Implementation ADV7511 with ZynqMP

Hello everyone,

I am trying to display on my monitor using the adv7511 pl design, made by analog. Small variante i am using a ZynqUltrascale MPSoC.

I am only concern by the display and not the sound so i took the liberty to remove the sound part, also the carrier board i am using as only HDMI_data[0:11] as input to the ADV7511, and not 16 like with the design of the zedboard for example.

What i have done is that i am using the Analog IP like in the base design and i created a system-top.vhd where i precised i was only going to use 12bits from the HDMI-data port of the HDMI-tx IP

this done, i added a part to my devicetree to add the ADV7511/HDMI-tx/clkgen/dmac:

/ {

	fpga_axi: fpga_axi@0 {
		status = "okay";
		#address-cells = <0x2>;
		#size-cells = <0x2>;
		compatible = "simple-bus";
		ranges;
		
		axi_iic_0: i2c@a0011000 {
			compatible = "xlnx,axi-iic-1.01.b", "xlnx,xps-iic-2.00.a";
			#address-cells = <0x1>;
			#size-cells = <0x0>;
			clocks = <0x3 0x47>;
			interrupt-parent = <0x4>;
			interrupts = <0x0 0x59 0x4>;
			reg = <0x0 0xa0011000 0x0 0x1000>;

			adv7511: adv7511@39 {
				compatible = "adi,adv7511";
				reg = <0x39>, <0x3f>;
				reg-names = "primary", "edid";

				adi,input-depth = <8>;
				adi,input-colorspace = "yuv422";
				adi,input-clock = "1x";
				adi,input-style = <1>;
				adi,input-justification = "right";
				adi,clock-delay = <0>;
				#sound-dai-cells = <0>;				

				ports {
				    #address-cells = <1>;
				    #size-cells = <0>;

				    port@0 {
					reg = <0>;
					adv7511_in: endpoint {
					    remote-endpoint = <&axi_hdmi_out>;
					};
				    };
				    port@1 {
					reg = <1>;
				    };
				};
			    };

		};

		axi_dma_0: dma@a0010000 {
			compatible = "adi,axi-dmac-1.00.a";
			reg = <0x0 0xa0010000 0x0 0x1000>;		
			#dma-cells = <1>;
			clocks = <0x3 0x47>;
			interrupt-parent = <0x4>;
			interrupts = <0 0x5a 0x4>;
			
			adi,channels {
				#size-cells = <0>;
				#address-cells = <1>;

				dma-channel@0 {
					reg = <0>;
					adi,source-bus-width = <64>;
					adi,source-bus-type = <0>;
					adi,destination-bus-width = <64>;
					adi,destination-bus-type = <1>;
				};
			};
		};

		axi_clkgen_0: axi_clkgen@a0000000 {
			compatible = "adi,axi-clkgen-2.00.a";
			#clock-cells = <0>;
			clocks = <0x3 0x48 0x3 0x47>;
			reg = <0x0 0xa0000000 0x0 0x10000>;
		};

		axi_hdmi_tx_0: axi_hdmi@a0020000 {
			compatible = "adi,axi-hdmi-tx-1.00.a";
			dmas = <&axi_dma_0 0>;
			dma-names = "video";
			clocks = <&axi_clkgen_0>;
			reg = <0x0 0xa0020000 0x0 0x10000>;
			port {
				axi_hdmi_out: endpoint {
				remote-endpoint = <&adv7511_in>;
        			};
    			};

		};

		misc_clk_0 {
			#clock-cells = <0x0>;
			clock-frequency = <0x5f5e100>;
			compatible = "fixed-clock";
			linux,phandle = <0x33>;
			phandle = <0x33>;
		};
		

		PERIPHERAL@ff380000 {
			compatible = "xlnx,PERIPHERAL-1.0";
			reg = <0x0 0xff380000 0x0 0x80000>;
		};

		PERIPHERAL@ff990000 {
			compatible = "xlnx,PERIPHERAL-1.0";
			reg = <0x0 0xff990000 0x0 0x10000>;
		};
	};
};

Implementation ADV7511 with ZynqMP

Hello everyone,

I am trying to display on my monitor using the adv7511 pl design, made by analog. Small variante i am using a ZynqUltrascale MPSoC.

I am only concern by the display and not the sound so i took the liberty to remove the sound part, also the carrier board i am using as only HDMI_data[0:11] as input to the ADV7511, and not 16 like with the design of the zedboard for example.

What i have done is that i am using the Analog IP like in the base design and i created a system-top.vhd where i precised i was only going to use 12bits from the HDMI-data port of the HDMI-tx IP

this done, i added a part to my devicetree to add the ADV7511/HDMI-tx/clkgen/dmac :

Fullscreen
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
misc_clk_0 {
#clock-cells = <0x0>;
clock-frequency = <0x5f5e100>;
compatible = "fixed-clock";
linux,phandle = <0x33>;
phandle = <0x33>;
};
PERIPHERAL@ff380000 {
compatible = "xlnx,PERIPHERAL-1.0";
reg = <0x0 0xff380000 0x0 0x80000>;
};
PERIPHERAL@ff990000 {
compatible = "xlnx,PERIPHERAL-1.0";
reg = <0x0 0xff990000 0x0 0x10000>;
};
};
};
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

At first i created the devicetree with petalinux so it added this misc_clk_0 but i am not using it after... not really sure why it had been generated.

i use the Linux kernel from Analog with the adi-zynqmp-config

booting my device it recognize the HDMI-tx ip, I have no notification of the chip but if i write the command : i2cdetect -y -r 2 (my i2c bus) the address 39 and 3f are marked as used.

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 4.14.0 (petalinux@petalinux-VirtualBox) (gcc version 7.3.1 20180314 (Linaro GCC 7.3-2018.04-rc3)) #4 SMP Wed May 29 08:54:53 CEST 2019
[    0.000000] Boot CPU: AArch64 Processor [410fd034]
[    0.000000] Machine model: xlnx,zynqmp
[    0.000000] efi: Getting EFI parameters from FDT:
[    0.000000] efi: UEFI not found.
[    0.000000] cma: Reserved 256 MiB at 0x000000006fc00000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] random: fast init done
[    0.000000] percpu: Embedded 20 pages/cpu @ffffffc07fe78000 s44568 r8192 d29160 u81920
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: enabling workaround for ARM erratum 845719
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 516867
[    0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk1p2 rw earlyprintk rootfstype=ext4 rootwait
[    0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[    0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes)
[    0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes)
[    0.000000] Memory: 1783644K/2096128K available (10172K kernel code, 708K rwdata, 4412K rodata, 448K init, 2157K bss, 50340K reserved, 262144K cma-reserved)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     modules : 0xffffff8000000000 - 0xffffff8008000000   (   128 MB)
[    0.000000]     vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000   (   250 GB)
[    0.000000]       .text : 0xffffff8008080000 - 0xffffff8008a70000   ( 10176 KB)
[    0.000000]     .rodata : 0xffffff8008a70000 - 0xffffff8008ed0000   (  4480 KB)
[    0.000000]       .init : 0xffffff8008ed0000 - 0xffffff8008f40000   (   448 KB)
[    0.000000]       .data : 0xffffff8008f40000 - 0xffffff8008ff1200   (   709 KB)
[    0.000000]        .bss : 0xffffff8008ff1200 - 0xffffff800920c630   (  2158 KB)
[    0.000000]     fixed   : 0xffffffbefe7fd000 - 0xffffffbefec00000   (  4108 KB)
[    0.000000]     PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000   (    16 MB)
[    0.000000]     vmemmap : 0xffffffbf00000000 - 0xffffffc000000000   (     4 GB maximum)
[    0.000000]               0xffffffbf00000000 - 0xffffffbf01bfc800   (    27 MB actual)
[    0.000000]     memory  : 0xffffffc000000000 - 0xffffffc07ff00000   (  2047 MB)
[    0.000000] Hierarchical RCU implementation.
[    0.000000]  RCU event tracing is enabled.
[    0.000000]  RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
[    0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
[    0.000000] GIC: Using split EOI/Deactivate mode
[    0.000000] arch_timer: cp15 timer(s) running at 33.33MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x7b00c3848, max_idle_ns: 440795203375 ns
[    0.000003] sched_clock: 56 bits at 33MHz, resolution 30ns, wraps every 2199023255545ns
[    0.000278] Console: colour dummy device 80x25
[    0.000295] Calibrating delay loop (skipped), value calculated using timer frequency.. 66.66 BogoMIPS (lpj=133333)
[    0.000303] pid_max: default: 32768 minimum: 301
[    0.000402] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes)
[    0.000412] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes)
[    0.000985] ASID allocator initialised with 65536 entries
[    0.001029] Hierarchical SRCU implementation.
[    0.001319] EFI services will not be available.
[    0.001340] zynqmp_plat_init Platform Management API v1.1
[    0.001346] zynqmp_plat_init Trustzone version v1.0
[    0.001441] smp: Bringing up secondary CPUs ...
[    0.001687] Detected VIPT I-cache on CPU1
[    0.001714] CPU1: Booted secondary processor [410fd034]
[    0.001985] Detected VIPT I-cache on CPU2
[    0.002002] CPU2: Booted secondary processor [410fd034]
[    0.002258] Detected VIPT I-cache on CPU3
[    0.002275] CPU3: Booted secondary processor [410fd034]
[    0.002317] smp: Brought up 1 node, 4 CPUs
[    0.002331] SMP: Total of 4 processors activated.
[    0.002336] CPU features: detected feature: 32-bit EL0 Support
[    0.002344] CPU: All CPU(s) started at EL2
[    0.002358] alternatives: patching kernel code
[    0.003051] devtmpfs: initialized
[    0.006582] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.006596] futex hash table entries: 1024 (order: 5, 131072 bytes)
[    0.011520] xor: measuring software checksum speed
[    0.048027]    8regs     :  2303.000 MB/sec
[    0.088056]    8regs_prefetch:  2053.000 MB/sec
[    0.128091]    32regs    :  2831.000 MB/sec
[    0.168116]    32regs_prefetch:  2379.000 MB/sec
[    0.168121] xor: using function: 32regs (2831.000 MB/sec)
[    0.168188] pinctrl core: initialized pinctrl subsystem
[    0.168690] NET: Registered protocol family 16
[    0.169574] vdso: 2 pages (1 code @ ffffff8008a76000, 1 data @ ffffff8008f44000)
[    0.169584] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.170338] DMA: preallocated 256 KiB pool for atomic allocations
[    0.191466] reset_zynqmp reset-controller: Xilinx zynqmp reset driver probed
[    0.191972] ARM CCI_400_r1 PMU driver probed
[    0.196481] zynqmp-pinctrl ff180000.pinctrl: zynqmp pinctrl initialized
[    0.203814] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[    0.268280] raid6: int64x1  gen()   455 MB/s
[    0.336301] raid6: int64x1  xor()   443 MB/s
[    0.404405] raid6: int64x2  gen()   687 MB/s
[    0.472432] raid6: int64x2  xor()   605 MB/s
[    0.540500] raid6: int64x4  gen()  1043 MB/s
[    0.608539] raid6: int64x4  xor()   765 MB/s
[    0.676572] raid6: int64x8  gen()   982 MB/s
[    0.744651] raid6: int64x8  xor()   751 MB/s
[    0.812678] raid6: neonx1   gen()   726 MB/s
[    0.880726] raid6: neonx1   xor()   851 MB/s
[    0.948794] raid6: neonx2   gen()  1168 MB/s
[    1.016852] raid6: neonx2   xor()  1208 MB/s
[    1.084908] raid6: neonx4   gen()  1507 MB/s
[    1.152949] raid6: neonx4   xor()  1442 MB/s
[    1.221016] raid6: neonx8   gen()  1666 MB/s
[    1.289074] raid6: neonx8   xor()  1535 MB/s
[    1.289078] raid6: using algorithm neonx8 gen() 1666 MB/s
[    1.289081] raid6: .... xor() 1535 MB/s, rmw enabled
[    1.289086] raid6: using neon recovery algorithm
[    1.289903] SCSI subsystem initialized
[    1.290075] usbcore: registered new interface driver usbfs
[    1.290106] usbcore: registered new interface driver hub
[    1.290138] usbcore: registered new device driver usb
[    1.290200] media: Linux media interface: v0.10
[    1.290226] Linux video capture interface: v2.00
[    1.290260] pps_core: LinuxPPS API ver. 1 registered
[    1.290264] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    1.290280] PTP clock support registered
[    1.290471] zynqmp-ipi ff9905c0.mailbox: Probed ZynqMP IPI Mailbox driver.
[    1.290591] FPGA manager framework
[    1.290698] fpga-region fpga-full: FPGA Region probed
[    1.290780] Advanced Linux Sound Architecture Driver Initialized.
[    1.291017] Bluetooth: Core ver 2.22
[    1.291036] NET: Registered protocol family 31
[    1.291040] Bluetooth: HCI device and connection manager initialized
[    1.291047] Bluetooth: HCI socket layer initialized
[    1.291053] Bluetooth: L2CAP socket layer initialized
[    1.291068] Bluetooth: SCO socket layer initialized
[    1.291610] clocksource: Switched to clocksource arch_sys_counter
[    1.291678] VFS: Disk quotas dquot_6.6.0
[    1.291719] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    1.295674] NET: Registered protocol family 2
[    1.295955] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
[    1.296062] TCP bind hash table entries: 16384 (order: 6, 262144 bytes)
[    1.296259] TCP: Hash tables configured (established 16384 bind 16384)
[    1.296327] UDP hash table entries: 1024 (order: 3, 32768 bytes)
[    1.296367] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes)
[    1.296475] NET: Registered protocol family 1
[    1.296631] RPC: Registered named UNIX socket transport module.
[    1.296636] RPC: Registered udp transport module.
[    1.296639] RPC: Registered tcp transport module.
[    1.296643] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    1.297005] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[    1.297144] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[    1.297768] audit: initializing netlink subsys (disabled)
[    1.298111] audit: type=2000 audit(1.288:1): state=initialized audit_enabled=0 res=1
[    1.298139] workingset: timestamp_bits=62 max_order=19 bucket_order=0
[    1.298778] NFS: Registering the id_resolver key type
[    1.298794] Key type id_resolver registered
[    1.298798] Key type id_legacy registered
[    1.298806] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    1.298823] jffs2: version 2.2. (NAND) (SUMMARY)  © 2001-2006 Red Hat, Inc.
[    1.322732] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
[    1.322743] io scheduler noop registered
[    1.322747] io scheduler deadline registered
[    1.322766] io scheduler cfq registered (default)
[    1.322771] io scheduler mq-deadline registered
[    1.322775] io scheduler kyber registered
[    1.324474] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success
[    1.324614] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success
[    1.324749] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success
[    1.324884] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success
[    1.325019] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success
[    1.325152] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success
[    1.325286] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success
[    1.325419] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success
[    1.325619] xilinx-zynqmp-dma ffa80000.dma: ZynqMP DMA driver Probe success
[    1.325754] xilinx-zynqmp-dma ffa90000.dma: ZynqMP DMA driver Probe success
[    1.325888] xilinx-zynqmp-dma ffaa0000.dma: ZynqMP DMA driver Probe success
[    1.326025] xilinx-zynqmp-dma ffab0000.dma: ZynqMP DMA driver Probe success
[    1.326159] xilinx-zynqmp-dma ffac0000.dma: ZynqMP DMA driver Probe success
[    1.326293] xilinx-zynqmp-dma ffad0000.dma: ZynqMP DMA driver Probe success
[    1.326428] xilinx-zynqmp-dma ffae0000.dma: ZynqMP DMA driver Probe success
[    1.326568] xilinx-zynqmp-dma ffaf0000.dma: ZynqMP DMA driver Probe success
[    1.351124] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[    1.353825] cacheinfo: Unable to detect cache hierarchy for CPU 0
[    1.357820] brd: module loaded
[    1.361168] loop: module loaded
[    1.361799] mtdoops: mtd device (mtddev=name/number) must be supplied
[    1.362668] m25p80 spi0.0: SPI-NOR-UniqueID 10000023420465060021001230061457a0
[    1.362946] m25p80 spi0.0: n25q512a (131072 Kbytes)
[    1.362964] 3 ofpart partitions found on MTD device spi0.0
[    1.362968] Creating 3 MTD partitions on "spi0.0":
[    1.362976] 0x000000000000-0x000000100000 : "boot"
[    1.363363] 0x000000100000-0x000000140000 : "bootenv"
[    1.363756] 0x000000140000-0x000001740000 : "kernel"
[    1.364945] libphy: Fixed MDIO Bus: probed
[    1.365885] tun: Universal TUN/TAP device driver, 1.6
[    1.366029] CAN device driver interface
[    1.366626] macb ff0e0000.ethernet: Not enabling partial store and forward
[    1.367056] libphy: MACB_mii_bus: probed
[    1.367072] [Firmware Warn]: /amba/ethernet@ff0e0000/ethernet-phy@0: Whitelisted compatible string. Please remove
[    1.427761] PLL: shutdown
[    1.427779] zynqmp_pll_disable() clock disable failed for dpll_int, ret = -13
[    1.435689] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 30 (54:10:ec:6c:e7:a4)
[    1.435697] Marvell 88E1510 ff0e0000.ethernet-ffffffff:01: attached PHY driver [Marvell 88E1510] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:01, irq=POLL)
[    1.436247] usbcore: registered new interface driver asix
[    1.436291] usbcore: registered new interface driver ax88179_178a
[    1.436317] usbcore: registered new interface driver cdc_ether
[    1.436341] usbcore: registered new interface driver net1080
[    1.436366] usbcore: registered new interface driver cdc_subset
[    1.436389] usbcore: registered new interface driver zaurus
[    1.436423] usbcore: registered new interface driver cdc_ncm
[    1.436695] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM
[    1.437232] usbcore: registered new interface driver uas
[    1.437267] usbcore: registered new interface driver usb-storage
[    1.437725] rtc_zynqmp ffa60000.rtc: rtc core: registered ffa60000.rtc as rtc0
[    1.437772] i2c /dev entries driver
[    1.438094] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 32
[    1.446018] IR NEC protocol handler initialized
[    1.446023] IR RC5(x/sz) protocol handler initialized
[    1.446027] IR RC6 protocol handler initialized
[    1.446031] IR JVC protocol handler initialized
[    1.446034] IR Sony protocol handler initialized
[    1.446038] IR SANYO protocol handler initialized
[    1.446041] IR Sharp protocol handler initialized
[    1.446045] IR MCE Keyboard/mouse protocol handler initialized
[    1.446049] IR XMP protocol handler initialized
[    1.446717] usbcore: registered new interface driver uvcvideo
[    1.446721] USB Video Class driver (1.1.1)
[    1.447147] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer at ffffff8009295000 with timeout 60s
[    1.447327] cdns-wdt ff150000.watchdog: Xilinx Watchdog Timer at ffffff800929d000 with timeout 10s
[    1.447491] Bluetooth: HCI UART driver ver 2.3
[    1.447497] Bluetooth: HCI UART protocol H4 registered
[    1.447501] Bluetooth: HCI UART protocol BCSP registered
[    1.447505] Bluetooth: HCI UART protocol ATH3K registered
[    1.447509] Bluetooth: HCI UART protocol Three-wire (H5) registered
[    1.447547] Bluetooth: HCI UART protocol Intel registered
[    1.447551] Bluetooth: HCI UART protocol QCA registered
[    1.447584] usbcore: registered new interface driver bcm203x
[    1.447636] usbcore: registered new interface driver bpa10x
[    1.447666] usbcore: registered new interface driver bfusb
[    1.447694] usbcore: registered new interface driver btusb
[    1.447699] Bluetooth: Generic Bluetooth SDIO driver ver 0.1
[    1.447745] usbcore: registered new interface driver ath3k
[    1.447923] sdhci: Secure Digital Host Controller Interface driver
[    1.447926] sdhci: Copyright(c) Pierre Ossman
[    1.447970] sdhci-pltfm: SDHCI platform and OF driver helper
[    1.495622] mmc0: SDHCI controller on ff160000.mmc [ff160000.mmc] using ADMA 64-bit
[    1.543620] mmc1: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit
[    1.549558] ledtrig-cpu: registered to indicate activity on CPUs
[    1.549680] usbcore: registered new interface driver usbhid
[    1.549684] usbhid: USB HID core driver
[    1.553618] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
[    1.554341] pktgen: Packet Generator for packet performance testing. Version: 2.75
[    1.558083] Netfilter messages via NETLINK v0.30.
[    1.558207] ip_tables: (C) 2000-2006 Netfilter Core Team
[    1.558396] Initializing XFRM netlink socket
[    1.558455] NET: Registered protocol family 10
[    1.558862] Segment Routing with IPv6
[    1.558905] ip6_tables: (C) 2000-2006 Netfilter Core Team
[    1.559067] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    1.559372] NET: Registered protocol family 17
[    1.559385] NET: Registered protocol family 15
[    1.559399] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[    1.559404] Ebtables v2.0 registered
[    1.559496] can: controller area network core (rev 20170425 abi 9)
[    1.559525] NET: Registered protocol family 29
[    1.559531] can: raw protocol (rev 20170425)
[    1.559535] can: broadcast manager protocol (rev 20170425 t)
[    1.559542] can: netlink gateway (rev 20170425) max_hops=1
[    1.559755] Bluetooth: RFCOMM TTY layer initialized
[    1.559763] Bluetooth: RFCOMM socket layer initialized
[    1.559773] Bluetooth: RFCOMM ver 1.11
[    1.559784] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[    1.559788] Bluetooth: BNEP filters: protocol multicast
[    1.559794] Bluetooth: BNEP socket layer initialized
[    1.559799] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[    1.559805] Bluetooth: HIDP socket layer initialized
[    1.559908] 9pnet: Installing 9P2000 support
[    1.559923] Key type dns_resolver registered
[    1.560299] registered taskstats version 1
[    1.560603] Btrfs loaded, crc32c=crc32c-generic
[    1.562058] mmc0: new HS200 MMC card at address 0001
[    1.565036] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 40, base_baud = 6249999) is a xuartps
[    1.575629] mmcblk0: mmc0:0001 Q2J54A 3.59 GiB
[    1.583835] mmcblk0boot0: mmc0:0001 Q2J54A partition 1 16.0 MiB
[    1.588576] mmcblk0boot1: mmc0:0001 Q2J54A partition 2 16.0 MiB
[    1.592310] mmcblk0rpmb: mmc0:0001 Q2J54A partition 3 512 KiB
[    1.597182] mmc1: Problem switching card into high-speed mode!
[    1.597290] mmc1: new SDHC card at address 0001
[    1.600206] mmcblk1: mmc1:0001 00000 7.45 GiB
[    1.602138]  mmcblk1: p1 p2
[    3.128813] console [ttyPS0] enabled
[    3.285766] Console: switching to colour frame buffer device 240x67
[    3.316658] axi-hdmi a0020000.axi_hdmi: fb0:  frame buffer device
[    3.322927] [drm] Initialized axi_hdmi_drm 1.0.0 20120930 for a0020000.axi_hdmi on minor 0
[    3.331410] dwc3-of-simple ff9d0000.usb0: dwc3_simple_set_phydata: Can't find usb3-phy
[    3.339850] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[    3.345263] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[    3.353113] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x22010010
[    3.361753] xhci-hcd xhci-hcd.0.auto: irq 46, io mem 0xfe200000
[    3.367727] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[    3.374433] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    3.381634] usb usb1: Product: xHCI Host Controller
[    3.386494] usb usb1: Manufacturer: Linux 4.14.0 xhci-hcd
[    3.391875] usb usb1: SerialNumber: xhci-hcd.0.auto
[    3.396988] hub 1-0:1.0: USB hub found
[    3.400672] hub 1-0:1.0: 1 port detected
[    3.404729] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[    3.410138] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[    3.417813] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[    3.425918] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
[    3.432622] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    3.439824] usb usb2: Product: xHCI Host Controller
[    3.444684] usb usb2: Manufacturer: Linux 4.14.0 xhci-hcd
[    3.450066] usb usb2: SerialNumber: xhci-hcd.0.auto
[    3.455151] hub 2-0:1.0: USB hub found
[    3.458832] hub 2-0:1.0: 1 port detected
[    3.463656] rtc_zynqmp ffa60000.rtc: setting system clock to 1970-01-01 00:00:25 UTC (25)
[    3.472132] PLL: shutdown
[    3.475424] ALSA device list:
[    3.478304]   No soundcards found.
[    3.619396] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
[    3.627423] VFS: Mounted root (ext4 filesystem) on device 179:34.
[    3.653241] devtmpfs: mounted
[    3.656262] Freeing unused kernel memory: 448K
[    4.781900] systemd[1]: System time before build time, advancing clock.

Welcome to Debian GNU/Linux 9 (stretch)!

NetworkManager-wait-online.service: Cannot add dependency job, ignoring: Unit NetworkManager-wait-online.service is masked.
[  OK  ] Listening on Syslog Socket.
[  OK  ] Started Dispatch Password Requests to Console Directory Watch.
[  OK  ] Reached target Swap.
[  OK  ] Listening on udev Kernel Socket.
[  OK  ] Created slice User and Session Slice.
[  OK  ] Listening on udev Control Socket.
[  OK  ] Listening on /dev/initctl Compatibility Named Pipe.
[  OK  ] Listening on Network Service Netlink Socket.
[  OK  ] Listening on Journal Socket (/dev/log).
[  OK  ] Listening on Journal Socket.
[  OK  ] Started Forward Password Requests to Wall Directory Watch.
[  OK  ] Reached target Encrypted Volumes.
[  OK  ] Reached target Remote File Systems.
[  OK  ] Listening on Journal Audit Socket.
[  OK  ] Created slice System Slice.
[  OK  ] Reached target Slices.
         Starting Create list of required st…ce nodes for the current kernel...
         Mounting Debug File System...
         Starting Remount Root and Kernel File Systems...
         Starting Set the console keyboard layout...
         Mounting POSIX Message Queue File System...
         Starting Journal Service...
dev-hugepages.mount: Couldn't determine result for ConditionVirtualization=!private-users, assuming failed: No such file or directory
[  OK  ] Created slice system-serial\x2dgetty.slice.
         Starting Nameserver information manager...
         Starting Load Kernel Modules...
[  OK  ] Created slice system-getty.slice.
[  OK  ] Started Create list of required sta…vice nodes for the current kernel.
[  OK  ] Started Remount Root and Kernel File Systems.
         Starting Load/Save Random Seed...
         Starting udev Coldplug all Devices...
         Starting Create Static Device Nodes in /dev...
[  OK  ] Started Load Kernel Modules.
         Starting Apply Kernel Variables...
         Mounting Configuration File System...
[  OK  ] Started Apply Kernel Variables.
[  OK  ] Started Journal Service.
[  OK  ] Started udev Coldplug all Devices.
         Starting Flush Journal to Persistent Storage...
[  OK  ] Started Load/Save Random Seed.
[  OK  ] Mounted POSIX Message Queue File System.
[  OK  ] Mounted Debug File System.
[  OK  ] Mounted Configuration File System.
[    6.566787] systemd-journald[1732]: Received request to flush runtime journal from PID 1
[  OK  ] Started Flush Journal to Persistent Storage.
[  OK  ] Started Create Static Device Nodes in /dev.
[  OK  ] Started Nameserver information manager.
         Starting udev Kernel Device Manager...
[  OK  ] Started Set the console keyboard layout.
[  OK  ] Reached target Local File Systems (Pre).
[  OK  ] Reached target Local File Systems.
         Starting Set console font and keymap...
         Starting Create Volatile Files and Directories...
         Starting Raise network interfaces...
[  OK  ] Started Set console font and keymap.
[  OK  ] Started Create Volatile Files and Directories.
         Starting Update UTMP about System Boot/Shutdown...
         Starting Network Time Synchronization...
[  OK  ] Started Update UTMP about System Boot/Shutdown.
[  OK  ] Started Network Time Synchronization.
[  OK  ] Reached target System Time Synchronized.
[  OK  ] Started udev Kernel Device Manager.
[  OK  ] Started Raise network interfaces.
         Starting Network Service...
[  OK  ] Reached target System Initialization.
[  OK  ] Started Daily apt download activities.
[  OK  ] Started Daily apt upgrade and clean activities.
[  OK  ] Listening on OpenBSD Secure Shell server socket.
[  OK  ] Listening on ACPID Listen Socket.
[  OK  ] Started Trigger anacron every hour.
[  OK  ] Started ACPI Events Check.
[  OK  ] Reached target Paths.
[  OK  ] Started Daily Cleanup of Temporary Directories.
[  OK  ] Reached target Timers.
[  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[  OK  ] Listening on D-Bus System Message Bus Socket.
[  OK  ] Reached target Sockets.
[  OK  ] Reached target Basic System.
         Starting RealtimeKit Scheduling Policy Service...
         Starting Initialize hardware monitoring sensors...
[  OK  ] Started Run anacron jobs.
         Starting LSB: Load kernel modules needed to enable cpufreq scaling...
         Starting Provide limited super user privileges to specific users...
[  OK  ] Started Regular background program processing daemon.
[  OK  ] Started D-Bus System Message Bus.
         Starting WPA supplicant...
         Starting Avahi mDNS/DNS-SD Stack...
         Starting LSB: Speech Dispatcher...
[  OK  ] Started ACPI event daemon.
         Starting System Logging Service...
         Starting Login Service...
         Starting Modem Manager...
         Starting Network Manager...
         Starting Restore /etc/resolv.conf i…fore the ppp link was shut down...
[  OK  ] Started Network Service.
[FAILED] Failed to start RealtimeKit Scheduling Policy Service.
See 'systemctl status rtkit-daemon.service' for details.
[  OK  ] Started Provide limited super user privileges to specific users.
[  OK  ] Started Initialize hardware monitoring sensors.
[  OK  ] Started Restore /etc/resolv.conf if…before the ppp link was shut down.
[  OK  ] Found device /dev/ttyPS0.
[  OK  ] Started System Logging Service.
[  OK  ] Started LSB: Speech Dispatcher.
[  OK  ] Started LSB: Load kernel modules needed to enable cpufreq scaling.
[  OK  ] Started Avahi mDNS/DNS-SD Stack.
[  OK  ] Started Login Service.
         Starting LSB: set CPUFreq kernel parameters...
[  OK  ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
[  OK  ] Started LSB: set CPUFreq kernel parameters.
[  OK  ] Started WPA supplicant.
         Starting Authorization Manager...
[  OK  ] Started Authorization Manager.
[  OK  ] Started Network Manager.
[  OK  ] Reached target Network.
[  OK  ] Reached target Network is Online.
         Starting LSB: disk temperature monitoring daemon...
         Starting LSB: exim Mail Transport Agent...
         Starting LSB: Advanced IEEE 802.11 management daemon...
         Starting /etc/rc.local Compatibility...
         Starting Network Name Resolution...
         Starting Permit User Sessions...
[  OK  ] Started LSB: Advanced IEEE 802.11 management daemon.
[  OK  ] Started /etc/rc.local Compatibility.
[  OK  ] Started Permit User Sessions.
[  OK  ] Started LSB: disk temperature monitoring daemon.
[  OK  ] Started Modem Manager.
         Starting Network Manager Script Dispatcher Service...
         Starting Light Display Manager...
[  OK  ] Started Getty on tty1.
[  OK  ] Started Serial Getty on ttyPS0.
[  OK  ] Reached target Login Prompts.
[  OK  ] Started Network Manager Script Dispatcher Service.
[  OK  ] Started Network Name Resolution.
         Starting Hostname Service...
[FAILED] Failed to start Hostname Service.
See 'systemctl status systemd-hostnamed.service' for details.
[  OK  ] Started Light Display Manager.
[  OK  ] Started LSB: exim Mail Transport Agent.
[  OK  ] Reached target Multi-User System.
[  OK  ] Reached target Graphical Interface.
         Starting Update UTMP about System Runlevel Changes...
[  OK  ] Started Update UTMP about System Runlevel Changes.

Debian GNU/Linux 9 linaro-developer ttyPS0

linaro-developer login: root (automatic login)

Last login: Mon Jun  3 13:58:19 UTC 2019 on ttyPS0
Linux linaro-developer 4.14.0 #4 SMP Wed May 29 08:54:53 CEST 2019 aarch64

The programs included with the Debian GNU/Linux system are free software;
the exact distribution terms for each program are described in the
individual files in /usr/share/doc/*/copyright.

Debian GNU/Linux comes with ABSOLUTELY NO WARRANTY, to the extent
permitted by applicable law.
root@linaro-developer:~#

however my screen stay green. I tried to use the command startx, i get an error telling that the driver for the axi-hdmi-drm-dri.so is not found.. when in the boot it seems to recognize it, at least create a framebuffer (dev/fb0 is there)

if someone has an idea this would really be helpful.

Best regards 

Sarah

  • 0
    •  Analog Employees 
    on Jun 4, 2019 8:38 AM over 1 year ago

    Hi Sarah,

    Can you please describe the hardware connection between FPGA and ADV7511 or post here part of the schematic that you use.

    I'm curious about the connections that you made. Also you use embedded syncs or separate sync signals?

    One important point is that our AXI_HDMI_TX core support only 36, 24 and 16 bit video bus lengths. So you can establish a 12 bit connection to ADV but for sure you'll lose some data. Please check AXI HDMI IP documentation here:  axi_hdmi_tx

    Regards,

    Bogdan

  • Hi Bogban,

    I am using the module TE0820 from trenz a  Ultrascale MPSoC Som connected on the board TE0710 also from trenz. here is the schematic for the ADV7511 chip:

    https://www.trenz-electronic.de/fileadmin/docs/Trenz_Electronic/Modules_and_Module_Carriers/4x5/4x5_Carriers/TE0701/REV06/Documents/SCH-TE0701-06.PDF

    the connection between the module and the board for the HDMI_D[0:11] aswell as VS,HS,CLKC, and DE are deduced from the Pin in/out file given by trenz  (link:https://shop.trenz-electronic.de/de/Download/?path=Trenz_Electronic/Pinout)

    and i need also to precise the CEC, HPD, LS_oe to enable the data transfert to the HDMI connector.

    (for this it is enable by default in my pl design)

    after i just made the connection using the devicetree and the kernel configuration (allowing the drm_i2c_adv7511 as module aswell as adi_axi_hdmi)

    after on the carrier i need to enable the FMC_VADJ and VIOTA to 1,8volts via some DIP switch, i measured it and it is set. Also since my monitor is lighting up and producing this green screen it proves that it is connected.

    One update since this morning: the misc_clk_0 that petalinux produce in my devicetree is actually the output of clk0 from clkgen i observed that it is at 100MHz and in the wiki it was precised that the pixel frequency should e at 148.5MHz for 1080p. i changed it but then kernel seems to have some troubles to implement the module :

    [    8.207769] adv7511 1-0039: 1-0039 supply avdd not found, using dummy regulator
    [    8.215053] adv7511 1-0039: 1-0039 supply dvdd not found, using dummy regulator
    [    8.222319] adv7511 1-0039: 1-0039 supply pvdd not found, using dummy regulator
    [    8.229603] adv7511 1-0039: 1-0039 supply bgvdd not found, using dummy regulator
    [    8.236984] adv7511 1-0039: 1-0039 supply dvdd-3v not found, using dummy regulator
    [    8.246950] Unable to handle kernel NULL pointer dereference at virtual address 00000000
    [    8.254965] Mem abort info:
    [    8.257736]   Exception class = IABT (current EL), IL = 32 bits
    [    8.263633]   SET = 0, FnV = 0
    [    8.266671]   EA = 0, S1PTW = 0
    [    8.269801] user pgtable: 4k pages, 39-bit VAs, pgd = ffffffc06ad5f000
    [    8.276306] [0000000000000000] *pgd=0000000000000000, *pud=0000000000000000
    [    8.283254] Internal error: Oops: 86000005 [#1] SMP
    [    8.288105] Modules linked in: adv7511 adi_axi_hdmi uio_pdrv_genirq
    [    8.294359] CPU: 1 PID: 58 Comm: kworker/1:1 Not tainted 4.14.0 #1
    [    8.300517] Hardware name: xlnx,zynqmp (DT)
    [    8.304692] Workqueue: events deferred_probe_work_func
    [    8.309806] task: ffffffc06dacce00 task.stack: ffffff8009388000
    [    8.315709] PC is at 0x0
    [    8.318231] LR is at axi_hdmi_encoder_create+0xa8/0x2d0 [adi_axi_hdmi]
    [    8.324736] pc : [<0000000000000000>] lr : [<ffffff8000af0820>] pstate: 60000145
    [    8.332112] sp : ffffff800938bb90
    [    8.335412] x29: ffffff800938bb90 x28: 0000000000000000
    [    8.340706] x27: 0000000000000000 x26: ffffff8008d7ce68
    [    8.346002] x25: ffffff80080b1b78 x24: ffffffc06adf5000
    [    8.351295] x23: ffffffc068020088 x22: ffffffc068020000
    [    8.356590] x21: ffffff8000af2028 x20: ffffffc06802b598
    [    8.361885] x19: ffffffc068020000 x18: 0000000000000001
    [    8.367180] x17: ffffff8008a78630 x16: 000000000000002d
    [    8.372475] x15: ffffffffffffffff x14: ffffffc068021008
    [    8.377769] x13: ffffffc068021007 x12: 0000000000000020
    [    8.383064] x11: 0000000005f5e0ff x10: 0000000000000001
    [    8.388359] x9 : ffffff800938bae0 x8 : 000000000000001d
    [    8.393654] x7 : ffffffc068021000 x6 : ffffffc068021005
    [    8.398951] x5 : 0000000000000000 x4 : 0000000000000000
    [    8.404243] x3 : 0000000000000000 x2 : ffffffc068020000
    [    8.409538] x1 : ffffffc06adf5000 x0 : ffffffc06cc75400
    [    8.414835] Process kworker/1:1 (pid: 58, stack limit = 0xffffff8009388000)
    [    8.421777] Call trace:
    [    8.424209] Exception stack(0xffffff800938ba50 to 0xffffff800938bb90)
    [    8.430632] ba40:                                   ffffffc06cc75400 ffffffc06adf5000
    [    8.438446] ba60: ffffffc068020000 0000000000000000 0000000000000000 0000000000000000
    [    8.446257] ba80: ffffffc068021005 ffffffc068021000 000000000000001d ffffff800938bae0
    [    8.454069] baa0: 0000000000000001 0000000005f5e0ff 0000000000000020 ffffffc068021007
    [    8.461881] bac0: ffffffc068021008 ffffffffffffffff 000000000000002d ffffff8008a78630
    [    8.469693] bae0: 0000000000000001 ffffffc068020000 ffffffc06802b598 ffffff8000af2028
    [    8.477505] bb00: ffffffc068020000 ffffffc068020088 ffffffc06adf5000 ffffff80080b1b78
    [    8.485317] bb20: ffffff8008d7ce68 0000000000000000 0000000000000000 ffffff800938bb90
    [    8.493129] bb40: ffffff8000af0820 ffffff800938bb90 0000000000000000 0000000060000145
    [    8.500941] bb60: ffffff800938bb90 ffffff8000af07f8 ffffffffffffffff ffffffc06802b598
    [    8.508752] bb80: ffffff800938bb90 0000000000000000
    [    8.513613] [<          (null)>]           (null)
    [    8.518307] [<ffffff8000af105c>] axi_hdmi_platform_probe+0x174/0x2e0 [adi_axi_hdmi]
    [    8.525943] [<ffffff80085502d8>] platform_drv_probe+0x58/0xb8
    [    8.531669] [<ffffff800854e714>] driver_probe_device+0x22c/0x2d8
    [    8.537658] [<ffffff800854e918>] __device_attach_driver+0x98/0xf0
    [    8.543734] [<ffffff800854c978>] bus_for_each_drv+0x48/0x98
    [    8.549289] [<ffffff800854e3c0>] __device_attach+0xc0/0x130
    [    8.554844] [<ffffff800854e9c8>] device_initial_probe+0x10/0x18
    [    8.560746] [<ffffff800854d8a8>] bus_probe_device+0x90/0x98
    [    8.566302] [<ffffff800854dd44>] deferred_probe_work_func+0xa4/0x148
    [    8.572640] [<ffffff80080b1a14>] process_one_work+0x1d4/0x338
    [    8.578367] [<ffffff80080b1bbc>] worker_thread+0x44/0x488
    [    8.583749] [<ffffff80080b7754>] kthread+0x12c/0x130
    [    8.588697] [<ffffff8008084a60>] ret_from_fork+0x10/0x18
    [    8.593993] Code: bad PC value
    [    8.597029] ---[ end trace 77afa80ab3994974 ]---

    After that the boot ended "normally" and if i do a lsmod it tells me that all the modules are there but my screen doesn't produce any output anymore :/

    best regards,

    Sarah

  • 0
    •  Analog Employees 
    on Jun 12, 2019 12:00 PM over 1 year ago in reply to SaWick

    Hi Sarah,

    Sorry for late response.

    First I would like to ask you to try to remove the misc_clk_0 device-tree node. The clockgen should not be fixed to a specific frequency in DT.

    Its out frequency should be set by axi-hdmi-tx driver using clock framework to the desired frequency according to HDMI frame-rate and resolution.

    Also I would like to ask you to install devmem2 and to set register 0x48 from axi-hdmi-tx IP to 0x2 with a command like: "devmem2 0xa0020048 w 0x2". In this mode the HDMI TX IP will generate a test pattern and we can test if this core is working and if the FPGA-ADV7511 connection is ok and ADV is correctly configures.

    More information related to HDMI TX IP can find here: axi_hdmi_tx

    Regards,

    Bogdan

  • Hi Btogorean,

    No problem^^

    i tested the test pattern from HDMI TX IP and the screen stay green, actually the screen gets green when i activate the test patern, i tried "sudo busybox devmem 0xa0020048 w 0x0" to see if this would change something and it did, the screen went off.

    I wrote again to activate the test pattern and the screen light up again and went back to green. 

    I suppose the problem is coming from this data length, which is only of 12bits on my board. 

    Also i looking at the board circuit from trenz and zedboard(used the ZedBoard design as base for the pl design):

    - On trenz we are sending the data on the D0 to D11 input from the ADV7511

    - On Zedboard we send the data on D8 to D23 input of the adv7511

    Maybe by doing so i am only selecting the green Color and missing the red or the blue? 

    Is it possible to know how the convertion is made between the output of our DMA controller and the HDMI_out of the axi_hdmi_tx?

    thank you a lot for your help

    Best regards,

    Sarah

  • +1
    •  Analog Employees 
    on Jun 18, 2019 9:22 AM over 1 year ago in reply to SaWick

    Hi Sarah,

    The test pattern should be composed of multiple colors not just green so is clear that something is wrong with input data mapping. 

    And the problem is, as you correctly pointed out the HW data pins connected between ADV and FPGA.

    Please check the ADV7511 Hardware Users Guide, section 6.1 "Input connections" where you can find all the possible input modes.

    There you can see that if you want to connect ADV7511 on less than 16 bit (8, 10, 12) you need to output data from FPGA on DDR (double data rate) or 2X pixel clock. Unfortunately neither of these modes is supported by our axi_hdmi_tx IP.

    The following configurations from Zed devicetree set the ADV7511 input Data Mapping as on table 7 from page 24 on ADV7511 User Guide

    adi,input-depth = 8;
    adi,input-colorspace = "yuv422";
    adi,input-clock = "1x";
    adi,input-style = 1;
    adi,input-justification = "right";

    But for your configuration you need something like to configure the ADV like on table 10 from ADV7511 User Guide:

    adi,input-depth = 8;
    adi,input-colorspace = "yuv422";
    adi,input-clock = "2x";
    adi,input-style = 2;
    adi,input-justification = "right";

    I must point out again that this operation mode is not supported by our axi_hdmi_tx IP but is how the DT configuration should look like for your hardware.

    Regards,

    Bogdan