AD9361
Recommended for New Designs
The AD9361 is a high performance, highly integrated radio
frequency (RF) Agile Transceiverâ„¢ designed for use in 3G and
4G base station applications....
Datasheet
AD9361 on Analog.com
Hello,
I am porting a current device to a new kernel and am having some issue with the AD9361. I am not seeing any transmits or receives in our software, where it worked before under an older kernel. I suspect it's something with the device tree. Could you double check and make sure this looks alright?
I have a TX DMA and associated dds device commented out, because the kernel panics with it, likely because I don't think we are using a TX DMA, that happens in the FPGA.
Like written, I get a boot error about the cf-ad9361-lpc device not working because TX tune failed. When I disable TX tune, eventually, when running my application, I see RX tune also failing. I also don't see anything being transmitted or received.
Thanks!
File 1:
/ {
amba: amba {
rx_dma: dma@7c400000 {
compatible = "adi,axi-dmac-1.00.a";
reg = <0x7c400000 0x10000>;
#dma-cells = <1>;
interrupt-parent = <&intc>;
interrupts = <0 33 0>;
clocks = <&clkc 16>;
dma-channel {
adi,buswidth = <64>;
adi,type = <0>;
};
};
/*
tx_dma: dma@7c420000 {
compatible = "adi,axi-dmac-1.00.a";
reg = <0x7c420000 0x10000>;
#dma-cells = <1>;
interrupt-parent = <&intc>;
interrupts = <0 56 0>;
clocks = <&clkc 16>;
dma-channel {
adi,buswidth = <64>;
adi,type = <1>;
adi,cyclic;
};
};
*/
cf_ad9361_adc_core_0: cf-ad9361-lpc@79020000 {
compatible = "adi,axi-ad9361-6.00.a";
reg = <0x79020000 0x6000>;
dmas = <&rx_dma 0>;
dma-names = "rx";
spibus-connected = <&adc0_ad9361>;
xlnx,dphase-timeout = <0x8>;
xlnx,num-mem = <0x1>;
xlnx,num-reg = <0x1>;
xlnx,s-axi-min-size = <0x1ff>;
xlnx,slv-awidth = <0x20>;
xlnx,slv-dwidth = <0x20>;
xlnx,use-wstrb = <0x0>;
};
/*
cf_ad9361_dac_core_0: cf-ad9361-dds-core-lpc@79024000 {
compatible = "adi,axi-ad9361-dds-6.00.a";
reg = <0x79024000 0x1000>;
clocks = <&adc0_ad9361 13>;
clock-names = "sampl_clk";
dmas = <&tx_dma 0>;
dma-names = "tx";
dac-sample-frequency = <491520000>;
xlnx,dphase-timeout = <0x8>;
xlnx,num-mem = <0x1>;
xlnx,num-reg = <0x1>;
xlnx,s-axi-min-size = <0x1ff>;
xlnx,slv-awidth = <0x20>;
xlnx,slv-dwidth = <0x20>;
xlnx,use-wstrb = <0x0>;
};
*/
};
};
and:
&spi0 {
adc0_ad9361: ad9361-phy@0 {
#address-cells = <1>;
#size-cells = <0>;
#clock-cells = <1>;
compatible = "ad9361";
/* SPI Setup */
reg = <0>;
spi-cpha;
spi-max-frequency = <10000000>;
/* Clocks */
clocks = <&ad9361_clkin 0>;
clock-names = "ad9361_ext_refclk";
clock-output-names = "rx_sampl_clk", "tx_sampl_clk";
//adi,debug-mode-enable;
/* Digital Interface Control */
/* adi,digital-interface-tune-skip-mode:
* 0 = TUNE RX&TX
* 1 = SKIP TX
* 2 = SKIP ALL
*/
adi,digital-interface-tune-skip-mode = <0>;
adi,pp-tx-swap-enable;
adi,pp-rx-swap-enable;
adi,rx-frame-pulse-mode-enable;
adi,lvds-mode-enable;
adi,lvds-bias-mV = <150>;
adi,lvds-rx-onchip-termination-enable;
adi,rx-data-delay = <10>;
adi,tx-fb-clock-delay = <7>;
//adi,fdd-rx-rate-2tx-enable;
adi,dcxo-coarse-and-fine-tune = <8 5920>;
//adi,xo-disable-use-ext-refclk-enable;
/* Mode Setup */
adi,2rx-2tx-mode-enable;
//adi,split-gain-table-mode-enable;
/* ENSM Mode */
adi,frequency-division-duplex-mode-enable;
//adi,ensm-pin-pulse-mode-enable;
//adi,ensm-enable-txnrx-control-enable;
/* adi,rx-rf-port-input-select:
* 0 = (RX1A_N & RX1A_P) and (RX2A_N & RX2A_P) enabled; balanced
* 1 = (RX1B_N & RX1B_P) and (RX2B_N & RX2B_P) enabled; balanced
* 2 = (RX1C_N & RX1C_P) and (RX2C_N & RX2C_P) enabled; balanced
*
* 3 = RX1A_N and RX2A_N enabled; unbalanced
* 4 = RX1A_P and RX2A_P enabled; unbalanced
* 5 = RX1B_N and RX2B_N enabled; unbalanced
* 6 = RX1B_P and RX2B_P enabled; unbalanced
* 7 = RX1C_N and RX2C_N enabled; unbalanced
* 8 = RX1C_P and RX2C_P enabled; unbalanced
*/
adi,rx-rf-port-input-select = <0>; /* (RX1A_N & RX1A_P) and (RX2A_N & RX2A_P) enabled; balanced */
/* adi,tx-rf-port-input-select:
* 0 TX1A, TX2A
* 1 TX1B, TX2B
*/
adi,tx-rf-port-input-select = <0>; /* TX1A, TX2A */
//adi,update-tx-gain-in-alert-enable;
adi,tx-attenuation-mdB = <10000>;
adi,rf-rx-bandwidth-hz = <1000000>;
adi,rf-tx-bandwidth-hz = <1000000>;
adi,rx-synthesizer-frequency-hz = /bits/ 64 <402795000>;
adi,tx-synthesizer-frequency-hz = /bits/ 64 <402795000>;
/* BBPLL ADC R2CLK R1CLK CLKRF RSAMPL */
adi,rx-path-clock-frequencies = <819200000 12800000 12800000 6400000 3200000 1600000>;
/* BBPLL DAC T2CLK T1CLK CLKTF TSAMPL */
adi,tx-path-clock-frequencies = <819200000 12800000 12800000 6400000 3200000 1600000>;
/* Gain Control */
/* adi,gc-rx[1|2]-mode:
* 0 = RF_GAIN_MGC
* 1 = RF_GAIN_FASTATTACK_AGC
* 2 = RF_GAIN_SLOWATTACK_AGC
* 3 = RF_GAIN_HYBRID_AGC
*/
adi,gc-rx1-mode = <0>;
adi,gc-rx2-mode = <0>;
adi,gc-adc-ovr-sample-size = <4>; /* sum 4 samples */
adi,gc-adc-small-overload-thresh = <47>; /* sum of squares */
adi,gc-adc-large-overload-thresh = <58>; /* sum of squares */
adi,gc-lmt-overload-high-thresh = <800>; /* mV */
adi,gc-lmt-overload-low-thresh = <704>; /* mV */
adi,gc-dec-pow-measurement-duration = <8192>; /* 0..524288 Samples */
adi,gc-low-power-thresh = <24>; /* 0..-64 dBFS vals are set pos */
//adi,gc-dig-gain-enable;
//adi,gc-max-dig-gain = <15>;
/* Manual Gain Control Setup */
//adi,mgc-rx1-ctrl-inp-enable; /* uncomment to use ctrl inputs */
//adi,mgc-rx2-ctrl-inp-enable; /* uncomment to use ctrl inputs */
adi,mgc-inc-gain-step = <2>;
adi,mgc-dec-gain-step = <2>;
/* adi,mgc-split-table-ctrl-inp-gain-mode:
* (relevant if adi,split-gain-table-mode-enable is set)
* 0 = AGC determine this
* 1 = only in LPF
* 2 = only in LMT
*/
adi,mgc-split-table-ctrl-inp-gain-mode = <0>;
/* Automatic Gain Control Setup */
adi,agc-attack-delay-extra-margin-us= <1>; /* us */
adi,agc-outer-thresh-high = <5>; /* -dBFS */
adi,agc-outer-thresh-high-dec-steps = <2>; /* 0..15 */
adi,agc-inner-thresh-high = <10>; /* -dBFS */
adi,agc-inner-thresh-high-dec-steps = <1>; /* 0..7 */
adi,agc-inner-thresh-low = <12>; /* -dBFS */
adi,agc-inner-thresh-low-inc-steps = <1>; /* 0..7 */
adi,agc-outer-thresh-low = <18>; /* -dBFS */
adi,agc-outer-thresh-low-inc-steps = <2>; /* 0..15 */
adi,agc-adc-small-overload-exceed-counter = <10>; /* 0..15 */
adi,agc-adc-large-overload-exceed-counter = <10>; /* 0..15 */
adi,agc-adc-large-overload-inc-steps = <2>; /* 0..15 */
//adi,agc-adc-lmt-small-overload-prevent-gain-inc-enable;
adi,agc-lmt-overload-large-exceed-counter = <10>; /* 0..15 */
adi,agc-lmt-overload-small-exceed-counter = <10>; /* 0..15 */
adi,agc-lmt-overload-large-inc-steps = <2>; /* 0..7 */
//adi,agc-dig-saturation-exceed-counter = <3>; /* 0..15 */
//adi,agc-dig-gain-step-size = <4>; /* 1..8 */
//adi,agc-sync-for-gain-counter-enable;
adi,agc-gain-update-interval-us = <1000>; /* 1ms */
//adi,agc-immed-gain-change-if-large-adc-overload-enable;
//adi,agc-immed-gain-change-if-large-lmt-overload-enable;
/* Fast AGC */
adi,fagc-dec-pow-measurement-duration = <64>; /* 64 Samples */
//adi,fagc-allow-agc-gain-increase-enable;
adi,fagc-lp-thresh-increment-steps = <1>;
adi,fagc-lp-thresh-increment-time = <5>;
adi,fagc-energy-lost-stronger-sig-gain-lock-exit-cnt = <8>;
adi,fagc-final-overrange-count = <3>;
//adi,fagc-gain-increase-after-gain-lock-enable;
adi,fagc-gain-index-type-after-exit-rx-mode = <0>;
adi,fagc-lmt-final-settling-steps = <1>;
adi,fagc-lock-level = <10>;
adi,fagc-lock-level-gain-increase-upper-limit = <5>;
adi,fagc-lock-level-lmt-gain-increase-enable;
adi,fagc-lpf-final-settling-steps = <1>;
adi,fagc-optimized-gain-offset = <5>;
adi,fagc-power-measurement-duration-in-state5 = <64>;
adi,fagc-rst-gla-engergy-lost-goto-optim-gain-enable;
adi,fagc-rst-gla-engergy-lost-sig-thresh-below-ll = <10>;
adi,fagc-rst-gla-engergy-lost-sig-thresh-exceeded-enable;
adi,fagc-rst-gla-if-en-agc-pulled-high-mode = <0>;
adi,fagc-rst-gla-large-adc-overload-enable;
adi,fagc-rst-gla-large-lmt-overload-enable;
adi,fagc-rst-gla-stronger-sig-thresh-above-ll = <10>;
adi,fagc-rst-gla-stronger-sig-thresh-exceeded-enable;
adi,fagc-state-wait-time-ns = <260>;
adi,fagc-use-last-lock-level-for-set-gain-enable;
/* RSSI */
/* adi,rssi-restart-mode:
* 0 = AGC_IN_FAST_ATTACK_MODE_LOCKS_THE_GAIN,
* 1 = EN_AGC_PIN_IS_PULLED_HIGH,
* 2 = ENTERS_RX_MODE,
* 3 = GAIN_CHANGE_OCCURS,
* 4 = SPI_WRITE_TO_REGISTER,
* 5 = GAIN_CHANGE_OCCURS_OR_EN_AGC_PIN_PULLED_HIGH,
*/
adi,rssi-restart-mode = <3>;
//adi,rssi-unit-is-rx-samples-enable;
adi,rssi-delay = <1>; /* 1us */
adi,rssi-wait = <1>; /* 1us */
adi,rssi-duration = <1000>; /* 1ms */
/* Control Outputs */
adi,ctrl-outs-index = <0>;
adi,ctrl-outs-enable-mask = <0xFF>;
/* AuxADC Temp Sense Control */
adi,temp-sense-measurement-interval-ms = <1000>;
adi,temp-sense-offset-signed = <0xCE>;
adi,temp-sense-periodic-measurement-enable;
/* AuxDAC Control */
adi,aux-dac-manual-mode-enable;
adi,aux-dac1-default-value-mV = <0>;
//adi,aux-dac1-active-in-rx-enable;
//adi,aux-dac1-active-in-tx-enable;
//adi,aux-dac1-active-in-alert-enable;
adi,aux-dac1-rx-delay-us = <0>;
adi,aux-dac1-tx-delay-us = <0>;
adi,aux-dac2-default-value-mV = <0>;
//adi,aux-dac2-active-in-rx-enable;
//adi,aux-dac2-active-in-tx-enable;
//adi,aux-dac2-active-in-alert-enable;
adi,aux-dac2-rx-delay-us = <0>;
adi,aux-dac2-tx-delay-us = <0>;
};
};
&adc0_ad9361 {
reset-gpios = <&gpio0 100 0>;
};
Please see here: https://wiki.analog.com/resources/eval/user-guides/ad-fmcomms2-ebz/interface_timing_validation
If tuning fails, it's most likely an issue with your HW or HDL design.
You could use skip mode = 2, to get the device probed and then further test your system.
adi,digital-interface-tune-skip-mode = <0>;
After you have probed the ad9361-phy you can use BIST to test the transceiver.
Then try to use the digital tune runtime API to test different interface speeds.
-Michael
I think I ignored a fairly important bit: We are using the axi_ad9361 IP core, but it's old (2011). I assume a new driver would require an up-to-date IP core as well, so let me try and update that.
With the new IP core, TX tuning seems to work (I get no error with the ad9361-lpc device), but RX tuning still fails when I run my application. Ideas?
Hi,
You are saying that both HDL and HW have been tested - how did you test them? If the digital tuning doesn't work, most likely the issue is caused by HDL or HW.
Dragos
Good question. The hardware has existed for a while, running an older Linux OS, and works just fine, so I think hardware can be ruled out.
As for HDL, I've been using the same bitfile we use with the legacy OS. Then I realized that we are using an old axi_ad9361 IP core in the HDL, so I just updated that to the 2018_R2_pack2 branch of the ADI HDL, along with axi_dmac and others.
My assumption is that a 2018_R2 HDL core plus the 2018_R2 branch of the ADI Linux fork as the OS should work.
Tuning was enabled in 2014/15 in our device tree, so I assume it worked then (no error messages about tuning with legacy OS).
Good question. The hardware has existed for a while, running an older Linux OS, and works just fine, so I think hardware can be ruled out.
As for HDL, I've been using the same bitfile we use with the legacy OS. Then I realized that we are using an old axi_ad9361 IP core in the HDL, so I just updated that to the 2018_R2_pack2 branch of the ADI HDL, along with axi_dmac and others.
My assumption is that a 2018_R2 HDL core plus the 2018_R2 branch of the ADI Linux fork as the OS should work.
Tuning was enabled in 2014/15 in our device tree, so I assume it worked then (no error messages about tuning with legacy OS).