modify the AD9361 simulink model to look at LNA output?

I'd like to be able to look at the output of the LNA in the AD9361 Simulink model. I've been able to modify the model to get the output from the IQ demod, but no further back towards the receive antenna. The issue is that when I take the output from the LNA, I still get the spectrum from roughly -5.5 to +5.5MHz. I'm not sure how to set the spectral display. It seems that the issue is with the inherited sample rate in the spectral display, but I don't see how to adjust that.

One other question. In the LNA, I see that NF (noise figure) is used as a variable to set the noise contribution of the LNA, but I don't see where in the model where NF is actually defined/quantified.

thanks,

Steve

Parents
  • 0
    •  Analog Employees 
    on Apr 17, 2019 3:17 AM over 1 year ago

    Can you indicate the block at the output of which you are connecting the spectrum analyzer.

    As for the NF variable, it can be found as follows. Right click RF_RX block, select Mask->View Mask. Then select Initialization tab in the Mask Editor. You'll find NF extrapolated from the noise figure values in the datasheet using interp1 MATLAB function.

    - Srikanth

  • 0
    •  Analog Employees 
    on Apr 17, 2019 11:24 AM over 1 year ago in reply to SrikanthPagadarai

    Hi Srikanth,

    This is what I'm doing. I've created an extra output from RF_Rx, from the LNA. I then moved the output of the block from DDC_Filters_Rx to this new output of RF_Rx. Thanks!

  • 0
    •  Analog Employees 
    on Apr 17, 2019 2:13 PM over 1 year ago in reply to stevereine

    Hi Steve,

    The x-axis limits in the spectrum analyzers are indeed inherited. You can modify them by doing two things.

    1. Double-click the CW Source block. Increase the Oversampling to value larger than the default value of 1.5.

    2. Double-click the ad9361_RX block. In the denominator for the setting, Step Size RF Simulation (s), you will see the default value of 1.5. Update this value to the new Oversampling value used in the CW Source block.

    The default range of  -5.76 MHz to 5.76 MHz can be calculated from the default settings of the CW Source block.

    x_lim_max =  0.5*Oversampling/ Sample time(s) = 0.5*1.5/1.302e-07 =  5.76e+06

    x_lim_min = -0.5*Oversampling/ Sample time(s) = 0.5*1.5/1.302e-07 = -5.76e+06

    - Srikanth

Reply
  • 0
    •  Analog Employees 
    on Apr 17, 2019 2:13 PM over 1 year ago in reply to stevereine

    Hi Steve,

    The x-axis limits in the spectrum analyzers are indeed inherited. You can modify them by doing two things.

    1. Double-click the CW Source block. Increase the Oversampling to value larger than the default value of 1.5.

    2. Double-click the ad9361_RX block. In the denominator for the setting, Step Size RF Simulation (s), you will see the default value of 1.5. Update this value to the new Oversampling value used in the CW Source block.

    The default range of  -5.76 MHz to 5.76 MHz can be calculated from the default settings of the CW Source block.

    x_lim_max =  0.5*Oversampling/ Sample time(s) = 0.5*1.5/1.302e-07 =  5.76e+06

    x_lim_min = -0.5*Oversampling/ Sample time(s) = 0.5*1.5/1.302e-07 = -5.76e+06

    - Srikanth

Children