Post Go back to editing

Spurious signals of Adalm-Pluto

Anonymous
Anonymous

    I recently purchased an Adalm-Pluto and started the first tests. As an initial test I used Adalm-Pluto for receiving the linear transponder of the Qatar-Oscar 100 geostationary satellite. I compared Adalm-Pluto signal reception with those of SDRPlay RSPDuo and a simple RTL-SDR usb dongle. I was disappointed to notice that Adalm-Pluto produces many spurious signals, whereas the other SDR hardware doesn't show any, even the $20,- SDR-RTL usb dongle.

    Question:

    1. Is there an issue with my Adalm-Pluto or have I just witnessed typical Adalm-Pluto behavior?
    2. Is there a way to illuminate the spurious signals?

    The following link will give access to three screenshots of SDR Console supporting the above statements: https://www.irista.com/gallery/judupjhis8xh.

    The screenshots show the "waterfall" of the SDR Console for any of the three tested SDR hardware components. Then observe that the waterfall of Adalm-Pluto shows many thin vertical lines, all representing spurious signals.

     

    Thank you,

    Erwin van der Linden

    Parents
    • It can be difficult to compare these radios directly since they have different design purposes and configurability. From our studies we have found that AD9361 has much more sensitivity than RTL-SDR, however the external LNA on RTL does help at low signal levels.

      I would make sure that you are loading a reasonable filter for Pluto, the necessary calibrations are enabled, and you are not saturating the receiver.

      -Travis

    Reply
    • It can be difficult to compare these radios directly since they have different design purposes and configurability. From our studies we have found that AD9361 has much more sensitivity than RTL-SDR, however the external LNA on RTL does help at low signal levels.

      I would make sure that you are loading a reasonable filter for Pluto, the necessary calibrations are enabled, and you are not saturating the receiver.

      -Travis

    Children
    No Data