Hi,
I've gotten my SPI interface to work finally by fixing some verilog but I still get errors when booting Linux. It seems the axi_adxcvr core is trying to enable a clock and it fails with error -5 this and causes the ad9467 driver to throw a -5 error before trying to communicate SPI. When I bypass this error check in the ad9467_probe function the operating system and driver are successfully able to communicate to both of my AD9250 ADCs. Obviously when the driver goes to tell the axi_adxcvr to enable the JESD204B link it fails with a -5 error.
I've turned on additional debugging in the drivers and I'm noticing the axi_adxcvr driver is trying to set the rate to 2MHz from a fixed 100MHz source.
axi_adxcvr 44a60000.axi_adxcvr: adxcvr_clk_recalc_rate: Parent Rate 100000000 Hz axi_adxcvr 44a60000.axi_adxcvr: adxcvr_clk_set_rate: Rate 2000000 Hz Parent Rate 100000000 Hz axi_adxcvr 44a60000.axi_adxcvr: adxcvr_clk_recalc_rate: Parent Rate 100000000 Hz axi_adxcvr 44a60000.axi_adxcvr: AXI-ADXCVR-RX (16.01.a) using GTX2 at 0x44A60000 mapped to 0xf09a0000. Number of Lanes: 4.
After a bit of time, the ad9467 driver starts and performs the probe function and throws the error -5 when it tries to call the function clk_prepare_enable(clk) which is calling the adxcvr_clk_enable function in the axi_adxcvr driver.
The axi_adxcvr driver does throw an error before returning control to the ad9467 driver:
axi_adxcvr 44a60000.axi_adxcvr: adxcvr_clk_enable: RX axi_adxcvr 44a60000.axi_adxcvr: RX Error: 0
I now know the 0 is the link status from the status register in the axi_adxcvr core. It should be 1 but that is not the case.
Let me also provide my current device tree just in case the error is there:
/ { clocks { clk_bus_0: clock@0 { compatible = "fixed-clock"; clock-frequency = <100000000>; clock-output-names = "s_axi_aclk_100M"; #clock-cells = <0>; }; }; }; &axi_ad9250_0_dma { compatible = "adi,axi-dmac-1.00.a"; reg = <0x7c420000 0x10000>; #dma-cells = <1>; interrupts = <0 57 0>; clocks = <&clk_bus_0>; adi,channels { #address-cells = <1>; #size-cells = <0>; dma-channel@0 { reg = <0>; adi,source-bus-width = <64>; adi,source-bus-type = <2>; adi,destination-bus-width = <64>; adi,destination-bus-type = <0>; }; }; }; &axi_ad9250_1_dma { compatible = "adi,axi-dmac-1.00.a"; reg = <0x7c430000 0x10000>; #dma-cells = <1>; interrupts = <0 57 0>; clocks = <&clk_bus_0>; adi,channels { #address-cells = <1>; #size-cells = <0>; dma-channel@0 { reg = <0>; adi,source-bus-width = <64>; adi,source-bus-type = <2>; adi,destination-bus-width = <64>; adi,destination-bus-type = <0>; }; }; }; &spi0 { compatible = "xlnx,zynq-spi-r1p6"; reg = <0xe0006000 0x1000>; status = "okay"; num-cs = <3>; #address-cells = <1>; #size-cells = <0>; adc0_ad9250: ad9250-0@0 { compatible = "adi,ad9250"; reg = <0>; spi-max-frequency = <10000000>; clocks = <&axi_jesd204_rx_0>, <&clk_bus_0>; clock-names = "jesd_adc_clk", "adc_clk"; }; adc1_ad9250: ad9250-1@1 { compatible = "adi,ad9250"; reg = <1>; spi-max-frequency = <10000000>; clocks = <&axi_jesd204_rx_0>, <&clk_bus_0>; clock-names = "jesd_adc_clk", "adc_clk"; }; }; &axi_ad9250_0 { compatible = "xlnx,axi-ad9250-1.00.a"; reg = <0x44a1000 0x10000>; status = "okay"; dmas = <&axi_ad9250_0_dma>; dma-names = "rx"; spibus-connected = <adc0_ad9250>; }; &axi_ad9250_1 { compatible = "xlnx,axi-ad9250-1.00.a"; reg = <0x44a2000 0x10000>; status = "okay"; dmas = <&axi_ad9250_1_dma>; dma-names = "rx"; spibus-connected = <adc1_ad9250>; }; &axi_jesd204_rx_0 { compatible = "adi,axi-jesd204-rx-1.0"; reg = <0x44aa0000 0x1000>; interrupts = <0 55 0>; clocks = <&clk_bus_0>, <&axi_adxcvr_0 1>, <&axi_adxcvr_0 0>; clock_names = "s_axi_aclk", "device_clk", "lane_clk"; #clock-cells = <0>; clock-output-names = "jesd_adc_lane_clk"; adi,octets-per-frame = <2>; adi,frames-per-multiframe = <32>; }; &axi_adxcvr { compatible = "adi,axi-adxcvr-1.0"; reg = <0x44a60000 0x1000>; clocks = <&clk_bus_0>; clock-names = "conv"; #clock-cells = <1>; clock-output-names = "adc_gt_clk", "rx_out_clk"; adi,sys-clk-select = <0>; adi,out-clk-select = <2>; adi,use-cpll-enable; }; &gpio0 { sysref-enable { gpio-hog; gpios = <86 6>; output-high; line-name = "sysref-enable"; }; };
Unfortunately I don't know what could be causing this issue except that the axi_adxcvr doesn't like fixed clocks. The 100 MHz clock I am using feeds into the gbt clock inputs of my GTX2 quads. It is also the clock that goes into a clocking wizard of my Zynq fabric and the clock also goes into the clock input of both of my AD9250 ADCs. The clock source is appropriately distributed using an ADCLK944 fanout buffer. The GTX2 gbtclk signals get this clock after it goes through a AD9515 clock divider which is currently set to not divide or delay the clock and just give the full 100 MHz frequency.
Any suggestions? I'm getting to the point to ask my lead to just make a new board with a AD9517 like the fmcjesdadc1 reference is configured.