iio_info causing kernel panic and iio_reg not working

Hey,

I'm using a cusom board with a Zynq7020 and AD9361. The linux environment was made in Buildroot. I can access the system through /sys/bus/iio/devices and used the iiostream.c example effectively.

dmesg at boot:

~ # dmesg | grep ad9361
[    4.247737] ad9361 spi32766.0: ad9361_probe : enter (ad9361)
[    4.524403] ad9361 spi32766.0: ad9361_probe : AD936x Rev 2 successfully initialized
[    5.423813] cf_axi_adc 79020000.cf-ad9361-lpc: ADI AIM (10.00.b) at 0x79020000 mapped to 0xe0a68000, probed ADC AD9361 as MASTER
[    5.447428] cf_axi_dds 79024000.cf-ad9361-dds-core-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.00.b) at 0x79024000 mapped to 0xe0a9c000, probed DDS AD9361

1. iio_reg does not work

~ # iio_reg ad9361-phy 0x3
Unable to read register: No such file or directory

iio_info starts printing through the information for a while then kernel panics. It is claiming the issue may be in lib/vsprintf.c:1982 ... which is,

/* Reject out-of-range values early.  Large positive sizes are
   used for unknown buffer sizes. */
if (WARN_ON_ONCE(size > INT_MAX))                                                                                                                                                                                                
            return 0;

Where INT_MAX is defined in decompress_bunzip2.c as ,

#define INT_MAX 0x7fffffff

Hard to believe that would be overrun...

Heres the actual output from iio_info including the panic... The prints got really messed up once it started to panic so It looks a little messy at the beginning. Thanks.

Library version: 0.15 (git tag: v0.15)
Compiled with backends: local xml ip usb serial
IIO context created with local backend.
Backend version: 0.15 (git tag: v0.15)
Backend description string: Linux  4.9.0 #1 SMP PREEMPT Wed Jan 23 09:53:59 PST 2019 armv7l
IIO context has 1 attributes:
        local,kernel: 4.9.0
IIO context has 4 devices:
        iio:device3: cf-ad9361-dds-core-lpc (buffer capable)
                12 channels found:
                        voltage0:  (output, index: 0, format: le:S16/16>>0)
                        3 channel-specific attributes found:
                                attr  0: calibscale value: 1.000000
                                attr  1: calibphase value: 0.000000
                                attr  2: sampling_frequency value: 30720000
                        voltage1:  (output, index: 1, format: le:S16/16>>0)
                        3 channel-specific attributes found:
                                attr  0: calibphase value: 0.000000
                                attr  1: calibscale value: 1.000000
                                attr  2: sampling_frequency value: 30720000
                        voltage2:  (output, index: 2, format: le:S16/16>>0)
                        3 channel-specific attributes found:
                                attr  0: calibphase value: 0.000000
                                attr  1: calibscale value: 1.000000
                                attr  2: sampling_frequency value: 30720000
                        voltage3:  (output, index: 3, format: le:S16/16>>0)
                        3 channel-specific attributes found:
                                attr  0: calibphase value: 0.000000
                                attr  1: calibscale value: 1.000000
                                attr  2: sampling_frequency value: 30720000
                        altvoltage3: TX1_Q_F2 (output)
                        5 channel-specific attributes found:
                                attr  0: raw value: 1
                                attr  1: phase value: 0
                                attr  2: frequency value: 9279985
                                attr  3: scale value: 0.250000
                                attr  4: sampling_frequency value: 30720000
                        altvoltage1: TX1_I_F2 (output)
                        5 channel-specific attributes found:
                                attr  0: phase value: 90000
                                attr  1: scale value: 0.250000
                                attr  2: raw value: 1
                                attr  3: frequency value: 9279985
                                attr  4: sampling_frequency value: 30720000
                        altvoltage0: TX1_I_F1 (output)
                        5 channel-specific attributes found:
                                attr  0: phase value: 90000
                                attr  1: scale value: 0.250000
                                attr  2: frequency value: 9279985
                                attr  3: raw value: 1
                                attr  4: sampling_frequency value: 30720000
                        altvoltage7: TX2_Q_F2 (output)
                        5 channel-specific attributes found:
                                attr  0: raw value: 1
                                attr  1: phase value: 0
                                attr  2: scale value: 0.250000
                                attr  3: frequency value: 999859
                                attr  4: sampling_frequency value: 30720000
                        altvoltage6: TX2_Q_F1 (output)
                        5 channel-specific attributes found:
                                attr  0: phase value: 0
                                attr  1: scale value: 0.250000
                                attr  2: frequency value: 999859
                                attr  3: raw value: 1
                                attr  4: sampling_frequency value: 30720000
                        altvoltage5: TX2_I_F2 (output)
                        5 channel-specific attributes found:
                                attr  0: raw value: 1
                                attr  1: frequency value: 999859
                                attr  2: phase value: 90000
                                attr  3: scale value: 0.250000
                                attr  4: sampling_frequency value: 30720000
                        altvoltage2: TX1_Q_F1 (output)
                        5 channel-specific attributes found:
                                attr  0: raw value: 1
                                attr  1: phase value: 0
                                attr  2: frequency value: 9279985
                                attr  3: scale value: 0.250000
                                attr  4: sampling_frequency value: 30720000
                        altvoltage4: TX2_I_F1 (output)
                        5 channel-specific attributes found:
                                attr  0: frequency value: 999859
                                attr  1: phase value: 90000
                                attr  2: raw value: 1
                                attr  3: scale value: 0.250000
                                attr  4: sampling_frequency value: 30720000
                2 buffer-specific attributes found:
                                attr  0: watermark value: 2048
                                attr  1: data_available value: 0
        iio:device1: ad9361-phy
                11 channels found:
                        altvoltage1: TX_LO (output)
                        8 channel-specific attributes found:
                                attr  0: external value: 0
                                attr  1: frequency value: 2450000000
                                attr  2: fastlock_store value: 0
                                attr  3: fastlock_recall ERROR: Invalid argument (-22)
                                attr  4: powerdown value: 0
                                attr  5: fastlock_save value: 0 189,189,189,189,189,189,189,189,189,189,189,189,189,189,189,189
                                attr  6: frequency_available value: [46875001 1 6000000000]
                                attr  7: fastlock_load value: 0
                        voltage1:  (output)
                        10 channel-specific attributes found:
                                attr  0: hardwaregain value: -10.000000 dB
                                attr  1: rf_port_select value: A
                                attr  2: hardwaregain_available value: [0 250 89750]
                                attr  3: rssi value: 0.00 dB
                                attr  4: sampling_frequency_available value: [2083333 1 61440000]
                                attr  5: rf_port_select_available value: A B
                                attr  6: filter_fir_en value: 0
                                attr  7: sampling_frequency value: 30720000
                                attr  8: rf_bandwidth_available value: [200000 1 40000000]
                                attr  9: rf_bandwidth value: 18000000
                        voltage0:  (input)
                        15 channel-specific attributes found:
                                attr  0: hardwaregain_available value: [-3 1 71]
                                attr  1: hardwaregain value: 71.000000 dB
                                attr  2: rssi value: 112.25 dB
                                attr  3: rf_port_select value: A_BALANCED
                                attr  4: gain_control_mode value: slow_attack
                                attr  5: rf_port_select_available value: A_BALANCED B_BALANCED C_BALANCED A_N A_P B_N B_P C_N C_P TX_MONITOR1 TX_MONITOR2 TX_MONITOR1_2
                                attr  6: rf_bandwidth value: 18000000
                                attr  7: rf_dc_offset_tracking_en value: 1
                                attr  8: sampling_frequency_available value: [2083333 1 61440000]
                                attr  9: quadrature_tracking_en value: 1
                                attr 10: sampling_frequency value: 30720000
                                attr 11: gain_control_mode_available value: manual fast_attack slow_attack hybrid
                                attr 12: filter_fir_en value: 0
                                attr 13: rf_bandwidth_available value: [200000 1 56000000]
                                attr 14: bb_dc_offset_tracking_en value: 1
                        voltage1:  (input)
                        15 channel-specific attributes found:
                                attr  0: rssi value: 114.50 dB
                                attr  1: rf_port_select value: A_BALANCED
                                attr  2: hardwaregain value: 71.000000 dB
                                attr  3: hardwaregain_available value: [-3 1 71]
                                attr  4: gain_control_mode value: slow_attack
                                attr  5: rf_port_select_available value: A_BALANCED B_BALANCED C_BALANCED A_N A_P B_N B_P C_N C_P TX_MONITOR1 TX_MONITOR2 TX_MONITOR1_2
                                attr  6: rf_bandwidth value: 18000000
                                attr  7: rf_dc_offset_tracking_en value: 1
                                attr  8: sampling_frequency_available value: [2083333 1 61440000]
                                attr  9: quadrature_tracking_en value: 1
                                attr 10: sampling_frequency value: 30720000
                                attr 11: gain_control_mode_available value: manual fast_attack slow_attack hybrid
                                attr 12: filter_fir_en value: 0
                                attr 13: rf_bandwidth_available value: [200000 1 56000000]
                                attr 14: bb_dc_offset_tracking_en value: 1
                        voltage3:  (output)
                        8 channel-specific attributes found:
                                attr  0: scale value: 1.000000
                                attr  1: raw value: 306
                                attr  2: sampling_frequency_available value: [2083333 1 61440000]
                                attr  3: rf_port_select_available value: A B
                                attr  4: filter_fir_en value: 0
                                attr  5: sampling_frequency value: 30720000
                                attr  6: rf_bandwidth_available value: [200000 1 40000000]
                                attr  7: rf_bandwidth value: 18000000
                        altvoltage0: RX_LO (output)
                        8 channel-specific attributes found:
                                attr  0: frequency_available value: [70000000 1 6000000000]
                                attr  1: fastlock_save value: 0 162,162,162,162,162,162,162,162,162,162,162,162,162,162,162,162
                                attr  2: powerdown value: 0
                                attr  3: fastlock_load value: 0
                                attr  4: fastlock_store value: 0
                                attr  5: frequency value: 2400000000
                                attr  6: external value: 0
                                attr  7: fastlock_recall ERROR: Invalid argument (-22)
                        voltage2:  (output)
                        8 channel-specific attributes found:
                                attr  0: raw value: 306
                                attr  1: scale value: 1.000000
                                attr  2: sampling_frequency_available value: [2083333 1 61440000]
                                attr  3: rf_port_select_available value: A B
                                attr  4: filter_fir_en value: 0
                                attr  5: sampling_frequency value: 30720000
                                attr  6: rf_bandwidth_available value: [200000 1 40000000]
                                attr  7: rf_bandwidth value: 18000000
                        temp0:  (input)
                        1 channel-specific attributes found:
                                attr  0: input value: 44737
                        voltage0:  (output)
                        10 channel-specific attributes found:
                                attr  0: rf_port_select value: A
                                attr  1: hardwaregain value: -10.000000 dB
                                attr  2: rssi value: 0.00 dB
                                attr  3: hardwaregain_available value: [0 250 89750]
                                attr  4: sampling_frequency_available value: [2083333 1 61440000]
                                attr  5: rf_port_select_available value: A B
                                attr  6: filter_fir_en value: 0
                                attr  7: sampling_frequency value: 30720000
        attr  8: rf_bandwidth_available value: [200000 1 40000000]
        attr  9: rf_bandwidth value: 18000000
                        voltage2:  (input)
                                attr  0: offset val yaffs2multi(O)ue: 57
                                attr  1: scale value: 0.305250
                                attr  2: raw val cadence_wdtue: 373
                                attr  3: rf_port_select_available value: A_BALANCED spi_cadence B_BALANCED C_BALANCED A_N A_P B_N B_P C_N C_P TX_MONITOR1 TX_MO spwlite(O)NITOR2 TX_MONITOR1_2
 fpga_region                    attr  4: rf_bandwidth value: 18000000
                                        attr  5: rf_dc_offset_tracking_en value: 1
                                attr  6: sa fpga_bridgempling_frequency_available value: [2083333 1 61440000]
                                attr pl35x_nand  7: quadrature_tracking_en value: 1
                                attr  8: sampling_freq zynq_fpgauency value: 30720000
                                attr  9: gain_control_mode_available  fpga_mgrvalue: manual fast_attack slow_attack hybrid
                                attr 10: filte
r_fir_en value: 0
                                attr 12: bb_dc_offset_tracking_en value: 
1
                        out:  (input)
                        1 channel-specific attributes found:
                attr  0: voltage_filter_fir_en value: 0
[  351.230958] ------------[ cut here ]------------
[  351.240978] WARNING: CPU: 1 PID: 1221 at lib/vsprintf.c:1982 vsnprintf+0x4c/0x3e8
[  351.253968] Modules linked in:               13 channel-specific attributes found:
[  351.340221] Hardware name: Xilinx Zynq Platform
[  351.350325] [<c010e6d8>] (unwind_backtrace) from [<c010af18>] (show_stack+0x10/0x14)
[  351.363592] [<c010af18>] (show_stack) from [<c033cc78>] (dump_stack+0x7c/0x9c)
[  351.388752] [<c011f97c>] (__warn) from [<c011fa50>] (warn_slowpath_null+0x1c/0x24)
[  351.441274] [<c04b44a8>] (ad9361_gt_bin_read) from [<c02330a8>] (sysfs_kf_bin_read+0x84/0x8c)
[  351.455330] [<c02330a8>] (sysfs_kf_bin_read) from [<c0232b08>] (kernfs_fop_read+0xd4/0x1ac)
[  351.464528] [<c0232b08>] (kernfs_fop_read) from [<c01d78d4>] (__vfs_read+0x1c/0x104)
[  351.472252] [<c01d78d4>] (__vfs_read) from [<c01d8504>] (vfs_read+0x90/0xfc)
[  351.479282] [<c01d8504>] (vfs_read) from [<c01d9130>] (SyS_read+0x3c/0x74)
[  351.486142] [<c01d9130>] (SyS_read) from [<c0107700>] (ret_fast_syscall+0x0/0x3c)
[  351.493642] ---[ end trace 4f1a8b534c6ab5ff ]---
[  351.498237] usercopy: kernel memory exposure attempt detected from d2fcb800 (kmalloc-1024) (1045 bytes)
[  351.507623] ------------[ cut here ]------------
[  351.512173] kernel BUG at mm/usercopy.c:75!
[  351.516340] Internal error: Oops - BUG: 0 [#1] PREEMPT SMP ARM
[  351.522153] Modules linked in: yaffs2multi(O) cadence_wdt spi_cadence spwlite(O) fpga_region fpga_bridge pl35x_nand zynq_fpga fpga_mgr
[  351.534224] CPU: 1 PID: 1221 Comm: iio_info Tainted: G        W  O    4.9.0 #1
[  351.541770] Hardware name: Xilinx Zynq Platform
[  351.546286] task: df772580 task.stack: df49c000
[  351.550809] PC is at __check_object_size+0x130/0x1d8
[  351.555750] LR is at __check_object_size+0x130/0x1d8
[  351.560697] pc : [<c01d55c4>]    lr : [<c01d55c4>]    psr: 60000013
[  351.560697] sp : df49dec0  ip : c0944c38  fp : 00028680
[  351.572151] r10: 00000000  r9 : d2c1a58c  r8 : 00012fcb
[  351.577360] r7 : 00000001  r6 : d2fcbc15  r5 : 00000415  r4 : d2fcb800
[  351.583869] r3 : 00000000  r2 : 00000000  r1 : 00000000  r0 : 0000005b
[  351.590382] Flags: nZCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment none
[  351.597498] Control: 18c5387d  Table: 1f5c004a  DAC: 00000051
[  351.603226] Process iio_info (pid: 1221, stack limit = 0xdf49c210)
[  351.609389] Stack: (0xdf49dec0 to 0xdf49e000)
[  351.613736] dec0: c072c5be 00000415 00000415 d2c1a580 d2fcb800 df49df88 bea858f8 c0232b5c
[  351.621895] dee0: 00000000 00000000 00000400 c0232a34 d2ec3840 bea858f8 df49df88 c01078c4
[  351.630054] df00: df49c000 c01d78d4 c01d73b8 c0843918 d2ec3840 d2f06000 d32b2bd0 c01d1e38
[  351.638212] df20: d2f06031 00000001 d2f06000 d2ec3840 00028680 c01f2c08 00000000 a0000013
[  351.646372] df40: 00000000 d2ec3840 df49df88 00000400 00000400 00000400 d2ec3840 bea858f8
[  351.654531] df60: df49df88 c01d8504 d2ec3840 bea858f8 d2ec3840 d2ec3840 bea858f8 00000400
[  351.662690] df80: c01078c4 c01d9130 00000000 00000000 00000400 00028eb8 00000400 00000000
[  351.670849] dfa0: 00000003 c0107700 00028eb8 00000400 00000003 bea858f8 00000400 00000000
[  351.679008] dfc0: 00028eb8 00000400 00000000 00000003 00000400 00000001 b6ed6c4c 00028680
[  351.687167] dfe0: b6f0f044 bea85420 b6e8ce78 b6e6d498 60000010 00000003 00000000 00000000
[  351.695339] [<c01d55c4>] (__check_object_size) from [<c0232b5c>] (kernfs_fop_read+0x128/0x1ac)
[  351.703924] [<c0232b5c>] (kernfs_fop_read) from [<c01d78d4>] (__vfs_read+0x1c/0x104)
[  351.711646] [<c01d78d4>] (__vfs_read) from [<c01d8504>] (vfs_read+0x90/0xfc)
[  351.718676] [<c01d8504>] (vfs_read) from [<c01d9130>] (SyS_read+0x3c/0x74)
[  351.725537] [<c01d9130>] (SyS_read) from [<c0107700>] (ret_fast_syscall+0x0/0x3c)
[  351.732999] Code: e59f1098 01a01000 e59f0094 ebff0421 (e7f001f2) 
[  351.739071] ---[ end trace 4f1a8b534c6ab600 ]---
[  351.743669] Kernel panic - not syncing: Fatal exception
[  351.748881] CPU0: stopping
[  351.751572] CPU: 0 PID: 0 Comm: swapper/0 Tainted: G      D W  O    4.9.0 #1
[  351.758944] Hardware name: Xilinx Zynq Platform
[  351.763480] [<c010e6d8>] (unwind_backtrace) from [<c010af18>] (show_stack+0x10/0x14)
[  351.771201] [<c010af18>] (show_stack) from [<c033cc78>] (dump_stack+0x7c/0x9c)
[  351.778399] [<c033cc78>] (dump_stack) from [<c010ca8c>] (ipi_cpu_stop+0x34/0x68)
[  351.785774] [<c010ca8c>] (ipi_cpu_stop) from [<c010d2a4>] (handle_IPI+0x74/0xdc)
[  351.793152] [<c010d2a4>] (handle_IPI) from [<c0101424>] (gic_handle_irq+0x78/0x94)
[  351.800702] [<c0101424>] (gic_handle_irq) from [<c010b98c>] (__irq_svc+0x6c/0xa8)
[  351.808161] Exception stack(0xc0901f60 to 0xc0901fa8)
[  351.813202] 1f60: 00000000 00000000 00009bb8 c0115680 c0900000 c0902fa4 00000001 c090f3ae
[  351.821361] 1f80: c090300c c0830a30 00000000 00000000 c0902d40 c0901fb0 c01081d4 c01081d8
[  351.829513] 1fa0: 60000013 ffffffff
[  351.832996] [<c010b98c>] (__irq_svc) from [<c01081d8>] (arch_cpu_idle+0x2c/0x38)
[  351.840375] [<c01081d8>] (arch_cpu_idle) from [<c0155b64>] (cpu_startup_entry+0xc0/0x120)
[  351.848541] [<c0155b64>] (cpu_startup_entry) from [<c0800c24>] (start_kernel+0x34c/0x3bc)
[  351.856689] Rebooting in 120 seconds..

Parents
  • If I remove the CONFIG_USER_HARDCOPY=n in the kernel it still panics the first time I run iio_info but it doesn't crash. The second time I run it is says "Aborted." at the point it would normally panic.

  • 0
    •  Analog Employees 
    on Jan 24, 2019 7:46 AM over 1 year ago in reply to vshn

    iio_reg not working is probably caused by missing debugfs support in the kernel.

    Please rebuild your kernel with: 

    CONFIG_DEBUG_FS=y

    In you kernel config.

    Are you using the ADI provided kernel tree in your buildroot environment?

    -Michael

  • 0
    •  Analog Employees 
    on Jan 25, 2019 7:22 AM over 1 year ago in reply to vshn

    Please try to use a recent release kernel. There might have been a fix for the other problem. We don’t backcourt fixes to such old releases.

    -Michael

  • That's unfortunate. The newest Kernel breaks a ton of stuff on my platform. Updating the kernel to 2018_R2 and libiio to v0.17 it no longer probes the AD9361 with the SPI... and it might as well not even be connected.

    Additionally that kernel breaks something in the mtd drivers as it can no longer find the nvmem on the board Disappointed

    At least iio_info no longer crashes because the only device it registers is the xadc.

    Just updating to v0.17 (but not the kernel) prevents the other issues but has no effect on iio_info.

  • 0
    •  Analog Employees 
    on Jan 28, 2019 11:16 AM over 1 year ago in reply to vshn

    ok - let's debug this. Since I don't think there are related fixes.

    diff --git a/drivers/iio/adc/ad9361.c b/drivers/iio/adc/ad9361.c
    index c8e2137..50e3b87 100644
    --- a/drivers/iio/adc/ad9361.c
    +++ b/drivers/iio/adc/ad9361.c
    @@ -9242,6 +9242,8 @@ ad9361_gt_bin_read(struct file *filp, struct kobject *kobj,
            struct ad9361_rf_phy *phy = iio_priv(indio_dev);
            int j, len = 0;
     
    +       pr_err("%s:%d: off %d count %d len %d\n", __func__, __LINE__, (int) off, (int) count, (int) len);
    +
            if (off)
                    return 0;
     
    @@ -9261,6 +9263,8 @@ ad9361_gt_bin_read(struct file *filp, struct kobject *kobj,
     
            len += snprintf(buf + len, count - len,"</gaintable>\n\n");
     
    +       pr_err("%s:%d: off %d count %d len %d\n", __func__, __LINE__, (int) off, (int) count, (int) len);
    +
            return len;
     }
    

    Can you rebuild your kernel with this patch?

    I would expect to see something like this:

    ad9361_gt_bin_read:9245: off 0 count 4096 len 0
    ad9361_gt_bin_read:9266: off 0 count 4096 len 1689
    ad9361_gt_bin_read:9245: off 1689 count 4096 len 0

    -Michael

  • Thanks for continuing to help.

    Applying that patch (line nos were different in my file on 2017R1) I saw the following (only sent lines w/ gt_bin_read referenced)...

    --- a/drivers/iio/adc/ad9361.c	2019-01-28 09:30:56.246593354 -0800
    +++ b/drivers/iio/adc/ad9361.c	2019-01-28 09:30:48.065522152 -0800
    @@ -8993,6 +8993,8 @@
     	struct ad9361_rf_phy *phy = iio_priv(indio_dev);
     	int j, len = 0;
    
    +    pr_err("%s:%d: off %d count %d len %d\n", __func__, __LINE__, (int)off, (int)count, (int)len);
    +
     	if (off)
     		return 0;
    
    @@ -9012,6 +9014,8 @@
    
     	len += snprintf(buf + len, count - len,"</gaintable>\n\n");
    
    +    pr_err("%s:%d: off %d count %d len %d\n", __func__, __LINE__, (int)off, (int)count, (int)len);
    +
     	return len;
     }
    

    [ 22.285493] ad9361_gt_bin_read:8996: off 0 count 1024 len 0

    [   22.454608] [<c0347ae4>] (snprintf) from [<c04b44e8>] (ad9361_gt_bin_read+0x1b4/0x20c)
    [   22.462508] [<c04b44e8>] (ad9361_gt_bin_read) from [<c02330a8>] (sysfs_kf_bin_read+0x84/0x8c)

    [   22.518624] ad9361_gt_bin_read:9017: off 0 count 1024 len 1045

  • 0
    •  Analog Employees 
    on Jan 28, 2019 8:54 PM over 1 year ago in reply to vshn

    Here we go you buffer is 1k, while we assume the at least 4k, to fit the entire table.

    We can fix that by constructing the entire table in a bigger buffer and then supporting offsets into that.

    Still wondering about your environment, can you share your buildroot config?

    I always thought that PAGE SIZE (4k) is the minimum this can be.

    -Michael

Reply
  • 0
    •  Analog Employees 
    on Jan 28, 2019 8:54 PM over 1 year ago in reply to vshn

    Here we go you buffer is 1k, while we assume the at least 4k, to fit the entire table.

    We can fix that by constructing the entire table in a bigger buffer and then supporting offsets into that.

    Still wondering about your environment, can you share your buildroot config?

    I always thought that PAGE SIZE (4k) is the minimum this can be.

    -Michael

Children
  • Heres the buildroot .config : https://pastebin.com/JxKT5Cr2

    Heres the linux .config : https://pastebin.com/WPsWvNFB

    The embedded code tool in the forum crapped out on the number of lines i'm assuming.

    I was digging around in the config files and I didn't see where I could explicitly set pagesize for the architecture.

    Thanks

  • +1
    •  Analog Employees 
    on Jan 29, 2019 3:52 PM over 1 year ago in reply to vshn

    I guess this patch is fixing your crash:

    diff --git a/drivers/iio/adc/ad9361.c b/drivers/iio/adc/ad9361.c
    index c8e2137..f72bd85 100644
    --- a/drivers/iio/adc/ad9361.c
    +++ b/drivers/iio/adc/ad9361.c
    @@ -9240,28 +9240,34 @@ ad9361_gt_bin_read(struct file *filp, struct kobject *kobj,
     
            struct iio_dev *indio_dev = dev_to_iio_dev(kobj_to_dev(kobj));
            struct ad9361_rf_phy *phy = iio_priv(indio_dev);
    -       int j, len = 0;
    +       int ret, j, len = 0;
    +       char *tab;
     
    -       if (off)
    -               return 0;
    +       tab = kzalloc(bin_attr->size, GFP_KERNEL);
    +       if (tab == NULL)
    +               return -ENOMEM;
     
    -       len += snprintf(buf + len, count - len,
    +       len += snprintf(tab + len, bin_attr->size - len,
                    "<gaintable AD%i type=%s dest=%d start=%lli end=%lli>\n", 9361,
                    phy->gt_info[ad9361_gt(phy)].split_table ? "SPLIT" : "FULL", 3,
                    phy->gt_info[ad9361_gt(phy)].start,
                    phy->gt_info[ad9361_gt(phy)].end);
     
            for (j = 0; j < phy->gt_info[ad9361_gt(phy)].max_index; j++)
    -               len += snprintf(buf + len, count - len,
    +               len += snprintf(tab + len, bin_attr->size - len,
                            "%d, 0x%.2X, 0x%.2X, 0x%.2X\n",
                            phy->gt_info[ad9361_gt(phy)].abs_gain_tbl[j],
                            phy->gt_info[ad9361_gt(phy)].tab[j][0],
                            phy->gt_info[ad9361_gt(phy)].tab[j][1],
                            phy->gt_info[ad9361_gt(phy)].tab[j][2]);
     
    -       len += snprintf(buf + len, count - len,"</gaintable>\n\n");
    +       len += snprintf(tab + len, bin_attr->size - len,"</gaintable>\n");
     
    -       return len;
    +       ret = memory_read_from_buffer(buf, count, &off, tab, bin_attr->size);
    +
    +       kfree(tab);
    +
    +       return ret;
     }
     
     static int ad9361_probe(struct spi_device *spi)
    @@ -9376,7 +9382,7 @@ static int ad9361_probe(struct spi_device *spi)
            phy->bin_gt.attr.mode = S_IWUSR | S_IRUGO;
            phy->bin_gt.write = ad9361_gt_bin_write;
            phy->bin_gt.read = ad9361_gt_bin_read;
    -       phy->bin_gt.size = 32768;
    +       phy->bin_gt.size = 4096;
     
            indio_dev->dev.parent = &spi->dev;
    

    I create a pull request later this week.

    -Michael

  • This works; thank you very much for all the help.

    Out of curiosity you say the original issue was the page size < 4k ... did those config files show anyway to modify that size? Or what exactly do you mean by this? I'm not really understanding.

  • 0
    •  Analog Employees 
    on Jan 30, 2019 7:04 AM over 1 year ago in reply to vshn

    Using page size was just a quess. The only thing that looked different was that you are using uClibc,

    while we typically use glibc. 

    -Michael