(ZCU102 + FMCOMMS3) Booting Issue : Login Prompt is not Coming

Hi all,

I created Linux Image using ADI Kernel ( 2018_R1) and Petalinux Tool. I added device-tree in my petalinux project (system-user.dtsi) and selected AD9361 drivers in the kernel configuration, then I built the project. Build Is successful and I copied the files on SD card and booted the device.

Below is given the boot message:

Release 2018.2 Oct 1 2018 - 14:59:42
NOTICE: ATF running on XCZU9EG/silicon v4/RTL5.1 at 0xfffea000
NOTICE: BL31: Secure code at 0x0
NOTICE: BL31: Non secure code at 0x8000000
NOTICE: BL31: v1.4(release):xilinx-v2018.1-4-g93a69a5a
NOTICE: BL31: Built : 04:21:54, Oct 3 2018
PMUFW: v1.0


U-Boot 2018.01 (Oct 03 2018 - 11:24:07 +0530) Xilinx ZynqMP ZCU102 rev1.0

I2C: ready
DRAM: 4 GiB
EL Level: EL2
Chip ID: zu9eg
MMC: sdhci@ff170000: 0 (SD)
SF: Detected n25q512a with page size 512 Bytes, erase size 128 KiB, total 128 MiB
*** Warning - bad CRC, using default environment

In: serial@ff000000
Out: serial@ff000000
Err: serial@ff000000
Model: ZynqMP ZCU102 Rev1.0
Board: Xilinx ZynqMP
Bootmode: LVL_SHFT_SD_MODE1
Net: ZYNQ GEM: ff0e0000, phyaddr c, interface rgmii-id
eth0: ethernet@ff0e0000
U-BOOT for eldaas_linux

Hit any key to stop autoboot: 0
Device: sdhci@ff170000
Manufacturer ID: 3
OEM: 5344
Name: SU08G
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 7.4 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes
reading image.ub
6985820 bytes read in 471 ms (14.1 MiB/s)
## Loading kernel from FIT Image at 10000000 ...
Using 'conf@system-top.dtb' configuration
Trying 'kernel@1' kernel subimage
Description: Linux kernel
Type: Kernel Image
Compression: gzip compressed
Data Start: 0x100000f8
Data Size: 6937400 Bytes = 6.6 MiB
Architecture: AArch64
OS: Linux
Load Address: 0x00080000
Entry Point: 0x00080000
Hash algo: sha1
Hash value: 168604421a335d58edbd2e2f8778fa1874f84808
Verifying Hash Integrity ... sha1+ OK
## Loading fdt from FIT Image at 10000000 ...
Using 'conf@system-top.dtb' configuration
Trying 'fdt@system-top.dtb' fdt subimage
Description: Flattened Device Tree blob
Type: Flat Device Tree
Compression: uncompressed
Data Start: 0x1069dd34
Data Size: 46516 Bytes = 45.4 KiB
Architecture: AArch64
Hash algo: sha1
Hash value: a48822adfc075490eab70af4ad38c2fa0677b247
Verifying Hash Integrity ... sha1+ OK
Booting using the fdt blob at 0x1069dd34
Uncompressing Kernel Image ... OK
Loading Device Tree to 000000007dd80000, end 000000007dd8e5b3 ... OK

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.0 (oe-user@oe-host) (gcc version 7.2.0 (GCC)) #3 SMP Wed Oct 3 09:46:54 IST 2018
[ 0.000000] Boot CPU: AArch64 Processor [410fd034]
[ 0.000000] Machine model: ZynqMP ZCU102 Rev1.0
[ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')
[ 0.000000] bootconsole [cdns0] enabled
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 256 MiB at 0x000000006dc00000
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] percpu: Embedded 21 pages/cpu @ffffffc87ff62000 s45080 r8192 d32744 u86016
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: enabling workaround for ARM erratum 845719
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1033987
[ 0.000000] Kernel command line: earlycon clk_ignore_unused root=/dev/mmcblk0p2 rw rootwait
[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)
[ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)
[ 0.000000] software IO TLB [mem 0x69c00000-0x6dc00000] (64MB) mapped at [ffffffc069c00000-ffffffc06dbfffff]
[ 0.000000] Memory: 3784528K/4193280K available (9916K kernel code, 640K rwdata, 3136K rodata, 512K init, 2160K bss, 146608K reserved, 262144K cma-reserved)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] modules : 0xffffff8000000000 - 0xffffff8008000000 ( 128 MB)
[ 0.000000] vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000 ( 250 GB)
[ 0.000000] .text : 0xffffff8008080000 - 0xffffff8008a30000 ( 9920 KB)
[ 0.000000] .rodata : 0xffffff8008a30000 - 0xffffff8008d50000 ( 3200 KB)
[ 0.000000] .init : 0xffffff8008d50000 - 0xffffff8008dd0000 ( 512 KB)
[ 0.000000] .data : 0xffffff8008dd0000 - 0xffffff8008e70200 ( 641 KB)
[ 0.000000] .bss : 0xffffff8008e70200 - 0xffffff800908c330 ( 2161 KB)
[ 0.000000] fixed : 0xffffffbefe7fd000 - 0xffffffbefec00000 ( 4108 KB)
[ 0.000000] PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000 ( 16 MB)
[ 0.000000] vmemmap : 0xffffffbf00000000 - 0xffffffc000000000 ( 4 GB maximum)
[ 0.000000] 0xffffffbf00000000 - 0xffffffbf1dc00000 ( 476 MB actual)
[ 0.000000] memory : 0xffffffc000000000 - 0xffffffc880000000 ( 34816 MB)
[ 0.000000] Hierarchical RCU implementation.
[ 0.000000] RCU event tracing is enabled.
[ 0.000000] RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
[ 0.000000] GIC: Using split EOI/Deactivate mode
[ 0.000000] arch_timer: cp15 timer(s) running at 99.99MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x170f8dc196, max_idle_ns: 440795203664 ns
[ 0.000003] sched_clock: 56 bits at 99MHz, resolution 10ns, wraps every 4398046511099ns
[ 0.008325] Console: colour dummy device 80x25
[ 0.012585] console [tty0] enabled
[ 0.015952] bootconsole [cdns0] disabled
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.0 (oe-user@oe-host) (gcc version 7.2.0 (GCC)) #3 SMP Wed Oct 3 09:46:54 IST 2018
[ 0.000000] Boot CPU: AArch64 Processor [410fd034]
[ 0.000000] Machine model: ZynqMP ZCU102 Rev1.0
[ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')
[ 0.000000] bootconsole [cdns0] enabled
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 256 MiB at 0x000000006dc00000
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] percpu: Embedded 21 pages/cpu @ffffffc87ff62000 s45080 r8192 d32744 u86016
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: enabling workaround for ARM erratum 845719
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1033987
[ 0.000000] Kernel command line: earlycon clk_ignore_unused root=/dev/mmcblk0p2 rw rootwait
[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)
[ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)
[ 0.000000] software IO TLB [mem 0x69c00000-0x6dc00000] (64MB) mapped at [ffffffc069c00000-ffffffc06dbfffff]
[ 0.000000] Memory: 3784528K/4193280K available (9916K kernel code, 640K rwdata, 3136K rodata, 512K init, 2160K bss, 146608K reserved, 262144K cma-reserved)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] modules : 0xffffff8000000000 - 0xffffff8008000000 ( 128 MB)
[ 0.000000] vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000 ( 250 GB)
[ 0.000000] .text : 0xffffff8008080000 - 0xffffff8008a30000 ( 9920 KB)
[ 0.000000] .rodata : 0xffffff8008a30000 - 0xffffff8008d50000 ( 3200 KB)
[ 0.000000] .init : 0xffffff8008d50000 - 0xffffff8008dd0000 ( 512 KB)
[ 0.000000] .data : 0xffffff8008dd0000 - 0xffffff8008e70200 ( 641 KB)
[ 0.000000] .bss : 0xffffff8008e70200 - 0xffffff800908c330 ( 2161 KB)
[ 0.000000] fixed : 0xffffffbefe7fd000 - 0xffffffbefec00000 ( 4108 KB)
[ 0.000000] PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000 ( 16 MB)
[ 0.000000] vmemmap : 0xffffffbf00000000 - 0xffffffc000000000 ( 4 GB maximum)
[ 0.000000] 0xffffffbf00000000 - 0xffffffbf1dc00000 ( 476 MB actual)
[ 0.000000] memory : 0xffffffc000000000 - 0xffffffc880000000 ( 34816 MB)
[ 0.000000] Hierarchical RCU implementation.
[ 0.000000] RCU event tracing is enabled.
[ 0.000000] RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
[ 0.000000] GIC: Using split EOI/Deactivate mode
[ 0.000000] arch_timer: cp15 timer(s) running at 99.99MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x170f8dc196, max_idle_ns: 440795203664 ns
[ 0.000003] sched_clock: 56 bits at 99MHz, resolution 10ns, wraps every 4398046511099ns
[ 0.008325] Console: colour dummy device 80x25
[ 0.012585] console [tty0] enabled
[ 0.015952] bootconsole [cdns0] disabled
[ 0.019862] Calibrating delay loop (skipped), value calculated using timer frequency.. 199.98 BogoMIPS (lpj=399960)
[ 0.019875] pid_max: default: 32768 minimum: 301
[ 0.019975] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.019993] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.020551] ASID allocator initialised with 65536 entries
[ 0.020599] Hierarchical SRCU implementation.
[ 0.020947] EFI services will not be available.
[ 0.020973] zynqmp_plat_init Platform Management API v1.0
[ 0.020982] zynqmp_plat_init Trustzone version v1.0
[ 0.021079] smp: Bringing up secondary CPUs ...
[ 0.021331] Detected VIPT I-cache on CPU1
[ 0.021358] CPU1: Booted secondary processor [410fd034]
[ 0.021630] Detected VIPT I-cache on CPU2
[ 0.021648] CPU2: Booted secondary processor [410fd034]
[ 0.021911] Detected VIPT I-cache on CPU3
[ 0.021929] CPU3: Booted secondary processor [410fd034]
[ 0.021970] smp: Brought up 1 node, 4 CPUs
[ 0.022002] SMP: Total of 4 processors activated.
[ 0.022010] CPU features: detected feature: 32-bit EL0 Support
[ 0.022021] CPU: All CPU(s) started at EL2
[ 0.022036] alternatives: patching kernel code
[ 0.022754] devtmpfs: initialized
[ 0.027376] random: get_random_u32 called from bucket_table_alloc+0x108/0x260 with crng_init=0
[ 0.027579] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.027600] futex hash table entries: 1024 (order: 5, 131072 bytes)
[ 0.027810] random: fast init done
[ 0.032969] xor: measuring software checksum speed
[ 0.071934] 8regs : 2302.000 MB/sec
[ 0.111964] 8regs_prefetch: 2052.000 MB/sec
[ 0.151995] 32regs : 2830.000 MB/sec
[ 0.192026] 32regs_prefetch: 2381.000 MB/sec
[ 0.192034] xor: using function: 32regs (2830.000 MB/sec)
[ 0.192099] pinctrl core: initialized pinctrl subsystem
[ 0.192597] NET: Registered protocol family 16
[ 0.193373] cpuidle: using governor menu
[ 0.193941] vdso: 2 pages (1 code @ ffffff8008a36000, 1 data @ ffffff8008dd4000)
[ 0.193957] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.194412] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.223920] reset_zynqmp reset-controller: Xilinx zynqmp reset driver probed
[ 0.224499] ARM CCI_400_r1 PMU driver probed
[ 0.229384] zynqmp-pinctrl ff180000.pinctrl: zynqmp pinctrl initialized
[ 0.237415] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.304243] raid6: int64x1 gen() 402 MB/s
[ 0.372223] raid6: int64x1 xor() 446 MB/s
[ 0.440269] raid6: int64x2 gen() 687 MB/s
[ 0.508336] raid6: int64x2 xor() 603 MB/s
[ 0.576377] raid6: int64x4 gen() 1042 MB/s
[ 0.644393] raid6: int64x4 xor() 742 MB/s
[ 0.712492] raid6: int64x8 gen() 980 MB/s
[ 0.780506] raid6: int64x8 xor() 745 MB/s
[ 0.848566] raid6: neonx1 gen() 726 MB/s
[ 0.916596] raid6: neonx1 xor() 851 MB/s
[ 0.984651] raid6: neonx2 gen() 1168 MB/s
[ 1.052701] raid6: neonx2 xor() 1207 MB/s
[ 1.120771] raid6: neonx4 gen() 1505 MB/s
[ 1.188792] raid6: neonx4 xor() 1441 MB/s
[ 1.256836] raid6: neonx8 gen() 1651 MB/s
[ 1.324887] raid6: neonx8 xor() 1534 MB/s
[ 1.324895] raid6: using algorithm neonx8 gen() 1651 MB/s
[ 1.324903] raid6: .... xor() 1534 MB/s, rmw enabled
[ 1.324910] raid6: using neon recovery algorithm
[ 1.326325] SCSI subsystem initialized
[ 1.326484] usbcore: registered new interface driver usbfs
[ 1.326522] usbcore: registered new interface driver hub
[ 1.326562] usbcore: registered new device driver usb
[ 1.326623] media: Linux media interface: v0.10
[ 1.326649] Linux video capture interface: v2.00
[ 1.326693] pps_core: LinuxPPS API ver. 1 registered
[ 1.326702] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 1.326723] PTP clock support registered
[ 1.326749] EDAC MC: Ver: 3.0.0
[ 1.327033] zynqmp-ipi ff9905c0.mailbox: Probed ZynqMP IPI Mailbox driver.
[ 1.327183] FPGA manager framework
[ 1.327286] fpga-region fpga-full: FPGA Region probed
[ 1.327382] Advanced Linux Sound Architecture Driver Initialized.
[ 1.327618] Bluetooth: Core ver 2.22
[ 1.327647] NET: Registered protocol family 31
[ 1.327655] Bluetooth: HCI device and connection manager initialized
[ 1.327667] Bluetooth: HCI socket layer initialized
[ 1.327676] Bluetooth: L2CAP socket layer initialized
[ 1.327694] Bluetooth: SCO socket layer initialized
[ 1.328213] clocksource: Switched to clocksource arch_sys_counter
[ 1.328282] VFS: Disk quotas dquot_6.6.0
[ 1.328325] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 1.332170] NET: Registered protocol family 2
[ 1.332486] TCP established hash table entries: 32768 (order: 6, 262144 bytes)
[ 1.332699] TCP bind hash table entries: 32768 (order: 7, 524288 bytes)
[ 1.333081] TCP: Hash tables configured (established 32768 bind 32768)
[ 1.333150] UDP hash table entries: 2048 (order: 4, 65536 bytes)
[ 1.333227] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes)
[ 1.333382] NET: Registered protocol family 1
[ 1.333607] RPC: Registered named UNIX socket transport module.
[ 1.333617] RPC: Registered udp transport module.
[ 1.333624] RPC: Registered tcp transport module.
[ 1.333631] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 1.334051] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[ 1.334197] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 1.334853] audit: initializing netlink subsys (disabled)
[ 1.335176] audit: type=2000 audit(1.316:1): state=initialized audit_enabled=0 res=1
[ 1.335220] workingset: timestamp_bits=62 max_order=20 bucket_order=0
[ 1.335842] NFS: Registering the id_resolver key type
[ 1.335863] Key type id_resolver registered
[ 1.335870] Key type id_legacy registered
[ 1.335882] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 1.335903] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
[ 1.359687] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
[ 1.359708] io scheduler noop registered
[ 1.359715] io scheduler deadline registered
[ 1.359735] io scheduler cfq registered (default)
[ 1.359743] io scheduler mq-deadline registered
[ 1.359751] io scheduler kyber registered
[ 1.360369] nwl-pcie fd0e0000.pcie: Link is DOWN
[ 1.360412] OF: PCI: host bridge /amba/pcie@fd0e0000 ranges:
[ 1.360433] OF: PCI: MEM 0xe0000000..0xefffffff -> 0xe0000000
[ 1.360445] OF: PCI: MEM 0x600000000..0x7ffffffff -> 0x600000000
[ 1.360571] nwl-pcie fd0e0000.pcie: PCI host bridge to bus 0000:00
[ 1.360586] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 1.360596] pci_bus 0000:00: root bus resource [mem 0xe0000000-0xefffffff]
[ 1.360607] pci_bus 0000:00: root bus resource [mem 0x600000000-0x7ffffffff pref]
[ 1.360863] pci 0000:00:00.0: PCI bridge to [bus 01-0c]
[ 1.361761] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed
[ 1.362161] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success
[ 1.362325] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success
[ 1.362484] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success
[ 1.362645] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success
[ 1.362803] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success
[ 1.362963] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success
[ 1.363123] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success
[ 1.363286] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success
[ 1.363506] xilinx-zynqmp-dma ffa80000.dma: ZynqMP DMA driver Probe success
[ 1.363664] xilinx-zynqmp-dma ffa90000.dma: ZynqMP DMA driver Probe success
[ 1.363816] xilinx-zynqmp-dma ffaa0000.dma: ZynqMP DMA driver Probe success
[ 1.363973] xilinx-zynqmp-dma ffab0000.dma: ZynqMP DMA driver Probe success
[ 1.364126] xilinx-zynqmp-dma ffac0000.dma: ZynqMP DMA driver Probe success
[ 1.364309] xilinx-zynqmp-dma ffad0000.dma: ZynqMP DMA driver Probe success
[ 1.364471] xilinx-zynqmp-dma ffae0000.dma: ZynqMP DMA driver Probe success
[ 1.364623] xilinx-zynqmp-dma ffaf0000.dma: ZynqMP DMA driver Probe success
[ 1.389044] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[ 1.392383] cacheinfo: Unable to detect cache hierarchy for CPU 0
[ 1.396282] brd: module loaded
[ 1.399477] loop: module loaded
[ 1.400406] ahci-ceva fd0c0000.ahci: couldn't get PHY in node ahci: -517
[ 1.400574] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.402172] m25p80 spi0.0: SPI-NOR-UniqueID 1044002c39910007f1ff170029ac71a285
[ 1.402320] m25p80 spi0.0: n25q512a (131072 Kbytes)
[ 1.402342] 3 ofpart partitions found on MTD device spi0.0
[ 1.402350] Creating 3 MTD partitions on "spi0.0":
[ 1.402363] 0x000000000000-0x000000100000 : "boot"
[ 1.402779] 0x000000100000-0x000000140000 : "bootenv"
[ 1.403144] 0x000000140000-0x000001740000 : "kernel"
[ 1.404343] libphy: Fixed MDIO Bus: probed
[ 1.405293] tun: Universal TUN/TAP device driver, 1.6
[ 1.405423] CAN device driver interface
[ 1.407428] macb ff0e0000.ethernet: Not enabling partial store and forward
[ 1.407799] libphy: MACB_mii_bus: probed
[ 1.409447] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 31 (00:0a:35:00:22:01)
[ 1.409464] TI DP83867 ff0e0000.ethernet-ffffffff:0c: attached PHY driver [TI DP83867] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:0c, irq=POLL)
[ 1.410093] usbcore: registered new interface driver asix
[ 1.410144] usbcore: registered new interface driver ax88179_178a
[ 1.410175] usbcore: registered new interface driver cdc_ether
[ 1.410207] usbcore: registered new interface driver net1080
[ 1.410237] usbcore: registered new interface driver cdc_subset
[ 1.410266] usbcore: registered new interface driver zaurus
[ 1.410304] usbcore: registered new interface driver cdc_ncm
[ 1.410588] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM
[ 1.411671] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.411682] ehci-pci: EHCI PCI platform driver
[ 1.411963] usbcore: registered new interface driver uas
[ 1.412002] usbcore: registered new interface driver usb-storage
[ 1.412500] rtc_zynqmp ffa60000.rtc: rtc core: registered ffa60000.rtc as rtc0
[ 1.412556] i2c /dev entries driver
[ 1.413547] IR NEC protocol handler initialized
[ 1.413556] IR RC5(x/sz) protocol handler initialized
[ 1.413563] IR RC6 protocol handler initialized
[ 1.413570] IR JVC protocol handler initialized
[ 1.413577] IR Sony protocol handler initialized
[ 1.413585] IR SANYO protocol handler initialized
[ 1.413592] IR Sharp protocol handler initialized
[ 1.413599] IR MCE Keyboard/mouse protocol handler initialized
[ 1.413606] IR XMP protocol handler initialized
[ 1.414666] usbcore: registered new interface driver uvcvideo
[ 1.414675] USB Video Class driver (1.1.1)
[ 1.415160] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer at ffffff8009135000 with timeout 10s
[ 1.415342] Bluetooth: HCI UART driver ver 2.3
[ 1.415353] Bluetooth: HCI UART protocol H4 registered
[ 1.415361] Bluetooth: HCI UART protocol BCSP registered
[ 1.415390] Bluetooth: HCI UART protocol LL registered
[ 1.415399] Bluetooth: HCI UART protocol ATH3K registered
[ 1.415407] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 1.415450] Bluetooth: HCI UART protocol Intel registered
[ 1.415458] Bluetooth: HCI UART protocol QCA registered
[ 1.415493] usbcore: registered new interface driver bcm203x
[ 1.415528] usbcore: registered new interface driver bpa10x
[ 1.415561] usbcore: registered new interface driver bfusb
[ 1.415594] usbcore: registered new interface driver btusb
[ 1.415603] Bluetooth: Generic Bluetooth SDIO driver ver 0.1
[ 1.415652] usbcore: registered new interface driver ath3k
[ 1.415778] EDAC MC: ECC not enabled
[ 1.415937] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT)
[ 1.416439] cpufreq: cpufreq_online: CPU0: Running at unlisted freq: 1199880 KHz
[ 1.416493] cpufreq: cpufreq_online: CPU0: Unlisted initial frequency changed to: 1199999 KHz
[ 1.416871] sdhci: Secure Digital Host Controller Interface driver
[ 1.416880] sdhci: Copyright(c) Pierre Ossman
[ 1.416887] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.464352] mmc0: SDHCI controller on ff170000.sdhci [ff170000.sdhci] using ADMA 64-bit
[ 1.470380] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.470522] usbcore: registered new interface driver usbhid
[ 1.470530] usbhid: USB HID core driver
[ 1.470995] ad9361 spi1.0: ad9361_probe : enter (ad9361)
[ 1.471843] ad9361 spi1.0: ad9361_reset: by SPI, this may cause unpredicted behavior!
[ 1.471881] ad9361 spi1.0: ad9361_probe : Unsupported PRODUCT_ID 0xFF
[ 1.474572] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
[ 1.477358] pktgen: Packet Generator for packet performance testing. Version: 2.75
[ 1.477560] Netfilter messages via NETLINK v0.30.
[ 1.477673] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 1.477855] Initializing XFRM netlink socket
[ 1.477913] NET: Registered protocol family 10
[ 1.478310] Segment Routing with IPv6
[ 1.478353] ip6_tables: (C) 2000-2006 Netfilter Core Team
[ 1.478532] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 1.478828] NET: Registered protocol family 17
[ 1.478844] NET: Registered protocol family 15
[ 1.478862] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[ 1.478876] Ebtables v2.0 registered
[ 1.478970] can: controller area network core (rev 20170425 abi 9)
[ 1.479004] NET: Registered protocol family 29
[ 1.479019] can: raw protocol (rev 20170425)
[ 1.479026] can: broadcast manager protocol (rev 20170425 t)
[ 1.479037] can: netlink gateway (rev 20170425) max_hops=1
[ 1.479240] Bluetooth: RFCOMM TTY layer initialized
[ 1.479256] Bluetooth: RFCOMM socket layer initialized
[ 1.479275] Bluetooth: RFCOMM ver 1.11
[ 1.479285] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 1.479293] Bluetooth: BNEP filters: protocol multicast
[ 1.479303] Bluetooth: BNEP socket layer initialized
[ 1.479311] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 1.479321] Bluetooth: HIDP socket layer initialized
[ 1.479425] 9pnet: Installing 9P2000 support
[ 1.479445] Key type dns_resolver registered
[ 1.479812] registered taskstats version 1
[ 1.481149] Btrfs loaded, crc32c=crc32c-generic
[ 1.488409] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 49, base_baud = 6249375) is a xuartps
[ 1.619605] mmc0: new high speed SDHC card at address aaaa
[ 1.633848] mmcblk0: mmc0:aaaa SU08G 7.40 GiB
[ 1.638060] mmcblk0: p1 p2 p3
[ 3.151100] console [ttyPS0] enabled
[ 3.155252] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 50, base_baud = 6249375) is a xuartps
[ 3.165848] xilinx-psgtr fd400000.zynqmp_phy: Lane:1 type:8 protocol:4 pll_locked:yes
[ 3.174062] PLL: shutdown
[ 3.178245] xilinx-dp-snd-codec fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0: Xilinx DisplayPort Sound Codec probed
[ 3.188844] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed
[ 3.196805] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed
[ 3.205015] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok
[ 3.217370] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok
[ 3.229991] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: Xilinx DisplayPort Sound Card probed
[ 3.240093] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000
[ 3.246965] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 3.253503] [drm] No driver support for vblank timestamp query.
[ 3.259464] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffff8008ae6268)
[ 4.344221] [drm] Cannot find any crtc or sizes
[ 4.348840] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display on minor 0
[ 4.356870] zynqmp-display fd4a0000.zynqmp-display: ZynqMP DisplayPort Subsystem driver probed
[ 4.365824] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:3 protocol:2 pll_locked:yes
[ 4.373639] ahci-ceva fd0c0000.ahci: AHCI 0001.0301 32 slots 2 ports 6 Gbps 0x3 impl platform mode
[ 4.382526] ahci-ceva fd0c0000.ahci: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst
[ 4.392859] scsi host0: ahci-ceva
[ 4.396294] scsi host1: ahci-ceva
[ 4.399626] ata1: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x100 irq 45
[ 4.407466] ata2: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x180 irq 45
[ 4.417043] xilinx-psgtr fd400000.zynqmp_phy: Lane:2 type:0 protocol:3 pll_locked:yes
[ 4.427011] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 4.432430] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[ 4.440276] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x22010010
[ 4.448928] xhci-hcd xhci-hcd.0.auto: irq 55, io mem 0xfe200000
[ 4.454910] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 4.461625] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 4.468827] usb usb1: Product: xHCI Host Controller
[ 4.473685] usb usb1: Manufacturer: Linux 4.14.0 xhci-hcd
[ 4.479067] usb usb1: SerialNumber: xhci-hcd.0.auto
[ 4.484195] hub 1-0:1.0: USB hub found
[ 4.487883] hub 1-0:1.0: 1 port detected
[ 4.491943] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 4.497359] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[ 4.505043] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 4.513145] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
[ 4.519854] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 4.527059] usb usb2: Product: xHCI Host Controller
[ 4.531917] usb usb2: Manufacturer: Linux 4.14.0 xhci-hcd
[ 4.537298] usb usb2: SerialNumber: xhci-hcd.0.auto
[ 4.542387] hub 2-0:1.0: USB hub found
[ 4.546077] hub 2-0:1.0: 1 port detected
[ 4.551083] pca953x 0-0020: 0-0020 supply vcc not found, using dummy regulator
[ 4.561198] pca953x 0-0020: interrupt support not compiled in
[ 4.566957] pca953x 0-0021: 0-0021 supply vcc not found, using dummy regulator
[ 4.576950] pca953x 0-0021: interrupt support not compiled in
[ 4.583412] ina2xx 3-0040: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.590115] ina2xx 3-0041: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.596807] ina2xx 3-0042: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.603501] ina2xx 3-0043: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.610195] ina2xx 3-0044: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.616896] ina2xx 3-0045: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.623598] ina2xx 3-0046: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.630295] ina2xx 3-0047: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.636992] ina2xx 3-004a: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.643681] ina2xx 3-004b: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.649984] i2c i2c-0: Added multiplexed i2c bus 3
[ 4.655340] ina2xx 4-0040: power monitor ina226 (Rshunt = 2000 uOhm)
[ 4.662043] ina2xx 4-0041: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.668741] ina2xx 4-0042: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.675434] ina2xx 4-0043: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.682127] ina2xx 4-0044: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.688822] ina2xx 4-0045: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.695520] ina2xx 4-0046: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.702216] ina2xx 4-0047: power monitor ina226 (Rshunt = 5000 uOhm)
[ 4.708516] i2c i2c-0: Added multiplexed i2c bus 4
[ 4.730410] ata2: SATA link down (SStatus 0 SControl 330)
[ 4.735748] ata1: SATA link down (SStatus 0 SControl 330)
[ 4.759067] i2c i2c-0: Added multiplexed i2c bus 5
[ 4.763900] i2c i2c-0: Added multiplexed i2c bus 6
[ 4.768612] pca954x 0-0075: registered 4 multiplexed busses for I2C mux pca9544
[ 4.775925] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 33
[ 4.783476] at24 7-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write
[ 4.790125] i2c i2c-1: Added multiplexed i2c bus 7
[ 4.795049] i2c i2c-1: Added multiplexed i2c bus 8
[ 4.801771] si570 9-005d: registered, current frequency 300000000 Hz
[ 4.808075] i2c i2c-1: Added multiplexed i2c bus 9
[ 4.826752] si570 10-005d: registered, current frequency 148500000 Hz
[ 4.833141] i2c i2c-1: Added multiplexed i2c bus 10
[ 4.838162] i2c i2c-1: Added multiplexed i2c bus 11
[ 4.843080] i2c i2c-1: Added multiplexed i2c bus 12
[ 4.847999] i2c i2c-1: Added multiplexed i2c bus 13
[ 4.852911] i2c i2c-1: Added multiplexed i2c bus 14
[ 4.857712] pca954x 1-0074: registered 8 multiplexed busses for I2C switch pca9548
[ 4.865579] i2c i2c-1: Added multiplexed i2c bus 15
[ 4.870499] i2c i2c-1: Added multiplexed i2c bus 16
[ 4.875421] i2c i2c-1: Added multiplexed i2c bus 17
[ 4.880647] i2c i2c-1: Added multiplexed i2c bus 18
[ 4.885566] i2c i2c-1: Added multiplexed i2c bus 19
[ 4.890496] i2c i2c-1: Added multiplexed i2c bus 20
[ 4.895411] i2c i2c-1: Added multiplexed i2c bus 21
[ 4.900333] i2c i2c-1: Added multiplexed i2c bus 22
[ 4.905135] pca954x 1-0075: registered 8 multiplexed busses for I2C switch pca9548
[ 4.912708] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 34
[ 4.919745] input: gpio-keys as /devices/platform/gpio-keys/input/input0
[ 4.926544] rtc_zynqmp ffa60000.rtc: setting system clock to 2018-10-03 07:34:06 UTC (1538552046)
[ 4.935340] of_cfs_init
[ 4.937780] of_cfs_init: OK
[ 4.940673] clk: Not disabling unused clocks
[ 4.944904] ALSA device list:
[ 4.947808] #0: DisplayPort monitor
[ 4.954515] EXT4-fs (mmcblk0p2): couldn't mount as ext3 due to feature incompatibilities
[ 5.151551] EXT4-fs (mmcblk0p2): recovery complete
[ 5.157608] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 5.165647] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 5.179997] devtmpfs: mounted
[ 5.183000] Freeing unused kernel memory: 512K
Mount failed for selinuxfs on /sys/fs/selinux: No such file or directory
[ 5.488247] [drm] Cannot find any crtc or sizes
* Setting up X socket directories... [ OK ]
* STARTDISTCC is set to false in /etc/default/distcc
* /usr/bin/distccd not starting
* Starting IIO Daemon iiod

After this no login prompt is coming.

What could be missing here? Is there way of verifying the built image contains all required modules and device-tree.

Note: I disabled the MATHWORKS driver while building this Linux Image. 

Your valuable suggestions are highly appreciated. Thank you.

Best Regards

-Siddhant

Parents
  • I have exactly same problem using distro from ADI, but I don't see obvious problems:

    Xilinx Zynq MP First Stage Boot Loader

    Release 2018.3   Dec  4 2019  -  23:48:13

    NOTICE:  ATF running on XCZU9EG/silicon v4/RTL5.1 at 0xfffea000

    NOTICE:  BL31: Secure code at 0x0

    NOTICE:  BL31: Non secure code at 0x8000000

    NOTICE:  BL31: v1.5(release):xilinx-v2018.3

    NOTICE:  BL31: Built : 15:00:47, Mar 18 2019

    PMUFW: v1.1

    U-Boot 2018.01 (Jun 29 2018 - 13:20:51 +0200) Xilinx ZynqMP ZCU102 rev1.0

    I2C:   ready

    DRAM:  4 GiB

    EL Level: EL2

    Chip ID: zu9eg

    MMC:   sdhci@ff170000: 0 (SD)

    *** Warning - bad CRC, using default environment

    In:    serial@ff000000

    Out:   serial@ff000000

    Err:   serial@ff000000

    Bootmode: LVL_SHFT_SD_MODE1

    Net:   ZYNQ GEM: ff0e0000, phyaddr c, interface rgmii-id

    Warning: ethernet@ff0e0000 using MAC address from ROM

    eth0: ethernet@ff0e0000

    Hit any key to stop autoboot:  0

    switch to partitions #0, OK

    mmc0 is current device

    Device: sdhci@ff170000

    Manufacturer ID: 1b

    OEM: 534d

    Name: GB1QT

    Tran Speed: 50000000

    Rd Block Len: 512

    SD version 3.0

    High Capacity: Yes

    Capacity: 29.8 GiB

    Bus Width: 4-bit

    Erase Group Size: 512 Bytes

    reading system.dtb

    44219 bytes read in 19 ms (2.2 MiB/s)

    reading Image

    16361984 bytes read in 1074 ms (14.5 MiB/s)

    ## Flattened Device Tree blob at 04000000

       Booting using the fdt blob at 0x4000000

       Loading Device Tree to 000000000fff2000, end 000000000ffffcba ... OK

    Starting kernel ...

    [    0.000000] Booting Linux on physical CPU 0x0

    [    0.000000] Linux version 4.14.0-g8a57ede (jenkins@romlxbuild1.adlk.analog.com) (gcc version 7.3.1 20180314 (Linaro GCC 7.3-2018.04-rc3)) #653 SMP Mon Feb 3 16:44:50 GMT 2020

    [    0.000000] Boot CPU: AArch64 Processor [410fd034]

    [    0.000000] Machine model: ZynqMP ZCU102 Rev1.0

    [    0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')

    [    0.000000] bootconsole [cdns0] enabled

    [    0.000000] efi: Getting EFI parameters from FDT:

    [    0.000000] efi: UEFI not found.

    [    0.000000] cma: Reserved 256 MiB at 0x0000000070000000

    [    0.000000] psci: probing for conduit method from DT.

    [    0.000000] psci: PSCIv1.1 detected in firmware.

    [    0.000000] psci: Using standard PSCI v0.2 function IDs

    [    0.000000] psci: MIGRATE_INFO_TYPE not supported.

    [    0.000000] percpu: Embedded 21 pages/cpu @ffffffc87ff61000 s45080 r8192 d32744 u86016

    [    0.000000] Detected VIPT I-cache on CPU0

    [    0.000000] CPU features: enabling workaround for ARM erratum 845719

    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1034240

    [    0.000000] Kernel command line: earlycon clk_ignore_unused root=/dev/mmcblk0p2 rw rootwait

    [    0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)

    [    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)

    [    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)

    [    0.000000] software IO TLB [mem 0x6bfff000-0x6ffff000] (64MB) mapped at [ffffffc06bfff000-ffffffc06fffefff]

    [    0.000000] Memory: 3783852K/4194304K available (10236K kernel code, 746K rwdata, 4448K rodata, 512K init, 2154K bss, 148308K reserved, 262144K cma-reserved)

    [    0.000000] Virtual kernel memory layout:

    [    0.000000]     modules : 0xffffff8000000000 - 0xffffff8008000000   (   128 MB)

    [    0.000000]     vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000   (   250 GB)

    [    0.000000]       .text : 0xffffff8008080000 - 0xffffff8008a80000   ( 10240 KB)

    [    0.000000]     .rodata : 0xffffff8008a80000 - 0xffffff8008ee0000   (  4480 KB)

    [    0.000000]       .init : 0xffffff8008ee0000 - 0xffffff8008f60000   (   512 KB)

    [    0.000000]       .data : 0xffffff8008f60000 - 0xffffff800901aa00   (   747 KB)

    [    0.000000]        .bss : 0xffffff800901aa00 - 0xffffff8009235530   (  2155 KB)

    [    0.000000]     fixed   : 0xffffffbefe7fd000 - 0xffffffbefec00000   (  4108 KB)

    [    0.000000]     PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000   (    16 MB)

    [    0.000000]     vmemmap : 0xffffffbf00000000 - 0xffffffc000000000   (     4 GB maximum)

    [    0.000000]               0xffffffbf00000000 - 0xffffffbf1dc00000   (   476 MB actual)

    [    0.000000]     memory  : 0xffffffc000000000 - 0xffffffc880000000   ( 34816 MB)

    [    0.000000] Hierarchical RCU implementation.

    [    0.000000] RCU event tracing is enabled.

    [    0.000000] RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.

    [    0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4

    [    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0

    [    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000

    [    0.000000] GIC: Using split EOI/Deactivate mode

    [    0.000000] arch_timer: cp15 timer(s) running at 99.99MHz (phys).

    [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x170f8de2d3, max_idle_ns: 440795206112 ns

    [    0.000003] sched_clock: 56 bits at 99MHz, resolution 10ns, wraps every 4398046511101ns

    [    0.008298] Console: colour dummy device 80x25

    [    0.012378] console [tty0] enabled

    [    0.015744] bootconsole [cdns0] disabled

    [    0.000000] Booting Linux on physical CPU 0x0

    [    0.000000] Linux version 4.14.0-g8a57ede (jenkins@romlxbuild1.adlk.analog.com) (gcc version 7.3.1 20180314 (Linaro GCC 7.3-2018.04-rc3)) #653 SMP Mon Feb 3 16:44:50 GMT 2020

    [    0.000000] Boot CPU: AArch64 Processor [410fd034]

    [    0.000000] Machine model: ZynqMP ZCU102 Rev1.0

    [    0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')

    [    0.000000] bootconsole [cdns0] enabled

    [    0.000000] efi: Getting EFI parameters from FDT:

    [    0.000000] efi: UEFI not found.

    [    0.000000] cma: Reserved 256 MiB at 0x0000000070000000

    [    0.000000] psci: probing for conduit method from DT.

    [    0.000000] psci: PSCIv1.1 detected in firmware.

    [    0.000000] psci: Using standard PSCI v0.2 function IDs

    [    0.000000] psci: MIGRATE_INFO_TYPE not supported.

    [    0.000000] percpu: Embedded 21 pages/cpu @ffffffc87ff61000 s45080 r8192 d32744 u86016

    [    0.000000] Detected VIPT I-cache on CPU0

    [    0.000000] CPU features: enabling workaround for ARM erratum 845719

    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1034240

    [    0.000000] Kernel command line: earlycon clk_ignore_unused root=/dev/mmcblk0p2 rw rootwait

    [    0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)

    [    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)

    [    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)

    [    0.000000] software IO TLB [mem 0x6bfff000-0x6ffff000] (64MB) mapped at [ffffffc06bfff000-ffffffc06fffefff]

    [    0.000000] Memory: 3783852K/4194304K available (10236K kernel code, 746K rwdata, 4448K rodata, 512K init, 2154K bss, 148308K reserved, 262144K cma-reserved)

    [    0.000000] Virtual kernel memory layout:

    [    0.000000]     modules : 0xffffff8000000000 - 0xffffff8008000000   (   128 MB)

    [    0.000000]     vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000   (   250 GB)

    [    0.000000]       .text : 0xffffff8008080000 - 0xffffff8008a80000   ( 10240 KB)

    [    0.000000]     .rodata : 0xffffff8008a80000 - 0xffffff8008ee0000   (  4480 KB)

    [    0.000000]       .init : 0xffffff8008ee0000 - 0xffffff8008f60000   (   512 KB)

    [    0.000000]       .data : 0xffffff8008f60000 - 0xffffff800901aa00   (   747 KB)

    [    0.000000]        .bss : 0xffffff800901aa00 - 0xffffff8009235530   (  2155 KB)

    [    0.000000]     fixed   : 0xffffffbefe7fd000 - 0xffffffbefec00000   (  4108 KB)

    [    0.000000]     PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000   (    16 MB)

    [    0.000000]     vmemmap : 0xffffffbf00000000 - 0xffffffc000000000   (     4 GB maximum)

    [    0.000000]               0xffffffbf00000000 - 0xffffffbf1dc00000   (   476 MB actual)

    [    0.000000]     memory  : 0xffffffc000000000 - 0xffffffc880000000   ( 34816 MB)

    [    0.000000] Hierarchical RCU implementation.

    [    0.000000] RCU event tracing is enabled.

    [    0.000000] RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.

    [    0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4

    [    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0

    [    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000

    [    0.000000] GIC: Using split EOI/Deactivate mode

    [    0.000000] arch_timer: cp15 timer(s) running at 99.99MHz (phys).

    [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x170f8de2d3, max_idle_ns: 440795206112 ns

    [    0.000003] sched_clock: 56 bits at 99MHz, resolution 10ns, wraps every 4398046511101ns

    [    0.008298] Console: colour dummy device 80x25

    [    0.012378] console [tty0] enabled

    [    0.015744] bootconsole [cdns0] disabled

    [    0.019654] Calibrating delay loop (skipped), value calculated using timer frequency.. 199.98 BogoMIPS (lpj=399960)

    [    0.019667] pid_max: default: 32768 minimum: 301

    [    0.019771] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes)

    [    0.019789] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes)

    [    0.020368] ASID allocator initialised with 65536 entries

    [    0.020415] Hierarchical SRCU implementation.

    [    0.020772] EFI services will not be available.

    [    0.020805] zynqmp_plat_init Platform Management API v1.1

    [    0.020813] zynqmp_plat_init Trustzone version v1.0

    [    0.020909] smp: Bringing up secondary CPUs ...

    [    0.021157] Detected VIPT I-cache on CPU1

    [    0.021185] CPU1: Booted secondary processor [410fd034]

    [    0.021455] Detected VIPT I-cache on CPU2

    [    0.021473] CPU2: Booted secondary processor [410fd034]

    [    0.021728] Detected VIPT I-cache on CPU3

    [    0.021746] CPU3: Booted secondary processor [410fd034]

    [    0.021789] smp: Brought up 1 node, 4 CPUs

    [    0.021819] SMP: Total of 4 processors activated.

    [    0.021827] CPU features: detected feature: 32-bit EL0 Support

    [    0.021837] CPU: All CPU(s) started at EL2

    [    0.021853] alternatives: patching kernel code

    [    0.022592] devtmpfs: initialized

    [    0.027513] random: get_random_u32 called from bucket_table_alloc+0x108/0x258 with crng_init=0

    [    0.027728] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns

    [    0.027750] futex hash table entries: 1024 (order: 5, 131072 bytes)

    [    0.027910] random: fast init done

    [    0.033207] xor: measuring software checksum speed

    [    0.071738]    8regs     :  2303.000 MB/sec

    [    0.111767]    8regs_prefetch:  2052.000 MB/sec

    [    0.151799]    32regs    :  2831.000 MB/sec

    [    0.191831]    32regs_prefetch:  2456.000 MB/sec

    [    0.191839] xor: using function: 32regs (2831.000 MB/sec)

    [    0.191915] pinctrl core: initialized pinctrl subsystem

    [    0.192419] NET: Registered protocol family 16

    [    0.192998] cpuidle: using governor menu

    [    0.193552] vdso: 2 pages (1 code @ ffffff8008a86000, 1 data @ ffffff8008f64000)

    [    0.193569] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.

    [    0.194035] DMA: preallocated 256 KiB pool for atomic allocations

    [    0.216062] zynqmp-pinctrl pinctrl: zynqmp pinctrl initialized

    [    0.216856] reset_zynqmp reset-controller: Xilinx zynqmp reset driver probed

    [    0.217490] ARM CCI_400_r1 PMU driver probed

    [    0.227665] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages

    [    0.295993] raid6: int64x1  gen()   457 MB/s

    [    0.364010] raid6: int64x1  xor()   443 MB/s

    [    0.432099] raid6: int64x2  gen()   689 MB/s

    [    0.500099] raid6: int64x2  xor()   605 MB/s

    [    0.568165] raid6: int64x4  gen()  1043 MB/s

    [    0.636212] raid6: int64x4  xor()   765 MB/s

    [    0.704269] raid6: int64x8  gen()   982 MB/s

    [    0.772298] raid6: int64x8  xor()   751 MB/s

    [    0.840349] raid6: neonx1   gen()   726 MB/s

    [    0.908407] raid6: neonx1   xor()   852 MB/s

    [    0.976442] raid6: neonx2   gen()  1168 MB/s

    [    1.044488] raid6: neonx2   xor()  1207 MB/s

    [    1.112569] raid6: neonx4   gen()  1505 MB/s

    [    1.180579] raid6: neonx4   xor()  1440 MB/s

    [    1.248650] raid6: neonx8   gen()  1665 MB/s

    [    1.316686] raid6: neonx8   xor()  1533 MB/s

    [    1.316694] raid6: using algorithm neonx8 gen() 1665 MB/s

    [    1.316701] raid6: .... xor() 1533 MB/s, rmw enabled

    [    1.316708] raid6: using neon recovery algorithm

    [    1.318077] SCSI subsystem initialized

    [    1.318241] usbcore: registered new interface driver usbfs

    [    1.318277] usbcore: registered new interface driver hub

    [    1.318316] usbcore: registered new device driver usb

    [    1.318378] media: Linux media interface: v0.10

    [    1.318403] Linux video capture interface: v2.00

    [    1.318442] pps_core: LinuxPPS API ver. 1 registered

    [    1.318450] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

    [    1.318469] PTP clock support registered

    [    1.318719] zynqmp-ipi ff9905c0.mailbox: Probed ZynqMP IPI Mailbox driver.

    [    1.318853] FPGA manager framework

    [    1.318963] fpga-region fpga-full: FPGA Region probed

    [    1.319050] Advanced Linux Sound Architecture Driver Initialized.

    [    1.319296] Bluetooth: Core ver 2.22

    [    1.319321] NET: Registered protocol family 31

    [    1.319329] Bluetooth: HCI device and connection manager initialized

    [    1.319340] Bluetooth: HCI socket layer initialized

    [    1.319349] Bluetooth: L2CAP socket layer initialized

    [    1.319372] Bluetooth: SCO socket layer initialized

    [    1.319898] clocksource: Switched to clocksource arch_sys_counter

    [    1.319975] VFS: Disk quotas dquot_6.6.0

    [    1.320017] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)

    [    1.323935] NET: Registered protocol family 2

    [    1.324230] TCP established hash table entries: 32768 (order: 6, 262144 bytes)

    [    1.324440] TCP bind hash table entries: 32768 (order: 7, 524288 bytes)

    [    1.324853] TCP: Hash tables configured (established 32768 bind 32768)

    [    1.324926] UDP hash table entries: 2048 (order: 4, 65536 bytes)

    [    1.325003] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes)

    [    1.325157] NET: Registered protocol family 1

    [    1.325377] RPC: Registered named UNIX socket transport module.

    [    1.325387] RPC: Registered udp transport module.

    [    1.325394] RPC: Registered tcp transport module.

    [    1.325401] RPC: Registered tcp NFSv4.1 backchannel transport module.

    [    1.325833] hw perfevents: no interrupt-affinity property for /pmu, guessing.

    [    1.325986] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available

    [    1.326609] audit: initializing netlink subsys (disabled)

    [    1.326967] audit: type=2000 audit(1.308:1): state=initialized audit_enabled=0 res=1

    [    1.327010] workingset: timestamp_bits=62 max_order=20 bucket_order=0

    [    1.327679] NFS: Registering the id_resolver key type

    [    1.327699] Key type id_resolver registered

    [    1.327706] Key type id_legacy registered

    [    1.327717] nfs4filelayout_init: NFSv4 File Layout Driver Registering...

    [    1.327738] jffs2: version 2.2. (NAND) (SUMMARY)  © 2001-2006 Red Hat, Inc.

    [    1.351751] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)

    [    1.351770] io scheduler noop registered

    [    1.351777] io scheduler deadline registered

    [    1.351797] io scheduler cfq registered (default)

    [    1.351806] io scheduler mq-deadline registered

    [    1.351813] io scheduler kyber registered

    [    1.352403] nwl-pcie fd0e0000.pcie: Link is DOWN

    [    1.352447] OF: PCI: host bridge /amba/pcie@fd0e0000 ranges:

    [    1.352468] OF: PCI:   MEM 0xe0000000..0xefffffff -> 0xe0000000

    [    1.352480] OF: PCI:   MEM 0x600000000..0x7ffffffff -> 0x600000000

    [    1.352613] nwl-pcie fd0e0000.pcie: PCI host bridge to bus 0000:00

    [    1.352627] pci_bus 0000:00: root bus resource [bus 00-ff]

    [    1.352637] pci_bus 0000:00: root bus resource [mem 0xe0000000-0xefffffff]

    [    1.352648] pci_bus 0000:00: root bus resource [mem 0x600000000-0x7ffffffff pref]

    [    1.352910] pci 0000:00:00.0: PCI bridge to [bus 01-0c]

    [    1.354158] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed

    [    1.354419] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success

    [    1.354580] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success

    [    1.354740] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success

    [    1.354901] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success

    [    1.355061] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success

    [    1.355222] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success

    [    1.355380] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success

    [    1.355543] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success

    [    1.380446] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled

    [    1.382904] cacheinfo: Unable to detect cache hierarchy for CPU 0

    [    1.386913] brd: module loaded

    [    1.390257] loop: module loaded

    [    1.390950] ahci-ceva fd0c0000.ahci: couldn't get PHY in node ahci: -517

    [    1.391109] mtdoops: mtd device (mtddev=name/number) must be supplied

    [    1.392415] m25p80 spi0.0: SPI-NOR-UniqueID 10440088170200151300240088e2ac8bc0

    [    1.392431] m25p80 spi0.0: found n25q512a, expected m25p80

    [    1.392599] m25p80 spi0.0: n25q512a (131072 Kbytes)

    [    1.392623] 4 ofpart partitions found on MTD device spi0.0

    [    1.392631] Creating 4 MTD partitions on "spi0.0":

    [    1.392643] 0x000000000000-0x000000100000 : "qspi-fsbl-uboot"

    [    1.393072] 0x000000100000-0x000000600000 : "qspi-linux"

    [    1.393441] 0x000000600000-0x000000620000 : "qspi-device-tree"

    [    1.393806] 0x000000620000-0x000000c00000 : "qspi-rootfs"

    [    1.395028] libphy: Fixed MDIO Bus: probed

    [    1.396021] tun: Universal TUN/TAP device driver, 1.6

    [    1.396155] CAN device driver interface

    [    1.398190] macb ff0e0000.ethernet: Not enabling partial store and forward

    [    1.398573] libphy: MACB_mii_bus: probed

    [    1.399077] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 23 (00:0a:35:05:1a:e6)

    [    1.399093] TI DP83867 ff0e0000.ethernet-ffffffff:0c: attached PHY driver [TI DP83867] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:0c, irq=POLL)

    [    1.399594] usbcore: registered new interface driver asix

    [    1.399644] usbcore: registered new interface driver ax88179_178a

    [    1.399677] usbcore: registered new interface driver cdc_ether

    [    1.399707] usbcore: registered new interface driver net1080

    [    1.399737] usbcore: registered new interface driver cdc_subset

    [    1.399766] usbcore: registered new interface driver zaurus

    [    1.399805] usbcore: registered new interface driver cdc_ncm

    [    1.400129] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM

    [    1.401613] usbcore: registered new interface driver uas

    [    1.401654] usbcore: registered new interface driver usb-storage

    [    1.402131] rtc_zynqmp ffa60000.rtc: rtc core: registered ffa60000.rtc as rtc0

    [    1.402184] i2c /dev entries driver

    [    1.403116] IR NEC protocol handler initialized

    [    1.403125] IR RC5(x/sz) protocol handler initialized

    [    1.403132] IR RC6 protocol handler initialized

    [    1.403139] IR JVC protocol handler initialized

    [    1.403146] IR Sony protocol handler initialized

    [    1.403153] IR SANYO protocol handler initialized

    [    1.403159] IR Sharp protocol handler initialized

    [    1.403166] IR MCE Keyboard/mouse protocol handler initialized

    [    1.403174] IR XMP protocol handler initialized

    [    1.403815] usbcore: registered new interface driver uvcvideo

    [    1.403823] USB Video Class driver (1.1.1)

    [    1.404314] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer at ffffff80092a5000 with timeout 60s

    [    1.404479] Bluetooth: HCI UART driver ver 2.3

    [    1.404489] Bluetooth: HCI UART protocol H4 registered

    [    1.404497] Bluetooth: HCI UART protocol BCSP registered

    [    1.404505] Bluetooth: HCI UART protocol ATH3K registered

    [    1.404512] Bluetooth: HCI UART protocol Three-wire (H5) registered

    [    1.404553] Bluetooth: HCI UART protocol Intel registered

    [    1.404561] Bluetooth: HCI UART protocol QCA registered

    [    1.404599] usbcore: registered new interface driver bcm203x

    [    1.404633] usbcore: registered new interface driver bpa10x

    [    1.404665] usbcore: registered new interface driver bfusb

    [    1.404699] usbcore: registered new interface driver btusb

    [    1.404707] Bluetooth: Generic Bluetooth SDIO driver ver 0.1

    [    1.404754] usbcore: registered new interface driver ath3k

    [    1.405539] sdhci: Secure Digital Host Controller Interface driver

    [    1.405548] sdhci: Copyright(c) Pierre Ossman

    [    1.405554] sdhci-pltfm: SDHCI platform and OF driver helper

    [    1.406784] ledtrig-cpu: registered to indicate activity on CPUs

    [    1.406908] usbcore: registered new interface driver usbhid

    [    1.406916] usbhid: USB HID core driver

    [    1.407593] ad9361 spi1.0: ad9361_probe : enter (ad9361)

    [    1.411889] axi_sysid 85000000.axi-sysid-0: [fmcomms2] on [zcu102] git <2e4ac278eb09c13471e381459b0da790ebad8373> clean [2019-12-04 23:16:58] UTC

    [    1.412274] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered

    [    1.413022] pktgen: Packet Generator for packet performance testing. Version: 2.75

    [    1.413292] Netfilter messages via NETLINK v0.30.

    [    1.413409] ip_tables: (C) 2000-2006 Netfilter Core Team

    [    1.413544] Initializing XFRM netlink socket

    [    1.413603] NET: Registered protocol family 10

    [    1.413995] Segment Routing with IPv6

    [    1.414041] ip6_tables: (C) 2000-2006 Netfilter Core Team

    [    1.414165] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver

    [    1.414468] NET: Registered protocol family 17

    [    1.414484] NET: Registered protocol family 15

    [    1.414501] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.

    [    1.414515] Ebtables v2.0 registered

    [    1.414598] can: controller area network core (rev 20170425 abi 9)

    [    1.414633] NET: Registered protocol family 29

    [    1.414647] can: raw protocol (rev 20170425)

    [    1.414655] can: broadcast manager protocol (rev 20170425 t)

    [    1.414666] can: netlink gateway (rev 20170425) max_hops=1

    [    1.414855] Bluetooth: RFCOMM TTY layer initialized

    [    1.414867] Bluetooth: RFCOMM socket layer initialized

    [    1.414882] Bluetooth: RFCOMM ver 1.11

    [    1.414896] Bluetooth: BNEP (Ethernet Emulation) ver 1.3

    [    1.414904] Bluetooth: BNEP filters: protocol multicast

    [    1.414914] Bluetooth: BNEP socket layer initialized

    [    1.414922] Bluetooth: HIDP (Human Interface Emulation) ver 1.2

    [    1.414931] Bluetooth: HIDP socket layer initialized

    [    1.415035] 9pnet: Installing 9P2000 support

    [    1.415054] Key type dns_resolver registered

    [    1.415420] registered taskstats version 1

    [    1.415729] Btrfs loaded, crc32c=crc32c-generic

    [    1.420242] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 40, base_baud = 6249999) is a xuartps

    [    2.971671] console [ttyPS0] enabled

    [    2.975780] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 41, base_baud = 6249999) is a xuartps

    [    2.986398] xilinx-psgtr fd400000.zynqmp_phy: Lane:1 type:8 protocol:4 pll_locked:yes

    [    2.994602] PLL: shutdown

    [    2.998912] zynqmp_clk_divider_set_rate() set divider failed for spi1_ref_div1, ret = -13

    [    3.007452] xilinx-dp-snd-codec fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0: Xilinx DisplayPort Sound Codec probed

    [    3.018127] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed

    [    3.026165] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed

    [    3.034511] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok

    [    3.046942] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok

    [    3.059617] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: Xilinx DisplayPort Sound Card probed

    [    3.069796] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000

    [    3.076793] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).

    [    3.083406] [drm] No driver support for vblank timestamp query.

    [    3.089374] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffff8008b32030)

    [    4.175909] [drm] Cannot find any crtc or sizes

    [    4.180610] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display on minor 0

    [    4.188718] zynqmp-display fd4a0000.zynqmp-display: ZynqMP DisplayPort Subsystem driver probed

    [    4.197679] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:3 protocol:2 pll_locked:yes

    [    4.205566] ahci-ceva fd0c0000.ahci: AHCI 0001.0301 32 slots 2 ports 6 Gbps 0x3 impl platform mode

    [    4.214530] ahci-ceva fd0c0000.ahci: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst

    [    4.224877] scsi host0: ahci-ceva

    [    4.228381] scsi host1: ahci-ceva

    [    4.231786] ata1: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x100 irq 37

    [    4.239705] ata2: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x180 irq 37

    [    4.249431] xilinx-psgtr fd400000.zynqmp_phy: Lane:2 type:0 protocol:3 pll_locked:yes

    [    4.257425] dwc3 fe200000.dwc3: stop_host(): INFO: Host already stopped

    [    4.264366] dwc3 fe200000.dwc3: stop_peripheral(): INFO: Peripheral already stopped

    [    4.308636] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller

    [    4.314133] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1

    [    4.322004] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x22010810

    [    4.330723] xhci-hcd xhci-hcd.0.auto: irq 48, io mem 0xfe200000

    [    4.336752] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

    [    4.343542] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

    [    4.350762] usb usb1: Product: xHCI Host Controller

    [    4.355641] usb usb1: Manufacturer: Linux 4.14.0-g8a57ede xhci-hcd

    [    4.361821] usb usb1: SerialNumber: xhci-hcd.0.auto

    [    4.366975] hub 1-0:1.0: USB hub found

    [    4.370739] hub 1-0:1.0: 1 port detected

    [    4.374833] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller

    [    4.380328] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2

    [    4.388095] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003

    [    4.394882] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1

    [    4.402101] usb usb2: Product: xHCI Host Controller

    [    4.406977] usb usb2: Manufacturer: Linux 4.14.0-g8a57ede xhci-hcd

    [    4.413158] usb usb2: SerialNumber: xhci-hcd.0.auto

    [    4.418260] hub 2-0:1.0: USB hub found

    [    4.422023] hub 2-0:1.0: 1 port detected

    [    4.427086] pca953x 0-0020: 0-0020 supply vcc not found, using dummy regulator

    [    4.437310] GPIO line 496 (sel0) hogged as output/low

    [    4.442690] GPIO line 497 (sel1) hogged as output/high

    [    4.448166] GPIO line 498 (sel2) hogged as output/high

    [    4.453632] GPIO line 499 (sel3) hogged as output/high

    [    4.458867] pca953x 0-0020: interrupt support not compiled in

    [    4.464705] pca953x 0-0021: 0-0021 supply vcc not found, using dummy regulator

    [    4.474650] pca953x 0-0021: interrupt support not compiled in

    [    4.481197] ina2xx 3-0040: power monitor ina226 (Rshunt = 5000 uOhm)

    [    4.487963] ina2xx 3-0041: power monitor ina226 (Rshunt = 5000 uOhm)

    [    4.494739] ina2xx 3-0042: power monitor ina226 (Rshunt = 5000 uOhm)

    [    4.501514] ina2xx 3-0043: power monitor ina226 (Rshunt = 5000 uOhm)

    [    4.508292] ina2xx 3-0044: power monitor ina226 (Rshunt = 5000 uOhm)

    [    4.515072] ina2xx 3-0045: power monitor ina226 (Rshunt = 5000 uOhm)

    [    4.521847] ina2xx 3-0046: power monitor ina226 (Rshunt = 5000 uOhm)

    [    4.528621] ina2xx 3-0047: power monitor ina226 (Rshunt = 5000 uOhm)

    [    4.531902] xhci-hcd xhci-hcd.0.auto: remove, state 4

    [    4.531916] usb usb2: USB disconnect, device number 1

    [    4.532297] xhci-hcd xhci-hcd.0.auto: USB bus 2 deregistered

    [    4.532307] xhci-hcd xhci-hcd.0.auto: remove, state 4

    [    4.532317] usb usb1: USB disconnect, device number 1

    [    4.532715] xhci-hcd xhci-hcd.0.auto: USB bus 1 deregistered

    [    4.532727] dwc3 fe200000.dwc3: stop_peripheral(): INFO: Peripheral already stopped

    [    4.562090] ata2: SATA link down (SStatus 0 SControl 330)

    [    4.562113] ata1: SATA link down (SStatus 0 SControl 330)

    [    4.585298] ina2xx 3-004a: power monitor ina226 (Rshunt = 5000 uOhm)

    [    4.592079] ina2xx 3-004b: power monitor ina226 (Rshunt = 5000 uOhm)

    [    4.598463] i2c i2c-0: Added multiplexed i2c bus 3

    [    4.603852] ina2xx 4-0040: power monitor ina226 (Rshunt = 2000 uOhm)

    [    4.610620] ina2xx 4-0041: power monitor ina226 (Rshunt = 5000 uOhm)

    [    4.617401] ina2xx 4-0042: power monitor ina226 (Rshunt = 5000 uOhm)

    [    4.624174] ina2xx 4-0043: power monitor ina226 (Rshunt = 5000 uOhm)

    [    4.630948] ina2xx 4-0044: power monitor ina226 (Rshunt = 5000 uOhm)

    [    4.637719] ina2xx 4-0045: power monitor ina226 (Rshunt = 5000 uOhm)

    [    4.644493] ina2xx 4-0046: power monitor ina226 (Rshunt = 5000 uOhm)

    [    4.651267] ina2xx 4-0047: power monitor ina226 (Rshunt = 5000 uOhm)

    [    4.657654] i2c i2c-0: Added multiplexed i2c bus 4

    [    4.703547] i2c i2c-0: Added multiplexed i2c bus 5

    [    4.708468] i2c i2c-0: Added multiplexed i2c bus 6

    [    4.713259] pca954x 0-0075: registered 4 multiplexed busses for I2C mux pca9544

    [    4.720593] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 25

    [    4.728168] at24 7-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write

    [    4.734904] i2c i2c-1: Added multiplexed i2c bus 7

    [    4.739883] i2c i2c-1: Added multiplexed i2c bus 8

    [    4.746744] si570 9-005d: registered, current frequency 300000000 Hz

    [    4.753125] i2c i2c-1: Added multiplexed i2c bus 9

    [    4.771885] si570 10-005d: registered, current frequency 148500000 Hz

    [    4.778357] i2c i2c-1: Added multiplexed i2c bus 10

    [    4.783434] i2c i2c-1: Added multiplexed i2c bus 11

    [    4.788431] i2c i2c-1: Added multiplexed i2c bus 12

    [    4.793429] i2c i2c-1: Added multiplexed i2c bus 13

    [    4.798419] i2c i2c-1: Added multiplexed i2c bus 14

    [    4.803300] pca954x 1-0074: registered 8 multiplexed busses for I2C switch pca9548

    [    4.812305] at24 15-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write

    [    4.819036] i2c i2c-1: Added multiplexed i2c bus 15

    [    4.824040] i2c i2c-1: Added multiplexed i2c bus 16

    [    4.829038] i2c i2c-1: Added multiplexed i2c bus 17

    [    4.834037] i2c i2c-1: Added multiplexed i2c bus 18

    [    4.839040] i2c i2c-1: Added multiplexed i2c bus 19

    [    4.844094] i2c i2c-1: Added multiplexed i2c bus 20

    [    4.849128] i2c i2c-1: Added multiplexed i2c bus 21

    [    4.854134] i2c i2c-1: Added multiplexed i2c bus 22

    [    4.859010] pca954x 1-0075: registered 8 multiplexed busses for I2C switch pca9548

    [    4.866603] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 26

    [    4.915914] mmc0: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit

    [    4.929764] ad9361 spi1.0: ad9361_probe : enter (ad9361)

    [    4.975197] mmc0: new SDHC card at address 0001

    [    4.979899] mmcblk0: mmc0:0001 GB1QT 29.8 GiB

    [    4.985754]  mmcblk0: p1 p2 p3

    [    5.163366] ad9361 spi1.0: ad9361_probe : AD936x Rev 2 successfully initialized

    [    5.188327] cf_axi_dds 99024000.cf-ad9361-dds-core-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x99024000 mapped to 0xffffff8009435000, probed DDS AD9361

    [    5.349323] [drm] Cannot find any crtc or sizes

    [    6.397209] cf_axi_adc 99020000.cf-ad9361-lpc: ADI AIM (10.01.b) at 0x99020000 mapped to 0xffffff800cf38000, probed ADC AD9361 as MASTER

    [    6.410309] input: gpio-keys as /devices/platform/gpio-keys/input/input0

    [    6.417195] rtc_zynqmp ffa60000.rtc: setting system clock to 2019-02-23 02:45:30 UTC (1550889930)

    [    6.426185] clk: Not disabling unused clocks

    [    6.430702] ALSA device list:

    [    6.433662]   #0: DisplayPort monitor

    [    6.438775] EXT4-fs (mmcblk0p2): couldn't mount as ext3 due to feature incompatibilities

    [    6.743571] EXT4-fs (mmcblk0p2): recovery complete

    [    6.751177] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)

    [    6.759294] VFS: Mounted root (ext4 filesystem) on device 179:2.

    [    6.786040] devtmpfs: mounted

    [    6.789119] Freeing unused kernel memory: 512K

    Mount failed for selinuxfs on /sys/fs/selinux:  No such file or directory

    * Setting up X socket directories...                                    [ OK ]

    * STARTDISTCC is set to false in /etc/default/distcc

    * /usr/bin/distccd not starting

    * Starting IIO Daemon iiod                                              [ OK ]

    And never login prompt.

  • 0
    •  Analog Employees 
    on Mar 4, 2020 6:55 PM 10 months ago in reply to MichalM

    @MichalM please do not post in answered threads as they get ignored by staff. Please create a new thread for your question and link to related threads if you want.

    -Travis

Reply Children
No Data