Hi all,
I created Linux Image using ADI Kernel ( 2018_R1) and Petalinux Tool. I added device-tree in my petalinux project (system-user.dtsi) and selected AD9361 drivers in the kernel configuration, then I built the project. Build Is successful and I copied the files on SD card and booted the device.
Below is given the boot message:
Release 2018.2 Oct 1 2018 - 14:59:42NOTICE: ATF running on XCZU9EG/silicon v4/RTL5.1 at 0xfffea000NOTICE: BL31: Secure code at 0x0NOTICE: BL31: Non secure code at 0x8000000NOTICE: BL31: v1.4(release):xilinx-v2018.1-4-g93a69a5aNOTICE: BL31: Built : 04:21:54, Oct 3 2018PMUFW: v1.0
U-Boot 2018.01 (Oct 03 2018 - 11:24:07 +0530) Xilinx ZynqMP ZCU102 rev1.0
I2C: readyDRAM: 4 GiBEL Level: EL2Chip ID: zu9egMMC: sdhci@ff170000: 0 (SD)SF: Detected n25q512a with page size 512 Bytes, erase size 128 KiB, total 128 MiB*** Warning - bad CRC, using default environment
In: serial@ff000000Out: serial@ff000000Err: serial@ff000000Model: ZynqMP ZCU102 Rev1.0Board: Xilinx ZynqMPBootmode: LVL_SHFT_SD_MODE1Net: ZYNQ GEM: ff0e0000, phyaddr c, interface rgmii-ideth0: ethernet@ff0e0000U-BOOT for eldaas_linux
Hit any key to stop autoboot: 0Device: sdhci@ff170000Manufacturer ID: 3OEM: 5344Name: SU08GTran Speed: 50000000Rd Block Len: 512SD version 3.0High Capacity: YesCapacity: 7.4 GiBBus Width: 4-bitErase Group Size: 512 Bytesreading image.ub6985820 bytes read in 471 ms (14.1 MiB/s)## Loading kernel from FIT Image at 10000000 ... Using 'conf@system-top.dtb' configuration Trying 'kernel@1' kernel subimage Description: Linux kernel Type: Kernel Image Compression: gzip compressed Data Start: 0x100000f8 Data Size: 6937400 Bytes = 6.6 MiB Architecture: AArch64 OS: Linux Load Address: 0x00080000 Entry Point: 0x00080000 Hash algo: sha1 Hash value: 168604421a335d58edbd2e2f8778fa1874f84808 Verifying Hash Integrity ... sha1+ OK## Loading fdt from FIT Image at 10000000 ... Using 'conf@system-top.dtb' configuration Trying 'fdt@system-top.dtb' fdt subimage Description: Flattened Device Tree blob Type: Flat Device Tree Compression: uncompressed Data Start: 0x1069dd34 Data Size: 46516 Bytes = 45.4 KiB Architecture: AArch64 Hash algo: sha1 Hash value: a48822adfc075490eab70af4ad38c2fa0677b247 Verifying Hash Integrity ... sha1+ OK Booting using the fdt blob at 0x1069dd34 Uncompressing Kernel Image ... OK Loading Device Tree to 000000007dd80000, end 000000007dd8e5b3 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0[ 0.000000] Linux version 4.14.0 (oe-user@oe-host) (gcc version 7.2.0 (GCC)) #3 SMP Wed Oct 3 09:46:54 IST 2018[ 0.000000] Boot CPU: AArch64 Processor [410fd034][ 0.000000] Machine model: ZynqMP ZCU102 Rev1.0[ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')[ 0.000000] bootconsole [cdns0] enabled[ 0.000000] efi: Getting EFI parameters from FDT:[ 0.000000] efi: UEFI not found.[ 0.000000] cma: Reserved 256 MiB at 0x000000006dc00000[ 0.000000] psci: probing for conduit method from DT.[ 0.000000] psci: PSCIv1.1 detected in firmware.[ 0.000000] psci: Using standard PSCI v0.2 function IDs[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.[ 0.000000] percpu: Embedded 21 pages/cpu @ffffffc87ff62000 s45080 r8192 d32744 u86016[ 0.000000] Detected VIPT I-cache on CPU0[ 0.000000] CPU features: enabling workaround for ARM erratum 845719[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1033987[ 0.000000] Kernel command line: earlycon clk_ignore_unused root=/dev/mmcblk0p2 rw rootwait[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)[ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)[ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)[ 0.000000] software IO TLB [mem 0x69c00000-0x6dc00000] (64MB) mapped at [ffffffc069c00000-ffffffc06dbfffff][ 0.000000] Memory: 3784528K/4193280K available (9916K kernel code, 640K rwdata, 3136K rodata, 512K init, 2160K bss, 146608K reserved, 262144K cma-reserved)[ 0.000000] Virtual kernel memory layout:[ 0.000000] modules : 0xffffff8000000000 - 0xffffff8008000000 ( 128 MB)[ 0.000000] vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000 ( 250 GB)[ 0.000000] .text : 0xffffff8008080000 - 0xffffff8008a30000 ( 9920 KB)[ 0.000000] .rodata : 0xffffff8008a30000 - 0xffffff8008d50000 ( 3200 KB)[ 0.000000] .init : 0xffffff8008d50000 - 0xffffff8008dd0000 ( 512 KB)[ 0.000000] .data : 0xffffff8008dd0000 - 0xffffff8008e70200 ( 641 KB)[ 0.000000] .bss : 0xffffff8008e70200 - 0xffffff800908c330 ( 2161 KB)[ 0.000000] fixed : 0xffffffbefe7fd000 - 0xffffffbefec00000 ( 4108 KB)[ 0.000000] PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000 ( 16 MB)[ 0.000000] vmemmap : 0xffffffbf00000000 - 0xffffffc000000000 ( 4 GB maximum)[ 0.000000] 0xffffffbf00000000 - 0xffffffbf1dc00000 ( 476 MB actual)[ 0.000000] memory : 0xffffffc000000000 - 0xffffffc880000000 ( 34816 MB)[ 0.000000] Hierarchical RCU implementation.[ 0.000000] RCU event tracing is enabled.[ 0.000000] RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0[ 0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000[ 0.000000] GIC: Using split EOI/Deactivate mode[ 0.000000] arch_timer: cp15 timer(s) running at 99.99MHz (phys).[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x170f8dc196, max_idle_ns: 440795203664 ns[ 0.000003] sched_clock: 56 bits at 99MHz, resolution 10ns, wraps every 4398046511099ns[ 0.008325] Console: colour dummy device 80x25[ 0.012585] console [tty0] enabled[ 0.015952] bootconsole [cdns0] disabled[ 0.000000] Booting Linux on physical CPU 0x0[ 0.000000] Linux version 4.14.0 (oe-user@oe-host) (gcc version 7.2.0 (GCC)) #3 SMP Wed Oct 3 09:46:54 IST 2018[ 0.000000] Boot CPU: AArch64 Processor [410fd034][ 0.000000] Machine model: ZynqMP ZCU102 Rev1.0[ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')[ 0.000000] bootconsole [cdns0] enabled[ 0.000000] efi: Getting EFI parameters from FDT:[ 0.000000] efi: UEFI not found.[ 0.000000] cma: Reserved 256 MiB at 0x000000006dc00000[ 0.000000] psci: probing for conduit method from DT.[ 0.000000] psci: PSCIv1.1 detected in firmware.[ 0.000000] psci: Using standard PSCI v0.2 function IDs[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.[ 0.000000] percpu: Embedded 21 pages/cpu @ffffffc87ff62000 s45080 r8192 d32744 u86016[ 0.000000] Detected VIPT I-cache on CPU0[ 0.000000] CPU features: enabling workaround for ARM erratum 845719[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1033987[ 0.000000] Kernel command line: earlycon clk_ignore_unused root=/dev/mmcblk0p2 rw rootwait[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)[ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)[ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)[ 0.000000] software IO TLB [mem 0x69c00000-0x6dc00000] (64MB) mapped at [ffffffc069c00000-ffffffc06dbfffff][ 0.000000] Memory: 3784528K/4193280K available (9916K kernel code, 640K rwdata, 3136K rodata, 512K init, 2160K bss, 146608K reserved, 262144K cma-reserved)[ 0.000000] Virtual kernel memory layout:[ 0.000000] modules : 0xffffff8000000000 - 0xffffff8008000000 ( 128 MB)[ 0.000000] vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000 ( 250 GB)[ 0.000000] .text : 0xffffff8008080000 - 0xffffff8008a30000 ( 9920 KB)[ 0.000000] .rodata : 0xffffff8008a30000 - 0xffffff8008d50000 ( 3200 KB)[ 0.000000] .init : 0xffffff8008d50000 - 0xffffff8008dd0000 ( 512 KB)[ 0.000000] .data : 0xffffff8008dd0000 - 0xffffff8008e70200 ( 641 KB)[ 0.000000] .bss : 0xffffff8008e70200 - 0xffffff800908c330 ( 2161 KB)[ 0.000000] fixed : 0xffffffbefe7fd000 - 0xffffffbefec00000 ( 4108 KB)[ 0.000000] PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000 ( 16 MB)[ 0.000000] vmemmap : 0xffffffbf00000000 - 0xffffffc000000000 ( 4 GB maximum)[ 0.000000] 0xffffffbf00000000 - 0xffffffbf1dc00000 ( 476 MB actual)[ 0.000000] memory : 0xffffffc000000000 - 0xffffffc880000000 ( 34816 MB)[ 0.000000] Hierarchical RCU implementation.[ 0.000000] RCU event tracing is enabled.[ 0.000000] RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0[ 0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000[ 0.000000] GIC: Using split EOI/Deactivate mode[ 0.000000] arch_timer: cp15 timer(s) running at 99.99MHz (phys).[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x170f8dc196, max_idle_ns: 440795203664 ns[ 0.000003] sched_clock: 56 bits at 99MHz, resolution 10ns, wraps every 4398046511099ns[ 0.008325] Console: colour dummy device 80x25[ 0.012585] console [tty0] enabled[ 0.015952] bootconsole [cdns0] disabled[ 0.019862] Calibrating delay loop (skipped), value calculated using timer frequency.. 199.98 BogoMIPS (lpj=399960)[ 0.019875] pid_max: default: 32768 minimum: 301[ 0.019975] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes)[ 0.019993] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes)[ 0.020551] ASID allocator initialised with 65536 entries[ 0.020599] Hierarchical SRCU implementation.[ 0.020947] EFI services will not be available.[ 0.020973] zynqmp_plat_init Platform Management API v1.0[ 0.020982] zynqmp_plat_init Trustzone version v1.0[ 0.021079] smp: Bringing up secondary CPUs ...[ 0.021331] Detected VIPT I-cache on CPU1[ 0.021358] CPU1: Booted secondary processor [410fd034][ 0.021630] Detected VIPT I-cache on CPU2[ 0.021648] CPU2: Booted secondary processor [410fd034][ 0.021911] Detected VIPT I-cache on CPU3[ 0.021929] CPU3: Booted secondary processor [410fd034][ 0.021970] smp: Brought up 1 node, 4 CPUs[ 0.022002] SMP: Total of 4 processors activated.[ 0.022010] CPU features: detected feature: 32-bit EL0 Support[ 0.022021] CPU: All CPU(s) started at EL2[ 0.022036] alternatives: patching kernel code[ 0.022754] devtmpfs: initialized[ 0.027376] random: get_random_u32 called from bucket_table_alloc+0x108/0x260 with crng_init=0[ 0.027579] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns[ 0.027600] futex hash table entries: 1024 (order: 5, 131072 bytes)[ 0.027810] random: fast init done[ 0.032969] xor: measuring software checksum speed[ 0.071934] 8regs : 2302.000 MB/sec[ 0.111964] 8regs_prefetch: 2052.000 MB/sec[ 0.151995] 32regs : 2830.000 MB/sec[ 0.192026] 32regs_prefetch: 2381.000 MB/sec[ 0.192034] xor: using function: 32regs (2830.000 MB/sec)[ 0.192099] pinctrl core: initialized pinctrl subsystem[ 0.192597] NET: Registered protocol family 16[ 0.193373] cpuidle: using governor menu[ 0.193941] vdso: 2 pages (1 code @ ffffff8008a36000, 1 data @ ffffff8008dd4000)[ 0.193957] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.[ 0.194412] DMA: preallocated 256 KiB pool for atomic allocations[ 0.223920] reset_zynqmp reset-controller: Xilinx zynqmp reset driver probed[ 0.224499] ARM CCI_400_r1 PMU driver probed[ 0.229384] zynqmp-pinctrl ff180000.pinctrl: zynqmp pinctrl initialized[ 0.237415] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages[ 0.304243] raid6: int64x1 gen() 402 MB/s[ 0.372223] raid6: int64x1 xor() 446 MB/s[ 0.440269] raid6: int64x2 gen() 687 MB/s[ 0.508336] raid6: int64x2 xor() 603 MB/s[ 0.576377] raid6: int64x4 gen() 1042 MB/s[ 0.644393] raid6: int64x4 xor() 742 MB/s[ 0.712492] raid6: int64x8 gen() 980 MB/s[ 0.780506] raid6: int64x8 xor() 745 MB/s[ 0.848566] raid6: neonx1 gen() 726 MB/s[ 0.916596] raid6: neonx1 xor() 851 MB/s[ 0.984651] raid6: neonx2 gen() 1168 MB/s[ 1.052701] raid6: neonx2 xor() 1207 MB/s[ 1.120771] raid6: neonx4 gen() 1505 MB/s[ 1.188792] raid6: neonx4 xor() 1441 MB/s[ 1.256836] raid6: neonx8 gen() 1651 MB/s[ 1.324887] raid6: neonx8 xor() 1534 MB/s[ 1.324895] raid6: using algorithm neonx8 gen() 1651 MB/s[ 1.324903] raid6: .... xor() 1534 MB/s, rmw enabled[ 1.324910] raid6: using neon recovery algorithm[ 1.326325] SCSI subsystem initialized[ 1.326484] usbcore: registered new interface driver usbfs[ 1.326522] usbcore: registered new interface driver hub[ 1.326562] usbcore: registered new device driver usb[ 1.326623] media: Linux media interface: v0.10[ 1.326649] Linux video capture interface: v2.00[ 1.326693] pps_core: LinuxPPS API ver. 1 registered[ 1.326702] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>[ 1.326723] PTP clock support registered[ 1.326749] EDAC MC: Ver: 3.0.0[ 1.327033] zynqmp-ipi ff9905c0.mailbox: Probed ZynqMP IPI Mailbox driver.[ 1.327183] FPGA manager framework[ 1.327286] fpga-region fpga-full: FPGA Region probed[ 1.327382] Advanced Linux Sound Architecture Driver Initialized.[ 1.327618] Bluetooth: Core ver 2.22[ 1.327647] NET: Registered protocol family 31[ 1.327655] Bluetooth: HCI device and connection manager initialized[ 1.327667] Bluetooth: HCI socket layer initialized[ 1.327676] Bluetooth: L2CAP socket layer initialized[ 1.327694] Bluetooth: SCO socket layer initialized[ 1.328213] clocksource: Switched to clocksource arch_sys_counter[ 1.328282] VFS: Disk quotas dquot_6.6.0[ 1.328325] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)[ 1.332170] NET: Registered protocol family 2[ 1.332486] TCP established hash table entries: 32768 (order: 6, 262144 bytes)[ 1.332699] TCP bind hash table entries: 32768 (order: 7, 524288 bytes)[ 1.333081] TCP: Hash tables configured (established 32768 bind 32768)[ 1.333150] UDP hash table entries: 2048 (order: 4, 65536 bytes)[ 1.333227] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes)[ 1.333382] NET: Registered protocol family 1[ 1.333607] RPC: Registered named UNIX socket transport module.[ 1.333617] RPC: Registered udp transport module.[ 1.333624] RPC: Registered tcp transport module.[ 1.333631] RPC: Registered tcp NFSv4.1 backchannel transport module.[ 1.334051] hw perfevents: no interrupt-affinity property for /pmu, guessing.[ 1.334197] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available[ 1.334853] audit: initializing netlink subsys (disabled)[ 1.335176] audit: type=2000 audit(1.316:1): state=initialized audit_enabled=0 res=1[ 1.335220] workingset: timestamp_bits=62 max_order=20 bucket_order=0[ 1.335842] NFS: Registering the id_resolver key type[ 1.335863] Key type id_resolver registered[ 1.335870] Key type id_legacy registered[ 1.335882] nfs4filelayout_init: NFSv4 File Layout Driver Registering...[ 1.335903] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.[ 1.359687] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)[ 1.359708] io scheduler noop registered[ 1.359715] io scheduler deadline registered[ 1.359735] io scheduler cfq registered (default)[ 1.359743] io scheduler mq-deadline registered[ 1.359751] io scheduler kyber registered[ 1.360369] nwl-pcie fd0e0000.pcie: Link is DOWN[ 1.360412] OF: PCI: host bridge /amba/pcie@fd0e0000 ranges:[ 1.360433] OF: PCI: MEM 0xe0000000..0xefffffff -> 0xe0000000[ 1.360445] OF: PCI: MEM 0x600000000..0x7ffffffff -> 0x600000000[ 1.360571] nwl-pcie fd0e0000.pcie: PCI host bridge to bus 0000:00[ 1.360586] pci_bus 0000:00: root bus resource [bus 00-ff][ 1.360596] pci_bus 0000:00: root bus resource [mem 0xe0000000-0xefffffff][ 1.360607] pci_bus 0000:00: root bus resource [mem 0x600000000-0x7ffffffff pref][ 1.360863] pci 0000:00:00.0: PCI bridge to [bus 01-0c][ 1.361761] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed[ 1.362161] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success[ 1.362325] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success[ 1.362484] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success[ 1.362645] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success[ 1.362803] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success[ 1.362963] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success[ 1.363123] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success[ 1.363286] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success[ 1.363506] xilinx-zynqmp-dma ffa80000.dma: ZynqMP DMA driver Probe success[ 1.363664] xilinx-zynqmp-dma ffa90000.dma: ZynqMP DMA driver Probe success[ 1.363816] xilinx-zynqmp-dma ffaa0000.dma: ZynqMP DMA driver Probe success[ 1.363973] xilinx-zynqmp-dma ffab0000.dma: ZynqMP DMA driver Probe success[ 1.364126] xilinx-zynqmp-dma ffac0000.dma: ZynqMP DMA driver Probe success[ 1.364309] xilinx-zynqmp-dma ffad0000.dma: ZynqMP DMA driver Probe success[ 1.364471] xilinx-zynqmp-dma ffae0000.dma: ZynqMP DMA driver Probe success[ 1.364623] xilinx-zynqmp-dma ffaf0000.dma: ZynqMP DMA driver Probe success[ 1.389044] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled[ 1.392383] cacheinfo: Unable to detect cache hierarchy for CPU 0[ 1.396282] brd: module loaded[ 1.399477] loop: module loaded[ 1.400406] ahci-ceva fd0c0000.ahci: couldn't get PHY in node ahci: -517[ 1.400574] mtdoops: mtd device (mtddev=name/number) must be supplied[ 1.402172] m25p80 spi0.0: SPI-NOR-UniqueID 1044002c39910007f1ff170029ac71a285[ 1.402320] m25p80 spi0.0: n25q512a (131072 Kbytes)[ 1.402342] 3 ofpart partitions found on MTD device spi0.0[ 1.402350] Creating 3 MTD partitions on "spi0.0":[ 1.402363] 0x000000000000-0x000000100000 : "boot"[ 1.402779] 0x000000100000-0x000000140000 : "bootenv"[ 1.403144] 0x000000140000-0x000001740000 : "kernel"[ 1.404343] libphy: Fixed MDIO Bus: probed[ 1.405293] tun: Universal TUN/TAP device driver, 1.6[ 1.405423] CAN device driver interface[ 1.407428] macb ff0e0000.ethernet: Not enabling partial store and forward[ 1.407799] libphy: MACB_mii_bus: probed[ 1.409447] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 31 (00:0a:35:00:22:01)[ 1.409464] TI DP83867 ff0e0000.ethernet-ffffffff:0c: attached PHY driver [TI DP83867] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:0c, irq=POLL)[ 1.410093] usbcore: registered new interface driver asix[ 1.410144] usbcore: registered new interface driver ax88179_178a[ 1.410175] usbcore: registered new interface driver cdc_ether[ 1.410207] usbcore: registered new interface driver net1080[ 1.410237] usbcore: registered new interface driver cdc_subset[ 1.410266] usbcore: registered new interface driver zaurus[ 1.410304] usbcore: registered new interface driver cdc_ncm[ 1.410588] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM[ 1.411671] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver[ 1.411682] ehci-pci: EHCI PCI platform driver[ 1.411963] usbcore: registered new interface driver uas[ 1.412002] usbcore: registered new interface driver usb-storage[ 1.412500] rtc_zynqmp ffa60000.rtc: rtc core: registered ffa60000.rtc as rtc0[ 1.412556] i2c /dev entries driver[ 1.413547] IR NEC protocol handler initialized[ 1.413556] IR RC5(x/sz) protocol handler initialized[ 1.413563] IR RC6 protocol handler initialized[ 1.413570] IR JVC protocol handler initialized[ 1.413577] IR Sony protocol handler initialized[ 1.413585] IR SANYO protocol handler initialized[ 1.413592] IR Sharp protocol handler initialized[ 1.413599] IR MCE Keyboard/mouse protocol handler initialized[ 1.413606] IR XMP protocol handler initialized[ 1.414666] usbcore: registered new interface driver uvcvideo[ 1.414675] USB Video Class driver (1.1.1)[ 1.415160] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer at ffffff8009135000 with timeout 10s[ 1.415342] Bluetooth: HCI UART driver ver 2.3[ 1.415353] Bluetooth: HCI UART protocol H4 registered[ 1.415361] Bluetooth: HCI UART protocol BCSP registered[ 1.415390] Bluetooth: HCI UART protocol LL registered[ 1.415399] Bluetooth: HCI UART protocol ATH3K registered[ 1.415407] Bluetooth: HCI UART protocol Three-wire (H5) registered[ 1.415450] Bluetooth: HCI UART protocol Intel registered[ 1.415458] Bluetooth: HCI UART protocol QCA registered[ 1.415493] usbcore: registered new interface driver bcm203x[ 1.415528] usbcore: registered new interface driver bpa10x[ 1.415561] usbcore: registered new interface driver bfusb[ 1.415594] usbcore: registered new interface driver btusb[ 1.415603] Bluetooth: Generic Bluetooth SDIO driver ver 0.1[ 1.415652] usbcore: registered new interface driver ath3k[ 1.415778] EDAC MC: ECC not enabled[ 1.415937] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT)[ 1.416439] cpufreq: cpufreq_online: CPU0: Running at unlisted freq: 1199880 KHz[ 1.416493] cpufreq: cpufreq_online: CPU0: Unlisted initial frequency changed to: 1199999 KHz[ 1.416871] sdhci: Secure Digital Host Controller Interface driver[ 1.416880] sdhci: Copyright(c) Pierre Ossman[ 1.416887] sdhci-pltfm: SDHCI platform and OF driver helper[ 1.464352] mmc0: SDHCI controller on ff170000.sdhci [ff170000.sdhci] using ADMA 64-bit[ 1.470380] ledtrig-cpu: registered to indicate activity on CPUs[ 1.470522] usbcore: registered new interface driver usbhid[ 1.470530] usbhid: USB HID core driver[ 1.470995] ad9361 spi1.0: ad9361_probe : enter (ad9361)[ 1.471843] ad9361 spi1.0: ad9361_reset: by SPI, this may cause unpredicted behavior![ 1.471881] ad9361 spi1.0: ad9361_probe : Unsupported PRODUCT_ID 0xFF[ 1.474572] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered[ 1.477358] pktgen: Packet Generator for packet performance testing. Version: 2.75[ 1.477560] Netfilter messages via NETLINK v0.30.[ 1.477673] ip_tables: (C) 2000-2006 Netfilter Core Team[ 1.477855] Initializing XFRM netlink socket[ 1.477913] NET: Registered protocol family 10[ 1.478310] Segment Routing with IPv6[ 1.478353] ip6_tables: (C) 2000-2006 Netfilter Core Team[ 1.478532] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver[ 1.478828] NET: Registered protocol family 17[ 1.478844] NET: Registered protocol family 15[ 1.478862] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.[ 1.478876] Ebtables v2.0 registered[ 1.478970] can: controller area network core (rev 20170425 abi 9)[ 1.479004] NET: Registered protocol family 29[ 1.479019] can: raw protocol (rev 20170425)[ 1.479026] can: broadcast manager protocol (rev 20170425 t)[ 1.479037] can: netlink gateway (rev 20170425) max_hops=1[ 1.479240] Bluetooth: RFCOMM TTY layer initialized[ 1.479256] Bluetooth: RFCOMM socket layer initialized[ 1.479275] Bluetooth: RFCOMM ver 1.11[ 1.479285] Bluetooth: BNEP (Ethernet Emulation) ver 1.3[ 1.479293] Bluetooth: BNEP filters: protocol multicast[ 1.479303] Bluetooth: BNEP socket layer initialized[ 1.479311] Bluetooth: HIDP (Human Interface Emulation) ver 1.2[ 1.479321] Bluetooth: HIDP socket layer initialized[ 1.479425] 9pnet: Installing 9P2000 support[ 1.479445] Key type dns_resolver registered[ 1.479812] registered taskstats version 1[ 1.481149] Btrfs loaded, crc32c=crc32c-generic[ 1.488409] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 49, base_baud = 6249375) is a xuartps[ 1.619605] mmc0: new high speed SDHC card at address aaaa[ 1.633848] mmcblk0: mmc0:aaaa SU08G 7.40 GiB[ 1.638060] mmcblk0: p1 p2 p3[ 3.151100] console [ttyPS0] enabled[ 3.155252] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 50, base_baud = 6249375) is a xuartps[ 3.165848] xilinx-psgtr fd400000.zynqmp_phy: Lane:1 type:8 protocol:4 pll_locked:yes[ 3.174062] PLL: shutdown[ 3.178245] xilinx-dp-snd-codec fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0: Xilinx DisplayPort Sound Codec probed[ 3.188844] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed[ 3.196805] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed[ 3.205015] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok[ 3.217370] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok[ 3.229991] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: Xilinx DisplayPort Sound Card probed[ 3.240093] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000[ 3.246965] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).[ 3.253503] [drm] No driver support for vblank timestamp query.[ 3.259464] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffff8008ae6268)[ 4.344221] [drm] Cannot find any crtc or sizes[ 4.348840] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display on minor 0[ 4.356870] zynqmp-display fd4a0000.zynqmp-display: ZynqMP DisplayPort Subsystem driver probed[ 4.365824] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:3 protocol:2 pll_locked:yes[ 4.373639] ahci-ceva fd0c0000.ahci: AHCI 0001.0301 32 slots 2 ports 6 Gbps 0x3 impl platform mode[ 4.382526] ahci-ceva fd0c0000.ahci: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst[ 4.392859] scsi host0: ahci-ceva[ 4.396294] scsi host1: ahci-ceva[ 4.399626] ata1: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x100 irq 45[ 4.407466] ata2: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x180 irq 45[ 4.417043] xilinx-psgtr fd400000.zynqmp_phy: Lane:2 type:0 protocol:3 pll_locked:yes[ 4.427011] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller[ 4.432430] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1[ 4.440276] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x22010010[ 4.448928] xhci-hcd xhci-hcd.0.auto: irq 55, io mem 0xfe200000[ 4.454910] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002[ 4.461625] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1[ 4.468827] usb usb1: Product: xHCI Host Controller[ 4.473685] usb usb1: Manufacturer: Linux 4.14.0 xhci-hcd[ 4.479067] usb usb1: SerialNumber: xhci-hcd.0.auto[ 4.484195] hub 1-0:1.0: USB hub found[ 4.487883] hub 1-0:1.0: 1 port detected[ 4.491943] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller[ 4.497359] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2[ 4.505043] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.[ 4.513145] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003[ 4.519854] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1[ 4.527059] usb usb2: Product: xHCI Host Controller[ 4.531917] usb usb2: Manufacturer: Linux 4.14.0 xhci-hcd[ 4.537298] usb usb2: SerialNumber: xhci-hcd.0.auto[ 4.542387] hub 2-0:1.0: USB hub found[ 4.546077] hub 2-0:1.0: 1 port detected[ 4.551083] pca953x 0-0020: 0-0020 supply vcc not found, using dummy regulator[ 4.561198] pca953x 0-0020: interrupt support not compiled in[ 4.566957] pca953x 0-0021: 0-0021 supply vcc not found, using dummy regulator[ 4.576950] pca953x 0-0021: interrupt support not compiled in[ 4.583412] ina2xx 3-0040: power monitor ina226 (Rshunt = 5000 uOhm)[ 4.590115] ina2xx 3-0041: power monitor ina226 (Rshunt = 5000 uOhm)[ 4.596807] ina2xx 3-0042: power monitor ina226 (Rshunt = 5000 uOhm)[ 4.603501] ina2xx 3-0043: power monitor ina226 (Rshunt = 5000 uOhm)[ 4.610195] ina2xx 3-0044: power monitor ina226 (Rshunt = 5000 uOhm)[ 4.616896] ina2xx 3-0045: power monitor ina226 (Rshunt = 5000 uOhm)[ 4.623598] ina2xx 3-0046: power monitor ina226 (Rshunt = 5000 uOhm)[ 4.630295] ina2xx 3-0047: power monitor ina226 (Rshunt = 5000 uOhm)[ 4.636992] ina2xx 3-004a: power monitor ina226 (Rshunt = 5000 uOhm)[ 4.643681] ina2xx 3-004b: power monitor ina226 (Rshunt = 5000 uOhm)[ 4.649984] i2c i2c-0: Added multiplexed i2c bus 3[ 4.655340] ina2xx 4-0040: power monitor ina226 (Rshunt = 2000 uOhm)[ 4.662043] ina2xx 4-0041: power monitor ina226 (Rshunt = 5000 uOhm)[ 4.668741] ina2xx 4-0042: power monitor ina226 (Rshunt = 5000 uOhm)[ 4.675434] ina2xx 4-0043: power monitor ina226 (Rshunt = 5000 uOhm)[ 4.682127] ina2xx 4-0044: power monitor ina226 (Rshunt = 5000 uOhm)[ 4.688822] ina2xx 4-0045: power monitor ina226 (Rshunt = 5000 uOhm)[ 4.695520] ina2xx 4-0046: power monitor ina226 (Rshunt = 5000 uOhm)[ 4.702216] ina2xx 4-0047: power monitor ina226 (Rshunt = 5000 uOhm)[ 4.708516] i2c i2c-0: Added multiplexed i2c bus 4[ 4.730410] ata2: SATA link down (SStatus 0 SControl 330)[ 4.735748] ata1: SATA link down (SStatus 0 SControl 330)[ 4.759067] i2c i2c-0: Added multiplexed i2c bus 5[ 4.763900] i2c i2c-0: Added multiplexed i2c bus 6[ 4.768612] pca954x 0-0075: registered 4 multiplexed busses for I2C mux pca9544[ 4.775925] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 33[ 4.783476] at24 7-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write[ 4.790125] i2c i2c-1: Added multiplexed i2c bus 7[ 4.795049] i2c i2c-1: Added multiplexed i2c bus 8[ 4.801771] si570 9-005d: registered, current frequency 300000000 Hz[ 4.808075] i2c i2c-1: Added multiplexed i2c bus 9[ 4.826752] si570 10-005d: registered, current frequency 148500000 Hz[ 4.833141] i2c i2c-1: Added multiplexed i2c bus 10[ 4.838162] i2c i2c-1: Added multiplexed i2c bus 11[ 4.843080] i2c i2c-1: Added multiplexed i2c bus 12[ 4.847999] i2c i2c-1: Added multiplexed i2c bus 13[ 4.852911] i2c i2c-1: Added multiplexed i2c bus 14[ 4.857712] pca954x 1-0074: registered 8 multiplexed busses for I2C switch pca9548[ 4.865579] i2c i2c-1: Added multiplexed i2c bus 15[ 4.870499] i2c i2c-1: Added multiplexed i2c bus 16[ 4.875421] i2c i2c-1: Added multiplexed i2c bus 17[ 4.880647] i2c i2c-1: Added multiplexed i2c bus 18[ 4.885566] i2c i2c-1: Added multiplexed i2c bus 19[ 4.890496] i2c i2c-1: Added multiplexed i2c bus 20[ 4.895411] i2c i2c-1: Added multiplexed i2c bus 21[ 4.900333] i2c i2c-1: Added multiplexed i2c bus 22[ 4.905135] pca954x 1-0075: registered 8 multiplexed busses for I2C switch pca9548[ 4.912708] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 34[ 4.919745] input: gpio-keys as /devices/platform/gpio-keys/input/input0[ 4.926544] rtc_zynqmp ffa60000.rtc: setting system clock to 2018-10-03 07:34:06 UTC (1538552046)[ 4.935340] of_cfs_init[ 4.937780] of_cfs_init: OK[ 4.940673] clk: Not disabling unused clocks[ 4.944904] ALSA device list:[ 4.947808] #0: DisplayPort monitor[ 4.954515] EXT4-fs (mmcblk0p2): couldn't mount as ext3 due to feature incompatibilities[ 5.151551] EXT4-fs (mmcblk0p2): recovery complete[ 5.157608] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)[ 5.165647] VFS: Mounted root (ext4 filesystem) on device 179:2.[ 5.179997] devtmpfs: mounted[ 5.183000] Freeing unused kernel memory: 512KMount failed for selinuxfs on /sys/fs/selinux: No such file or directory[ 5.488247] [drm] Cannot find any crtc or sizes * Setting up X socket directories... [ OK ] * STARTDISTCC is set to false in /etc/default/distcc * /usr/bin/distccd not starting * Starting IIO Daemon iiod
After this no login prompt is coming.
What could be missing here? Is there way of verifying the built image contains all required modules and device-tree.
Note: I disabled the MATHWORKS driver while building this Linux Image.
Your valuable suggestions are highly appreciated. Thank you.
Best Regards
-Siddhant
Hi,
the resource length should not have any impact, since we only use less than 4k memory.
The auto-generated stuff uses the size of reserved IO memory...
Looking at your bootlog shows that all drivers…
I would try to see where the issue is kernel of dt.
Use our Image with your dt and vice versa.
Then you know where to look at.
You need everything under the fpga_axi node in here:
https://github.com/analogdevicesinc/linux/blob/master/arch/arm64/boot/dts/xilinx/zynqmp-zcu102-rev10-ad9361-fmcomms2-3.dts#L33
In addition the drivers…
Looks like you're missing a few things in the device tree. Otherwise you wouldn't get the errors and warnings.
[ 1.471843] ad9361 spi1.0: ad9361_reset: by SPI, this may cause unpredicted behavior!
This for example indicates that the reset GPIO is missing.
In general we recommend starting without device trees.
Not 100% sure why you don't get the login prompt - for me it looks like your ext4 partition is damaged.
Try to re-image the SD card.
-Michael
Hi Micheal,
Waiting for your comment on device-tree, Could you please tell me what is wrong here? or any debugging technique which would help me in fixing the problem.
Thank you.
Hi Michael,
Ty for quick response!
Yes, the boot files you shared is working fine in driver probing, but the image I created using petalinux tool is having issue, it is not able to probe the driver.
My main problem still persists How to debug this probing issue. I am trying to modify device-tree , rebuild the image and test. But No Success so far.
I would continue my debugging with the resources you provided :)
Regards
I used your Image with my system.dtb and same probing error came, product unsuported at FF. So, with this I think problem is in Device-Tree. I would look into this now.
Thanks for smart stuff. Kudos!
Hello Michael,
Hope you are doing great!
I have a little progress in my work, Now I see AD9361 is initialized successfully, but cf-ad9361-dds-core-lpc and cf-ad9361-lpc are not probed, What I should do to check this issue? How should I add entry in the device-tree for such devices?
The duplicated entry in DT you pointed out earlier would really make difference, am little skeptical on this, since I tried to delete those nodes but still I see them in device-tree.
Thank you
Xilinx Zynq MP First Stage Boot Loader Release 2018.2 Oct 16 2018 - 10:07:27 NOTICE: ATF running on XCZU9EG/silicon v4/RTL5.1 at 0xfffea000 NOTICE: BL31: Secure code at 0x0 NOTICE: BL31: Non secure code at 0x8000000 NOTICE: BL31: v1.4(release):xilinx-v2018.1-4-g93a69a5a NOTICE: BL31: Built : 07:45:19, Oct 16 2018 PMUFW: v1.0 U-Boot 2018.01 (Oct 16 2018 - 13:12:57 +0530) Xilinx ZynqMP ZCU102 rev1.0 I2C: ready DRAM: 4 GiB EL Level: EL2 Chip ID: zu9eg MMC: sdhci@ff170000: 0 (SD) SF: Detected n25q512a with page size 512 Bytes, erase size 128 KiB, total 128 MiB *** Warning - bad CRC, using default environment In: serial@ff000000 Out: serial@ff000000 Err: serial@ff000000 Model: ZynqMP ZCU102 Rev1.0 Board: Xilinx ZynqMP Bootmode: LVL_SHFT_SD_MODE1 Net: ZYNQ GEM: ff0e0000, phyaddr c, interface rgmii-id eth0: ethernet@ff0e0000 U-BOOT for lnx_ad9361 Hit any key to stop autoboot: 0 Device: sdhci@ff170000 Manufacturer ID: 3 OEM: 5344 Name: SD08G Tran Speed: 25000000 Rd Block Len: 512 SD version 3.0 High Capacity: Yes Capacity: 7.4 GiB Bus Width: 4-bit Erase Group Size: 512 Bytes reading image.ub 74615488 bytes read in 6606 ms (10.8 MiB/s) ## Loading kernel from FIT Image at 10000000 ... Using 'conf@system-top.dtb' configuration Trying 'kernel@1' kernel subimage Description: Linux kernel Type: Kernel Image Compression: gzip compressed Data Start: 0x100000f8 Data Size: 7191650 Bytes = 6.9 MiB Architecture: AArch64 OS: Linux Load Address: 0x00080000 Entry Point: 0x00080000 Hash algo: sha1 Hash value: 028cffe5d2741814a43641ba19739b2d579a0c38 Verifying Hash Integrity ... sha1+ OK ## Loading ramdisk from FIT Image at 10000000 ... Using 'conf@system-top.dtb' configuration Trying 'ramdisk@1' ramdisk subimage Description: petalinux-user-image Type: RAMDisk Image Compression: gzip compressed Data Start: 0x106e7af0 Data Size: 67373629 Bytes = 64.3 MiB Architecture: AArch64 OS: Linux Load Address: unavailable Entry Point: unavailable Hash algo: sha1 Hash value: 641b075ab179d630c0b8b9f03a3d2ecb55b44d14 Verifying Hash Integrity ... sha1+ OK ## Loading fdt from FIT Image at 10000000 ... Using 'conf@system-top.dtb' configuration Trying 'fdt@system-top.dtb' fdt subimage Description: Flattened Device Tree blob Type: Flat Device Tree Compression: uncompressed Data Start: 0x106dbe60 Data Size: 48076 Bytes = 46.9 KiB Architecture: AArch64 Hash algo: sha1 Hash value: 4d3b841177020bb040f100e317ee4b36380bfb36 Verifying Hash Integrity ... sha1+ OK Booting using the fdt blob at 0x106dbe60 Uncompressing Kernel Image ... OK Loading Ramdisk to 79d4c000, end 7dd8ca3d ... OK Loading Device Tree to 0000000079d3d000, end 0000000079d4bbcb ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.14.0 (oe-user@oe-host) (gcc version 7.2.0 (GCC)) #3 SMP Tue Oct 16 10:01:49 IST 2018 [ 0.000000] Boot CPU: AArch64 Processor [410fd034] [ 0.000000] Machine model: ZynqMP ZCU102 Rev1.0 [ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8') [ 0.000000] bootconsole [cdns0] enabled [ 0.000000] efi: Getting EFI parameters from FDT: [ 0.000000] efi: UEFI not found. [ 0.000000] cma: Reserved 256 MiB at 0x0000000069c00000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: MIGRATE_INFO_TYPE not supported. [ 0.000000] percpu: Embedded 21 pages/cpu @ffffffc87ff5f000 s45080 r8192 d32744 u86016 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: enabling workaround for ARM erratum 845719 [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1033987 [ 0.000000] Kernel command line: earlycon clk_ignore_unused [ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes) [ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes) [ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes) [ 0.000000] software IO TLB [mem 0x65c00000-0x69c00000] (64MB) mapped at [ffffffc065c00000-ffffffc069bfffff] [ 0.000000] Memory: 3718036K/4193280K available (10172K kernel code, 874K rwdata, 3352K rodata, 512K init, 2162K bss, 213100K reserved, 262144K cma-reserved) [ 0.000000] Virtual kernel memory layout: [ 0.000000] modules : 0xffffff8000000000 - 0xffffff8008000000 ( 128 MB) [ 0.000000] vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000 ( 250 GB) [ 0.000000] .text : 0xffffff8008080000 - 0xffffff8008a70000 ( 10176 KB) [ 0.000000] .rodata : 0xffffff8008a70000 - 0xffffff8008dc0000 ( 3392 KB) [ 0.000000] .init : 0xffffff8008dc0000 - 0xffffff8008e40000 ( 512 KB) [ 0.000000] .data : 0xffffff8008e40000 - 0xffffff8008f1aa00 ( 875 KB) [ 0.000000] .bss : 0xffffff8008f1aa00 - 0xffffff80091375b8 ( 2163 KB) [ 0.000000] fixed : 0xffffffbefe7fd000 - 0xffffffbefec00000 ( 4108 KB) [ 0.000000] PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000 ( 16 MB) [ 0.000000] vmemmap : 0xffffffbf00000000 - 0xffffffc000000000 ( 4 GB maximum) [ 0.000000] 0xffffffbf00000000 - 0xffffffbf1dc00000 ( 476 MB actual) [ 0.000000] memory : 0xffffffc000000000 - 0xffffffc880000000 ( 34816 MB) [ 0.000000] Hierarchical RCU implementation. [ 0.000000] RCU event tracing is enabled. [ 0.000000] RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4. [ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000 [ 0.000000] GIC: Using split EOI/Deactivate mode [ 0.000000] arch_timer: cp15 timer(s) running at 99.99MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x170f8dc196, max_idle_ns: 440795203664 ns [ 0.000003] sched_clock: 56 bits at 99MHz, resolution 10ns, wraps every 4398046511099ns [ 0.008334] Console: colour dummy device 80x25 [ 0.012594] console [tty0] enabled [ 0.015961] bootconsole [cdns0] disabled [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.14.0 (oe-user@oe-host) (gcc version 7.2.0 (GCC)) #3 SMP Tue Oct 16 10:01:49 IST 2018 [ 0.000000] Boot CPU: AArch64 Processor [410fd034] [ 0.000000] Machine model: ZynqMP ZCU102 Rev1.0 [ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8') [ 0.000000] bootconsole [cdns0] enabled [ 0.000000] efi: Getting EFI parameters from FDT: [ 0.000000] efi: UEFI not found. [ 0.000000] cma: Reserved 256 MiB at 0x0000000069c00000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: MIGRATE_INFO_TYPE not supported. [ 0.000000] percpu: Embedded 21 pages/cpu @ffffffc87ff5f000 s45080 r8192 d32744 u86016 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: enabling workaround for ARM erratum 845719 [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1033987 [ 0.000000] Kernel command line: earlycon clk_ignore_unused [ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes) [ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes) [ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes) [ 0.000000] software IO TLB [mem 0x65c00000-0x69c00000] (64MB) mapped at [ffffffc065c00000-ffffffc069bfffff] [ 0.000000] Memory: 3718036K/4193280K available (10172K kernel code, 874K rwdata, 3352K rodata, 512K init, 2162K bss, 213100K reserved, 262144K cma-reserved) [ 0.000000] Virtual kernel memory layout: [ 0.000000] modules : 0xffffff8000000000 - 0xffffff8008000000 ( 128 MB) [ 0.000000] vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000 ( 250 GB) [ 0.000000] .text : 0xffffff8008080000 - 0xffffff8008a70000 ( 10176 KB) [ 0.000000] .rodata : 0xffffff8008a70000 - 0xffffff8008dc0000 ( 3392 KB) [ 0.000000] .init : 0xffffff8008dc0000 - 0xffffff8008e40000 ( 512 KB) [ 0.000000] .data : 0xffffff8008e40000 - 0xffffff8008f1aa00 ( 875 KB) [ 0.000000] .bss : 0xffffff8008f1aa00 - 0xffffff80091375b8 ( 2163 KB) [ 0.000000] fixed : 0xffffffbefe7fd000 - 0xffffffbefec00000 ( 4108 KB) [ 0.000000] PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000 ( 16 MB) [ 0.000000] vmemmap : 0xffffffbf00000000 - 0xffffffc000000000 ( 4 GB maximum) [ 0.000000] 0xffffffbf00000000 - 0xffffffbf1dc00000 ( 476 MB actual) [ 0.000000] memory : 0xffffffc000000000 - 0xffffffc880000000 ( 34816 MB) [ 0.000000] Hierarchical RCU implementation. [ 0.000000] RCU event tracing is enabled. [ 0.000000] RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4. [ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000 [ 0.000000] GIC: Using split EOI/Deactivate mode [ 0.000000] arch_timer: cp15 timer(s) running at 99.99MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x170f8dc196, max_idle_ns: 440795203664 ns [ 0.000003] sched_clock: 56 bits at 99MHz, resolution 10ns, wraps every 4398046511099ns [ 0.008334] Console: colour dummy device 80x25 [ 0.012594] console [tty0] enabled [ 0.015961] bootconsole [cdns0] disabled [ 0.019870] Calibrating delay loop (skipped), value calculated using timer frequency.. 199.98 BogoMIPS (lpj=399960) [ 0.019883] pid_max: default: 32768 minimum: 301 [ 0.019984] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes) [ 0.020002] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes) [ 0.020577] ASID allocator initialised with 65536 entries [ 0.020630] Hierarchical SRCU implementation. [ 0.022215] EFI services will not be available. [ 0.022242] zynqmp_plat_init Platform Management API v1.0 [ 0.022250] zynqmp_plat_init Trustzone version v1.0 [ 0.022354] smp: Bringing up secondary CPUs ... [ 0.177301] Detected VIPT I-cache on CPU1 [ 0.177332] CPU1: Booted secondary processor [410fd034] [ 0.290042] Detected VIPT I-cache on CPU2 [ 0.290059] CPU2: Booted secondary processor [410fd034] [ 0.416536] Detected VIPT I-cache on CPU3 [ 0.416554] CPU3: Booted secondary processor [410fd034] [ 0.416595] smp: Brought up 1 node, 4 CPUs [ 0.416627] SMP: Total of 4 processors activated. [ 0.416636] CPU features: detected feature: 32-bit EL0 Support [ 0.416646] CPU: All CPU(s) started at EL2 [ 0.416662] alternatives: patching kernel code [ 0.417368] devtmpfs: initialized [ 0.422500] random: get_random_u32 called from bucket_table_alloc+0x108/0x260 with crng_init=0 [ 0.422659] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.422678] futex hash table entries: 1024 (order: 5, 131072 bytes) [ 0.428039] xor: measuring software checksum speed [ 0.464203] 8regs : 2302.000 MB/sec [ 0.504232] 8regs_prefetch: 2052.000 MB/sec [ 0.544263] 32regs : 2830.000 MB/sec [ 0.584295] 32regs_prefetch: 2381.000 MB/sec [ 0.584303] xor: using function: 32regs (2830.000 MB/sec) [ 0.584372] pinctrl core: initialized pinctrl subsystem [ 0.584586] random: fast init done [ 0.584863] NET: Registered protocol family 16 [ 0.585411] cpuidle: using governor menu [ 0.585942] vdso: 2 pages (1 code @ ffffff8008a76000, 1 data @ ffffff8008e44000) [ 0.585963] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.586423] DMA: preallocated 256 KiB pool for atomic allocations [ 0.616088] reset_zynqmp reset-controller: Xilinx zynqmp reset driver probed [ 0.616672] ARM CCI_400_r1 PMU driver probed [ 0.621642] zynqmp-pinctrl ff180000.pinctrl: zynqmp pinctrl initialized [ 0.630604] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages [ 0.696460] raid6: int64x1 gen() 400 MB/s [ 0.764535] raid6: int64x1 xor() 443 MB/s [ 0.832582] raid6: int64x2 gen() 686 MB/s [ 0.900588] raid6: int64x2 xor() 602 MB/s [ 0.968674] raid6: int64x4 gen() 1042 MB/s [ 1.036696] raid6: int64x4 xor() 742 MB/s [ 1.104788] raid6: int64x8 gen() 980 MB/s [ 1.172809] raid6: int64x8 xor() 745 MB/s [ 1.240894] raid6: neonx1 gen() 727 MB/s [ 1.308910] raid6: neonx1 xor() 851 MB/s [ 1.376969] raid6: neonx2 gen() 1166 MB/s [ 1.445020] raid6: neonx2 xor() 1207 MB/s [ 1.513104] raid6: neonx4 gen() 1511 MB/s [ 1.581129] raid6: neonx4 xor() 1442 MB/s [ 1.649212] raid6: neonx8 gen() 1653 MB/s [ 1.717229] raid6: neonx8 xor() 1534 MB/s [ 1.717237] raid6: using algorithm neonx8 gen() 1653 MB/s [ 1.717245] raid6: .... xor() 1534 MB/s, rmw enabled [ 1.717252] raid6: using neon recovery algorithm [ 1.718699] SCSI subsystem initialized [ 1.718870] usbcore: registered new interface driver usbfs [ 1.718907] usbcore: registered new interface driver hub [ 1.718945] usbcore: registered new device driver usb [ 1.719015] media: Linux media interface: v0.10 [ 1.719043] Linux video capture interface: v2.00 [ 1.719083] pps_core: LinuxPPS API ver. 1 registered [ 1.719091] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 1.719112] PTP clock support registered [ 1.719139] EDAC MC: Ver: 3.0.0 [ 1.719424] zynqmp-ipi ff9905c0.mailbox: Probed ZynqMP IPI Mailbox driver. [ 1.719578] FPGA manager framework [ 1.719683] fpga-region fpga-full: FPGA Region probed [ 1.719780] Advanced Linux Sound Architecture Driver Initialized. [ 1.720030] Bluetooth: Core ver 2.22 [ 1.720058] NET: Registered protocol family 31 [ 1.720066] Bluetooth: HCI device and connection manager initialized [ 1.720078] Bluetooth: HCI socket layer initialized [ 1.720088] Bluetooth: L2CAP socket layer initialized [ 1.720105] Bluetooth: SCO socket layer initialized [ 1.720550] clocksource: Switched to clocksource arch_sys_counter [ 1.720621] VFS: Disk quotas dquot_6.6.0 [ 1.720662] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 1.724711] NET: Registered protocol family 2 [ 1.725007] TCP established hash table entries: 32768 (order: 6, 262144 bytes) [ 1.725219] TCP bind hash table entries: 32768 (order: 7, 524288 bytes) [ 1.725602] TCP: Hash tables configured (established 32768 bind 32768) [ 1.725670] UDP hash table entries: 2048 (order: 4, 65536 bytes) [ 1.725748] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes) [ 1.725898] NET: Registered protocol family 1 [ 1.726063] RPC: Registered named UNIX socket transport module. [ 1.726072] RPC: Registered udp transport module. [ 1.726079] RPC: Registered tcp transport module. [ 1.726087] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 1.726188] Trying to unpack rootfs image as initramfs... [ 4.785184] Freeing initrd memory: 65792K [ 4.785717] hw perfevents: no interrupt-affinity property for /pmu, guessing. [ 4.785878] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available [ 4.786597] audit: initializing netlink subsys (disabled) [ 4.786681] audit: type=2000 audit(4.772:1): state=initialized audit_enabled=0 res=1 [ 4.786997] workingset: timestamp_bits=62 max_order=20 bucket_order=0 [ 4.787660] NFS: Registering the id_resolver key type [ 4.787681] Key type id_resolver registered [ 4.787688] Key type id_legacy registered [ 4.787700] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 4.787722] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc. [ 4.814120] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246) [ 4.814139] io scheduler noop registered [ 4.814146] io scheduler deadline registered [ 4.814167] io scheduler cfq registered (default) [ 4.814175] io scheduler mq-deadline registered [ 4.814183] io scheduler kyber registered [ 4.814852] nwl-pcie fd0e0000.pcie: Link is DOWN [ 4.814898] OF: PCI: host bridge /amba/pcie@fd0e0000 ranges: [ 4.814921] OF: PCI: MEM 0xe0000000..0xefffffff -> 0xe0000000 [ 4.814934] OF: PCI: MEM 0x600000000..0x7ffffffff -> 0x600000000 [ 4.815066] nwl-pcie fd0e0000.pcie: PCI host bridge to bus 0000:00 [ 4.815081] pci_bus 0000:00: root bus resource [bus 00-ff] [ 4.815091] pci_bus 0000:00: root bus resource [mem 0xe0000000-0xefffffff] [ 4.815102] pci_bus 0000:00: root bus resource [mem 0x600000000-0x7ffffffff pref] [ 4.815365] pci 0000:00:00.0: PCI bridge to [bus 01-0c] [ 4.816320] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed [ 4.816903] xilinx-zynqmp-dma ffa80000.dma: ZynqMP DMA driver Probe success [ 4.817057] xilinx-zynqmp-dma ffa90000.dma: ZynqMP DMA driver Probe success [ 4.817213] xilinx-zynqmp-dma ffaa0000.dma: ZynqMP DMA driver Probe success [ 4.817366] xilinx-zynqmp-dma ffab0000.dma: ZynqMP DMA driver Probe success [ 4.817520] xilinx-zynqmp-dma ffac0000.dma: ZynqMP DMA driver Probe success [ 4.817677] xilinx-zynqmp-dma ffad0000.dma: ZynqMP DMA driver Probe success [ 4.817830] xilinx-zynqmp-dma ffae0000.dma: ZynqMP DMA driver Probe success [ 4.817984] xilinx-zynqmp-dma ffaf0000.dma: ZynqMP DMA driver Probe success [ 4.842988] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled [ 4.844569] arm-smmu fd800000.smmu: probing hardware configuration... [ 4.844584] arm-smmu fd800000.smmu: SMMUv2 with: [ 4.844593] arm-smmu fd800000.smmu: stage 1 translation [ 4.844602] arm-smmu fd800000.smmu: stage 2 translation [ 4.844611] arm-smmu fd800000.smmu: nested translation [ 4.844623] arm-smmu fd800000.smmu: stream matching with 48 register groups [ 4.844635] arm-smmu fd800000.smmu: 16 context banks (0 stage-2 only) [ 4.844647] arm-smmu fd800000.smmu: Supported page sizes: 0x61311000 [ 4.844657] arm-smmu fd800000.smmu: Stage-1: 48-bit VA -> 48-bit IPA [ 4.844666] arm-smmu fd800000.smmu: Stage-2: 48-bit IPA -> 48-bit PA [ 4.846840] cacheinfo: Unable to detect cache hierarchy for CPU 0 [ 4.850874] brd: module loaded [ 4.854219] loop: module loaded [ 4.855098] iommu: Adding device fd0c0000.ahci to group 0 [ 4.855280] ahci-ceva fd0c0000.ahci: couldn't get PHY in node ahci: -517 [ 4.855434] mtdoops: mtd device (mtddev=name/number) must be supplied [ 4.856644] iommu: Adding device ff0f0000.spi to group 1 [ 4.857230] m25p80 spi0.0: SPI-NOR-UniqueID 1044002c39910007f1ff170029ac71a285 [ 4.857409] m25p80 spi0.0: n25q512a (131072 Kbytes) [ 4.857432] 3 ofpart partitions found on MTD device spi0.0 [ 4.857441] Creating 3 MTD partitions on "spi0.0": [ 4.857453] 0x000000000000-0x000000100000 : "boot" [ 4.857896] 0x000000100000-0x000000140000 : "bootenv" [ 4.858277] 0x000000140000-0x000001740000 : "kernel" [ 4.859510] libphy: Fixed MDIO Bus: probed [ 4.860498] tun: Universal TUN/TAP device driver, 1.6 [ 4.860742] CAN device driver interface [ 4.862541] iommu: Adding device ff0e0000.ethernet to group 2 [ 4.862898] macb ff0e0000.ethernet: Not enabling partial store and forward [ 4.863284] libphy: MACB_mii_bus: probed [ 4.866596] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 31 (00:0a:35:00:22:01) [ 4.866617] TI DP83867 ff0e0000.ethernet-ffffffff:0c: attached PHY driver [TI DP83867] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:0c, irq=POLL) [ 4.867323] usbcore: registered new interface driver asix [ 4.867373] usbcore: registered new interface driver ax88179_178a [ 4.867405] usbcore: registered new interface driver cdc_ether [ 4.867435] usbcore: registered new interface driver net1080 [ 4.867465] usbcore: registered new interface driver cdc_subset [ 4.867495] usbcore: registered new interface driver zaurus [ 4.867536] usbcore: registered new interface driver cdc_ncm [ 4.867842] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM [ 4.868997] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 4.869016] ehci-pci: EHCI PCI platform driver [ 4.869318] usbcore: registered new interface driver uas [ 4.869357] usbcore: registered new interface driver usb-storage [ 4.869853] rtc_zynqmp ffa60000.rtc: rtc core: registered ffa60000.rtc as rtc0 [ 4.869912] i2c /dev entries driver [ 4.870917] IR NEC protocol handler initialized [ 4.870926] IR RC5(x/sz) protocol handler initialized [ 4.870934] IR RC6 protocol handler initialized [ 4.870941] IR JVC protocol handler initialized [ 4.870948] IR Sony protocol handler initialized [ 4.870955] IR SANYO protocol handler initialized [ 4.870962] IR Sharp protocol handler initialized [ 4.870969] IR MCE Keyboard/mouse protocol handler initialized [ 4.870976] IR XMP protocol handler initialized [ 4.872088] usbcore: registered new interface driver uvcvideo [ 4.872096] USB Video Class driver (1.1.1) [ 4.872613] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer at ffffff80091b5000 with timeout 10s [ 4.872803] Bluetooth: HCI UART driver ver 2.3 [ 4.872814] Bluetooth: HCI UART protocol H4 registered [ 4.872821] Bluetooth: HCI UART protocol BCSP registered [ 4.872848] Bluetooth: HCI UART protocol LL registered [ 4.872857] Bluetooth: HCI UART protocol ATH3K registered [ 4.872865] Bluetooth: HCI UART protocol Three-wire (H5) registered [ 4.872909] Bluetooth: HCI UART protocol Intel registered [ 4.872918] Bluetooth: HCI UART protocol QCA registered [ 4.872955] usbcore: registered new interface driver bcm203x [ 4.872989] usbcore: registered new interface driver bpa10x [ 4.873022] usbcore: registered new interface driver bfusb [ 4.873057] usbcore: registered new interface driver btusb [ 4.873066] Bluetooth: Generic Bluetooth SDIO driver ver 0.1 [ 4.873114] usbcore: registered new interface driver ath3k [ 4.873240] EDAC MC: ECC not enabled [ 4.873402] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT) [ 4.873891] cpufreq: cpufreq_online: CPU0: Running at unlisted freq: 1199880 KHz [ 4.873947] cpufreq: cpufreq_online: CPU0: Unlisted initial frequency changed to: 1199999 KHz [ 4.874339] sdhci: Secure Digital Host Controller Interface driver [ 4.874348] sdhci: Copyright(c) Pierre Ossman [ 4.874355] sdhci-pltfm: SDHCI platform and OF driver helper [ 4.875177] iommu: Adding device ff170000.sdhci to group 3 [ 4.924559] mmc0: SDHCI controller on ff170000.sdhci [ff170000.sdhci] using ADMA 64-bit [ 4.930667] ledtrig-cpu: registered to indicate activity on CPUs [ 4.930808] usbcore: registered new interface driver usbhid [ 4.930816] usbhid: USB HID core driver [ 4.931409] ad9361 spi1.0: ad9361_probe : enter (ad9361) [ 4.933965] fake-fmc-carrier: mezzanine 0 [ 4.933976] Manufacturer: fake-vendor [ 4.933983] Product name: fake-design-for-testing [ 4.934038] fmc fake-design-for-testing-f001: Driver has no ID: matches all [ 4.934065] fmc_trivial: probe of fake-design-for-testing-f001 failed with error -95 [ 4.934093] fmc fake-design-for-testing-f001: Driver has no ID: matches all [ 4.934113] fmc_write_eeprom fake-design-for-testing-f001: fmc_write_eeprom: no busid passed, refusing all cards [ 4.934145] fmc fake-design-for-testing-f001: Driver has no ID: matches all [ 4.935259] fmc_chardev fake-design-for-testing-f001: Created misc device "fake-design-for-testing-f001" [ 4.935547] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered [ 4.937054] pktgen: Packet Generator for packet performance testing. Version: 2.75 [ 4.938009] Netfilter messages via NETLINK v0.30. [ 4.938125] ip_tables: (C) 2000-2006 Netfilter Core Team [ 4.938267] Initializing XFRM netlink socket [ 4.938335] NET: Registered protocol family 10 [ 4.938730] Segment Routing with IPv6 [ 4.938774] ip6_tables: (C) 2000-2006 Netfilter Core Team [ 4.938896] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 4.939206] NET: Registered protocol family 17 [ 4.939222] NET: Registered protocol family 15 [ 4.939239] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this. [ 4.939253] Ebtables v2.0 registered [ 4.939497] can: controller area network core (rev 20170425 abi 9) [ 4.939527] NET: Registered protocol family 29 [ 4.939543] can: raw protocol (rev 20170425) [ 4.939550] can: broadcast manager protocol (rev 20170425 t) [ 4.939561] can: netlink gateway (rev 20170425) max_hops=1 [ 4.939695] Bluetooth: RFCOMM TTY layer initialized [ 4.939707] Bluetooth: RFCOMM socket layer initialized [ 4.939722] Bluetooth: RFCOMM ver 1.11 [ 4.939732] Bluetooth: BNEP (Ethernet Emulation) ver 1.3 [ 4.939740] Bluetooth: BNEP filters: protocol multicast [ 4.939750] Bluetooth: BNEP socket layer initialized [ 4.939758] Bluetooth: HIDP (Human Interface Emulation) ver 1.2 [ 4.939768] Bluetooth: HIDP socket layer initialized [ 4.939882] 9pnet: Installing 9P2000 support [ 4.939902] Key type dns_resolver registered [ 4.940228] registered taskstats version 1 [ 4.941584] Btrfs loaded, crc32c=crc32c-generic [ 4.948818] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 50, base_baud = 6249375) is a xuartps [ 5.076775] mmc0: new SDHC card at address e624 [ 5.090949] mmcblk0: mmc0:e624 SD08G 7.40 GiB [ 5.109753] mmcblk0: p1 p2 p3 [ 6.689993] console [ttyPS0] enabled [ 6.694158] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 51, base_baud = 6249375) is a xuartps [ 6.704607] iommu: Adding device fd500000.dma to group 4 [ 6.710107] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success [ 6.717078] iommu: Adding device fd510000.dma to group 5 [ 6.722493] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success [ 6.729465] iommu: Adding device fd520000.dma to group 6 [ 6.734871] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success [ 6.741845] iommu: Adding device fd530000.dma to group 7 [ 6.747250] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success [ 6.754229] iommu: Adding device fd540000.dma to group 8 [ 6.759645] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success [ 6.766641] iommu: Adding device fd550000.dma to group 9 [ 6.772092] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success [ 6.779071] iommu: Adding device fd560000.dma to group 10 [ 6.784610] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success [ 6.791585] iommu: Adding device fd570000.dma to group 11 [ 6.797107] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success [ 6.804266] xilinx-psgtr fd400000.zynqmp_phy: Lane:1 type:8 protocol:4 pll_locked:yes [ 6.812487] PLL: shutdown [ 6.816705] xilinx-dp-snd-codec fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0: Xilinx DisplayPort Sound Codec probed [ 6.827302] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed [ 6.835273] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed [ 6.843546] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok [ 6.855901] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok [ 6.868531] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: Xilinx DisplayPort Sound Card probed [ 6.878637] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000 [ 6.885539] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013). [ 6.892071] [drm] No driver support for vblank timestamp query. [ 6.898031] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffff8008b28230) [ 7.984559] [drm] Cannot find any crtc or sizes [ 7.989186] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display on minor 0 [ 7.997220] zynqmp-display fd4a0000.zynqmp-display: ZynqMP DisplayPort Subsystem driver probed [ 8.006183] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:3 protocol:2 pll_locked:yes [ 8.024054] ahci-ceva fd0c0000.ahci: AHCI 0001.0301 32 slots 2 ports 6 Gbps 0x3 impl platform mode [ 8.032946] ahci-ceva fd0c0000.ahci: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst [ 8.043225] scsi host0: ahci-ceva [ 8.046644] scsi host1: ahci-ceva [ 8.049986] ata1: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x100 irq 45 [ 8.057831] ata2: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x180 irq 45 [ 8.067149] iommu: Adding device fe200000.dwc3 to group 12 [ 8.072976] xilinx-psgtr fd400000.zynqmp_phy: Lane:2 type:0 protocol:3 pll_locked:yes [ 8.082976] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 8.088394] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1 [ 8.096147] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x22010010 [ 8.104790] xhci-hcd xhci-hcd.0.auto: irq 58, io mem 0xfe200000 [ 8.110784] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 8.117493] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 8.124700] usb usb1: Product: xHCI Host Controller [ 8.129554] usb usb1: Manufacturer: Linux 4.14.0 xhci-hcd [ 8.134935] usb usb1: SerialNumber: xhci-hcd.0.auto [ 8.140077] hub 1-0:1.0: USB hub found [ 8.143768] hub 1-0:1.0: 1 port detected [ 8.147833] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 8.153244] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2 [ 8.160921] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM. [ 8.169029] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003 [ 8.175739] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 8.182943] usb usb2: Product: xHCI Host Controller [ 8.187801] usb usb2: Manufacturer: Linux 4.14.0 xhci-hcd [ 8.193184] usb usb2: SerialNumber: xhci-hcd.0.auto [ 8.198277] hub 2-0:1.0: USB hub found [ 8.201963] hub 2-0:1.0: 1 port detected [ 8.206969] pca953x 0-0020: 0-0020 supply vcc not found, using dummy regulator [ 8.216864] pca953x 0-0020: interrupt support not compiled in [ 8.222622] pca953x 0-0021: 0-0021 supply vcc not found, using dummy regulator [ 8.232536] pca953x 0-0021: interrupt support not compiled in [ 8.239007] ina2xx 3-0040: power monitor ina226 (Rshunt = 5000 uOhm) [ 8.245710] ina2xx 3-0041: power monitor ina226 (Rshunt = 5000 uOhm) [ 8.252403] ina2xx 3-0042: power monitor ina226 (Rshunt = 5000 uOhm) [ 8.259106] ina2xx 3-0043: power monitor ina226 (Rshunt = 5000 uOhm) [ 8.265814] ina2xx 3-0044: power monitor ina226 (Rshunt = 5000 uOhm) [ 8.272508] ina2xx 3-0045: power monitor ina226 (Rshunt = 5000 uOhm) [ 8.279208] ina2xx 3-0046: power monitor ina226 (Rshunt = 5000 uOhm) [ 8.285903] ina2xx 3-0047: power monitor ina226 (Rshunt = 5000 uOhm) [ 8.292599] ina2xx 3-004a: power monitor ina226 (Rshunt = 5000 uOhm) [ 8.299299] ina2xx 3-004b: power monitor ina226 (Rshunt = 5000 uOhm) [ 8.305607] i2c i2c-0: Added multiplexed i2c bus 3 [ 8.310961] ina2xx 4-0040: power monitor ina226 (Rshunt = 2000 uOhm) [ 8.317667] ina2xx 4-0041: power monitor ina226 (Rshunt = 5000 uOhm) [ 8.324367] ina2xx 4-0042: power monitor ina226 (Rshunt = 5000 uOhm) [ 8.331064] ina2xx 4-0043: power monitor ina226 (Rshunt = 5000 uOhm) [ 8.337764] ina2xx 4-0044: power monitor ina226 (Rshunt = 5000 uOhm) [ 8.344467] ina2xx 4-0045: power monitor ina226 (Rshunt = 5000 uOhm) [ 8.351163] ina2xx 4-0046: power monitor ina226 (Rshunt = 5000 uOhm) [ 8.357863] ina2xx 4-0047: power monitor ina226 (Rshunt = 5000 uOhm) [ 8.364166] i2c i2c-0: Added multiplexed i2c bus 4 [ 8.378795] ata1: SATA link down (SStatus 0 SControl 330) [ 8.384147] ata2: SATA link down (SStatus 0 SControl 330) [ 8.410334] i2c i2c-0: Added multiplexed i2c bus 5 [ 8.415167] i2c i2c-0: Added multiplexed i2c bus 6 [ 8.419881] pca954x 0-0075: registered 4 multiplexed busses for I2C mux pca9544 [ 8.427197] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 33 [ 8.434775] at24 7-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write [ 8.441428] i2c i2c-1: Added multiplexed i2c bus 7 [ 8.446358] i2c i2c-1: Added multiplexed i2c bus 8 [ 8.453092] si570 9-005d: registered, current frequency 300000000 Hz [ 8.459395] i2c i2c-1: Added multiplexed i2c bus 9 [ 8.478069] si570 10-005d: registered, current frequency 148500000 Hz [ 8.484458] i2c i2c-1: Added multiplexed i2c bus 10 [ 8.489479] i2c i2c-1: Added multiplexed i2c bus 11 [ 8.494398] i2c i2c-1: Added multiplexed i2c bus 12 [ 8.499313] i2c i2c-1: Added multiplexed i2c bus 13 [ 8.504223] i2c i2c-1: Added multiplexed i2c bus 14 [ 8.509023] pca954x 1-0074: registered 8 multiplexed busses for I2C switch pca9548 [ 8.517279] at24 15-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write [ 8.523928] i2c i2c-1: Added multiplexed i2c bus 15 [ 8.528887] i2c i2c-1: Added multiplexed i2c bus 16 [ 8.533806] i2c i2c-1: Added multiplexed i2c bus 17 [ 8.539045] i2c i2c-1: Added multiplexed i2c bus 18 [ 8.543964] i2c i2c-1: Added multiplexed i2c bus 19 [ 8.548885] i2c i2c-1: Added multiplexed i2c bus 20 [ 8.553807] i2c i2c-1: Added multiplexed i2c bus 21 [ 8.558734] i2c i2c-1: Added multiplexed i2c bus 22 [ 8.563531] pca954x 1-0075: registered 8 multiplexed busses for I2C switch pca9548 [ 8.571104] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 34 [ 8.577595] ad9361 spi1.0: ad9361_probe : enter (ad9361) [ 8.583712] ad9361 spi1.0: No GPIOs defined for ext band ctrl [ 8.805018] ad9361 spi1.0: ad9361_probe : AD936x Rev 2 successfully initialized [ 9.131977] [drm] Cannot find any crtc or sizes [ 9.647489] input: gpio-keys as /devices/platform/gpio-keys/input/input0 [ 9.711605] rtc_zynqmp ffa60000.rtc: setting system clock to 2018-10-16 13:47:55 UTC (1539697675) [ 9.720396] of_cfs_init [ 9.722838] of_cfs_init: OK [ 9.725729] clk: Not disabling unused clocks [ 9.729952] ALSA device list: [ 9.732865] #0: DisplayPort monitor [ 9.736968] Freeing unused kernel memory: 512K INIT: version 2.88 booting Starting udev [ 9.846684] udevd[1912]: starting version 3.2.2 [ 9.855924] udevd[1913]: starting eudev-3.2.2 [ 12.532622] EXT4-fs (mmcblk0p2): recovery complete [ 12.537349] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 12.652668] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck. Starting internet superserver: inetd. Configuring packages on first boot.... (This may take several minutes. Please do not power off the machine.) Running postinst /etc/rpm-postinsts/100-sysvinit-inittab... update-rc.d: /etc/init.d/run-postinsts exists during rc.d purge (continuing) INIT: Entering runlevel: 5 Configuring network interfaces... [ 13.082712] pps pps0: new PPS source ptp0 [ 13.086667] macb ff0e0000.ethernet: gem-ptp-timer ptp clock registered. [ 13.093350] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready RTNETLINK answers: Network is unreachable Starting system message bus: dbus. Starting Dropbear SSH server: Generating key, this may take a while... Public key portion is: ssh-rsa AAAAB3NzaC1yc2EAAAADAQABAAABAQC+H/cTU5nRBiBc3mBBAi3ukNKY+r5Ub9vfG/eXBQkFectTJpOID5vhklWfoR4Hj11E7Hc7/YrLMcc5NglXWF0wKnbPe69hNd0ZICJIDGJIyQeBKYBXnGJzchEg6cCII0+nlquSrz/l2rqH8iXzJY/DntJklu51e2I5A2fx9DH0YIUnJ/QfXqycP/hAsF1Iit05Goa6odTdmcIUuJUCXKQBsai53fyj5N+M3SofYOyO2tWweYDkDZ1ZHrUqTb1BpJi/Mhc7v8Ca5Q9HrLQebO3g+U43MfPbbSwrPpp/pXrJNC5Q0dHCzKw/d3rrmhr5Jpl/baUVDd1ihT5DznEHomFh root@lnx_ad9361 Fingerprint: md5 6a:de:11:4b:b4:37:d3:7a:ea:26:0a:cb:aa:86:f1:24 dropbear. Starting syslogd/klogd: done * Starting Avahi mDNS/DNS-SD Daemon: avahi-daemon [ ok ] * Starting Avahi Unicast DNS Configuration Daemon: avahi-dnsconfd [ ok ] Starting tcf-agent: OK PetaLinux 2018.2 lnx_ad9361 /dev/ttyPS0 lnx_ad9361 login: root Password: root@lnx_ad9361:~# root@lnx_ad9361:~# root@lnx_ad9361:~# root@lnx_ad9361:~# dmesg | grep ad9361 [ 4.931409] ad9361 spi1.0: ad9361_probe : enter (ad9361) [ 8.577595] ad9361 spi1.0: ad9361_probe : enter (ad9361) [ 8.583712] ad9361 spi1.0: No GPIOs defined for ext band ctrl [ 8.805018] ad9361 spi1.0: ad9361_probe : AD936x Rev 2 successfully initialized root@lnx_ad9361:~# ls /sys/bus/i i2c/ iio/ root@lnx_ad9361:~# ls /sys/bus/iio/devices/ iio:device0 iio:device1 root@lnx_ad9361:~# root@lnx_ad9361:~# root@lnx_ad9361:~# cd /sys/bus/iio//devices/iio:device1 root@lnx_ad9361:/sys/bus/iio/devices/iio:device1# ls calib_mode calib_mode_available dcxo_tune_coarse dcxo_tune_coarse_available dcxo_tune_fine dcxo_tune_fine_available dev ensm_mode ensm_mode_available filter_fir_config gain_table_config in_out_voltage_filter_fir_en in_temp0_input in_voltage0_gain_control_mode in_voltage0_hardwaregain in_voltage0_hardwaregain_available in_voltage0_rf_port_select in_voltage0_rssi in_voltage2_offset in_voltage2_raw in_voltage2_scale in_voltage_bb_dc_offset_tracking_en in_voltage_filter_fir_en in_voltage_gain_control_mode_available in_voltage_quadrature_tracking_en in_voltage_rf_bandwidth in_voltage_rf_bandwidth_available in_voltage_rf_dc_offset_tracking_en in_voltage_rf_port_select_available in_voltage_sampling_frequency in_voltage_sampling_frequency_available multichip_sync name of_node out_altvoltage0_RX_LO_external out_altvoltage0_RX_LO_fastlock_load out_altvoltage0_RX_LO_fastlock_recall out_altvoltage0_RX_LO_fastlock_save out_altvoltage0_RX_LO_fastlock_store out_altvoltage0_RX_LO_frequency out_altvoltage0_RX_LO_frequency_available out_altvoltage0_RX_LO_powerdown out_altvoltage1_TX_LO_external out_altvoltage1_TX_LO_fastlock_load out_altvoltage1_TX_LO_fastlock_recall out_altvoltage1_TX_LO_fastlock_save out_altvoltage1_TX_LO_fastlock_store out_altvoltage1_TX_LO_frequency out_altvoltage1_TX_LO_frequency_available out_altvoltage1_TX_LO_powerdown out_voltage0_hardwaregain out_voltage0_hardwaregain_available out_voltage0_rf_port_select out_voltage0_rssi out_voltage2_raw out_voltage2_scale out_voltage3_raw out_voltage3_scale out_voltage_filter_fir_en out_voltage_rf_bandwidth out_voltage_rf_bandwidth_available out_voltage_rf_port_select_available out_voltage_sampling_frequency out_voltage_sampling_frequency_available power rssi_gain_step_error rx_path_rates subsystem trx_rate_governor trx_rate_governor_available tx_path_rates uevent xo_correction xo_correction_available root@lnx_ad9361:/sys/bus/iio/devices/iio:device1# cat name ad9361-phy root@lnx_ad9361:/sys/bus/iio/devices/iio:device1# root@lnx_ad9361:/sys/bus/iio/devices/iio:device1# root@lnx_ad9361:/sys/bus/iio/devices/iio:device1# root@lnx_ad9361:/sys/bus/iio/devices/iio:device1# root@lnx_ad9361:/sys/bus/iio/devices/iio:device1#
In addition the drivers need to be enabled in your kernel config:
CONFIG_AXI_DMAC=y
CONFIG_AD9361=y
CONFIG_CF_AXI_ADC=y
CONFIG_CF_AXI_DDS=y
I am sharing my work observation and need your comment, I guess am making progress but still things are not working as per expectation.
I have enabled the drivers in petalinux project, following is the output of user kernel config file:
CONFIG_IIO_BUFFER_DMA=yCONFIG_IIO_BUFFER_DMAENGINE=yCONFIG_IIO_HW_CONSUMER=yCONFIG_CF_AXI_ADC=yCONFIG_AD9361=y# CONFIG_AD9361_EXT_BAND_CONTROL is not setCONFIG_CF_AXI_DDS=y# CONFIG_CF_AXI_DDS_AD9122 is not set# CONFIG_CF_AXI_DDS_AD9144 is not set# CONFIG_CF_AXI_DDS_AD9162 is not set# CONFIG_CF_AXI_DDS_AD9739A is not setCONFIG_JESD204=y# CONFIG_ALTERA_ARRIA10_JESD204_PHY is not set# CONFIG_AXI_ADXCVR is not set# CONFIG_AXI_JESD204B is not set# CONFIG_AXI_JESD204_TX is not set# CONFIG_AXI_JESD204_RX is not setCONFIG_DYNAMIC_DEBUG=y
This gives me confidence that driver is selected so next doubt is device-tree, but the device tree which is generated by Petalinux is now working with the kernel you shared here,
In boot-log message I can see :
AD9361 successfully initialized,
cf-ad9361-dds-core-lpc and cf-ad9361-lpc both are mapped and probed.
This gave me confidence that Device-Tree is okay. Now, I am not sure where to troubleshoot the issue, since my observation put me in chaos
Kindly share some hints/suggestions which would help me to come out this debugging loop.
Can you do a ls in:
/sys/bus/platform/drivers
/sys/bus/platform/devices
/sys/bus/spi/drivers
/sys/bus/spi/devices
Thanks Michael, Kudos!
Finally it worked :) , Your suggestions indeed was very helpful.
CONFIG_AXI_DMAC was not selected.
My Next Objective is to use this Linux with IIO-Scope, How can I integrate the LIB-IIO framework with my custom Linux? As per my study I have to cross-compile the Lib-IIO library and add it in my Linux, am I thinking right?
Again, Thanks a lot.
One way is to clone and cross compile it, however Libiio is Available as: