AD9517 Linux Driver libiio

Hi,

I would like to configure several Options of the AD9517 using Linux/libiio. As far as I see the libiio driver only allows enabling/disabling the outputs and setting the output frequency. All other functions of the ad9517 driver are not accessible via libiio (or am I missing something?). I could set the device settings using direct register access, which works fine but it seems to be an ugly solution to me. So how is this driver meant to be included and accessed from a libiio based software?

Best

Oliver

Parents Reply Children