Hi,
Background:-
1. I brought up four slots design on custom board with changes to original zcu102.
2. I made necessary changes in the linux device tree and all the 12 iio devices are detected.
slot 0 => ad9361-phy[ad9361 rfic] + cf-ad9361-dds-core-lpc [Tx DMA] + cf-ad9361-lpc [Rx DMA].
slot 1 => ad9361-phy0[ad9361 rfic] + cf-ad9361-dds-core-lpc0 [Tx DMA] + cf-ad9361-lpc0 [Rx DMA]
slot 2 => ad9361-phy1[ad9361 rfic] + cf-ad9361-dds-core-lpc1 [Tx DMA] + cf-ad9361-lpc1 [Rx DMA]
slot 3 => ad9361-phy2[ad9361 rfic] + cf-ad9361-dds-core-lpc2 [Tx DMA] + cf-ad9361-lpc2 [Rx DMA]
3. I am using libiio way of configuring txwaveform, txfreq, rxfreq and bandwidth and other settings.
4. I have ensured that the when i run commands for setting bw+fir and sending waveform it is ONLY affecting its related iio:device<x> attributes not the other slot's.
say slot 0 affects only attributes of ad9361-phy[ad9361 rfic] + cf-ad9361-dds-core-lpc [Tx DMA] + cf-ad9361-lpc [Rx DMA] and nothing else.
5. in vivado design, i ensured that everyblock has its own clkdiv feed by its own axi_ad9361 lclk and its own set of tx paths like dac_dma, dac_upack and dac_fifo. same with receive path
no slot path shares any clocks/signals with other slot path [block diagram system.pdf attached1].
in other words, each path is different from others and it is independent.
6. all of the slots are detected as individual MASTERS [something like this]
[ 6.563475] cf_axi_dds 99024000.cf-ad9361-dds-core-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.00.b) at 0x99024000 mapped to 0xffffff8008e8e000, probed DDS AD9361
[ 6.618076] cf_axi_dds 99d24000.cf-ad9361-dds-core-lpc0: Analog Devices CF_AXI_DDS_DDS MASTER (9.00.b) at 0x99D24000 mapped to 0xffffff8008eaa000, probed DDS AD9361
7. when i run txdma using libiio on each slot individuall they work perfectly [no issues there].
Problem/issue: -
8. when i keep one slot tx path running [say 15mhz] and other tx path running [5mhz], i see issue that 5mhz path is influencing 15mhz path signal. i see the 15mhz signal is corrupted, surprisingly 5mhz signal looks clean. same is affect with other bandwidths, however the affect is different, split constellation. so it is not isolated to 15mhz and 5mhz combination.
This happens irrespective of which path dma i start first. order does not matter.
9. i looked into DMAC channel registers to this [Base (common to all cores) [Analog Devices Wiki] ]
and [High-Speed DMA Controller Peripheral [Analog Devices Wiki] ]
15mhz path has the following
9c420414 0x7C100000 [start address]
9c420418 0x00383FFF [length]
5mhz path has the following
99d40414 0x7CD00000 [start address]
99d40418 0x0012BFFF [length]
i also ensured that start address <= CURRENT_SRC_ADDRESS [AXI DMAC 0x438] < start address + length
in other words, DMA buffer wise, they are way apart and they conform to multiple of 4k bytes alignment.
10. i put ILA and traced back to DMAC output of 64 bits and here is what i see. Here i am generating a pure sinusoidal signal on 15mhz path [slot 0] and a typical lte signal on 5mhz path [slot 1].
As you can see the waveform is clean if i just run the slot0 tx dma alone. [BEFORE case in pic] -> working case
if slot0 tx dma is run along with 5mhz signal, you can see the gaps [AFTER case in pic] -> non working case
few notes: -
1. However signal is contiguous even with that gap, say iq sample before that idle period and after that idle period are contiguous.

few questions:
1. to operate each path as its own MASTER, is there anything need to be done specifically in dts. [i have attached final output dts].
2. does core_ID of each instance of AXI_DMAC has to be different. does that matter to linux?
3. what can cause the DMAC to pause for few clock cycles and resume back?
4.what is the effect of core_ID [i read from these posts]
https://wiki.analog.com/resources/fpga/docs/axi_ad9361
"ID Core ID should be unique for each AD9361 IP in the system 0"
IDLE CASE ILA waveforms: -
Working case 15mhz

non working 15mhz:-


dts:-
bd: -
Thanks
Edit Notes
added dts this time[edited by: ENGINEER at 6:14 PM (GMT -4) on 28 Aug 2018]