Configuring AD9364 using ADSP-BF537 using NO-OS drivers

I want to configure AD9364 using ADSP-BF537 using NO-OS drivers. Is it recommended to use any specific processor for AD9364. Does someone faced any issue while configuring AD9364 using ADSP-537.

Does someone have experience of configuring AD9364 using cypress PSoC 4.

Thanks

Parents
  • 0
    •  Analog Employees 
    on Jun 14, 2016 9:03 AM

    Hi,

    The No-OS drivers are host system independent and should work fine on any system as long as a C compiler is available. We test our designs on the Xilinx Zynq with the ADI HDL reference designs. When you want to use a custom SoC you have to define a small hardware-abstraction-layer that implements functions like SPI bus access etc to be able to use the AD9361/AD9364 No-OS drivers.

    - Lars

Reply
  • 0
    •  Analog Employees 
    on Jun 14, 2016 9:03 AM

    Hi,

    The No-OS drivers are host system independent and should work fine on any system as long as a C compiler is available. We test our designs on the Xilinx Zynq with the ADI HDL reference designs. When you want to use a custom SoC you have to define a small hardware-abstraction-layer that implements functions like SPI bus access etc to be able to use the AD9361/AD9364 No-OS drivers.

    - Lars

Children
No Data