LNA enabling in picozed+LNA_PA module

We integrated picozed with AD_PZSDR2400TDD-EBZ, When we enable the channel 2 LNA we are not getting the enable control on the test port of the RF card.

We set the GPIO direction and ON control for the GPO signals in parameters.h

GPIO_CTL0_PIN =0

GPIO_CTL1_PIN =1

GPIO_CTL2_PIN =1

GPIO_CTL3_PIN =0

Please help us to enable LNA

Thank you



The following commands have been added in NO OS Driver main.c For disabling LNA: gpio_direction(94, 1); gpio_set_value(94, 0); gpio_direction(95, 1); gpio_set_value(95, 0); For selecting TX/Rx mode : gpio_direction(97, 1); gpio_set_value(97, 0); Please check the above commands whether it is correct or not.
[edited by: pratibha at 5:12 AM (GMT 0) on 22 Jul 2019]