ADRV9371 & ZC706 Building NO-OS project

Hi I am trying to run ADRV9371 with ZC706
Following the guide: analog-staging.dw1.cosmocode.de/.../no-os-setup

1. Downloaded github.com/.../hdl HW design, built under Vivado 2018.3,
2. Built fine, produced .hdf
3. Downloaded: github.com/.../no-OS master branch
4. Downloaded: www.analog.com/.../transceiver-evaluation-software.html, mykonos_api_source_1.5.2.3566
5. SDK 2018.3, opened new project, picture 1
6. Copied no-OS-master\ad9371\sw into my \src , picture 2
7. Copied ad9528 and mykonos folder to the src folder of my project, picture3
8. Upon build I got, fatal error: io.h: No such file or directory platform_drivers.h /6ADI/src/platform_altera line 45 C/C++ Problem

Q.
1. Could not run MATLAB Profile Generator yet, is it essential? I dont have the necessary version of MATLAB for now, I can use any frequency and any setting for the beginning, any .c, .h, welcome
For now I just need to see setup transmiting & receiving.

2. Is there a just ready-to-use, ready-to-modify project, I followed the guide and ended up error,
I also tried no-OS-master\projects\ad9371\src, included paths, ended up with other inclusion errors, those leading infinite errors upon solving one.

  • 0
    •  Analog Employees 
    on Jul 9, 2019 11:13 AM
    Could not run MATLAB Profile Generator yet, is it essential? I dont have the necessary version of MATLAB for now, I can use any frequency and any setting for the beginning, any .c, .h, welcome
    For now I just need to see setup transmiting & receiving.

    You can use the standard profiles available in TES GUI to generate the init 'c' files. Please refer to UG-992 for more details.

    Moving to No-Os space for more comments.

  • 0
    •  Analog Employees 
    on Jul 18, 2019 7:40 AM

    Hello,

    Apologies for the late response.

    It seems the problem comes from including the 'platform_altera' folder, but if you are using ZC706 you should not include that folder at all.

    Try deleting it from the project and leave only the 'platform_xilinx' folder. Let us know if you have any more problems.

    Regards,

    Andrei.