adrv9371x on kcu105 giving 0x20 RxFramerStatus and OrxFramerStatus with no-OS

Hello,

I've been using the Linux drivers on the KCU105 with adrv9371x evaluation board and all has been working well with the 2018_R2 branches of both the hdl and linux branches. Linux fully boots and all drivers probe and I can run IIO Oscope and config and radio and get IQ samples.

I recently switched to the no-OS code and mykonos API driver v3566, and when I use this and just run headless.c (as described at https://wiki.analog.com/resources/eval/user-guides/mykonos/no-os-setup) I consistently get the following.

Please wait...
RX_XCVR (GTH3) initialization OK
TX_XCVR (GTH3) initialization OK
RX_OS_XCVR (GTH3) initialization OK
MCS successful
CLKPLL locked
AD9371 ARM version 5.1.1
PLLs locked
Calibrations completed successfully
RxFramerStatus = 0x20
OrxFramerStatus = 0x20
dac_setup dac core initialized (245 MHz).
adc_setup adc core initialized (123 MHz).
Done

Can someone please check this? I'm now needing to remove the Microblaze, DDR, etc from my design and am going to leverage the no-OS code to setup/config the radio over PCIe, but I'd like to begin at a good starting point.

Thanks,

Nick