JESD204B Rx-link status is always "CGS"

Hello, everyone!

I am working with zc706 and ADRV9009 evaluation boards using the master no-os software.

I have encountered this problem:

    Using the TES to create the init .c files, then repace the talise_config.c in no-os project. Compile and run,the rx and os JESD204B status is "CGS", not "DATA".

I am stuck for long times about this problem, could you help me resolve this problem.

Please see my configuration:

AD9528:

ADRV9009:

JESD204B:

Receive data with 2100MHz signal applied on RX1:

All works OK!

Then i use "TOOLS->create init.c files" to create the init files,  replace the orignal No-os talise_config.c with the one created by TES. Also the talise_stream_binary.h has been correctly changed too. the result is:

the rx and os JESD204B status is "CGS".

But if  i do nothing changed with the orignal No-os source files,the result is:

the rx and os JESD204B status is "DATA".

 

Please see the code.

headless.c:

/**
 * \file headless.c
 *
 * \brief Contains example code for user integration with their application
 *
 * Copyright 2015-2017 Analog Devices Inc.
 * Released under the AD9378-AD9379 API license, for more information see the "LICENSE.txt" file in this zip file.
 *
 */

#include "talise.h"
#include "talise_jesd204.h"
#include "talise_arm.h"
#include "talise_radioctrl.h"
#include "talise_cals.h"

#include "talise_config.h"
#include "talise_error.h"
/****< Insert User Includes Here >***/

#include <stdio.h>
#include "adi_hal.h"
#include "platform_drivers.h"
#include "parameters.h"
#include "util.h"
#include "ad9528.h"
#ifdef ALTERA_PLATFORM
#include "clk_altera_a10_fpll.h"
#include "altera_adxcvr.h"
#else
#include "clk_axi_clkgen.h"
#include "axi_adxcvr.h"
#endif
#include "axi_jesd204_rx.h"
#include "axi_jesd204_tx.h"
#include "axi_dac_core.h"
#include "axi_adc_core.h"
#include "axi_dmac.h"

#include "talise_config_ad9528.h"
#include "talise_arm_binary.h"
#include "talise_stream_binary.h"

/**********************************************************/
/**********************************************************/
/********** Talise Data Structure Initializations ********/
/**********************************************************/
/**********************************************************/

int main(void)
{
	adiHalErr_t ad9528Error;
	ad9528Device_t clockAD9528_ = {
		NULL,
		NULL,
		NULL,
		&clockSpiSettings,
		&clockPll1Settings,
		&clockPll2Settings,
		&clockOutputSettings,
		&clockSysrefSettings
	};
	ad9528Device_t *clockAD9528_device = &clockAD9528_;
#ifdef ALTERA_PLATFORM
	struct altera_a10_fpll_init rx_device_clk_pll_init = {
		"rx_device_clk_pll",
		RX_A10_FPLL_BASEADDR,
		clockAD9528_device->outputSettings->outFrequency_Hz[1]
	};
	struct altera_a10_fpll_init tx_device_clk_pll_init = {
		"tx_device_clk_pll",
		TX_A10_FPLL_BASEADDR,
		clockAD9528_device->outputSettings->outFrequency_Hz[1]
	};
	struct altera_a10_fpll_init rx_os_device_clk_pll_init = {
		"rx_os_device_clk_pll",
		RX_OS_A10_FPLL_BASEADDR,
		clockAD9528_device->outputSettings->outFrequency_Hz[1]
	};
	struct altera_a10_fpll *rx_device_clk_pll;
	struct altera_a10_fpll *tx_device_clk_pll;
	struct altera_a10_fpll *rx_os_device_clk_pll;
#else
	struct axi_clkgen_init rx_clkgen_init = {
		"rx_clkgen",
		RX_CLKGEN_BASEADDR,
		clockAD9528_device->outputSettings->outFrequency_Hz[1]
	};
	struct axi_clkgen_init tx_clkgen_init = {
		"tx_clkgen",
		TX_CLKGEN_BASEADDR,
		clockAD9528_device->outputSettings->outFrequency_Hz[1]
	};
	struct axi_clkgen_init rx_os_clkgen_init = {
		"rx_os_clkgen",
		RX_OS_CLKGEN_BASEADDR,
		clockAD9528_device->outputSettings->outFrequency_Hz[1]
	};
	struct axi_clkgen *rx_clkgen;
	struct axi_clkgen *tx_clkgen;
	struct axi_clkgen *rx_os_clkgen;
#endif
	uint32_t rx_lane_rate_khz = talInit.rx.rxProfile.rxOutputRate_kHz *
				    talInit.jesd204Settings.framerA.M * (20 /
						    hweight8(talInit.jesd204Settings.framerA.serializerLanesEnabled));
	uint32_t rx_div40_rate_hz = rx_lane_rate_khz * (1000 / 40);
	uint32_t tx_lane_rate_khz = talInit.tx.txProfile.txInputRate_kHz *
				    talInit.jesd204Settings.deframerA.M * (20 /
						    hweight8(talInit.jesd204Settings.deframerA.deserializerLanesEnabled));
	uint32_t tx_div40_rate_hz = tx_lane_rate_khz * (1000 / 40);
	uint32_t rx_os_lane_rate_khz = talInit.obsRx.orxProfile.orxOutputRate_kHz *
				       talInit.jesd204Settings.framerB.M * (20 /
						       hweight8(talInit.jesd204Settings.framerB.serializerLanesEnabled));
	uint32_t rx_os_div40_rate_hz = rx_os_lane_rate_khz * (1000 / 40);
	struct jesd204_rx_init rx_jesd_init = {
		"rx_jesd",
		RX_JESD_BASEADDR,
		4,
		32,
		1,
		rx_div40_rate_hz / 1000,
		rx_lane_rate_khz,
	};
	struct jesd204_tx_init tx_jesd_init = {
		"tx_jesd",
		TX_JESD_BASEADDR,
		2,
		32,
		4,
		14,
		16,
		true,
		2,
		1,
		tx_div40_rate_hz / 1000,
		tx_lane_rate_khz,
	};

	struct jesd204_rx_init rx_os_jesd_init = {
		"rx_os_jesd",
		RX_OS_JESD_BASEADDR,
		2,
		32,
		1,
		rx_os_div40_rate_hz / 1000,
		rx_os_lane_rate_khz,
	};
	struct axi_jesd204_rx *rx_jesd;
	struct axi_jesd204_tx *tx_jesd;
	struct axi_jesd204_rx *rx_os_jesd;
#ifdef ALTERA_PLATFORM
	struct adxcvr_init rx_adxcvr_init = {
		"rx_adxcvr",
		RX_XCVR_BASEADDR,
		{RX_ADXCFG_0_BASEADDR, RX_ADXCFG_1_BASEADDR, 0, 0},
		0,
		rx_lane_rate_khz,
		talInit.clocks.deviceClock_kHz,
	};
	struct adxcvr_init tx_adxcvr_init = {
		"tx_adxcvr",
		TX_XCVR_BASEADDR,
		{TX_ADXCFG_0_BASEADDR, TX_ADXCFG_1_BASEADDR, TX_ADXCFG_2_BASEADDR, TX_ADXCFG_3_BASEADDR},
		TX_PLL_BASEADDR,
		tx_lane_rate_khz,
		talInit.clocks.deviceClock_kHz,
	};
	struct adxcvr_init rx_os_adxcvr_init = {
		"rx_os_adxcvr",
		RX_OS_XCVR_BASEADDR,
		{RX_OS_ADXCFG_0_BASEADDR, RX_OS_ADXCFG_1_BASEADDR, 0, 0},
		0,
		rx_os_lane_rate_khz,
		talInit.clocks.deviceClock_kHz,
	};
#else
	struct adxcvr_init rx_adxcvr_init = {
		"rx_adxcvr",
		RX_XCVR_BASEADDR,
		0,
		3,
		1,
		1,
		rx_lane_rate_khz,
		talInit.clocks.deviceClock_kHz,
	};
	struct adxcvr_init tx_adxcvr_init = {
		"tx_adxcvr",
		TX_XCVR_BASEADDR,
		3,
		3,
		0,
		0,
		tx_lane_rate_khz,
		talInit.clocks.deviceClock_kHz,
	};
	struct adxcvr_init rx_os_adxcvr_init = {
		"rx_os_adxcvr",
		RX_OS_XCVR_BASEADDR,
		0,
		3,
		1,
		1,
		rx_os_lane_rate_khz,
		talInit.clocks.deviceClock_kHz,
	};
#endif
	struct adxcvr *rx_adxcvr;
	struct adxcvr *tx_adxcvr;
	struct adxcvr *rx_os_adxcvr;
	struct axi_adc_init rx_adc_init = {
		"rx_adc",
		RX_CORE_BASEADDR,
		4,
	};
	struct axi_adc *rx_adc;
	struct axi_dac_init tx_dac_init = {
		"rx_dac",
		TX_CORE_BASEADDR,
		4,
	};
	struct axi_dac *tx_dac;
	struct axi_dmac_init rx_dmac_init = {
		"rx_dmac",
		RX_DMA_BASEADDR,
		DMA_DEV_TO_MEM,
		0,
	};
	struct axi_dmac *rx_dmac;
	struct adi_hal hal;
	taliseDevice_t talDev = {
		.devHalInfo = &hal,
		.devStateInfo = {0}
	};
	uint32_t talAction = TALACT_NO_ACTION;
	uint8_t errorFlag = 0;
	uint8_t mcsStatus = 0;
	uint8_t pllLockStatus = 0;
	uint16_t deframerStatus = 0;
	uint8_t framerStatus = 0;
	uint32_t count = sizeof(armBinary);
	taliseArmVersionInfo_t talArmVersionInfo;
	uint32_t initCalMask =  TAL_TX_BB_FILTER | TAL_ADC_TUNER | TAL_TIA_3DB_CORNER
				| TAL_DC_OFFSET | TAL_TX_ATTENUATION_DELAY | TAL_RX_GAIN_DELAY | TAL_FLASH_CAL |
				TAL_PATH_DELAY | TAL_TX_LO_LEAKAGE_INTERNAL | TAL_TX_QEC_INIT |
				TAL_LOOPBACK_RX_LO_DELAY | TAL_LOOPBACK_RX_RX_QEC_INIT |
				TAL_RX_LO_DELAY | TAL_RX_QEC_INIT;
	uint32_t trackingCalMask =  TAL_TRACK_RX1_QEC |
				    TAL_TRACK_RX2_QEC |
				    TAL_TRACK_TX1_QEC |
				    TAL_TRACK_TX2_QEC;

	uint32_t api_vers[4];
	uint8_t rev;
	int32_t status;

	printf("Hello\n");

	/**********************************************************/
	/**********************************************************/
	/************ Talise Initialization Sequence *************/
	/**********************************************************/
	/**********************************************************/

	/** < Insert User System Clock(s) Initialization Code Here >
	 * System Clock should provide a device clock and SYSREF signal
	 * to the Talise device.
	 **/

	/* Init the AD9528 data structure */
	ad9528Error = AD9528_initDeviceDataStruct(clockAD9528_device,
			clockAD9528_device->pll1Settings->vcxo_Frequency_Hz,
			clockAD9528_device->pll1Settings->refA_Frequency_Hz,
			clockAD9528_device->outputSettings->outFrequency_Hz[1]);
	if (ad9528Error != ADIHAL_OK) {
		printf("error: AD9528_initDeviceDataStruct() failed\n");
		goto error_0;
	}

	/* Perform a hard reset on the AD9528 DUT */
	ad9528Error = AD9528_resetDevice(clockAD9528_device);
	if (ad9528Error != ADIHAL_OK) {
		printf("error: AD9528_resetDevice() failed\n");
		goto error_1;
	}

	/* Initialize the AD9528 by writing all SPI registers */
	ad9528Error = AD9528_initialize(clockAD9528_device);
	if (ad9528Error == ADIHAL_ERR) {
		printf("error: AD9528_initialize() failed\n");
		goto error_1;
	}

	if (ad9528Error == ADIHAL_WARNING)
		printf("warning: AD9528_initialize() issues. "
		       "Possible cause: REF_CLK not connected\n");

#ifdef ALTERA_PLATFORM
	/* Initialize A10 FPLLs */
	status = altera_a10_fpll_init(&rx_device_clk_pll,
				      &rx_device_clk_pll_init);
	if (status != SUCCESS) {
		printf("error: %s: altera_a10_fpll_init() failed\n",
		       rx_os_device_clk_pll_init.name);
		goto error_1;
	}
	status = altera_a10_fpll_init(&tx_device_clk_pll,
				      &tx_device_clk_pll_init);
	if (status != SUCCESS) {
		printf("error: %s: altera_a10_fpll_init() failed\n",
		       rx_os_device_clk_pll_init.name);
		goto error_2;
	}
	status = altera_a10_fpll_init(&rx_os_device_clk_pll,
				      &rx_os_device_clk_pll_init);
	if (status != SUCCESS) {
		printf("error: %s: altera_a10_fpll_init() failed\n",
		       rx_os_device_clk_pll_init.name);
		goto error_3;
	}

	altera_a10_fpll_disable(rx_device_clk_pll);
	status = altera_a10_fpll_set_rate(rx_device_clk_pll,
					  rx_div40_rate_hz);
	if (status != SUCCESS) {
		printf("error: %s: altera_a10_fpll_set_rate() failed\n",
		       rx_device_clk_pll->name);
		goto error_4;
	}
	altera_a10_fpll_enable(rx_device_clk_pll);
	altera_a10_fpll_disable(tx_device_clk_pll);
	status = altera_a10_fpll_set_rate(tx_device_clk_pll,
					  tx_div40_rate_hz);
	if (status != SUCCESS) {
		printf("error: %s: altera_a10_fpll_set_rate() failed\n",
		       tx_device_clk_pll->name);
		goto error_4;
	}
	altera_a10_fpll_enable(tx_device_clk_pll);
	altera_a10_fpll_disable(rx_os_device_clk_pll);
	status = altera_a10_fpll_set_rate(rx_os_device_clk_pll,
					  rx_os_div40_rate_hz);
	if (status != SUCCESS) {
		printf("error: %s: altera_a10_fpll_set_rate() failed\n",
		       rx_os_device_clk_pll->name);
		goto error_4;
	}
	altera_a10_fpll_enable(rx_os_device_clk_pll);
#else
	/* Initialize CLKGEN */
	status = axi_clkgen_init(&rx_clkgen, &rx_clkgen_init);
	if (status != SUCCESS) {
		printf("error: %s: axi_clkgen_init() failed\n", rx_clkgen_init.name);
		goto error_1;
	}
	status = axi_clkgen_init(&tx_clkgen, &tx_clkgen_init);
	if (status != SUCCESS) {
		printf("error: %s: axi_clkgen_init() failed\n", tx_clkgen_init.name);
		goto error_2;
	}
	status = axi_clkgen_init(&rx_os_clkgen, &rx_os_clkgen_init);
	if (status != SUCCESS) {
		printf("error: %s: axi_clkgen_set_rate() failed\n", rx_os_clkgen_init.name);
		goto error_3;
	}

	status = axi_clkgen_set_rate(rx_clkgen, rx_div40_rate_hz);
	if (status != SUCCESS) {
		printf("error: %s: axi_clkgen_set_rate() failed\n", rx_clkgen->name);
		goto error_4;
	}
	status = axi_clkgen_set_rate(tx_clkgen, tx_div40_rate_hz);
	if (status != SUCCESS) {
		printf("error: %s: axi_clkgen_set_rate() failed\n", tx_clkgen->name);
		goto error_4;
	}
	status = axi_clkgen_set_rate(rx_os_clkgen, rx_os_div40_rate_hz);
	if (status != SUCCESS) {
		printf("error: %s: axi_clkgen_set_rate() failed\n", rx_os_clkgen->name);
		goto error_4;
	}
#endif

	/*** < Insert User BBIC JESD204B Initialization Code Here > ***/

	/* Initialize JESD */
	status = axi_jesd204_rx_init(&rx_jesd, &rx_jesd_init);
	if (status != SUCCESS) {
		printf("error: %s: axi_jesd204_rx_init() failed\n", rx_jesd_init.name);
		goto error_4;
	}
	status = axi_jesd204_tx_init(&tx_jesd, &tx_jesd_init);
	if (status != SUCCESS) {
		printf("error: %s: axi_jesd204_rx_init() failed\n", rx_jesd_init.name);
		goto error_5;
	}
	status = axi_jesd204_rx_init(&rx_os_jesd, &rx_os_jesd_init);
	if (status != SUCCESS) {
		printf("error: %s: axi_jesd204_rx_init() failed\n", rx_jesd_init.name);
		goto error_6;
	}

	/* Initialize ADXCR */
	status = adxcvr_init(&rx_adxcvr, &rx_adxcvr_init);
	if (status != SUCCESS) {
		printf("error: %s: adxcvr_init() failed\n", rx_adxcvr_init.name);
		goto error_7;
	}
	status = adxcvr_init(&tx_adxcvr, &tx_adxcvr_init);
	if (status != SUCCESS) {
		printf("error: %s: adxcvr_init() failed\n", tx_adxcvr_init.name);
		goto error_8;
	}
	status = adxcvr_init(&rx_os_adxcvr, &rx_os_adxcvr_init);
	if (status != SUCCESS) {
		printf("error: %s: adxcvr_init() failed\n", rx_os_adxcvr_init.name);
		goto error_9;
	}
#ifndef ALTERA_PLATFORM
	status = adxcvr_clk_enable(rx_adxcvr);
	if (status != SUCCESS) {
		printf("error: %s: adxcvr_clk_enable() failed\n", rx_adxcvr->name);
		goto error_10;
	}
	status = adxcvr_clk_enable(tx_adxcvr);
	if (status != SUCCESS) {
		printf("error: %s: adxcvr_clk_enable() failed\n", tx_adxcvr->name);
		goto error_10;
	}
	status = adxcvr_clk_enable(rx_os_adxcvr);
	if (status != SUCCESS) {
		printf("error: %s: adxcvr_clk_enable() failed\n", rx_os_adxcvr->name);
		goto error_10;
	}
#endif
	/*******************************/
	/**** Talise Initialization ***/
	/*******************************/

	/*Open Talise Hw Device*/
	talAction = TALISE_openHw(&talDev);
	if(talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
		printf("error: TALISE_openHw() failed\n");
		goto error_10;
	}

	/* Toggle RESETB pin on Talise device */
	talAction = TALISE_resetDevice(&talDev);
	if (talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
		printf("error: TALISE_resetDevice() failed\n");
		goto error_11;
	}

	mdelay(100);

	axi_jesd204_tx_lane_clk_enable(tx_jesd);

	/* TALISE_initialize() loads the Talise device data structure
	 * settings for the Rx/Tx/ORx profiles, FIR filters, digital
	 * filter enables, calibrates the CLKPLL, loads the user provided Rx
	 * gain tables, and configures the JESD204b serializers/framers/deserializers
	 * and deframers.
	 */
	talAction = TALISE_initialize(&talDev, &talInit);
	if (talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
		printf("error: TALISE_initialize() failed\n");
		goto error_11;
	}

	/*******************************/
	/***** CLKPLL Status Check *****/
	/*******************************/
	talAction = TALISE_getPllsLockStatus(&talDev, &pllLockStatus);
	if (talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
		printf("error: TALISE_getPllsLockStatus() failed\n");
		goto error_11;
	}

	/* Assert that Talise CLKPLL is locked */
	if ((pllLockStatus & 0x01) == 0) {
		/* <user code - CLKPLL not locked - ensure lock before proceeding */
		printf("error: CLKPLL not locked\n");
		goto error_11;
	}

	/*******************************************************/
	/**** Perform MultiChip Sync (MCS) on Talise Device ***/
	/*******************************************************/
	talAction = TALISE_enableMultichipSync(&talDev, 1, &mcsStatus);
	if (talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
		printf("error: TALISE_enableMultichipSync() failed\n");
		goto error_11;
	}

	/*< user code - Request minimum 3 SYSREF pulses from Clock Device - > */
	AD9528_sysrefReq(clockAD9528_device, SYSREF_PULSE);

	/*******************/
	/**** Verify MCS ***/
	/*******************/
	talAction = TALISE_enableMultichipSync(&talDev, 0, &mcsStatus);
	if ((mcsStatus & 0x0B) != 0x0B) {
		/*< user code - MCS failed - ensure MCS before proceeding*/
		printf("warning: TALISE_enableMultichipSync() failed\n");
	}

	/*******************************************************/
	/**** Prepare Talise Arm binary and Load Arm and	****/
	/**** Stream processor Binaryes 					****/
	/*******************************************************/
	if (pllLockStatus & 0x01) {
		talAction = TALISE_initArm(&talDev, &talInit);
		if (talAction != TALACT_NO_ACTION) {
			/*** < User: decide what to do based on Talise recovery action returned > ***/
			printf("error: TALISE_initArm() failed\n");
			goto error_11;
		}

		/*< user code- load Talise stream binary into streamBinary[4096] >*/
		/*< user code- load ARM binary byte array into armBinary[114688] >*/

		talAction = TALISE_loadStreamFromBinary(&talDev, &streamBinary[0]);
		if (talAction != TALACT_NO_ACTION) {
			/*** < User: decide what to do based on Talise recovery action returned > ***/
			printf("error: TALISE_loadStreamFromBinary() failed\n");
			goto error_11;
		}

		talAction = TALISE_loadArmFromBinary(&talDev, &armBinary[0], count);
		if (talAction != TALACT_NO_ACTION) {
			/*** < User: decide what to do based on Talise recovery action returned > ***/
			printf("error: TALISE_loadArmFromBinary() failed\n");
			goto error_11;
		}

		/* TALISE_verifyArmChecksum() will timeout after 200ms
		 * if ARM checksum is not computed
		 */
		talAction = TALISE_verifyArmChecksum(&talDev);
		if (talAction != TAL_ERR_OK) {
			/*< user code- ARM did not load properly - check armBinary & clock/profile settings >*/
			printf("error: TALISE_verifyArmChecksum() failed\n");
			goto error_11;
		}

	} else {
		/*< user code- check settings for proper CLKPLL lock  > ***/
		printf("error: CLKPLL not locked\n");
		goto error_11;
	}

	TALISE_getDeviceRev(&talDev, &rev);
	TALISE_getArmVersion_v2(&talDev, &talArmVersionInfo);
	TALISE_getApiVersion(&talDev,
			     &api_vers[0], &api_vers[1], &api_vers[2], &api_vers[3]);

	printf("talise: Device Revision %d, Firmware %u.%u.%u, API %u.%u.%u.%u\n",
	       rev, talArmVersionInfo.majorVer,
	       talArmVersionInfo.minorVer, talArmVersionInfo.rcVer,
	       api_vers[0], api_vers[1], api_vers[2], api_vers[3]);

	/*******************************/
	/**Set RF PLL LO Frequencies ***/
	/*******************************/
	talAction = TALISE_setRfPllFrequency(&talDev, TAL_RF_PLL, 2000000000);
	if (talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
		printf("error: TALISE_setRfPllFrequency() failed\n");
		goto error_11;
	}

	/*** < wait 200ms for PLLs to lock - user code here > ***/

	talAction = TALISE_getPllsLockStatus(&talDev, &pllLockStatus);
	if ((pllLockStatus & 0x07) != 0x07) {
		/*< user code - ensure lock of all PLLs before proceeding>*/
		printf("error: RFPLL not locked\n");
		goto error_11;
	}

	/****************************************************/
	/**** Run Talise ARM Initialization Calibrations ***/
	/****************************************************/
	talAction = TALISE_runInitCals(&talDev, initCalMask);
	if (talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
		printf("error: TALISE_runInitCals() failed\n");
		goto error_11;
	}

	talAction = TALISE_waitInitCals(&talDev, 20000, &errorFlag);
	if (talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
		printf("error: TALISE_waitInitCals() failed\n");
		goto error_11;
	}

	if (errorFlag) {
		/*< user code - Check error flag to determine ARM  error> */
		printf("error: Calibrations not completed\n");
		goto error_11;
	} else {
		/*< user code - Calibrations completed successfully > */
		printf("talise: Calibrations completed successfully\n");
	}

	/***************************************************/
	/**** Enable  Talise JESD204B Framer ***/
	/***************************************************/

	talAction = TALISE_enableFramerLink(&talDev, TAL_FRAMER_A, 0);
	if (talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
		printf("error: TALISE_enableFramerLink() failed\n");
		goto error_11;
	}

	talAction |= TALISE_enableFramerLink(&talDev, TAL_FRAMER_A, 1);
	if (talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
		printf("error: TALISE_enableFramerLink() failed\n");
		goto error_11;
	}

	/*************************************************/
	/**** Enable SYSREF to Talise JESD204B Framer ***/
	/*************************************************/
	/*** < User: Make sure SYSREF is stopped/disabled > ***/

	talAction = TALISE_enableSysrefToFramer(&talDev, TAL_FRAMER_A, 1);
	if (talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
		printf("error: TALISE_enableSysrefToFramer() failed\n");
		goto error_11;
	}

	/***************************************************/
	/**** Enable  Talise JESD204B Deframer ***/
	/***************************************************/

	talAction = TALISE_enableDeframerLink(&talDev, TAL_DEFRAMER_A, 0);
	if (talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
		printf("error: TALISE_enableDeframerLink() failed\n");
		goto error_11;
	}

	talAction |= TALISE_enableDeframerLink(&talDev, TAL_DEFRAMER_A, 1);
	if (talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
		printf("error: TALISE_enableDeframerLink() failed\n");
		goto error_11;
	}
	/***************************************************/
	/**** Enable SYSREF to Talise JESD204B Deframer ***/
	/***************************************************/
	talAction = TALISE_enableSysrefToDeframer(&talDev, TAL_DEFRAMER_A, 1);
	if (talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
		printf("error: TALISE_enableDeframerLink() failed\n");
		goto error_11;
	}

	/*** < User Sends SYSREF Here > ***/

	AD9528_sysrefReq(clockAD9528_device, SYSREF_CONT_ON);

	mdelay(100);

	axi_jesd204_rx_lane_clk_enable(rx_jesd);
	axi_jesd204_rx_lane_clk_enable(rx_os_jesd);

	mdelay(100);

	AD9528_sysrefReq(clockAD9528_device, SYSREF_CONT_OFF);

	mdelay(100);

	/*** < Insert User JESD204B Sync Verification Code Here > ***/

	/**************************************/
	/**** Check Talise Deframer Status ***/
	/**************************************/
	talAction = TALISE_readDeframerStatus(&talDev, TAL_DEFRAMER_A, &deframerStatus);
	if (talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
		printf("error: TALISE_readDeframerStatus() failed\n");
		goto error_11;
	}

	if ((deframerStatus & 0xF7) != 0x86)
		printf("warning: TAL_DEFRAMER_A status 0x%X\n", deframerStatus);

	/************************************/
	/**** Check Talise Framer Status ***/
	/************************************/
	talAction = TALISE_readFramerStatus(&talDev, TAL_FRAMER_A, &framerStatus);
	if (talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
		printf("error: TALISE_readFramerStatus() failed\n");
		goto error_11;
	}

	if ((framerStatus & 0x07) != 0x05) {
		printf("warning: TAL_FRAMER_A status 0x%X\n", framerStatus);
	}

	/*** < User: When links have been verified, proceed > ***/

	/***********************************************
	* Allow Rx1/2 QEC tracking and Tx1/2 QEC	   *
	* tracking to run when in the radioOn state	*
	* Tx calibrations will only run if radioOn and *
	* the obsRx path is set to OBS_INTERNAL_CALS   *
	* **********************************************/

	talAction = TALISE_enableTrackingCals(&talDev, trackingCalMask);
	if (talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
		printf("error: TALISE_enableTrackingCals() failed\n");
		goto error_11;
	}

	/* Function to turn radio on, Enables transmitters and receivers */
	/* that were setup during TALISE_initialize() */
	talAction = TALISE_radioOn(&talDev);
	if (talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
		printf("error: TALISE_radioOn() failed\n");
		goto error_11;
	}

	talAction = TALISE_setRxTxEnable(&talDev, TAL_RX1_EN, TAL_TX2);
	if (talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
		printf("error: TALISE_setRxTxEnable() failed\n");
		goto error_10;
	}

	AD9528_sysrefReq(clockAD9528_device, SYSREF_CONT_ON);

	axi_jesd204_rx_watchdog(rx_jesd);
	axi_jesd204_rx_watchdog(rx_os_jesd);


	/* Print JESD status */
	axi_jesd204_rx_status_read(rx_jesd);

	axi_jesd204_tx_status_read(tx_jesd);
	axi_jesd204_rx_status_read(rx_os_jesd);

	/* Initialize the DAC DDS */
	axi_dac_init(&tx_dac, &tx_dac_init);

	/* Initialize the ADC core */
	axi_adc_init(&rx_adc, &rx_adc_init);

	mdelay(1000);

	/* Initialize the DMAC and transfer 16384 samples from ADC to MEM */
	axi_dmac_init(&rx_dmac, &rx_dmac_init);
	axi_dmac_transfer(rx_dmac,
			  DDR_MEM_BASEADDR + 0x800000,
			  16384 * 8);

	/***********************************************
	* Shutdown Procedure *
	* **********************************************/
	/* Function to turn radio on, Disables transmitters and receivers */
	talAction = TALISE_radioOff(&talDev);
	if (talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
	}
	/* Put Talise in safe state for power down */
	talAction = TALISE_shutdown(&talDev);
	if (talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
	}

	/*Close Talise Hw Device*/
	talAction = TALISE_closeHw(&talDev);
	if(talAction != TALACT_NO_ACTION) {
		/*** < User: decide what to do based on Talise recovery action returned > ***/
	}

	adxcvr_remove(rx_os_adxcvr);
	adxcvr_remove(tx_adxcvr);
	adxcvr_remove(rx_adxcvr);
	axi_jesd204_rx_remove(rx_os_jesd);
	axi_jesd204_tx_remove(tx_jesd);
	axi_jesd204_rx_remove(rx_jesd);
#ifdef ALTERA_PLATFORM
	altera_a10_fpll_remove(rx_device_clk_pll);
	altera_a10_fpll_remove(tx_device_clk_pll);
	altera_a10_fpll_remove(rx_os_device_clk_pll);
#else
	axi_clkgen_remove(rx_os_clkgen);
	axi_clkgen_remove(tx_clkgen);
	axi_clkgen_remove(rx_clkgen);
#endif
	AD9528_remove(clockAD9528_device);

	printf("Bye\n");

	return SUCCESS;

error_11:
	TALISE_closeHw(&talDev);
error_10:
	adxcvr_remove(rx_os_adxcvr);
error_9:
	adxcvr_remove(tx_adxcvr);
error_8:
	adxcvr_remove(rx_adxcvr);
error_7:
	axi_jesd204_rx_remove(rx_os_jesd);
error_6:
	axi_jesd204_tx_remove(tx_jesd);
error_5:
	axi_jesd204_rx_remove(rx_jesd);
error_4:
#ifdef ALTERA_PLATFORM
	altera_a10_fpll_remove(rx_os_device_clk_pll);
#else
	axi_clkgen_remove(rx_os_clkgen);
#endif
error_3:
#ifdef ALTERA_PLATFORM
	altera_a10_fpll_remove(tx_device_clk_pll);
#else
	axi_clkgen_remove(tx_clkgen);
#endif
error_2:
#ifdef ALTERA_PLATFORM
	altera_a10_fpll_remove(rx_device_clk_pll);
#else
	axi_clkgen_remove(rx_clkgen);
#endif
error_1:
	AD9528_remove(clockAD9528_device);
error_0:
	return FAILURE;
}

the orignal talise_config.c:

/**
 * \file talise_config.c
 * \brief Contains Talise configuration settings for the Talise API
 *
 * Copyright 2015-2017 Analog Devices Inc.
 * Released under the AD9378-AD9379 API license, for more information see the "LICENSE.txt" file in this zip file.
 *
 * The top level structure taliseDevice_t talDevice uses keyword
 * extern to allow the application layer main() to have visibility
 * to these settings.
 *
 * This file may not be fully complete for the end user application and
 * may need to updated for AGC, GPIO, and DAC full scale settings.
 * To create a full initialisation routine, the user should also refer to the
 * Iron Python initialisation routine generated by the GUI, and also the Talise User Guide.
 *
 */

#include "talise_types.h"
#include "talise_config.h"
#include "talise_error.h"
#include "talise_agc.h"
#ifdef ADI_ZYNQ_PLATFORM
#include "zynq_platform.h"
#endif

int16_t txFirCoefs[80] = {0, 0, 0, 1, 0, -3, 1, 7, -3, -13, 7, 25, -14, -42, 27, 69, -46, -107, 74, 160, -115, -229, 184, 336, -264, -468, 382, 653, -538, -904, 754, 1269, -1056, -1842, 1486, 2879, -2031, -4846, 3816, 16221, 16221, 3816, -4846, -2031, 2879, 1486, -1842, -1056, 1269, 754, -904, -538, 653, 382, -468, -264, 336, 184, -229, -115, 160, 74, -107, -46, 69, 27, -42, -14, 25, 7, -13, -3, 7, 1, -3, 0, 1, 0, 0, 0};

int16_t rxFirCoefs[48] = {-8, -22, 32, 50, -68, -106, 141, 199, -258, -352, 430, 572, -691, -903, 1069, 1392, -1644, -2172, 2569, 3574, -4364, -7129, 9355, 31095, 31095, 9355, -7129, -4364, 3574, 2569, -2172, -1644, 1392, 1069, -903, -691, 572, 430, -352, -258, 199, 141, -106, -68, 50, 32, -22, -8};

int16_t obsrxFirCoefs[48] = {-9, -18, 31, 42, -65, -89, 132, 168, -240, -298, 396, 486, -632, -770, 968, 1163, -1530, -1862, 2369, 3051, -4066, -5983, 9689, 29830, 29830, 9689, -5983, -4066, 3051, 2369, -1862, -1530, 1163, 968, -770, -632, 486, 396, -298, -240, 168, 132, -89, -65, 42, 31, -18, -9};

#ifdef ADI_ZYNQ_PLATFORM /** < Insert Customer Platform HAL State Container here>*/
/*
 * Platform Layer SPI settings - this structure is specific to ADI's platform layer code.
 * User should replace with their own structure or settings for their hardware
 */
zynqSpiSettings_t spiDev1 = {
	.chipSelectIndex = 1,
	.writeBitPolarity = 0,
	.longInstructionWord = 1,
	.CPHA = 0,
	.CPOL = 0,
	.mode = 0,
	.spiClkFreq_Hz = 25000000
};

/*
 * Platform Layer settings - this structure is specific to ADI's platform layer code.
 * User should replace with their own structure or settings for their hardware
 * The structure is held in taliseDevice_t below as a void pointer, allowing
 * the customer to pass any information for their specific hardware down to the
 * hardware layer code.
 */
zynqAdiDev_t talDevHalInfo = {
	.devIndex = 1,
	.spiSettings = &spiDev1,
	.spiErrCode = 0,
	.timerErrCode = 0,
	.gpioErrCode = 0,
	.logLevel = ADIHAL_LOG_ALL
};
#endif
/**
 *  TalDevice a structure used by the Talise API to hold the platform hardware
 *  structure information, as well as an internal Talise API state container
 *  (devStateInfo) of runtime information used by the API.
 **/
taliseDevice_t talDevice = {
#ifdef ADI_ZYNQ_PLATFORM
	/* Void pointer of users platform HAL settings to pass to HAL layer calls
	 * Talise API does not use the devHalInfo member */
	.devHalInfo = &talDevHalInfo,
#else
	.devHalInfo = NULL,     /*/** < Insert Customer Platform HAL State Container here>*/
#endif
	/* devStateInfo is maintained internal to the Talise API, just create the memory */
	.devStateInfo = {0}

};

taliseInit_t talInit = {
	/* SPI settings */
	.spiSettings =
	{
		.MSBFirst            = 1,  /* 1 = MSBFirst, 0 = LSBFirst */
		.enSpiStreaming      = 0,  /* Not implemented in ADIs platform layer. SW feature to improve SPI throughput */
		.autoIncAddrUp       = 1,  /* Not implemented in ADIs platform layer. For SPI Streaming, set address increment direction. 1= next addr = addr+1, 0:addr=addr-1 */
		.fourWireMode        = 1,  /* 1: Use 4-wire SPI, 0: 3-wire SPI (SDIO pin is bidirectional). NOTE: ADI's FPGA platform always uses 4-wire mode */
		.cmosPadDrvStrength  = TAL_CMOSPAD_DRV_2X /* Drive strength of CMOS pads when used as outputs (SDIO, SDO, GP_INTERRUPT, GPIO 1, GPIO 0) */
	},

	/* Rx settings */
	.rx =
	{
		.rxProfile =
		{
			.rxFir =
			{
				.gain_dB = -6,                /* filter gain */
				.numFirCoefs = 48,            /* number of coefficients in the FIR filter */
				.coefs = &rxFirCoefs[0]
			},
			.rxFirDecimation = 2,            /* Rx FIR decimation (1,2,4) */
			.rxDec5Decimation = 4,            /* Decimation of Dec5 or Dec4 filter (5,4) */
			.rhb1Decimation = 2,            /* RX Half band 1 decimation (1 or 2) */
			.rxOutputRate_kHz = 122880,            /* Rx IQ data rate in kHz */
			.rfBandwidth_Hz = 100000000,    /* The Rx RF passband bandwidth for the profile */
			.rxBbf3dBCorner_kHz = 100000,    /* Rx BBF 3dB corner in kHz */
			.rxAdcProfile = {265, 146, 181, 90, 1280, 366, 1257, 27, 1258, 17, 718, 39, 48, 46, 27, 161, 0, 0, 0, 0, 40, 0, 7, 6, 42, 0, 7, 6, 42, 0, 25, 27, 0, 0, 25, 27, 0, 0, 165, 44, 31, 905},            /* pointer to custom ADC profile */
			.rxDdcMode = TAL_RXDDC_BYPASS,   /* Rx DDC mode */
			.rxNcoShifterCfg =
			{
				.bandAInputBandWidth_kHz = 0,
				.bandAInputCenterFreq_kHz = 0,
				.bandANco1Freq_kHz = 0,
				.bandANco2Freq_kHz = 0,
				.bandBInputBandWidth_kHz = 0,
				.bandBInputCenterFreq_kHz = 0,
				.bandBNco1Freq_kHz = 0,
				.bandBNco2Freq_kHz = 0
			}
		},
		.framerSel = TAL_FRAMER_A,            /* Rx JESD204b framer configuration */
		.rxGainCtrl =
		{
			.gainMode = TAL_MGC,            /* taliserxGainMode_t gainMode */
			.rx1GainIndex = 255,            /* uint8_t rx1GainIndex */
			.rx2GainIndex = 255,            /* uint8_t rx2GainIndex */
			.rx1MaxGainIndex = 255,            /* uint8_t rx1MaxGainIndex */
			.rx1MinGainIndex = 195,            /* uint8_t rx1MinGainIndex */
			.rx2MaxGainIndex = 255,            /* uint8_t rx2MaxGainIndex */
			.rx2MinGainIndex = 195            /* uint8_t rx2MinGainIndex */
		},
		.rxChannels = TAL_RX1RX2,                /* The desired Rx Channels to enable during initialization */
	},


	/* Tx settings */
	.tx =
	{
		.txProfile =
		{
			.dacDiv = 1,                        /* The divider used to generate the DAC clock */
			.txFir =
			{
				.gain_dB = 6,                        /* filter gain */
				.numFirCoefs = 80,                    /* number of coefficients in the FIR filter */
				.coefs = &txFirCoefs[0]
			},
			.txFirInterpolation = 2,                    /* The Tx digital FIR filter interpolation (1,2,4) */
			.thb1Interpolation = 2,                    /* Tx Halfband1 filter interpolation (1,2) */
			.thb2Interpolation = 2,                    /* Tx Halfband2 filter interpolation (1,2)*/
			.thb3Interpolation = 2,                    /* Tx Halfband3 filter interpolation (1,2)*/
			.txInt5Interpolation = 1,                    /* Tx Int5 filter interpolation (1,5) */
			.txInputRate_kHz = 122880,                    /* Primary Signal BW */
			.primarySigBandwidth_Hz = 50000000,    /* The Rx RF passband bandwidth for the profile */
			.rfBandwidth_Hz = 100000000,            /* The Tx RF passband bandwidth for the profile */
			.txDac3dBCorner_kHz = 187000,                /* The DAC filter 3dB corner in kHz */
			.txBbf3dBCorner_kHz = 56000,                /* The BBF 3dB corner in kHz */
			.loopBackAdcProfile = {265, 146, 181, 90, 1280, 366, 1257, 27, 1258, 17, 718, 39, 48, 46, 27, 161, 0, 0, 0, 0, 40, 0, 7, 6, 42, 0, 7, 6, 42, 0, 25, 27, 0, 0, 25, 27, 0, 0, 165, 44, 31, 905}
		},
		.deframerSel = TAL_DEFRAMER_A,                    /* Talise JESD204b deframer config for the Tx data path */
		.txChannels = TAL_TX1TX2,                            /* The desired Tx channels to enable during initialization */
		.txAttenStepSize = TAL_TXATTEN_0P05_DB,            /* Tx Attenuation step size */
		.tx1Atten_mdB = 0,                            /* Initial Tx1 Attenuation */
		.tx2Atten_mdB = 0,                            /* Initial Tx2 Attenuation */
		.disTxDataIfPllUnlock = TAL_TXDIS_TX_RAMP_DOWN_TO_ZERO    /* Options to disable the transmit data when the RFPLL unlocks. */
	},


	/* ObsRx settings */
	.obsRx =
	{
		.orxProfile =
		{
			.rxFir =
			{
				.gain_dB = 6,                /* filter gain */
				.numFirCoefs = 48,            /* number of coefficients in the FIR filter */
				.coefs = &obsrxFirCoefs[0]
			},
			.rxFirDecimation = 2,            /* Rx FIR decimation (1,2,4) */
			.rxDec5Decimation = 4,            /* Decimation of Dec5 or Dec4 filter (5,4) */
			.rhb1Decimation = 2,            /* RX Half band 1 decimation (1 or 2) */
			.orxOutputRate_kHz = 122880,            /* Rx IQ data rate in kHz */
			.rfBandwidth_Hz = 100000000,    /* The Rx RF passband bandwidth for the profile */
			.rxBbf3dBCorner_kHz = 225000,    /* Rx BBF 3dB corner in kHz */
			.orxLowPassAdcProfile = {265, 146, 181, 90, 1280, 366, 1257, 27, 1258, 17, 718, 39, 48, 46, 27, 161, 0, 0, 0, 0, 40, 0, 7, 6, 42, 0, 7, 6, 42, 0, 25, 27, 0, 0, 25, 27, 0, 0, 165, 44, 31, 905},
			.orxBandPassAdcProfile = {265, 146, 181, 90, 1280, 366, 1257, 27, 1258, 17, 718, 39, 48, 46, 27, 161, 0, 0, 0, 0, 40, 0, 7, 6, 42, 0, 7, 6, 42, 0, 25, 27, 0, 0, 25, 27, 0, 0, 165, 44, 31, 905},
			.orxDdcMode = TAL_ORXDDC_DISABLED,   /* ORx DDC mode */
			.orxMergeFilter  = {0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0}
		},
		.orxGainCtrl =
		{
			.gainMode = TAL_MGC,
			.orx1GainIndex = 255,
			.orx2GainIndex = 255,
			.orx1MaxGainIndex = 255,
			.orx1MinGainIndex = 195,
			.orx2MaxGainIndex = 255,
			.orx2MinGainIndex = 195
		},
		.framerSel = TAL_FRAMER_B,                /* ObsRx JESD204b framer configuration */
		.obsRxChannelsEnable = TAL_ORX1ORX2,        /* The desired ObsRx Channels to enable during initialization */
		.obsRxLoSource = TAL_OBSLO_RF_PLL                /* The ORx mixers can use the TX_PLL */
	},

	/* Digital Clock Settings */
	.clocks =
	{
		.deviceClock_kHz = 122880,            /* CLKPLL and device reference clock frequency in kHz */
		.clkPllVcoFreq_kHz = 9830400,        /* CLKPLL VCO frequency in kHz */
		.clkPllHsDiv = TAL_HSDIV_2P5,            /* CLKPLL high speed clock divider */
		.rfPllUseExternalLo = 0,                /* 1= Use external LO for RF PLL, 0 = use internal LO generation for RF PLL */
		.rfPllPhaseSyncMode = TAL_RFPLLMCS_NOSYNC                /* RFPLL MCS (Phase sync) mode */
	},

	/* JESD204B settings */
	.jesd204Settings =
	{
		/* Framer A settings */
		.framerA =
		{
			.bankId = 1,                    /* JESD204B Configuration Bank ID -extension to Device ID (Valid 0..15) */
			.deviceId = 0,                    /* JESD204B Configuration Device ID - link identification number. (Valid 0..255) */
			.lane0Id = 0,                    /* JESD204B Configuration starting Lane ID.  If more than one lane used, each lane will increment from the Lane0 ID. (Valid 0..31) */
			.M = 4,                            /* number of ADCs (0, 2, or 4) - 2 ADCs per receive chain */
			.K = 32,                        /* number of frames in a multiframe (default=32), F*K must be a multiple of 4. (F=2*M/numberOfLanes) */
			.F = 4,                            /* F (number of bytes per frame) */
			.Np = 16,                            /* Np (converter sample resolution) */
			.scramble = 1,                    /* scrambling off if framerScramble= 0, if framerScramble>0 scramble is enabled. */
			.externalSysref = 1,            /* 0=use internal SYSREF, 1= use external SYSREF */
			.serializerLanesEnabled = 0x03,    /* serializerLanesEnabled - bit per lane, [0] = Lane0 enabled, [1] = Lane1 enabled */
			.serializerLaneCrossbar = 0xE4,    /* serializerLaneCrossbar */
			.lmfcOffset = 31,                /* lmfcOffset - LMFC offset value for deterministic latency setting */
			.newSysrefOnRelink = 0,            /* newSysrefOnRelink */
			.syncbInSelect = 0,                /* syncbInSelect; */
			.overSample = 0,                    /* 1=overSample, 0=bitRepeat */
			.syncbInLvdsMode = 1,
			.syncbInLvdsPnInvert = 0,
			.enableManualLaneXbar = 0 /* 0=auto, 1=manual */
		},
		/* Framer B settings */
		.framerB =
		{
			.bankId = 0,                    /* JESD204B Configuration Bank ID -extension to Device ID (Valid 0..15) */
			.deviceId = 0,                    /* JESD204B Configuration Device ID - link identification number. (Valid 0..255) */
			.lane0Id = 0,                    /* JESD204B Configuration starting Lane ID.  If more than one lane used, each lane will increment from the Lane0 ID. (Valid 0..31) */
			.M = 2,                            /* number of ADCs (0, 2, or 4) - 2 ADCs per receive chain */
			.K = 32,                        /* number of frames in a multiframe (default=32), F*K must be a multiple of 4. (F=2*M/numberOfLanes) */
			.F = 2,                            /* F (number of bytes per frame) */
			.Np = 16,                            /* Np (converter sample resolution) */
			.scramble = 1,                    /* scrambling off if framerScramble= 0, if framerScramble>0 scramble is enabled. */
			.externalSysref = 1,            /* 0=use internal SYSREF, 1= use external SYSREF */
			.serializerLanesEnabled = 0x0C,    /* serializerLanesEnabled - bit per lane, [0] = Lane0 enabled, [1] = Lane1 enabled */
			.serializerLaneCrossbar = 0xE4,    /* serializerLaneCrossbar */
			.lmfcOffset = 31,                /* lmfcOffset - LMFC offset value for deterministic latency setting */
			.newSysrefOnRelink = 0,            /* newSysrefOnRelink */
			.syncbInSelect = 1,                /* syncbInSelect; */
			.overSample = 0,                    /* 1=overSample, 0=bitRepeat */
			.syncbInLvdsMode = 1,
			.syncbInLvdsPnInvert = 0,
			.enableManualLaneXbar = 0 /* 0=auto, 1=manual */
		},
		/* Deframer A settings */
		.deframerA =
		{
			.bankId = 0,                    /* bankId extension to Device ID (Valid 0..15) */
			.deviceId = 0,                    /* deviceId  link identification number. (Valid 0..255) */
			.lane0Id = 0,                    /* lane0Id Lane0 ID. (Valid 0..31) */
			.M = 4,                            /* M  number of DACss (0, 2, or 4) - 2 DACs per transmit chain */
			.K = 32,                        /* K  #frames in a multiframe (default=32), F*K=multiple of 4. (F=2*M/numberOfLanes) */
			.scramble = 1,                    /* scramble  scrambling off if scramble= 0 */
			.externalSysref = 1,            /* externalSysref  0= use internal SYSREF, 1= external SYSREF */
			.deserializerLanesEnabled = 0x0F,    /* deserializerLanesEnabled  bit per lane, [0] = Lane0 enabled */
			.deserializerLaneCrossbar = 0xE4,    /* deserializerLaneCrossbar */
			.lmfcOffset = 17,                /* lmfcOffset	 LMFC offset value to adjust deterministic latency */
			.newSysrefOnRelink = 0,            /* newSysrefOnRelink */
			.syncbOutSelect = 0,                /* SYNCBOUT0/1 select */
			.Np = 16,                /* Np (converter sample resolution) */
			.syncbOutLvdsMode = 1,
			.syncbOutLvdsPnInvert = 0,
			.syncbOutCmosSlewRate = 0,
			.syncbOutCmosDriveLevel = 0,
			.enableManualLaneXbar = 0 /* 0=auto, 1=manual */
		},
		/* Deframer B settings */
		.deframerB =
		{
			.bankId = 0,                    /* bankId extension to Device ID (Valid 0..15) */
			.deviceId = 0,                    /* deviceId  link identification number. (Valid 0..255) */
			.lane0Id = 0,                    /* lane0Id Lane0 ID. (Valid 0..31) */
			.M = 0,                            /* M  number of DACss (0, 2, or 4) - 2 DACs per transmit chain */
			.K = 32,                        /* K  #frames in a multiframe (default=32), F*K=multiple of 4. (F=2*M/numberOfLanes) */
			.scramble = 1,                    /* scramble  scrambling off if scramble= 0 */
			.externalSysref = 1,            /* externalSysref  0= use internal SYSREF, 1= external SYSREF */
			.deserializerLanesEnabled = 0x00,    /* deserializerLanesEnabled  bit per lane, [0] = Lane0 enabled */
			.deserializerLaneCrossbar = 0xE4,    /* deserializerLaneCrossbar */
			.lmfcOffset = 0,                /* lmfcOffset	 LMFC offset value to adjust deterministic latency */
			.newSysrefOnRelink = 0,            /* newSysrefOnRelink */
			.syncbOutSelect = 1,                /* SYNCBOUT0/1 select */
			.Np = 16,                /* Np (converter sample resolution) */
			.syncbOutLvdsMode = 1,
			.syncbOutLvdsPnInvert = 0,
			.syncbOutCmosSlewRate = 0,
			.syncbOutCmosDriveLevel = 0,
			.enableManualLaneXbar = 0 /* 0=auto, 1=manual */
		},
		.serAmplitude = 15,                    /* Serializer amplitude setting. Default = 15. Range is 0..15 */
		.serPreEmphasis = 1,                /* Serializer pre-emphasis setting. Default = 1 Range is 0..4 */
		.serInvertLanePolarity = 0,            /* Serializer Lane PN inversion select. Default = 0. Where, bit[0] = 1 will invert lane [0], bit[1] = 1 will invert lane 1, etc. */
		.desInvertLanePolarity = 0,            /* Deserializer Lane PN inversion select.  bit[0] = 1 Invert PN of Lane 0, bit[1] = Invert PN of Lane 1, etc */
		.desEqSetting = 1,                    /* Deserializer Equalizer setting. Applied to all deserializer lanes. Range is 0..4 */
		.sysrefLvdsMode = 1,                /* Use LVDS inputs on Talise for SYSREF */
		.sysrefLvdsPnInvert = 0              /*0= Do not PN invert SYSREF */
	}
};

//Only needs to be called if user wants to setup AGC parameters
static taliseAgcCfg_t rxAgcCtrl = {
	4,
	255,
	195,
	255,
	195,
	30720,  /* AGC gain update time in us (125us-250us - based on IQ data rate - set for 125us @ 245.76 Mhz) */
	10,
	10,
	16,
	0,
	1,
	0,
	0,
	0,
	1,
	31,
	246,
	4,
	1,          /*!<1- bit field to enable the multiple time constants in AGC loop for fast attack and fast recovery to max gain. */
	/* agcPower */
	{
		1,      /*!<1-bit field, enables the Rx power measurement block. */
		1,      /*!<1-bit field, allows using Rx PFIR for power measurement. */
		0,      /*!<1-bit field, allows to use the output of the second digital offset block in the Rx datapath for power measurement. */
		9,      /*!<AGC power measurement detect lower 0 threshold. Default = -12dBFS == 5, 7-bit register value where max = 0x7F, min = 0x00 */
		2,      /*!<AGC power measurement detect lower 1 threshold. Default = (offset) 4dB == 0, 4-bit register value where  max = 0xF, min = 0x00 */
		4,      /*!<AGC power measurement detect lower 0 recovery gain step. Default = 2dB - based on gain table step  size, 5-bit register value where max = 0x1F, min = 0x00 */
		4,      /*!<AGC power measurement detect lower 1 recovery gain step. Default = 4dB - based on gain table step size, 5-bit register value where max = 0x1F, min = 0x00 */
		5,      /*!< power measurement duration used by the decimated power block. Default = 0x05, 5-bit register value where max = 0x1F, min = 0x00 */
		5,      /*!<Allows power detection of data for a specific slice of the gain update counter. 16-bit register value (currently not used) */
		1,      /*!<Allows power detection of data for a specific slice of the gain update counter. 16-bit register value (currently not used) */
		5,      /*!<Allows power detection of data for a specific slice of the gain update counter. 16-bit register value (currently not used) */
		1,      /*!<Allows power detection of data for a specific slice of the gain update counter. 16-bit register value (currently not used) */
		2,      /*!<Default value should be 2*/
		0,
		0
	},
	/* agcPeak */
	{
		205,        /*!<1st update interval for the multiple time constant in AGC loop mode, Default:205. */
		2,          /*!<sets the 2nd update interval for the multiple time constant in AGC loop mode. Calculated as a multiple of  agcUnderRangeLowInterval  , Default: 4 */
		4,          /*!<sets the 3rd update interval for the multiple time constant in AGC loop mode. Calculated as a multiple of agcUnderRangeMidInterval and agcUnderRangeLowInterval, Default: 4 */
		39,         /*!<AGC APD high threshold. Default=0x1F, 6-bit register value where max=0x3F, min =0x00 */
		49,         /*!<AGC APD peak detect high threshold. default = 0x1F, 6-bit register value where max = 0x3F, min = 0x00.  Set to 3dB below apdHighThresh */
		23,         /*!<AGC APD peak detect low threshold. default = 3dB below high threshold, 6-bit register value where max =0x3F, min = 0x00 */
		19,         /*!<AGC APD peak detect low threshold. default = 3dB below high threshold, 6-bit register value where max = 0x3F, min = 0x00 . Set to 3dB below apdLowThresh  */
		6,          /*!<AGC APD peak detect upper threshold count. Default = 0x06 8-bit register value where max = 0xFF, min = 0x20  */
		3,          /*!<AGC APD peak detect lower threshold count. Default = 0x03, 8-bit register value where max = 0xFF, min = 0x00  */
		4,          /*!<AGC APD peak detect attack gain step. Default = 2dB step - based on gain table step size, 5-bit register  value, where max = 0x1F, min = 0x00  */
		2,          /*!<AGC APD gain index step size. Recommended to be same as hb2GainStepRecovery. Default = 0x00, 5-bit register value where max = 0x1F, min = 0x00  */
		1,          /*!<1-bit field, enables or disables the HB2 overload detector.  */
		1,          /*!<3-bit field. Sets the window of clock cycles (at the HB2 output rate) to meet the overload count. */
		1,          /*!<4-bit field. Sets the number of actual overloads required to trigger the overload signal.  */
		181,        /*!<AGC decimator output high threshold. Default = 0xB5, 8-bit register value where max = 0xFF, min = 0x00 */
		45,         /*!<AGC decimator output low threshold. Default = 0x80, 8-bit register value where max = 0xFF, min = 0x00 */
		90,         /*!<AGC decimator output low threshold. Default = 0x80, 8-bit register value where max = 0xFF, min = 0x00 */
		128,        /*!<AGC decimator output low threshold. Default = 0x80, 8-bit register value where max = 0xFF, min = 0x00 */
		6,          /*!<AGC HB2 output upper threshold count. Default = 0x06, 8-bit register value where max = 0xFF, min =  0x20 */
		3,          /*!<AGC HB2 output lower threshold count. Default = 0x03, 8-bit register value where max = 0xFF, min = 0x00 */
		2,          /*!<AGC decimator gain index step size. Default = 0x00, 5-bit register value where max = 0x1F, min = 0x00 */
		4,          /*!<AGC HB2 gain index step size, when the HB2 Low Overrange interval 0 triggers a programmable number  of times. Default = 0x08, 5-bit register value where max = 0x1F, min = 0x00 */
		8,          /*!<AGC HB2 gain index step size, when the HB2 Low Overrange interval 1 triggers a programmable number of times. Default = 0x04, 5-bit register value where max = 0x1F, min = 0x00 */
		4,          /*!<AGC decimator output attack gain step. Default = 2dB step - based on gain table step size, 5-bit register value, where max = 0x1F, min = 0x00 */
		1,
		0,
		0
	}
};

the talise_config.c generated by TES:

/**
 * \file talise_config.c
 * \brief Contains Talise configuration settings for the Talise API
 *
 * Copyright 2015-2017 Analog Devices Inc.
 * Released under the AD9378-AD9379 API license, for more information see the "LICENSE.txt" file in this zip file.
 *
 * The top level structure taliseDevice_t talDevice uses keyword
 * extern to allow the application layer main() to have visibility
 * to these settings.
 *
 * This file may not be fully complete for the end user application and 
 * may need to updated for AGC, GPIO, and DAC full scale settings. 
 * To create a full initialisation routine, the user should also refer to the 
 * Iron Python initialisation routine generated by the GUI, and also the Talise User Guide.
 *
 */

#include "talise_types.h"
#include "talise_config.h"
#include "talise_error.h"
#include "talise_agc.h"
#ifdef ADI_ZYNQ_PLATFORM
#include "zynq_platform.h"
#endif

int16_t txFirCoefs[20] = {-39, 24, -62, 112, -175, 298, -574, 1284, -2814, 20281, -2814, 1284, -574, 298, -175, 112, -62, 24, -39, 0};

int16_t rxFirCoefs[48] = {-2, 23, 46, -17, -104, 10, 208, 23, -370, -97, 607, 240, -942, -489, 1407, 910, -2065, -1637, 3058, 2995, -4912, -6526, 9941, 30489, 30489, 9941, -6526, -4912, 2995, 3058, -1637, -2065, 910, 1407, -489, -942, 240, 607, -97, -370, 23, 208, 10, -104, -17, 46, 23, -2};

int16_t obsrxFirCoefs[24] = {-15, 9, -13, 19, -28, 38, -73, 110, -195, 409, -1006, 17711, -1006, 409, -195, 110, -73, 38, -28, 19, -13, 9, -15, 0};

#ifdef ADI_ZYNQ_PLATFORM /** < Insert Customer Platform HAL State Container here>*/
/*
 * Platform Layer SPI settings - this structure is specific to ADI's platform layer code.
 * User should replace with their own structure or settings for their hardware
 */
zynqSpiSettings_t spiDev1 =
{
	.chipSelectIndex = 1,
	.writeBitPolarity = 0,
	.longInstructionWord = 1,
	.CPHA = 0,
	.CPOL = 0,
	.mode = 0,
	.spiClkFreq_Hz = 25000000
};

/*
 * Platform Layer settings - this structure is specific to ADI's platform layer code.
 * User should replace with their own structure or settings for their hardware
 * The structure is held in taliseDevice_t below as a void pointer, allowing
 * the customer to pass any information for their specific hardware down to the
 * hardware layer code.
 */
zynqAdiDev_t talDevHalInfo =
{
	.devIndex = 1,
	.spiSettings = &spiDev1,
	.spiErrCode = 0,
	.timerErrCode = 0,
	.gpioErrCode = 0,
	.logLevel = ADIHAL_LOG_ALL
};
#endif
/**
 *  TalDevice a structure used by the Talise API to hold the platform hardware
 *  structure information, as well as an internal Talise API state container
 *  (devStateInfo) of runtime information used by the API.
 **/
taliseDevice_t talDevice =
{
#ifdef ADI_ZYNQ_PLATFORM
    /* Void pointer of users platform HAL settings to pass to HAL layer calls
     * Talise API does not use the devHalInfo member */
	.devHalInfo = &talDevHalInfo,
#else
	.devHalInfo = NULL,     /*/** < Insert Customer Platform HAL State Container here>*/
#endif
	/* devStateInfo is maintained internal to the Talise API, just create the memory */
	.devStateInfo = {0}

};

taliseInit_t talInit =
{
	/* SPI settings */
    .spiSettings =
    {
		.MSBFirst            = 1,  /* 1 = MSBFirst, 0 = LSBFirst */
		.enSpiStreaming      = 0,  /* Not implemented in ADIs platform layer. SW feature to improve SPI throughput */
		.autoIncAddrUp       = 1,  /* Not implemented in ADIs platform layer. For SPI Streaming, set address increment direction. 1= next addr = addr+1, 0:addr=addr-1 */
		.fourWireMode        = 1,  /* 1: Use 4-wire SPI, 0: 3-wire SPI (SDIO pin is bidirectional). NOTE: ADI's FPGA platform always uses 4-wire mode */
		.cmosPadDrvStrength  = TAL_CMOSPAD_DRV_2X /* Drive strength of CMOS pads when used as outputs (SDIO, SDO, GP_INTERRUPT, GPIO 1, GPIO 0) */
	},
	
    /* Rx settings */
    .rx = 
    {
        .rxProfile =
        {
            .rxFir = 
            {
                .gain_dB = -6,                /* filter gain */
                .numFirCoefs = 48,            /* number of coefficients in the FIR filter */
                .coefs = &rxFirCoefs[0]
            },
            .rxFirDecimation = 2,            /* Rx FIR decimation (1,2,4) */
            .rxDec5Decimation = 4,            /* Decimation of Dec5 or Dec4 filter (5,4) */
            .rhb1Decimation = 1,            /* RX Half band 1 decimation (1 or 2) */
            .rxOutputRate_kHz = 245760,            /* Rx IQ data rate in kHz */
            .rfBandwidth_Hz = 200000000,    /* The Rx RF passband bandwidth for the profile */
            .rxBbf3dBCorner_kHz = 200000,    /* Rx BBF 3dB corner in kHz */
            .rxAdcProfile = {182, 142, 173, 90, 1280, 982, 1335, 96, 1369, 48, 1012, 18, 48, 48, 37, 208, 0, 0, 0, 0, 52, 0, 7, 6, 42, 0, 7, 6, 42, 0, 25, 27, 0, 0, 25, 27, 0, 0, 165, 44, 31, 905},            /* pointer to custom ADC profile */
            .rxDdcMode = TAL_RXDDC_BYPASS,   /* Rx DDC mode */
            .rxNcoShifterCfg =
            {
                .bandAInputBandWidth_kHz = 0,
                .bandAInputCenterFreq_kHz = 0,
                .bandANco1Freq_kHz = 0,
                .bandANco2Freq_kHz = 0,
                .bandBInputBandWidth_kHz = 0,
                .bandBInputCenterFreq_kHz = 0,
                .bandBNco1Freq_kHz = 0,
                .bandBNco2Freq_kHz = 0
            }
        },
        .framerSel = TAL_FRAMER_A,            /* Rx JESD204b framer configuration */
        .rxGainCtrl = 
        {
            .gainMode = TAL_MGC,            /* taliserxGainMode_t gainMode */
            .rx1GainIndex = 255,            /* uint8_t rx1GainIndex */
            .rx2GainIndex = 255,            /* uint8_t rx2GainIndex */
            .rx1MaxGainIndex = 255,            /* uint8_t rx1MaxGainIndex */
            .rx1MinGainIndex = 195,            /* uint8_t rx1MinGainIndex */
            .rx2MaxGainIndex = 255,            /* uint8_t rx2MaxGainIndex */
            .rx2MinGainIndex = 195            /* uint8_t rx2MinGainIndex */
        },
        .rxChannels = TAL_RX1,                /* The desired Rx Channels to enable during initialization */
    },


    /* Tx settings */
    .tx = 
    {
        .txProfile =
        {
            .dacDiv = 1,                        /* The divider used to generate the DAC clock */
            .txFir = 
            {
                .gain_dB = 6,                        /* filter gain */
                .numFirCoefs = 20,                    /* number of coefficients in the FIR filter */
                .coefs = &txFirCoefs[0]
            },
            .txFirInterpolation = 1,                    /* The Tx digital FIR filter interpolation (1,2,4) */
            .thb1Interpolation = 2,                    /* Tx Halfband1 filter interpolation (1,2) */
            .thb2Interpolation = 2,                    /* Tx Halfband2 filter interpolation (1,2)*/
            .thb3Interpolation = 1,                    /* Tx Halfband3 filter interpolation (1,2)*/
            .txInt5Interpolation = 1,                    /* Tx Int5 filter interpolation (1,5) */
            .txInputRate_kHz = 491520,                    /* Primary Signal BW */
            .primarySigBandwidth_Hz = 200000000,    /* The Rx RF passband bandwidth for the profile */
            .rfBandwidth_Hz = 450000000,            /* The Tx RF passband bandwidth for the profile */
            .txDac3dBCorner_kHz = 450000,                /* The DAC filter 3dB corner in kHz */
            .txBbf3dBCorner_kHz = 225000,                /* The BBF 3dB corner in kHz */
            .loopBackAdcProfile = {150, 178, 181, 90, 1280, 1338, 1699, 493, 1386, 162, 934, 4, 48, 46, 35, 201, 0, 0, 0, 0, 50, 0, 0, 6, 24, 0, 0, 6, 24, 0, 25, 27, 0, 0, 25, 27, 0, 0, 165, 44, 15, 905}
        },
        .deframerSel = TAL_DEFRAMER_A,                    /* Talise JESD204b deframer config for the Tx data path */
        .txChannels = TAL_TX2,                            /* The desired Tx channels to enable during initialization */
        .txAttenStepSize = TAL_TXATTEN_0P05_DB,            /* Tx Attenuation step size */
        .tx1Atten_mdB = 0,                            /* Initial Tx1 Attenuation */
        .tx2Atten_mdB = 0,                            /* Initial Tx2 Attenuation */
        .disTxDataIfPllUnlock = TAL_TXDIS_TX_RAMP_DOWN_TO_ZERO    /* Options to disable the transmit data when the RFPLL unlocks. */
    },


    /* ObsRx settings */
    .obsRx = 
    {
        .orxProfile =
        {
            .rxFir = 
            {
                .gain_dB = 6,                /* filter gain */
                .numFirCoefs = 24,            /* number of coefficients in the FIR filter */
                .coefs = &obsrxFirCoefs[0]
            },
            .rxFirDecimation = 1,            /* Rx FIR decimation (1,2,4) */
            .rxDec5Decimation = 4,            /* Decimation of Dec5 or Dec4 filter (5,4) */
            .rhb1Decimation = 1,            /* RX Half band 1 decimation (1 or 2) */
            .orxOutputRate_kHz = 491520,            /* Rx IQ data rate in kHz */
            .rfBandwidth_Hz = 450000000,    /* The Rx RF passband bandwidth for the profile */
            .rxBbf3dBCorner_kHz = 225000,    /* Rx BBF 3dB corner in kHz */
            .orxLowPassAdcProfile = {155, 163, 181, 90, 1280, 1254, 1572, 340, 1431, 142, 973, 8, 48, 47, 36, 205, 0, 0, 0, 0, 51, 0, 0, 6, 24, 0, 0, 6, 24, 0, 25, 27, 0, 0, 25, 27, 0, 0, 165, 44, 15, 905},
            .orxBandPassAdcProfile = {124, 131, 154, 90, 1280, 2779, 1986, 0, 1037, 839, 988, 109, 11, 15, 28, 179, 0, 0, 0, 0, 45, 0, 0, 0, 24, 0, 0, 0, 24, 0, 25, 27, 0, 0, 25, 27, 0, 0, 165, 44, 15, 905},
            .orxDdcMode = TAL_ORXDDC_DISABLED,   /* ORx DDC mode */
            .orxMergeFilter  = {-167, 419, -208, -498, 968, -320, -1273, 2154, -402, -4155, 9170, 21413}
        },
        .orxGainCtrl = 
        {
            .gainMode = TAL_MGC,
            .orx1GainIndex = 255,
            .orx2GainIndex = 255,
            .orx1MaxGainIndex = 255,
            .orx1MinGainIndex = 195,
            .orx2MaxGainIndex = 255,
            .orx2MinGainIndex = 195
        },
        .framerSel = TAL_FRAMER_B,                /* ObsRx JESD204b framer configuration */
        .obsRxChannelsEnable = TAL_ORX2,        /* The desired ObsRx Channels to enable during initialization */
        .obsRxLoSource = TAL_OBSLO_RF_PLL                /* The ORx mixers can use the TX_PLL */
    },

    /* Digital Clock Settings */
    .clocks = 
    {
        .deviceClock_kHz = 122880,            /* CLKPLL and device reference clock frequency in kHz */
        .clkPllVcoFreq_kHz = 9830400,        /* CLKPLL VCO frequency in kHz */
        .clkPllHsDiv = TAL_HSDIV_2P5,            /* CLKPLL high speed clock divider */
        .rfPllUseExternalLo = 0,                /* 1= Use external LO for RF PLL, 0 = use internal LO generation for RF PLL */
        .rfPllPhaseSyncMode = TAL_RFPLLMCS_NOSYNC                /* RFPLL MCS (Phase sync) mode */
    },

    /* JESD204B settings */
    .jesd204Settings = 
    {
        /* Framer A settings */
        .framerA = 
        {
            .bankId = 1,                    /* JESD204B Configuration Bank ID -extension to Device ID (Valid 0..15) */
            .deviceId = 0,                    /* JESD204B Configuration Device ID - link identification number. (Valid 0..255) */
            .lane0Id = 0,                    /* JESD204B Configuration starting Lane ID.  If more than one lane used, each lane will increment from the Lane0 ID. (Valid 0..31) */
            .M = 2,                            /* number of ADCs (0, 2, or 4) - 2 ADCs per receive chain */
            .K = 32,                        /* number of frames in a multiframe (default=32), F*K must be a multiple of 4. (F=2*M/numberOfLanes) */
            .F = 4,                            /* F (number of bytes per frame) */
            .Np = 16,                            /* Np (converter sample resolution) */
            .scramble = 1,                    /* scrambling off if framerScramble= 0, if framerScramble>0 scramble is enabled. */
            .externalSysref = 1,            /* 0=use internal SYSREF, 1= use external SYSREF */
            .serializerLanesEnabled = 0x04,    /* serializerLanesEnabled - bit per lane, [0] = Lane0 enabled, [1] = Lane1 enabled */
            .serializerLaneCrossbar = 0xE4,    /* serializerLaneCrossbar */
            .lmfcOffset = 31,                /* lmfcOffset - LMFC offset value for deterministic latency setting */
            .newSysrefOnRelink = 0,            /* newSysrefOnRelink */
            .syncbInSelect = 0,                /* syncbInSelect; */
            .overSample = 0,                    /* 1=overSample, 0=bitRepeat */
            .syncbInLvdsMode = 1,
            .syncbInLvdsPnInvert = 0,
            .enableManualLaneXbar = 0 /* 0=auto, 1=manual */
        },
        /* Framer B settings */
        .framerB = 
        {
            .bankId = 0,                    /* JESD204B Configuration Bank ID -extension to Device ID (Valid 0..15) */
            .deviceId = 0,                    /* JESD204B Configuration Device ID - link identification number. (Valid 0..255) */
            .lane0Id = 0,                    /* JESD204B Configuration starting Lane ID.  If more than one lane used, each lane will increment from the Lane0 ID. (Valid 0..31) */
            .M = 2,                            /* number of ADCs (0, 2, or 4) - 2 ADCs per receive chain */
            .K = 32,                        /* number of frames in a multiframe (default=32), F*K must be a multiple of 4. (F=2*M/numberOfLanes) */
            .F = 2,                            /* F (number of bytes per frame) */
            .Np = 16,                            /* Np (converter sample resolution) */
            .scramble = 1,                    /* scrambling off if framerScramble= 0, if framerScramble>0 scramble is enabled. */
            .externalSysref = 1,            /* 0=use internal SYSREF, 1= use external SYSREF */
            .serializerLanesEnabled = 0x03,    /* serializerLanesEnabled - bit per lane, [0] = Lane0 enabled, [1] = Lane1 enabled */
            .serializerLaneCrossbar = 0xE4,    /* serializerLaneCrossbar */
            .lmfcOffset = 31,                /* lmfcOffset - LMFC offset value for deterministic latency setting */
            .newSysrefOnRelink = 0,            /* newSysrefOnRelink */
            .syncbInSelect = 1,                /* syncbInSelect; */
            .overSample = 0,                    /* 1=overSample, 0=bitRepeat */
            .syncbInLvdsMode = 1,
            .syncbInLvdsPnInvert = 0,
            .enableManualLaneXbar = 0 /* 0=auto, 1=manual */
        },
        /* Deframer A settings */
        .deframerA = 
        {
            .bankId = 0,                    /* bankId extension to Device ID (Valid 0..15) */
            .deviceId = 0,                    /* deviceId  link identification number. (Valid 0..255) */
            .lane0Id = 0,                    /* lane0Id Lane0 ID. (Valid 0..31) */
            .M = 2,                            /* M  number of DACss (0, 2, or 4) - 2 DACs per transmit chain */
            .K = 32,                        /* K  #frames in a multiframe (default=32), F*K=multiple of 4. (F=2*M/numberOfLanes) */
            .scramble = 1,                    /* scramble  scrambling off if scramble= 0 */
            .externalSysref = 1,            /* externalSysref  0= use internal SYSREF, 1= external SYSREF */
            .deserializerLanesEnabled = 0x03,    /* deserializerLanesEnabled  bit per lane, [0] = Lane0 enabled */
            .deserializerLaneCrossbar = 0xE4,    /* deserializerLaneCrossbar */
            .lmfcOffset = 17,                /* lmfcOffset	 LMFC offset value to adjust deterministic latency */
            .newSysrefOnRelink = 0,            /* newSysrefOnRelink */
            .syncbOutSelect = 0,                /* SYNCBOUT0/1 select */
            .Np = 16,                /* Np (converter sample resolution) */
            .syncbOutLvdsMode = 1,
            .syncbOutLvdsPnInvert = 0,
            .syncbOutCmosSlewRate = 0,
            .syncbOutCmosDriveLevel = 0,
            .enableManualLaneXbar = 0 /* 0=auto, 1=manual */
        },
        /* Deframer B settings */
        .deframerB = 
        {
            .bankId = 0,                    /* bankId extension to Device ID (Valid 0..15) */
            .deviceId = 0,                    /* deviceId  link identification number. (Valid 0..255) */
            .lane0Id = 0,                    /* lane0Id Lane0 ID. (Valid 0..31) */
            .M = 0,                            /* M  number of DACss (0, 2, or 4) - 2 DACs per transmit chain */
            .K = 32,                        /* K  #frames in a multiframe (default=32), F*K=multiple of 4. (F=2*M/numberOfLanes) */
            .scramble = 1,                    /* scramble  scrambling off if scramble= 0 */
            .externalSysref = 1,            /* externalSysref  0= use internal SYSREF, 1= external SYSREF */
            .deserializerLanesEnabled = 0x00,    /* deserializerLanesEnabled  bit per lane, [0] = Lane0 enabled */
            .deserializerLaneCrossbar = 0xE4,    /* deserializerLaneCrossbar */
            .lmfcOffset = 0,                /* lmfcOffset	 LMFC offset value to adjust deterministic latency */
            .newSysrefOnRelink = 0,            /* newSysrefOnRelink */
            .syncbOutSelect = 1,                /* SYNCBOUT0/1 select */
            .Np = 16,                /* Np (converter sample resolution) */
            .syncbOutLvdsMode = 1,
            .syncbOutLvdsPnInvert = 0,
            .syncbOutCmosSlewRate = 0,
            .syncbOutCmosDriveLevel = 0,
            .enableManualLaneXbar = 0 /* 0=auto, 1=manual */
        },
        .serAmplitude = 15,                    /* Serializer amplitude setting. Default = 15. Range is 0..15 */
        .serPreEmphasis = 1,                /* Serializer pre-emphasis setting. Default = 1 Range is 0..4 */
        .serInvertLanePolarity = 0,            /* Serializer Lane PN inversion select. Default = 0. Where, bit[0] = 1 will invert lane [0], bit[1] = 1 will invert lane 1, etc. */
        .desInvertLanePolarity = 0,            /* Deserializer Lane PN inversion select.  bit[0] = 1 Invert PN of Lane 0, bit[1] = Invert PN of Lane 1, etc */
        .desEqSetting = 1,                    /* Deserializer Equalizer setting. Applied to all deserializer lanes. Range is 0..4 */
        .sysrefLvdsMode = 1,                /* Use LVDS inputs on Talise for SYSREF */
        .sysrefLvdsPnInvert = 0              /*0= Do not PN invert SYSREF */
    }
};

//Only needs to be called if user wants to setup AGC parameters
static taliseAgcCfg_t rxAgcCtrl =
{
    4,
    255,
    195,
    255,
    195,
    30720,  /* AGC gain update time in us (125us-250us - based on IQ data rate - set for 125us @ 245.76 Mhz) */
    10,
    10,
    16,
    0,
    1,
    0,
    0,
    0,
    1,
    31,
    246,
    4,
    1,          /*!<1- bit field to enable the multiple time constants in AGC loop for fast attack and fast recovery to max gain. */
    /* agcPower */
    {
        1,      /*!<1-bit field, enables the Rx power measurement block. */
        1,      /*!<1-bit field, allows using Rx PFIR for power measurement. */
        0,      /*!<1-bit field, allows to use the output of the second digital offset block in the Rx datapath for power measurement. */
        9,      /*!<AGC power measurement detect lower 0 threshold. Default = -12dBFS == 5, 7-bit register value where max = 0x7F, min = 0x00 */
        2,      /*!<AGC power measurement detect lower 1 threshold. Default = (offset) 4dB == 0, 4-bit register value where  max = 0xF, min = 0x00 */
        4,      /*!<AGC power measurement detect lower 0 recovery gain step. Default = 2dB - based on gain table step  size, 5-bit register value where max = 0x1F, min = 0x00 */
        4,      /*!<AGC power measurement detect lower 1 recovery gain step. Default = 4dB - based on gain table step size, 5-bit register value where max = 0x1F, min = 0x00 */
        5,      /*!< power measurement duration used by the decimated power block. Default = 0x05, 5-bit register value where max = 0x1F, min = 0x00 */
        5,      /*!<Allows power detection of data for a specific slice of the gain update counter. 16-bit register value (currently not used) */
        1,      /*!<Allows power detection of data for a specific slice of the gain update counter. 16-bit register value (currently not used) */
        5,      /*!<Allows power detection of data for a specific slice of the gain update counter. 16-bit register value (currently not used) */
        1,      /*!<Allows power detection of data for a specific slice of the gain update counter. 16-bit register value (currently not used) */
        2,      /*!<Default value should be 2*/
        0,
        0
    },
    /* agcPeak */
    {
        205,        /*!<1st update interval for the multiple time constant in AGC loop mode, Default:205. */
        2,          /*!<sets the 2nd update interval for the multiple time constant in AGC loop mode. Calculated as a multiple of  agcUnderRangeLowInterval  , Default: 4 */
        4,          /*!<sets the 3rd update interval for the multiple time constant in AGC loop mode. Calculated as a multiple of agcUnderRangeMidInterval and agcUnderRangeLowInterval, Default: 4 */
        39,         /*!<AGC APD high threshold. Default=0x1F, 6-bit register value where max=0x3F, min =0x00 */
        49,         /*!<AGC APD peak detect high threshold. default = 0x1F, 6-bit register value where max = 0x3F, min = 0x00.  Set to 3dB below apdHighThresh */
        23,         /*!<AGC APD peak detect low threshold. default = 3dB below high threshold, 6-bit register value where max =0x3F, min = 0x00 */
        19,         /*!<AGC APD peak detect low threshold. default = 3dB below high threshold, 6-bit register value where max = 0x3F, min = 0x00 . Set to 3dB below apdLowThresh  */
        6,          /*!<AGC APD peak detect upper threshold count. Default = 0x06 8-bit register value where max = 0xFF, min = 0x20  */
        3,          /*!<AGC APD peak detect lower threshold count. Default = 0x03, 8-bit register value where max = 0xFF, min = 0x00  */
        4,          /*!<AGC APD peak detect attack gain step. Default = 2dB step - based on gain table step size, 5-bit register  value, where max = 0x1F, min = 0x00  */
        2,          /*!<AGC APD gain index step size. Recommended to be same as hb2GainStepRecovery. Default = 0x00, 5-bit register value where max = 0x1F, min = 0x00  */
        1,          /*!<1-bit field, enables or disables the HB2 overload detector.  */
        1,          /*!<3-bit field. Sets the window of clock cycles (at the HB2 output rate) to meet the overload count. */
        1,          /*!<4-bit field. Sets the number of actual overloads required to trigger the overload signal.  */
        181,        /*!<AGC decimator output high threshold. Default = 0xB5, 8-bit register value where max = 0xFF, min = 0x00 */
        45,         /*!<AGC decimator output low threshold. Default = 0x80, 8-bit register value where max = 0xFF, min = 0x00 */
        90,         /*!<AGC decimator output low threshold. Default = 0x80, 8-bit register value where max = 0xFF, min = 0x00 */
        128,        /*!<AGC decimator output low threshold. Default = 0x80, 8-bit register value where max = 0xFF, min = 0x00 */
        6,          /*!<AGC HB2 output upper threshold count. Default = 0x06, 8-bit register value where max = 0xFF, min =  0x20 */
        3,          /*!<AGC HB2 output lower threshold count. Default = 0x03, 8-bit register value where max = 0xFF, min = 0x00 */
        2,          /*!<AGC decimator gain index step size. Default = 0x00, 5-bit register value where max = 0x1F, min = 0x00 */
        4,          /*!<AGC HB2 gain index step size, when the HB2 Low Overrange interval 0 triggers a programmable number  of times. Default = 0x08, 5-bit register value where max = 0x1F, min = 0x00 */
        8,          /*!<AGC HB2 gain index step size, when the HB2 Low Overrange interval 1 triggers a programmable number of times. Default = 0x04, 5-bit register value where max = 0x1F, min = 0x00 */
        4,          /*!<AGC decimator output attack gain step. Default = 2dB step - based on gain table step size, 5-bit register value, where max = 0x1F, min = 0x00 */
        1,
        0,
        0
    }
};

Thanks and Best Regards.

Parents Reply Children