Is Xilinx DMA compatible with libiio

Hi, larsc,

if attach a "xilinx dma" to a iio device(such as ad9265), is libiio compatible with it?

  • 0
    •  Analog Employees 
    on Dec 4, 2015 8:16 AM

    Hi,

    I've branched this into a new discussion since it is unrelated to the original question.

    The libiio is not tied to a specific DMA. The interface on the driver side is generic and can be implementing using any DMA. For DMA controllers that implement a DMAengine driver there is even a helper library that allows to use them for IIO device without having to write any custom code.

    - Lars

  • ,Aha, I'm glad to hear that!

    I have been stuck at the axi_dmac problem for a long period of time,

    I'll replace axi_dmac with xilinx dma conjuction with libiio, to see if this

    can help solve my problem.