libiio: "Device or resource busy" when creating buffers

Hello!

We are using an FMCOMMS4 board with the Zedboard SoC.

For our application, we're writing our software in C using libiio. Most of the work is based off the provided sample code, found here: libiio/ad9361-iiostream.c at master · analogdevicesinc/libiio · GitHub 

Here's the problem: if another program that uses the libiio buffers gets run (and even if it is closed, or even force-quit) then our program ceases to open buffers. Furthermore, if our program crashes or gets force-quit, the buffers are still rendered unavailable.

The only solution we've found is to reboot the SoC.  Reloading the iio kernel module is impossible (I think it was compiled into the kernel), and restarting iiod does not fix the problem. Killing all processes that could possibly be using libiio doesn't help.

Does anyone know how to fix this problem without rebooting the system?

P.S. For prosperity, I have attached our C code to this post.

iiowrite.c.zip
Parents
  • Hello- I have a similar problem that is actually more accurate to the thread topic so I will add it here.

    I am also modifying the ad9361-iiostream.c example as a simple experiment to create a third iio buffer.

    However I have no competing applications such as iio-oscilloscope using the resources, but console output shows that "Could not create RF buffer: Device or resource busy" on the first attempt to run the code. mahkoe seems to have successfully created the buffers , but can't open them after running another program that uses the resources.. I cant create them at all even though it is the only program I run, not even the first time after a fresh boot from power off of target and host.. I am using zc702 and FMCOMMS2.

    Console output below:

    root@analog:~/tmp# ./ad9361-iiostream
    * Acquiring IIO context
    * Acquiring AD9361 streaming devices
    * Configuring AD9361 for streaming
    * Acquiring AD9361 phy channel 0
    * Acquiring AD9361 RX lo channel
    * Acquiring AD9361 phy channel 0
    * Acquiring AD9361 TX lo channel
    * Initializing AD9361 IIO streaming channels
    * Enabling IIO streaming channels
    * Creating non-cyclic IIO buffers with 1 MiS
    * Receive buffer created
    * Transmit buffer created
    Could not create RF buffer: Device or resource busy
    * Destroying buffers
    * Disabling streaming channels
    * Destroying context

    It seems straightforward and common to create multiple buffers, can anyone see what the issue is here? I appreciate your suggestions.

    I've attached my code and anything that I thought should be modified to create the third buffer (which I call RF) is commented with //RF

    I don't see where to attach the code, so it is copied below:

    /*
    * libiio - AD9361 IIO streaming example
    *
    * Copyright (C) 2014 IABG mbH
    * Author: Michael Feilen <feilen_at_iabg.de>
    *
    * This library is free software; you can redistribute it and/or
    * modify it under the terms of the GNU Lesser General Public
    * License as published by the Free Software Foundation; either
    * version 2.1 of the License, or (at your option) any later version.
    *
    * This library is distributed in the hope that it will be useful,
    * but WITHOUT ANY WARRANTY; without even the implied warranty of
    * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
    * Lesser General Public License for more details.
    *
    **/

    #include <stdbool.h>
    #include <stdint.h>
    #include <string.h>
    #include <signal.h>
    #include <stdio.h>

    #ifdef __APPLE__
    #include <iio/iio.h>
    #else
    #include <iio.h>
    #endif

    /* helper macros */
    #define MHZ(x) ((long long)(x*1000000.0 + .5))
    #define GHZ(x) ((long long)(x*1000000000.0 + .5))

    #define ASSERT(expr) { \
    if (!(expr)) { \
    (void) fprintf(stderr, "assertion failed (%s:%d)\n", __FILE__, __LINE__); \
    (void) abort(); \
    } \
    }

    /* RX is input, TX is output */
    enum iodev { RX, TX };

    /* common RX and TX streaming params */
    struct stream_cfg {
    long long bw_hz; // Analog banwidth in Hz
    long long fs_hz; // Baseband sample rate in Hz
    long long lo_hz; // Local oscillator frequency in Hz
    const char* rfport; // Port name
    };

    /* static scratch mem for strings */
    static char tmpstr[64];

    /* IIO structs required for streaming */
    static struct iio_context *ctx = NULL;
    static struct iio_channel *rx0_i = NULL;
    static struct iio_channel *rx0_q = NULL;
    static struct iio_channel *tx0_i = NULL;
    static struct iio_channel *tx0_q = NULL;
    static struct iio_channel *rf0_i = NULL; //RF
    static struct iio_channel *rf0_q = NULL; //RF

    static struct iio_buffer *rxbuf = NULL;
    static struct iio_buffer *txbuf = NULL;

    static struct iio_buffer *rfbuf = NULL; /*RF*/

    static bool stop;

    /* cleanup and exit */
    static void shutdown()
    {
    printf("* Destroying buffers\n");
    if (rxbuf) { iio_buffer_destroy(rxbuf); }
    if (txbuf) { iio_buffer_destroy(txbuf); }
    if (rfbuf) { iio_buffer_destroy(rfbuf); } /*RF*/

    printf("* Disabling streaming channels\n");
    if (rx0_i) { iio_channel_disable(rx0_i); }
    if (rx0_q) { iio_channel_disable(rx0_q); }
    if (tx0_i) { iio_channel_disable(tx0_i); }
    if (tx0_q) { iio_channel_disable(tx0_q); }
    if (rf0_i) { iio_channel_disable(rf0_i); } //RF
    if (rf0_q) { iio_channel_disable(rf0_q); } //RF

    printf("* Destroying context\n");
    if (ctx) { iio_context_destroy(ctx); }
    exit(0);
    }

    static void handle_sig(int sig)
    {
    printf("Waiting for process to finish...\n");
    stop = true;
    }

    /* check return value of attr_write function */
    static void errchk(int v, const char* what) {
    if (v < 0) { fprintf(stderr, "Error %d writing to channel \"%s\"\nvalue may not be supported.\n", v, what); shutdown(); }
    }

    /* write attribute: long long int */
    static void wr_ch_lli(struct iio_channel *chn, const char* what, long long val)
    {
    errchk(iio_channel_attr_write_longlong(chn, what, val), what);
    }

    /* write attribute: string */
    static void wr_ch_str(struct iio_channel *chn, const char* what, const char* str)
    {
    errchk(iio_channel_attr_write(chn, what, str), what);
    }

    /* helper function generating channel names */
    static char* get_ch_name(const char* type, int id)
    {
    snprintf(tmpstr, sizeof(tmpstr), "%s%d", type, id);
    return tmpstr;
    }

    /* returns ad9361 phy device */
    static struct iio_device* get_ad9361_phy(struct iio_context *ctx)
    {
    struct iio_device *dev = iio_context_find_device(ctx, "ad9361-phy");
    ASSERT(dev && "No ad9361-phy found");
    return dev;
    }

    /* finds AD9361 streaming IIO devices */
    static bool get_ad9361_stream_dev(struct iio_context *ctx, enum iodev d, struct iio_device **dev)
    {
    switch (d) {
    case TX: *dev = iio_context_find_device(ctx, "cf-ad9361-dds-core-lpc"); return *dev != NULL;
    case RX: *dev = iio_context_find_device(ctx, "cf-ad9361-lpc"); return *dev != NULL;
    default: ASSERT(0); return false;
    }
    }

    /* finds AD9361 streaming IIO channels */
    static bool get_ad9361_stream_ch(struct iio_context *ctx, enum iodev d, struct iio_device *dev, int chid, struct iio_channel **chn)
    {
    *chn = iio_device_find_channel(dev, get_ch_name("voltage", chid), d == TX);
    if (!*chn)
    *chn = iio_device_find_channel(dev, get_ch_name("altvoltage", chid), d == TX);
    return *chn != NULL;
    }

    /* finds AD9361 phy IIO configuration channel with id chid */
    static bool get_phy_chan(struct iio_context *ctx, enum iodev d, int chid, struct iio_channel **chn)
    {
    switch (d) {
    case RX: *chn = iio_device_find_channel(get_ad9361_phy(ctx), get_ch_name("voltage", chid), false); return *chn != NULL;
    case TX: *chn = iio_device_find_channel(get_ad9361_phy(ctx), get_ch_name("voltage", chid), true); return *chn != NULL;
    default: ASSERT(0); return false;
    }
    }

    /* finds AD9361 local oscillator IIO configuration channels */
    static bool get_lo_chan(struct iio_context *ctx, enum iodev d, struct iio_channel **chn)
    {
    switch (d) {
    // LO chan is always output, i.e. true
    case RX: *chn = iio_device_find_channel(get_ad9361_phy(ctx), get_ch_name("altvoltage", 0), true); return *chn != NULL;
    case TX: *chn = iio_device_find_channel(get_ad9361_phy(ctx), get_ch_name("altvoltage", 1), true); return *chn != NULL;
    default: ASSERT(0); return false;
    }
    }

    /* applies streaming configuration through IIO */
    bool cfg_ad9361_streaming_ch(struct iio_context *ctx, struct stream_cfg *cfg, enum iodev type, int chid)
    {
    struct iio_channel *chn = NULL;

    // Configure phy and lo channels
    printf("* Acquiring AD9361 phy channel %d\n", chid);
    if (!get_phy_chan(ctx, type, chid, &chn)) { return false; }
    wr_ch_str(chn, "rf_port_select", cfg->rfport);
    wr_ch_lli(chn, "rf_bandwidth", cfg->bw_hz);
    wr_ch_lli(chn, "sampling_frequency", cfg->fs_hz);

    // Configure LO channel
    printf("* Acquiring AD9361 %s lo channel\n", type == TX ? "TX" : "RX");
    if (!get_lo_chan(ctx, type, &chn)) { return false; }
    wr_ch_lli(chn, "frequency", cfg->lo_hz);
    return true;
    }

    /* simple configuration and streaming */
    int main (int argc, char **argv)
    {
    // Streaming devices
    struct iio_device *tx;
    struct iio_device *rx;
    struct iio_device *rf; /*RF */

    // RX and TX sample counters
    size_t nrx = 0;
    size_t ntx = 0;
    size_t nrf = 0; /*RF */

    // Stream configurations
    struct stream_cfg rxcfg;
    struct stream_cfg txcfg;
    struct stream_cfg rfcfg;

    // Listen to ctrl+c and ASSERT
    signal(SIGINT, handle_sig);

    // RX stream config
    rxcfg.bw_hz = MHZ(2); // 2 MHz rf bandwidth
    rxcfg.fs_hz = MHZ(2.5); // 2.5 MS/s rx sample rate
    rxcfg.lo_hz = GHZ(2.5); // 2.5 GHz rf frequency
    rxcfg.rfport = "A_BALANCED"; // port A (select for rf freq.)

    // TX stream config
    txcfg.bw_hz = MHZ(1.5); // 1.5 MHz rf bandwidth
    txcfg.fs_hz = MHZ(2.5); // 2.5 MS/s tx sample rate
    txcfg.lo_hz = GHZ(2.5); // 2.5 GHz rf frequency
    txcfg.rfport = "A"; // port A (select for rf freq.)

    printf("* Acquiring IIO context\n");
    ASSERT((ctx = iio_create_default_context()) && "No context");
    ASSERT(iio_context_get_devices_count(ctx) > 0 && "No devices");

    printf("* Acquiring AD9361 streaming devices\n");
    ASSERT(get_ad9361_stream_dev(ctx, TX, &tx) && "No tx dev found");
    ASSERT(get_ad9361_stream_dev(ctx, RX, &rx) && "No rx dev found");
    ASSERT(get_ad9361_stream_dev(ctx, RX, &rf) && "No rf dev found"); //RF

    printf("* Configuring AD9361 for streaming\n");
    ASSERT(cfg_ad9361_streaming_ch(ctx, &rxcfg, RX, 0) && "RX port 0 not found");
    ASSERT(cfg_ad9361_streaming_ch(ctx, &txcfg, TX, 0) && "TX port 0 not found");
    //ASSERT(cfg_ad9361_streaming_ch(ctx, &rfcfg, RX, 0) && "RF port 0 not found"); // RF


    printf("* Initializing AD9361 IIO streaming channels\n");
    ASSERT(get_ad9361_stream_ch(ctx, RX, rx, 0, &rx0_i) && "RX chan i not found");
    ASSERT(get_ad9361_stream_ch(ctx, RX, rx, 1, &rx0_q) && "RX chan q not found");
    ASSERT(get_ad9361_stream_ch(ctx, TX, tx, 0, &tx0_i) && "TX chan i not found");
    ASSERT(get_ad9361_stream_ch(ctx, TX, tx, 1, &tx0_q) && "TX chan q not found");
    ASSERT(get_ad9361_stream_ch(ctx, RX, rf, 0, &rf0_i) && "RX chan i not found"); //RF
    ASSERT(get_ad9361_stream_ch(ctx, RX, rf, 1, &rf0_q) && "RX chan q not found"); //RF


    printf("* Enabling IIO streaming channels\n");
    iio_channel_enable(rx0_i);
    iio_channel_enable(rx0_q);
    iio_channel_enable(tx0_i);
    iio_channel_enable(tx0_q);
    iio_channel_enable(rf0_i); //RF
    iio_channel_enable(rf0_q); //RF


    printf("* Creating non-cyclic IIO buffers with 1 MiS\n");

    rxbuf = iio_device_create_buffer(rx, 1024, false);//RF reduce size by *1024
    if (!rxbuf) {
    perror("Could not create RX buffer");
    shutdown();
    }

    printf("* Receive buffer created\n");





    txbuf = iio_device_create_buffer(tx, 1024, false); //RF reduce size by *1024
    if (!txbuf) {
    perror("Could not create TX buffer");
    shutdown();
    }

    printf("* Transmit buffer created\n");




    //RF trouble using rx device
    rfbuf = iio_device_create_buffer(rx, 1024, false);
    if (!rfbuf) {
    perror("Could not create RF buffer");
    shutdown();
    }

    printf("* Aux buffer created\n");


    printf("* Starting IO streaming (press CTRL+C to cancel)\n");
    while (!stop)
    {
    ssize_t nbytes_rx, nbytes_tx, nbytes_rf;
    char *p_dat, *p_end;
    ptrdiff_t p_inc;

    // Schedule TX buffer
    nbytes_tx = iio_buffer_push(txbuf);
    if (nbytes_tx < 0) { printf("Error pushing buf %d\n", (int) nbytes_tx); shutdown(); }

    // Refill RX buffer
    nbytes_rx = iio_buffer_refill(rxbuf);
    if (nbytes_rx < 0) { printf("Error refilling buf %d\n",(int) nbytes_rx); shutdown(); }

    /* Refill RF buffer
    nbytes_rf = iio_buffer_refill(rfbuf);
    if (nbytes_rf < 0) { printf("Error refilling buf %d\n",(int) nbytes_rf); shutdown(); }
    */

    printf("* round 2\n");

    // READ: Get pointers to RX buf and read IQ from RX buf port 0
    p_inc = iio_buffer_step(rxbuf);
    p_end = iio_buffer_end(rxbuf);
    for (p_dat = (char *)iio_buffer_first(rxbuf, rx0_i); p_dat < p_end; p_dat += p_inc) {
    // Example: swap I and Q
    const int16_t i = ((int16_t*)p_dat)[0]; // Real (I)
    const int16_t q = ((int16_t*)p_dat)[1]; // Imag (Q)
    ((int16_t*)p_dat)[0] = q;
    ((int16_t*)p_dat)[1] = i;
    }

    // WRITE: Get pointers to TX buf and write IQ to TX buf port 0
    p_inc = iio_buffer_step(txbuf);
    p_end = iio_buffer_end(txbuf);
    for (p_dat = (char *)iio_buffer_first(txbuf, tx0_i); p_dat < p_end; p_dat += p_inc) {
    // Example: fill with zeros
    // 12-bit sample needs to be MSB alligned so shift by 4
    // wiki.analog.com/.../basic_iq_datafiles
    ((int16_t*)p_dat)[0] = 0 << 4; // Real (I)
    ((int16_t*)p_dat)[1] = 0 << 4; // Imag (Q)
    }

    // Sample counter increment and status output
    nrx += nbytes_rx / iio_device_get_sample_size(rx);
    ntx += nbytes_tx / iio_device_get_sample_size(tx);

    nrf += nbytes_rf / iio_device_get_sample_size(rf); //RF


    printf("\tRX %8.2f MSmp, TX %8.2f MSmp\n, RF %8.2f MSmp\n", nrx/1e6, ntx/1e6, nrf/1e6);
    }

    shutdown();

    return 0;
    }

Reply
  • Hello- I have a similar problem that is actually more accurate to the thread topic so I will add it here.

    I am also modifying the ad9361-iiostream.c example as a simple experiment to create a third iio buffer.

    However I have no competing applications such as iio-oscilloscope using the resources, but console output shows that "Could not create RF buffer: Device or resource busy" on the first attempt to run the code. mahkoe seems to have successfully created the buffers , but can't open them after running another program that uses the resources.. I cant create them at all even though it is the only program I run, not even the first time after a fresh boot from power off of target and host.. I am using zc702 and FMCOMMS2.

    Console output below:

    root@analog:~/tmp# ./ad9361-iiostream
    * Acquiring IIO context
    * Acquiring AD9361 streaming devices
    * Configuring AD9361 for streaming
    * Acquiring AD9361 phy channel 0
    * Acquiring AD9361 RX lo channel
    * Acquiring AD9361 phy channel 0
    * Acquiring AD9361 TX lo channel
    * Initializing AD9361 IIO streaming channels
    * Enabling IIO streaming channels
    * Creating non-cyclic IIO buffers with 1 MiS
    * Receive buffer created
    * Transmit buffer created
    Could not create RF buffer: Device or resource busy
    * Destroying buffers
    * Disabling streaming channels
    * Destroying context

    It seems straightforward and common to create multiple buffers, can anyone see what the issue is here? I appreciate your suggestions.

    I've attached my code and anything that I thought should be modified to create the third buffer (which I call RF) is commented with //RF

    I don't see where to attach the code, so it is copied below:

    /*
    * libiio - AD9361 IIO streaming example
    *
    * Copyright (C) 2014 IABG mbH
    * Author: Michael Feilen <feilen_at_iabg.de>
    *
    * This library is free software; you can redistribute it and/or
    * modify it under the terms of the GNU Lesser General Public
    * License as published by the Free Software Foundation; either
    * version 2.1 of the License, or (at your option) any later version.
    *
    * This library is distributed in the hope that it will be useful,
    * but WITHOUT ANY WARRANTY; without even the implied warranty of
    * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
    * Lesser General Public License for more details.
    *
    **/

    #include <stdbool.h>
    #include <stdint.h>
    #include <string.h>
    #include <signal.h>
    #include <stdio.h>

    #ifdef __APPLE__
    #include <iio/iio.h>
    #else
    #include <iio.h>
    #endif

    /* helper macros */
    #define MHZ(x) ((long long)(x*1000000.0 + .5))
    #define GHZ(x) ((long long)(x*1000000000.0 + .5))

    #define ASSERT(expr) { \
    if (!(expr)) { \
    (void) fprintf(stderr, "assertion failed (%s:%d)\n", __FILE__, __LINE__); \
    (void) abort(); \
    } \
    }

    /* RX is input, TX is output */
    enum iodev { RX, TX };

    /* common RX and TX streaming params */
    struct stream_cfg {
    long long bw_hz; // Analog banwidth in Hz
    long long fs_hz; // Baseband sample rate in Hz
    long long lo_hz; // Local oscillator frequency in Hz
    const char* rfport; // Port name
    };

    /* static scratch mem for strings */
    static char tmpstr[64];

    /* IIO structs required for streaming */
    static struct iio_context *ctx = NULL;
    static struct iio_channel *rx0_i = NULL;
    static struct iio_channel *rx0_q = NULL;
    static struct iio_channel *tx0_i = NULL;
    static struct iio_channel *tx0_q = NULL;
    static struct iio_channel *rf0_i = NULL; //RF
    static struct iio_channel *rf0_q = NULL; //RF

    static struct iio_buffer *rxbuf = NULL;
    static struct iio_buffer *txbuf = NULL;

    static struct iio_buffer *rfbuf = NULL; /*RF*/

    static bool stop;

    /* cleanup and exit */
    static void shutdown()
    {
    printf("* Destroying buffers\n");
    if (rxbuf) { iio_buffer_destroy(rxbuf); }
    if (txbuf) { iio_buffer_destroy(txbuf); }
    if (rfbuf) { iio_buffer_destroy(rfbuf); } /*RF*/

    printf("* Disabling streaming channels\n");
    if (rx0_i) { iio_channel_disable(rx0_i); }
    if (rx0_q) { iio_channel_disable(rx0_q); }
    if (tx0_i) { iio_channel_disable(tx0_i); }
    if (tx0_q) { iio_channel_disable(tx0_q); }
    if (rf0_i) { iio_channel_disable(rf0_i); } //RF
    if (rf0_q) { iio_channel_disable(rf0_q); } //RF

    printf("* Destroying context\n");
    if (ctx) { iio_context_destroy(ctx); }
    exit(0);
    }

    static void handle_sig(int sig)
    {
    printf("Waiting for process to finish...\n");
    stop = true;
    }

    /* check return value of attr_write function */
    static void errchk(int v, const char* what) {
    if (v < 0) { fprintf(stderr, "Error %d writing to channel \"%s\"\nvalue may not be supported.\n", v, what); shutdown(); }
    }

    /* write attribute: long long int */
    static void wr_ch_lli(struct iio_channel *chn, const char* what, long long val)
    {
    errchk(iio_channel_attr_write_longlong(chn, what, val), what);
    }

    /* write attribute: string */
    static void wr_ch_str(struct iio_channel *chn, const char* what, const char* str)
    {
    errchk(iio_channel_attr_write(chn, what, str), what);
    }

    /* helper function generating channel names */
    static char* get_ch_name(const char* type, int id)
    {
    snprintf(tmpstr, sizeof(tmpstr), "%s%d", type, id);
    return tmpstr;
    }

    /* returns ad9361 phy device */
    static struct iio_device* get_ad9361_phy(struct iio_context *ctx)
    {
    struct iio_device *dev = iio_context_find_device(ctx, "ad9361-phy");
    ASSERT(dev && "No ad9361-phy found");
    return dev;
    }

    /* finds AD9361 streaming IIO devices */
    static bool get_ad9361_stream_dev(struct iio_context *ctx, enum iodev d, struct iio_device **dev)
    {
    switch (d) {
    case TX: *dev = iio_context_find_device(ctx, "cf-ad9361-dds-core-lpc"); return *dev != NULL;
    case RX: *dev = iio_context_find_device(ctx, "cf-ad9361-lpc"); return *dev != NULL;
    default: ASSERT(0); return false;
    }
    }

    /* finds AD9361 streaming IIO channels */
    static bool get_ad9361_stream_ch(struct iio_context *ctx, enum iodev d, struct iio_device *dev, int chid, struct iio_channel **chn)
    {
    *chn = iio_device_find_channel(dev, get_ch_name("voltage", chid), d == TX);
    if (!*chn)
    *chn = iio_device_find_channel(dev, get_ch_name("altvoltage", chid), d == TX);
    return *chn != NULL;
    }

    /* finds AD9361 phy IIO configuration channel with id chid */
    static bool get_phy_chan(struct iio_context *ctx, enum iodev d, int chid, struct iio_channel **chn)
    {
    switch (d) {
    case RX: *chn = iio_device_find_channel(get_ad9361_phy(ctx), get_ch_name("voltage", chid), false); return *chn != NULL;
    case TX: *chn = iio_device_find_channel(get_ad9361_phy(ctx), get_ch_name("voltage", chid), true); return *chn != NULL;
    default: ASSERT(0); return false;
    }
    }

    /* finds AD9361 local oscillator IIO configuration channels */
    static bool get_lo_chan(struct iio_context *ctx, enum iodev d, struct iio_channel **chn)
    {
    switch (d) {
    // LO chan is always output, i.e. true
    case RX: *chn = iio_device_find_channel(get_ad9361_phy(ctx), get_ch_name("altvoltage", 0), true); return *chn != NULL;
    case TX: *chn = iio_device_find_channel(get_ad9361_phy(ctx), get_ch_name("altvoltage", 1), true); return *chn != NULL;
    default: ASSERT(0); return false;
    }
    }

    /* applies streaming configuration through IIO */
    bool cfg_ad9361_streaming_ch(struct iio_context *ctx, struct stream_cfg *cfg, enum iodev type, int chid)
    {
    struct iio_channel *chn = NULL;

    // Configure phy and lo channels
    printf("* Acquiring AD9361 phy channel %d\n", chid);
    if (!get_phy_chan(ctx, type, chid, &chn)) { return false; }
    wr_ch_str(chn, "rf_port_select", cfg->rfport);
    wr_ch_lli(chn, "rf_bandwidth", cfg->bw_hz);
    wr_ch_lli(chn, "sampling_frequency", cfg->fs_hz);

    // Configure LO channel
    printf("* Acquiring AD9361 %s lo channel\n", type == TX ? "TX" : "RX");
    if (!get_lo_chan(ctx, type, &chn)) { return false; }
    wr_ch_lli(chn, "frequency", cfg->lo_hz);
    return true;
    }

    /* simple configuration and streaming */
    int main (int argc, char **argv)
    {
    // Streaming devices
    struct iio_device *tx;
    struct iio_device *rx;
    struct iio_device *rf; /*RF */

    // RX and TX sample counters
    size_t nrx = 0;
    size_t ntx = 0;
    size_t nrf = 0; /*RF */

    // Stream configurations
    struct stream_cfg rxcfg;
    struct stream_cfg txcfg;
    struct stream_cfg rfcfg;

    // Listen to ctrl+c and ASSERT
    signal(SIGINT, handle_sig);

    // RX stream config
    rxcfg.bw_hz = MHZ(2); // 2 MHz rf bandwidth
    rxcfg.fs_hz = MHZ(2.5); // 2.5 MS/s rx sample rate
    rxcfg.lo_hz = GHZ(2.5); // 2.5 GHz rf frequency
    rxcfg.rfport = "A_BALANCED"; // port A (select for rf freq.)

    // TX stream config
    txcfg.bw_hz = MHZ(1.5); // 1.5 MHz rf bandwidth
    txcfg.fs_hz = MHZ(2.5); // 2.5 MS/s tx sample rate
    txcfg.lo_hz = GHZ(2.5); // 2.5 GHz rf frequency
    txcfg.rfport = "A"; // port A (select for rf freq.)

    printf("* Acquiring IIO context\n");
    ASSERT((ctx = iio_create_default_context()) && "No context");
    ASSERT(iio_context_get_devices_count(ctx) > 0 && "No devices");

    printf("* Acquiring AD9361 streaming devices\n");
    ASSERT(get_ad9361_stream_dev(ctx, TX, &tx) && "No tx dev found");
    ASSERT(get_ad9361_stream_dev(ctx, RX, &rx) && "No rx dev found");
    ASSERT(get_ad9361_stream_dev(ctx, RX, &rf) && "No rf dev found"); //RF

    printf("* Configuring AD9361 for streaming\n");
    ASSERT(cfg_ad9361_streaming_ch(ctx, &rxcfg, RX, 0) && "RX port 0 not found");
    ASSERT(cfg_ad9361_streaming_ch(ctx, &txcfg, TX, 0) && "TX port 0 not found");
    //ASSERT(cfg_ad9361_streaming_ch(ctx, &rfcfg, RX, 0) && "RF port 0 not found"); // RF


    printf("* Initializing AD9361 IIO streaming channels\n");
    ASSERT(get_ad9361_stream_ch(ctx, RX, rx, 0, &rx0_i) && "RX chan i not found");
    ASSERT(get_ad9361_stream_ch(ctx, RX, rx, 1, &rx0_q) && "RX chan q not found");
    ASSERT(get_ad9361_stream_ch(ctx, TX, tx, 0, &tx0_i) && "TX chan i not found");
    ASSERT(get_ad9361_stream_ch(ctx, TX, tx, 1, &tx0_q) && "TX chan q not found");
    ASSERT(get_ad9361_stream_ch(ctx, RX, rf, 0, &rf0_i) && "RX chan i not found"); //RF
    ASSERT(get_ad9361_stream_ch(ctx, RX, rf, 1, &rf0_q) && "RX chan q not found"); //RF


    printf("* Enabling IIO streaming channels\n");
    iio_channel_enable(rx0_i);
    iio_channel_enable(rx0_q);
    iio_channel_enable(tx0_i);
    iio_channel_enable(tx0_q);
    iio_channel_enable(rf0_i); //RF
    iio_channel_enable(rf0_q); //RF


    printf("* Creating non-cyclic IIO buffers with 1 MiS\n");

    rxbuf = iio_device_create_buffer(rx, 1024, false);//RF reduce size by *1024
    if (!rxbuf) {
    perror("Could not create RX buffer");
    shutdown();
    }

    printf("* Receive buffer created\n");





    txbuf = iio_device_create_buffer(tx, 1024, false); //RF reduce size by *1024
    if (!txbuf) {
    perror("Could not create TX buffer");
    shutdown();
    }

    printf("* Transmit buffer created\n");




    //RF trouble using rx device
    rfbuf = iio_device_create_buffer(rx, 1024, false);
    if (!rfbuf) {
    perror("Could not create RF buffer");
    shutdown();
    }

    printf("* Aux buffer created\n");


    printf("* Starting IO streaming (press CTRL+C to cancel)\n");
    while (!stop)
    {
    ssize_t nbytes_rx, nbytes_tx, nbytes_rf;
    char *p_dat, *p_end;
    ptrdiff_t p_inc;

    // Schedule TX buffer
    nbytes_tx = iio_buffer_push(txbuf);
    if (nbytes_tx < 0) { printf("Error pushing buf %d\n", (int) nbytes_tx); shutdown(); }

    // Refill RX buffer
    nbytes_rx = iio_buffer_refill(rxbuf);
    if (nbytes_rx < 0) { printf("Error refilling buf %d\n",(int) nbytes_rx); shutdown(); }

    /* Refill RF buffer
    nbytes_rf = iio_buffer_refill(rfbuf);
    if (nbytes_rf < 0) { printf("Error refilling buf %d\n",(int) nbytes_rf); shutdown(); }
    */

    printf("* round 2\n");

    // READ: Get pointers to RX buf and read IQ from RX buf port 0
    p_inc = iio_buffer_step(rxbuf);
    p_end = iio_buffer_end(rxbuf);
    for (p_dat = (char *)iio_buffer_first(rxbuf, rx0_i); p_dat < p_end; p_dat += p_inc) {
    // Example: swap I and Q
    const int16_t i = ((int16_t*)p_dat)[0]; // Real (I)
    const int16_t q = ((int16_t*)p_dat)[1]; // Imag (Q)
    ((int16_t*)p_dat)[0] = q;
    ((int16_t*)p_dat)[1] = i;
    }

    // WRITE: Get pointers to TX buf and write IQ to TX buf port 0
    p_inc = iio_buffer_step(txbuf);
    p_end = iio_buffer_end(txbuf);
    for (p_dat = (char *)iio_buffer_first(txbuf, tx0_i); p_dat < p_end; p_dat += p_inc) {
    // Example: fill with zeros
    // 12-bit sample needs to be MSB alligned so shift by 4
    // wiki.analog.com/.../basic_iq_datafiles
    ((int16_t*)p_dat)[0] = 0 << 4; // Real (I)
    ((int16_t*)p_dat)[1] = 0 << 4; // Imag (Q)
    }

    // Sample counter increment and status output
    nrx += nbytes_rx / iio_device_get_sample_size(rx);
    ntx += nbytes_tx / iio_device_get_sample_size(tx);

    nrf += nbytes_rf / iio_device_get_sample_size(rf); //RF


    printf("\tRX %8.2f MSmp, TX %8.2f MSmp\n, RF %8.2f MSmp\n", nrx/1e6, ntx/1e6, nrf/1e6);
    }

    shutdown();

    return 0;
    }

Children