Receiving samples from Obsrx and Rx Triggering in Pyadi-iio

Hi, 

I have managed to use pyadi-iio in both remote computer and device itself (  ZC706+AD9375) . Transmit and receive functions are okay for both remote computer and arm processor on ZC706 , thanks for the library.  I wonder two things: 

1)  Is there any easy way to receive samples  from obs-rx using the pyadi-iio.

2) Can I use a trigger signal as in the windows TES APİ with pyadi-iio . (like  AdiCmdServerClient.RXTRIGGER.EXT_SMA,  AdiCmdServerClient.RXTRIGGER.TX_LOOP) 

Thank you .

Parents Reply Children