What is the maximum sampling rate/Interface rate of AD9364?

I have been working with AD9364. I'm setting parallel port configuration register are as follows : 0x010 = 0xC8, 0x011 = 0x00, 0x012 = 0x10 mean I'm using dual port , double data rate full duplex mode.I would like to know about

1) what is the maximum interface rate that AD9364 can support?

2)will the interface rate depend on enable or disable fir filter?

Parents Reply Children