ZCU102 + AD9371 + 2018.3 SD card boot issues

Hi all,

The image works fine for some time after that I get the following error while using the AD9371 with SD card.

mmc0: Timeout waiting for hardware interrupt.
[  253.247442] mmc0: sdhci: ============ SDHCI REGISTER DUMP ===========
[  253.253866] mmc0: sdhci: Sys addr:  0x00000050 | Version:  0x00001002
[  253.260289] mmc0: sdhci: Blk size:  0x00007200 | Blk cnt:  0x00000000
[  253.266713] mmc0: sdhci: Argument:  0x00642700 | Trn mode: 0x0000002b
[  253.273137] mmc0: sdhci: Present:   0x01ff0000 | Host ctl: 0x0000001f
[  253.279561] mmc0: sdhci: Power:     0x0000000f | Blk gap:  0x00000080
[  253.285985] mmc0: sdhci: Wake-up:   0x00000000 | Clock:    0x00000207
[  253.292409] mmc0: sdhci: Timeout:   0x00000009 | Int stat: 0x00000003
[  253.298832] mmc0: sdhci: Int enab:  0x02ff008b | Sig enab: 0x02ff008b
[  253.305256] mmc0: sdhci: AC12 err:  0x00000000 | Slot int: 0x00000001
[  253.311680] mmc0: sdhci: Caps:      0x35ecc881 | Caps_1:   0x00002007
[  253.318104] mmc0: sdhci: Cmd:       0x0000193a | Max curr: 0x00000000
[  253.324528] mmc0: sdhci: Resp[0]:   0x00000900 | Resp[1]:  0x0076b27f
[  253.330951] mmc0: sdhci: Resp[2]:   0x325b5900 | Resp[3]:  0x00000900
[  253.337375] mmc0: sdhci: Host ctl2: 0x00000000
[  253.341803] mmc0: sdhci: ADMA Err:  0x00000000 | ADMA Ptr: 0x00000000700a4278
[  253.348920] mmc0: sdhci: ============================================

Seems to be an SD card issue, I changed the SD card multiple times. We have three boards here tried changing the boards too but no luck. Can someone please help me with this issue.

This is a custom image that I made using petalinux with analog devices linux (master branch) and u-boot-xlnx (2018.3).

Regards

Arjun Nadh