Queries on RSSI readback in SSH and Reading RSSI value in python script

I have 2 questions and that would be: When I use SSH to connect to the ADALM Pluto and see the RSSI value through using the command "cat in_voltage0_rssi", sometimes it displays 115.25dB or 51.75dB but most of the time it displays 51.75dB without any input power. What is the problem behind this? The 2nd question would be, if I want to read the RSSI value in a python script, what code should I write in the python script to read the RSSI value? Is it using " iio_channel_attr_read(iio_device_find_channel(phy, "voltage0",false), "rssi", &rssi)"?

Parents Reply
  • +1
    •  Analog Employees 
    on Jun 12, 2019 4:26 PM in reply to MJohn887
    So the RSSI varies according to different frequencies as well?

    Yes, the AD9363 has higher attenuation at higher frequencies.

    Is there any commands for me to access and see the lookup table of the Pluto.?

    This table does not exist on the device, you must create it in the baseband processor or host PC with external instrumentation.

    By the way, I tried terminating the Receive SMA and went to check the RSSI reading. It still displays 51.75dB.

    I've tried this on multiple devices, all read below -99 dB. RSSI gets lower at higher frequencies.

    -Travis

Children
No Data