If I am using the ADRV9361-Z7035 and ADVR1CRR-BOB how do I get an external reference to the AD9361?
There seems to be no way to apply a reference to the AD9361_CLK signal.
Thanks.
Refer schematic from below link.
https://wiki.analog.com/resources/eval/user-guides/adrv936x_rfsom/hardware
Hi Vinod,
Correct, I did see the schematic and it looks like this signal is pinned out to pin 63 on JX4. The confusing part is when plugged into JX4 on the BOB there is no way to apply a clock?
Vinod, any comment on my question below? I don't see a way to inject a clock signal to this pin?
From schematics what I understand is there is provision for external reference but that is not taken out into the break out board. So you may need to solder it out using a pigtail from the SOM board itself .
I am moving this post to Linux Software driver forum. The team there developed this board and they will be able to comment better.
That pin is routed only on the ADVR1CRR-FMC. If you want to use it on the -BOB you would need to solder a coax on that pin.