ADRV1CRR-FMC with ADRV9361 SOM - NO Output on HDMI

I have downloaded the latest linux image from

https://wiki.analog.com/resources/tools-software/linux-software/zynq_images

2018_R1

--------

There is no output on HDMI -

Following I have attached boot log on tera term -


U-Boot 2014.07-dirty (Nov 20 2014 - 17:05:21)

Board:	Xilinx Zynq
I2C:   ready
DRAM:  ECC disabled 512 MiB
MMC:   zynq_sdhci: 0
SF: Detected N25Q256A with page size 256 Bytes, erase size 4 KiB, total 32 MiB
In:    serial
Out:   serial
Err:   serial
Net:   Gem.e000b000
Hit any key to stop autoboot:  3  2  1  0 
Device: zynq_sdhci
Manufacturer ID: 1b
OEM: 534d
Name: 00000 
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 7.5 GiB
Bus Width: 4-bit
Unknown command 'load' - try 'help'
Copying Linux from SD to RAM...
reading uImage
4109416 bytes read in 358 ms (10.9 MiB/s)
reading devicetree.dtb
22214 bytes read in 18 ms (1.2 MiB/s)
libfdt fdt_setprop(): FDT_ERR_NOSPACE
Loaded AD9361 refclk frequency and model into devicetree
reading uramdisk.image.gz
** Unable to read file uramdisk.image.gz **
## Booting kernel from Legacy Image at 02080000 ...
   Image Name:   Linux-4.9.0-g2398d50
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    4109352 Bytes = 3.9 MiB
   Load Address: 00008000
   Entry Point:  00008000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 02000000
   Booting using the fdt blob at 0x2000000
   Loading Kernel Image ... OK
   Loading Device Tree to 1ed1b000, end 1ed236c5 ... OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
Booting Linux on physical CPU 0x0

Linux version 4.9.0-g2398d50 (jenkins@romlx1) (gcc version 6.2.1 20161114 (Linaro GCC Snapshot 6.2-2016.11) ) #189 SMP PREEMPT Tue Jun 26 09:52:32 IST 2018

CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

OF: fdt:Machine model: Zynq

bootconsole [earlycon0] enabled

cma: Reserved 128 MiB at 0x38000000

Memory policy: Data cache writealloc

percpu: Embedded 13 pages/cpu @ef7cc000 s23564 r8192 d21492 u53248

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260608

Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlyprintk rootfstype=ext4 rootwait

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 899640K/1048576K available (5603K kernel code, 242K rwdata, 2208K rodata, 256K init, 154K bss, 17864K reserved, 131072K cma-reserved, 131072K highmem)

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)

    vmalloc : 0xf0800000 - 0xff800000   ( 240 MB)

    lowmem  : 0xc0000000 - 0xf0000000   ( 768 MB)

    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

    modules : 0xbf000000 - 0xbfe00000   (  14 MB)

      .text : 0xc0008000 - 0xc0580f0c   (5604 kB)

      .init : 0xc07d2000 - 0xc0812000   ( 256 kB)

      .data : 0xc0812000 - 0xc084ea80   ( 243 kB)

       .bss : 0xc084ea80 - 0xc08753b4   ( 155 kB)

Preemptible hierarchical RCU implementation.

	Build-time adjustment of leaf fanout to 32.

	RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.

RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=2

NR_IRQS:16 nr_irqs:16 16

efuse mapped to f0802000

slcr mapped to f0804000

L2C: platform modifies aux control register: 0x72360000 -> 0x72760000

L2C: DT/platform modifies aux control register: 0x72360000 -> 0x72760000

L2C-310 erratum 769419 enabled

L2C-310 enabling early BRESP for Cortex-A9

L2C-310 full line of zeros enabled for Cortex-A9

L2C-310 ID prefetch enabled, offset 1 lines

L2C-310 dynamic clock gating enabled, standby mode enabled

L2C-310 cache controller enabled, 8 ways, 512 kB

L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76760001

zynq_clock_init: clkc starts at f0804100

Zynq clock init

sched_clock: 64 bits at 333MHz, resolution 3ns, wraps every 4398046511103ns

clocksource: arm_global_timer: mask: 0xffffffffffffffff max_cycles: 0x4ce07af025, max_idle_ns: 440795209040 ns

Switching to timer-based delay loop, resolution 3ns

clocksource: ttc_clocksource: mask: 0xffff max_cycles: 0xffff, max_idle_ns: 537538477 ns

timer #0 at f080c000, irq=17

Console: colour dummy device 80x30

Calibrating delay loop (skipped), value calculated using timer frequency.. 666.66 BogoMIPS (lpj=3333333)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)

Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)

CPU: Testing write buffer coherency: ok

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

Setting up static identity map for 0x82c0 - 0x8318

CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

Brought up 2 CPUs

SMP: Total of 2 processors activated (1333.33 BogoMIPS).

CPU: All CPU(s) started in SVC mode.

devtmpfs: initialized

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns

pinctrl core: initialized pinctrl subsystem

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

cpuidle: using governor ladder

hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 4 bytes.

zynq-ocm f800c000.ocmc: ZYNQ OCM pool: 256 KiB @ 0xf0880000

zynq-pinctrl 700.pinctrl: zynq pinctrl initialized

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

media: Linux media interface: v0.10

Linux video capture interface: v2.00

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

PTP clock support registered

EDAC MC: Ver: 3.0.0

Advanced Linux Sound Architecture Driver Initialized.

clocksource: Switched to clocksource arm_global_timer

NET: Registered protocol family 2

TCP established hash table entries: 8192 (order: 3, 32768 bytes)

TCP bind hash table entries: 8192 (order: 4, 65536 bytes)

TCP: Hash tables configured (established 8192 bind 8192)

UDP hash table entries: 512 (order: 2, 16384 bytes)

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Registered protocol family 1

hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available

futex hash table entries: 512 (order: 3, 32768 bytes)

workingset: timestamp_bits=30 max_order=18 bucket_order=0

bounce: pool size: 64 pages

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

dma-pl330 f8003000.dmac: Loaded driver for PL330 DMAC-241330

dma-pl330 f8003000.dmac: 	DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16

xilinx-vdma 43000000.axivdma: missing xlnx,flush-fsync property

xilinx-vdma 43000000.axivdma: missing xlnx,addrwidth property

xilinx-vdma 43000000.axivdma: Xilinx AXI VDMA Engine Driver Probed!!

e0001000.serial: ttyPS0 at MMIO 0xe0001000 (irq = 25, base_baud = 6249999) is a xuartps
àconsole [ttyPS0] enabled
console [ttyPS0] enabled

bootconsole [earlycon0] disabled
bootconsole [earlycon0] disabled

xdevcfg f8007000.devcfg: ioremap 0xf8007000 to f0875000
[drm] Initialized
brd: module loaded
loop: module loaded
m25p80 spi32765.0: SPI-NOR-UniqueID 104473f6078f00070300110054ff8d4a1b
m25p80 spi32765.0: n25q256a (32768 Kbytes)
6 ofpart partitions found on MTD device spi32765.0
Creating 6 MTD partitions on "spi32765.0":
0x000000000000-0x0000000e0000 : "qspi-fsbl-uboot"
0x0000000e0000-0x000000100000 : "qspi-uboot-env"
0x000000100000-0x000000600000 : "qspi-linux"
0x000000600000-0x000000620000 : "qspi-device-tree"
0x000000620000-0x000001300000 : "qspi-rootfs"
0x000001300000-0x000002000000 : "qspi-bitstream"
MACsec IEEE 802.1AE
libphy: Fixed MDIO Bus: probed
libphy: mdio_driver_register: xgmiitorgmii
tun: Universal TUN/TAP device driver, 1.6
tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
libphy: MACB_mii_bus: probed
macb e000b000.ethernet eth0: Cadence GEM rev 0x00020118 at 0xe000b000 irq 28 (00:02:b5:01:c6:b7)
Marvell 88E1510 e000b000.etherne:00: attached PHY driver [Marvell 88E1510] (mii_bus:phy_addr=e000b000.etherne:00, irq=-1)
macb e000c000.ethernet: invalid hw address, using random
libphy: MACB_mii_bus: probed
mdio_bus e000c000.etherne:08: mdio_device_register
xgmiitorgmii e000c000.etherne:08: Couldn't find phydev
macb e000c000.ethernet eth1: Cadence GEM rev 0x00020118 at 0xe000c000 irq 29 (1a:ea:6d:f8:f5:51)
Marvell 88E1510 e000c000.etherne:01: attached PHY driver [Marvell 88E1510] (mii_bus:phy_addr=e000c000.etherne:01, irq=-1)
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usbserial
usbcore: registered new interface driver usbserial_generic
usbserial: USB Serial support registered for generic
usbcore: registered new interface driver ftdi_sio
usbserial: USB Serial support registered for FTDI USB Serial Device
e0002000.usb supply vbus not found, using dummy regulator
ULPI transceiver vendor/product ID 0x0424/0x0007
Found SMSC USB3320 ULPI transceiver.
ULPI integrity check: passed.
ci_hdrc ci_hdrc.0: EHCI Host Controller
ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
i2c /dev entries driver
i2c i2c-0: Added multiplexed i2c bus 1
i2c i2c-0: Added multiplexed i2c bus 2
i2c i2c-0: Added multiplexed i2c bus 3
i2c i2c-0: Added multiplexed i2c bus 4
i2c i2c-0: Added multiplexed i2c bus 5
at24 6-0050: 4096 byte 24c32 EEPROM, writable, 1 bytes/write
i2c i2c-0: Added multiplexed i2c bus 6
i2c i2c-0: Added multiplexed i2c bus 7
i2c i2c-0: Added multiplexed i2c bus 8
pca954x 0-0070: registered 8 multiplexed busses for I2C switch pca9548
usbcore: registered new interface driver uvcvideo
USB Video Class driver (1.1.1)
gspca_main: v2.14.0 registered
cdns-wdt f8005000.watchdog: Xilinx Watchdog Timer at f090e000 with timeout 10s
Xilinx Zynq CpuIdle Driver started
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc0: SDHCI controller on e0100000.sdhci [e0100000.sdhci] using DMA
ledtrig-cpu: registered to indicate activity on CPUs
hidraw: raw HID events driver (C) Jiri Kosina
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
ad9361 spi32766.0: ad9361_probe : enter (ad9361)
random: fast init done
mmc0: new high speed SDHC card at address 59b4
mmcblk0: mmc0:59b4 00000 7.48 GiB 
 mmcblk0: p1 p2
ad9361 spi32766.0: ad9361_probe : AD936x Rev 2 successfully initialized
ad9517 spi32766.1: AD9517 successfully initialized
cf_axi_dds 79024000.cf-ad9361-dds-core-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.00.b) at 0x79024000 mapped to 0xf09ac000, probed DDS AD9361
NET: Registered protocol family 17
Registering SWP/SWPB emulation handler
Console: switching to colour frame buffer device 128x48
axi-hdmi 70e00000.axi_hdmi: fb0:  frame buffer device
[drm] Initialized axi_hdmi_drm 1.0.0 20120930 on minor 0
EDID block is all zeroes
axi-hdmi 70e00000.axi_hdmi: HDMI-A-1: EDID block 0 invalid.
cf_axi_adc 79020000.cf-ad9361-lpc: ADI AIM (10.00.b) at 0x79020000 mapped to 0xf0cd8000, probed ADC AD9361 as MASTER
asoc-simple-card adv7511_hdmi_snd: hdmi-hifi.0 <-> 75c00000.axi-spdif-tx mapping ok
asoc-simple-card zed_sound: adau-hifi <-> 77600000.axi-i2s mapping ok
input: gpio_keys as /devices/soc0/gpio_keys/input/input0
hctosys: unable to open rtc device (rtc0)
ALSA device list:
  #0: HDMI monitor
  #1: ZED ADAU1761
EXT4-fs (mmcblk0p2): recovery complete
EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
VFS: Mounted root (ext4 filesystem) on device 179:2.
devtmpfs: mounted
Freeing unused kernel memory: 256K (c07d2000 - c0812000)
This architecture does not have kernel memory protection.
Mount failed for selinuxfs on /sys/fs/selinux:  No such file or directory
init: hwclock main process (920) terminated with status 1
systemd-udevd[1384]: could not open moddep file '/lib/modules/4.9.0-g2398d50/modules.dep.bin'
 * Setting up X socket directories...        
[ OK ]
 * STARTDISTCC is set to false in /etc/default/distcc
 * /usr/bin/distccd not starting
 * Starting IIO Daemon iiod        
[ OK ]


Last login: Thu Jan  1 00:00:13 UTC 1970 on tty1
Welcome to Linaro 14.04 (GNU/Linux 4.9.0-g2398d50 armv7l)

 * Documentation:  https://wiki.analog.com/ https://ez.analog.com/

New release '16.04.4 LTS' available.
Run 'do-release-upgrade' to upgrade to it.

78root@analog:~# 

Can I know what is the issue?

Regards
Kashyap