Jesd Eye scan gtk: eyescan_info does not exist

Hi Analog.

I've build the Jesd eye scan application ( latest commit ) on a clean UB18 VM,  mounted the target device trough sshfs but I can't seem t get a connection with the target JESD device

The file on target: eyescan_info does not exist but the devices are present in the file system.

One thing I've noticed: The "display" drop down menu stays empty.

Any ideas about this? Any help would be welcome

Thanks


Deville

zynqdev@ubuntu:~$ ls mnt/sys/bus/platform/devices/84a60000.axi-adxcvr-rx/
driver  driver_override  modalias  of_node  power  subsystem  uevent

Parents
  • 0
    •  Analog Employees 
    on Apr 26, 2019 3:04 PM

    You need to use at least our 2018_R2 or master linux branch:

    root@analog:~# ls -al /sys/bus/platform/devices/84a60000.axi-adxcvr-rx/
    total 0
    drwxr-xr-x 3 root root 0 Apr 26 15:01 .
    drwxr-xr-x 18 root root 0 Apr 26 14:53 ..
    lrwxrwxrwx 1 root root 0 Apr 26 15:01 driver -> ../../../../bus/platform/drivers/axi_adxcvr
    -rw-r--r-- 1 root root 4096 Apr 26 15:01 driver_override
    -rw-r--r-- 1 root root 4096 Apr 26 15:01 enable
    -r--r--r-- 1 root root 2091000 Apr 26 15:01 eye_data
    -r--r--r-- 1 root root 4096 Apr 26 14:53 eyescan_info
    -r--r--r-- 1 root root 4096 Apr 26 15:01 modalias
    lrwxrwxrwx 1 root root 0 Apr 26 15:01 of_node -> ../../../../firmware/devicetree/base/fpga-axi@0/axi-adxcvr-rx@84a60000
    drwxr-xr-x 2 root root 0 Apr 26 15:01 power
    -rw-r--r-- 1 root root 4096 Apr 26 15:01 prescale
    -rw------- 1 root root 4096 Apr 26 15:01 reg_access
    lrwxrwxrwx 1 root root 0 Apr 26 15:01 subsystem -> ../../../../bus/platform
    -rw-r--r-- 1 root root 4096 Apr 26 14:53 uevent

  • Hi

    Thanks for your reply.  The SD card on the ZCU102 has been provided with a Linux build with checkout tag  c2041af164e2 there has been a few updates in the branch since. I don't know if it matters

    The eyscan application is build from the latest master commit.

    | | | | * b9e70649ae9a (HEAD -> 2018_R2, origin/2018_R2) net: ethernet: xilinx: Revert ADI's fixes
    | | | | * 1de0d0bbf63a arm: dts: adi-fmcomms11.dtsi: Fix location of fixed-factor-clock
    | | | | * 5ff896cb85a4 spi: spi-axi-engine: Fix buffer address incrementation
    | | | | * 042b7b12a5e9 staging: iio: ad7192: Fix ad7193 channel address
    | | | | * df76e4d45f53 iio: adc: ad9361: Fix max filter HB rates and update the available attr.
    | | | | * dc7a1f8d3fa9 firmware/TaliseStream.bin: Update Talise stream
    | | | | * 69b34672a1e2 iio: adc: adrv9009: Update for Filter Wizard Ver. 2.3
    | | | | * 10503d413d5e firmware/Talise*: Update Firmware to ARM Revision: 6.0.2
    | | | | * 9dc40bad2090 iio: adc: talise: Update Talise API version: 3.6.0.5
    | | | | * 67e707275528 iio: adc: talise: Remove unused files
    | | | | * 54af1a584c68 arm: configs: zynq_pluto_defconfig: Enable USB_NET_CDCETHER and RNDIS_HOST
    | | | | * 9775cb505906 iio: adc: ad9361: Fix bug in ad9361_gt_bin_read()
    | | | | * c2041af164e2 arm: configs: zynq_pluto_defconfig: Enable ext4 filesystem support

    Still no success but I see @JV-IE having the same issues. I'm in the process of building a new kernel with the latest tag.

    Until then I'm watching this thread ;-) Carry on boys ...

Reply
  • Hi

    Thanks for your reply.  The SD card on the ZCU102 has been provided with a Linux build with checkout tag  c2041af164e2 there has been a few updates in the branch since. I don't know if it matters

    The eyscan application is build from the latest master commit.

    | | | | * b9e70649ae9a (HEAD -> 2018_R2, origin/2018_R2) net: ethernet: xilinx: Revert ADI's fixes
    | | | | * 1de0d0bbf63a arm: dts: adi-fmcomms11.dtsi: Fix location of fixed-factor-clock
    | | | | * 5ff896cb85a4 spi: spi-axi-engine: Fix buffer address incrementation
    | | | | * 042b7b12a5e9 staging: iio: ad7192: Fix ad7193 channel address
    | | | | * df76e4d45f53 iio: adc: ad9361: Fix max filter HB rates and update the available attr.
    | | | | * dc7a1f8d3fa9 firmware/TaliseStream.bin: Update Talise stream
    | | | | * 69b34672a1e2 iio: adc: adrv9009: Update for Filter Wizard Ver. 2.3
    | | | | * 10503d413d5e firmware/Talise*: Update Firmware to ARM Revision: 6.0.2
    | | | | * 9dc40bad2090 iio: adc: talise: Update Talise API version: 3.6.0.5
    | | | | * 67e707275528 iio: adc: talise: Remove unused files
    | | | | * 54af1a584c68 arm: configs: zynq_pluto_defconfig: Enable USB_NET_CDCETHER and RNDIS_HOST
    | | | | * 9775cb505906 iio: adc: ad9361: Fix bug in ad9361_gt_bin_read()
    | | | | * c2041af164e2 arm: configs: zynq_pluto_defconfig: Enable ext4 filesystem support

    Still no success but I see @JV-IE having the same issues. I'm in the process of building a new kernel with the latest tag.

    Until then I'm watching this thread ;-) Carry on boys ...

Children