Can't IIC Oscilloscope Windows 10 version with ZCU102+ADRV9009

I have a ZCU102 and an ADRV9009.

I followed this

https://wiki.analog.com/resources/eval/user-guides/adrv9009/quickstart/zynqmp

And run the commands 

root@analog:~# iio_info | grep iio:device
iio:device3: adrv9009-phy
iio:device1: ad9528-1
iio:device6: axi-adrv9009-rx-hpc (buffer capable)
iio:device4: axi-adrv9009-rx-obs-hpc (buffer capable)
iio:device2: ad7291
iio:device0: ams
iio:device5: axi-adrv9009-tx-hpc (buffer capable)

root@analog:~# fru-dump -b /sys/bus/i2c/devices/16-0050/eeprom
read 256 bytes from /sys/bus/i2c/devices/16-0050/eeprom
Date of Man : Wed Aug 30 14:05:00 2017
Manufacturer : Analog Devices
Product Name : 9379RC0,9528
Serial Number : 1716630014
Part Number : 9379
FRU File ID : Empty Field
PCB Rev : 01B
PCB ID : 9379CE01B
Uses LVDS : Y

Then I would like to use the IIO  Oscillscope on my PC connected with Ethernet to the ZCU102+ADRV9009.

What IP address to use to connect to ZCU102 ?

Thanks

Parents Reply Children