ERROR: 4: TALISE_loadArmFromBinary(): ARM unknown error during bootup

Getting this error running the headless example program.  The radioStatus value that was read from the device comes back 0xFF, thus the error at line 442 in talise_arm.c.  No other errors or warnings up to that point.  It does continue on but then throws another error "Talise init calibration error encountered" during the TALISE_checkInitCalComplete() function.  Probably meaningless since it appears that the boot didn't happen.  The binaries used to load the device came from the Analog Devices linux repo on the 2018_R1 branch.

I can provide the talise_config.c file if needed.

    - Brad