iio:device0: SPI Read Verify failed (0x0) problem on custom carrier and ad9234 evaluation board

Hi,

I am trying to build a custom  design for the ad9234 evaluation board on a custom zynq-7000 carrier board. While going through hdl design and building my custom linux and devicetree I am now working on the SPI communication.

When I do "dmesg | grep spi" ig got the following output : iio iio:device0: SPI Read Verify failed (0x0) what might causing  this message?

I think I have a proper SPI communication, the signals looking good and I fixed an error where my linux read 0xCE it handled it as wrong device (this was because of the wrong devicetree driver settings for the ADC) But no I got the IIO error.

Here are the main parts devicetree I am using right now:

#include <dt-bindings/iio/frequency/ad9528.h>

/ {
	clocks {

	};
};

&fmc_spi {

	adc0_ad9234: ad9234@0 {
			#address-cells = <1>;
			#size-cells = <0>;
			compatible = "adi,ad9234";
			reg = <0>;
			spi-max-frequency = <1000000>;
			spi-cpol;
			spi-cpha;
			//adi,master-slave-2x-quirk;
			clocks = <&axi_ad9680_jesd_rx_axi>, <&clk0_ad9528 13>, <&clk0_ad9528 12>;
			clock-names = "jesd_adc_clk", "adc_clk", "adc_sysref";
	};

	clk0_ad9528: ad9528-1@1 {
		#address-cells = <1>;
		#size-cells = <0>;
		#clock-cells = <1>;
		compatible = "ad9528";

		spi-cpol;
		spi-cpha;
		spi-max-frequency = <10000000>;
		adi,spi-3wire-enable;
		reg = <1>;

		clock-output-names = "ad9528-1_out0", "ad9528-1_out1", "ad9528-1_out2", "ad9528-1_out3", "ad9528-1_out4", "ad9528-1_out5", "ad9528-1_out6", "ad9528-1_out7", "ad9528-1_out8", "ad9528-1_out9", "ad9528-1_out10", "ad9528-1_out11", "ad9528-1_out12", "ad9528-1_out13";
		adi,vcxo-freq = <122880000>;

		adi,refa-enable;
		adi,refa-diff-rcv-enable;
		adi,refa-r-div = <1>;
		adi,osc-in-cmos-neg-inp-enable;

		/* PLL1 config */
		adi,pll1-feedback-div = <4>;
		adi,pll1-charge-pump-current-nA = <5000>;


		/* PLL2 config */
		adi,pll2-vco-div-m1 = <3>; /* use 5 for 184320000 output device clock */
		adi,pll2-n2-div = <10>; /* N / M1 */
		adi,pll2-r1-div = <1>;
		adi,pll2-charge-pump-current-nA = <805000>;

		/* SYSREF config */
		adi,sysref-src = <SYSREF_SRC_INTERNAL>;
		adi,sysref-pattern-mode = <SYSREF_PATTERN_CONTINUOUS>;
		adi,sysref-k-div = <512>;
		adi,sysref-request-enable;
		adi,sysref-nshot-mode = <SYSREF_NSHOT_4_PULSES>;
		adi,sysref-request-trigger-mode = <SYSREF_LEVEL_HIGH>;

		adi,rpole2 = <RPOLE2_900_OHM>;
		adi,rzero = <RZERO_1850_OHM>;
		adi,cpole1 = <CPOLE1_16_PF>;

		adi,status-mon-pin0-function-select = <1>; /* PLL1 & PLL2 Locked */
		adi,status-mon-pin1-function-select = <7>; /* REFA Correct */

		ad9528_0_c13: channel@13 {
			reg = <13>;
			adi,extended-name = "DEV_CLK";
			adi,driver-mode = <DRIVER_MODE_LVDS>;
			adi,divider-phase = <0>;
			adi,channel-divider = <10>;
			adi,signal-source = <SOURCE_VCO>;
		};

		ad9528_0_c1: channel@1 {
			reg = <1>;
			adi,extended-name = "FMC_CLK";
			adi,driver-mode = <DRIVER_MODE_LVDS>;
			adi,divider-phase = <0>;
			adi,channel-divider = <10>;
			adi,signal-source = <SOURCE_VCO>;
		};

		ad9528_0_c12: channel@12 {
			reg = <12>;
			adi,extended-name = "DEV_SYSREF";
			adi,driver-mode = <DRIVER_MODE_LVDS>;
			adi,divider-phase = <0>;
			adi,channel-divider = <10>;
			adi,signal-source = <SOURCE_SYSREF_VCO>;
		};

		ad9528_0_c3: channel@3 {
			reg = <3>;
			adi,extended-name = "FMC_SYSREF";
			adi,driver-mode = <DRIVER_MODE_LVDS>;
			adi,divider-phase = <0>;
			adi,channel-divider = <10>;
			adi,signal-source = <SOURCE_SYSREF_VCO>;
		};
	};
};

/*
 * CAUTION: This file is automatically generated by Xilinx.
 * Version:  
 * Today is: Thu Oct 11 09:51:08 2018
 */


/ {
	amba_pl: amba_pl {
		#address-cells = <1>;
		#size-cells = <1>;
		compatible = "simple-bus";
		ranges ;
		
		axi_ad9680_dma: axi_dmac@7c400000 {
			compatible = "adi,axi-dmac-1.00.a";
			reg = <0x7c400000 0x1000>;

			#dma-cells = <1>;
			interrupts = <0 57 0>;
			clocks = <&clkc 16>;

			dma-channel {
				adi,source-bus-width = <64>;
				adi,destination-bus-width = <64>;
				adi,type = <0>;
			};
		};

		axi_ad9680_core: axi_ad9680@44a10000 {
			compatible = "xlnx,axi-ad9234-1.00.a";
			reg = <0x44a10000 0x10000>;
			dmas = <&axi_ad9680_dma 0>;
			dma-names = "rx";
			spibus-connected = <&adc0_ad9234>;
		};
		
		axi_ad9680_jesd_rx_axi: axi_jesd204_rx@44aa0000 {
			compatible = "adi,axi-jesd204-rx-1.0";
			reg = <0x44aa0000 0x4000>;

			interrupt-names = "irq";
			interrupt-parent = <&intc>;
			interrupts = <0 59 4>;
			

			clocks = <&clkc 16>, <&axi_ad9680_xcvr 1>, <&axi_ad9680_xcvr 0>;
			clock-names = "s_axi_aclk", "device_clk", "lane_clk";

			adi,octets-per-frame = <1>;
			adi,frames-per-multiframe = <32>;
			adi,converter-resolution = <12>;
			adi,bits-per-sample = <16>;
			adi,converters-per-device = <1>;

			#clock-cells = <0>;
			clock-output-names = "jesd_adc_lane_clk";
		};
		axi_ad9680_xcvr: axi_adxcvr@44a50000 {
			compatible = "adi,axi-adxcvr-1.0";
			reg = <0x44a50000 0x10000>;

			clocks = <&clk0_ad9528 1>;
			clock-names = "conv";

			#clock-cells = <1>;
			clock-output-names = "adc_gt_clk", "rx_out_clk";

			adi,sys-clk-select = <0>;
			adi,out-clk-select = <8>;
			adi,use-lpm-enable;
			adi,use-cpll-enable;
		};
	};
};

Thanks,

Nils

Parents
  • For Information, this is the whole dmesg output after booting the system:

    Booting Linux on physical CPU 0x0
    Linux version 4.9.0-xilinx-g7cf8748-dirty (nils@parallels-vm) (gcc version 5.4.0 20160609 (Ubuntu/Linaro 5.4.0-6ubuntu1~16.04.9) ) #3 SMP PREEMPT Wed Oct 10 10:28:34 CEST 2018
    CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
    CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    OF: fdt:Machine model: xlnx,zynq-7000
    bootconsole [earlycon0] enabled
    cma: Reserved 16 MiB at 0x3f000000
    Memory policy: Data cache writealloc
    On node 0 totalpages: 262144
    free_area_init_node: node 0, pgdat c092f400, node_mem_map ef7f7000
      Normal zone: 1536 pages used for memmap
      Normal zone: 0 pages reserved
      Normal zone: 196608 pages, LIFO batch:31
      HighMem zone: 65536 pages, LIFO batch:15
    percpu: Embedded 14 pages/cpu @ef7d1000 s25932 r8192 d23220 u57344
    pcpu-alloc: s25932 r8192 d23220 u57344 alloc=14*4096
    pcpu-alloc: [0] 0 [0] 1 
    Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260608
    Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlyprintk rootfstype=ext4 rootwait
    PID hash table entries: 4096 (order: 2, 16384 bytes)
    Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
    Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
    Memory: 1009116K/1048576K available (5120K kernel code, 192K rwdata, 1356K rodata, 1024K init, 214K bss, 23076K reserved, 16384K cma-reserved, 245760K highmem)
    Virtual kernel memory layout:
        vector  : 0xffff0000 - 0xffff1000   (   4 kB)
        fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
        vmalloc : 0xf0800000 - 0xff800000   ( 240 MB)
        lowmem  : 0xc0000000 - 0xf0000000   ( 768 MB)
        pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
        modules : 0xbf000000 - 0xbfe00000   (  14 MB)
          .text : 0xc0008000 - 0xc0600000   (6112 kB)
          .init : 0xc0800000 - 0xc0900000   (1024 kB)
          .data : 0xc0900000 - 0xc0930000   ( 192 kB)
           .bss : 0xc0930000 - 0xc0965a38   ( 215 kB)
    Preemptible hierarchical RCU implementation.
    	Build-time adjustment of leaf fanout to 32.
    	RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
    RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=2
    NR_IRQS:16 nr_irqs:16 16
    efuse mapped to f0801000
    slcr mapped to f0803000
    L2C: platform modifies aux control register: 0x72360000 -> 0x72760000
    L2C: DT/platform modifies aux control register: 0x72360000 -> 0x72760000
    L2C-310 erratum 769419 enabled
    L2C-310 enabling early BRESP for Cortex-A9
    L2C-310 full line of zeros enabled for Cortex-A9
    L2C-310 ID prefetch enabled, offset 1 lines
    L2C-310 dynamic clock gating enabled, standby mode enabled
    L2C-310 cache controller enabled, 8 ways, 512 kB
    L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76760001
    zynq_clock_init: clkc starts at f0803100
    Zynq clock init
    sched_clock: 64 bits at 333MHz, resolution 3ns, wraps every 4398046511103ns
    clocksource: arm_global_timer: mask: 0xffffffffffffffff max_cycles: 0x4ce07af025, max_idle_ns: 440795209040 ns
    Switching to timer-based delay loop, resolution 3ns
    clocksource: ttc_clocksource: mask: 0xffff max_cycles: 0xffff, max_idle_ns: 537538477 ns
    timer #0 at f080b000, irq=17
    Console: colour dummy device 80x30
    Calibrating delay loop (skipped), value calculated using timer frequency.. 666.66 BogoMIPS (lpj=3333333)
    pid_max: default: 32768 minimum: 301
    Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
    Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
    CPU: Testing write buffer coherency: ok
    CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
    Setting up static identity map for 0x100000 - 0x100058
    CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
    Brought up 2 CPUs
    SMP: Total of 2 processors activated (1333.33 BogoMIPS).
    CPU: All CPU(s) started in SVC mode.
    devtmpfs: initialized
    VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
    clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
    pinctrl core: initialized pinctrl subsystem
    NET: Registered protocol family 16
    DMA: preallocated 256 KiB pool for atomic coherent allocations
    cpuidle: using governor menu
    hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
    hw-breakpoint: maximum watchpoint size is 4 bytes.
    zynq-ocm f800c000.ocmc: ZYNQ OCM pool: 256 KiB @ 0xf0880000
    zynq-pinctrl 700.pinctrl: zynq pinctrl initialized
    vgaarb: loaded
    SCSI subsystem initialized
    usbcore: registered new interface driver usbfs
    usbcore: registered new interface driver hub
    usbcore: registered new device driver usb
    pps_core: LinuxPPS API ver. 1 registered
    pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    PTP clock support registered
    EDAC MC: Ver: 3.0.0
    FPGA manager framework
    fpga-region fpga-full: FPGA Region probed
    clocksource: Switched to clocksource arm_global_timer
    NET: Registered protocol family 2
    TCP established hash table entries: 8192 (order: 3, 32768 bytes)
    TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
    TCP: Hash tables configured (established 8192 bind 8192)
    UDP hash table entries: 512 (order: 2, 16384 bytes)
    UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
    NET: Registered protocol family 1
    RPC: Registered named UNIX socket transport module.
    RPC: Registered udp transport module.
    RPC: Registered tcp transport module.
    RPC: Registered tcp NFSv4.1 backchannel transport module.
    PCI: CLS 0 bytes, default 64
    Trying to unpack rootfs image as initramfs...
    Freeing initrd memory: 4788K (dfb53000 - e0000000)
    hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
    futex hash table entries: 512 (order: 3, 32768 bytes)
    workingset: timestamp_bits=30 max_order=18 bucket_order=0
    jffs2: version 2.2. (NAND) (SUMMARY)  © 2001-2006 Red Hat, Inc.
    bounce: pool size: 64 pages
    io scheduler noop registered
    io scheduler deadline registered
    io scheduler cfq registered (default)
    dma-pl330 f8003000.dmac: Loaded driver for PL330 DMAC-241330
    dma-pl330 f8003000.dmac: 	DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16
    e0000000.serial: ttyPS0 at MMIO 0xe0000000 (irq = 25, base_baud = 6249999) is a xuartps
    console [ttyPS0] enabled
    bootconsole [earlycon0] disabled
    [drm] Initialized
    brd: module loaded
    loop: module loaded
    libphy: Fixed MDIO Bus: probed
    libphy: MACB_mii_bus: probed
    macb e000b000.ethernet eth0: Cadence GEM rev 0x00020118 at 0xe000b000 irq 28 (00:0a:35:00:01:22)
    Marvell 88E1510 e000b000.etherne:00: attached PHY driver [Marvell 88E1510] (mii_bus:phy_addr=e000b000.etherne:00, irq=-1)
    e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
    e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
    ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    ehci-pci: EHCI PCI platform driver
    usbcore: registered new interface driver usb-storage
    e0002000.usb supply vbus not found, using dummy regulator
    ULPI transceiver vendor/product ID 0x0424/0x0007
    Found SMSC USB3320 ULPI transceiver.
    ULPI integrity check: passed.
    ci_hdrc ci_hdrc.0: EHCI Host Controller
    ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
    ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
    hub 1-0:1.0: USB hub found
    hub 1-0:1.0: 1 port detected
    mousedev: PS/2 mouse device common for all mice
    i2c /dev entries driver
    cdns-wdt f8005000.watchdog: Xilinx Watchdog Timer at f0990000 with timeout 10s
    EDAC MC: ECC not enabled
    Xilinx Zynq CpuIdle Driver started
    sdhci: Secure Digital Host Controller Interface driver
    sdhci: Copyright(c) Pierre Ossman
    sdhci-pltfm: SDHCI platform and OF driver helper
    mmc0: SDHCI controller on e0100000.sdhci [e0100000.sdhci] using ADMA
    ledtrig-cpu: registered to indicate activity on CPUs
    usbcore: registered new interface driver usbhid
    usbhid: USB HID core driver
    spi1.1 supply vcc not found, using dummy regulator
    iio iio:device0: SPI Read Verify failed (0x0)
    ad9528: probe of spi1.1 failed with error -5
    fpga_manager fpga0: Xilinx Zynq FPGA Manager registered
    NET: Registered protocol family 10
    sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    NET: Registered protocol family 17
    Registering SWP/SWPB emulation handler
    of_cfs_init
    mmc0: new high speed SDHC card at address 0001
    of_cfs_init: OK
    mmcblk0: mmc0:0001 SD16G 14.6 GiB 
    Freeing unused kernel memory: 1024K (c0800000 - c0900000)
     mmcblk0: p1 p2
    usb 1-1: new high-speed USB device number 2 using ci_hdrc
    EXT4-fs (mmcblk0p2): recovery complete
    EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    hub 1-1:1.0: USB hub found
    hub 1-1:1.0: 4 ports detected
    FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
    random: dd: uninitialized urandom read (512 bytes read)
    IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
    macb e000b000.ethernet eth0: link up (1000/Full)
    IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
    random: dropbearkey: uninitialized urandom read (32 bytes read)
    random: dropbearkey: uninitialized urandom read (32 bytes read)
    random: dropbearkey: uninitialized urandom read (32 bytes read)
    random: dropbear: uninitialized urandom read (32 bytes read)
    random: tcf-agent: uninitialized urandom read (16 bytes read)
    random: dropbear: uninitialized urandom read (32 bytes read)
    random: dropbear: uninitialized urandom read (32 bytes read)

Reply Children