ADRV9361-Z7035 U-Boot default configuration

Hey,

I was wondering if there is a branch of the xilinx/u-boot-xlnx which contans the defconfig for this hardware in the breakout board? I searched in https://github.com/analogdevicesinc/u-boot-xlnx to no avail.

Will one for another zynq board work? Such as a zedboard?

Thanks

Parents Reply
  • image:
    {
        [bootloader]./fsbl.elf
        ./system.bit
        ./u-boot.elf
        [load=0x300000]./buildroot.itb
    }

    Where the buildroot.its file is,

    /*
     * Simple U-boot uImage source file containing a single kernel and FDT blob
     *
    github.com/.../source_file_format.txt
     * www.systutorials.com/.../
     */

    /dts-v1/;

    / {
        description = "Simple image with single Linux kernel and FDT blob";
        #address-cells = <1>;

        images {
            kernel@1 {
                description = "Linux kernel";
                data = /incbin/("./buildroot/output/images/zImage");
                type = "kernel";
                arch = "arm";
                os = "linux";
                compression = "none";
                load = <0x1000000>;
                entry = <0x1000000>;
                hash@1 {
                    algo = "crc32";
                };
            };
            initramfs@1 {
                description = "Initramfs";
                data = /incbin/("./buildroot/output/images/rootfs.cpio.xz");
                type = "ramdisk";
                arch = "arm";
                os = "linux";
                load = <0x1500000>;
                entry = <0x1500000>;
                compression = "gzip";
                hash@1 {
                    algo = "crc32";
                };
            };
            fdt@1 {
                description = "Flattened Device Tree blob";
                data = /incbin/("./buildroot/output/images/dtb.dtb");
                type = "flat_dt";
                arch = "arm";
                compression = "none";
                hash@1 {
                    algo = "crc32";
                };
            };
        };

        configurations {
            default = "conf@1";
            conf@1 {
                description = "Boot Linux kernel with FDT blob";
                kernel = "kernel@1";
                ramdisk = "initramfs@1";
                fdt = "fdt@1";
            };
        };
    };

    EDIT:

    Tried ditching the dts and using only a bif and matching the address offsets in the dtsi to the same result. uImage was generated using the 0x100000 offset.

    image:
    {
        [bootloader]./fsbl.elf
        ./u-boot.elf
        [load=0x100000]../../buildroot/output/images/uImage
        [load=0x600000]../../buildroot/output/images/dtb.dtb
        [load=0x620000]../../buildroot/output/images/rootfs.cpio.xz
        [load=0x1300000]./system.bit
    }

Children