when using analog devices meta-adi, Petalinux ERROR: Failed to create workspace directory

Hi, I worked with petalinux-v2019.2 + vivado-v2019.2(.xsa file) 

I used analog devices referance design. When I configured the project, it failed.

[INFO] generating Kconfig for project
[INFO] menuconfig project


*** End of the configuration.
*** Execute 'make' to start the build or try 'make help'.

[INFO] sourcing bitbake
[INFO] generating plnxtool conf
[INFO] generating meta-plnx-generated layer
[INFO] generating user layers
[INFO] generating workspace directory
ERROR: Failed to create workspace directory
ERROR: Failed to config project.

$ petalinux-create --type project --template zynqMP --name zcu102-ref

$ petalinux-config --get-hw-description= /home/esra/Documents/zcu102for20192/

configure

DTG Settings-->(zcu102-rev1.0) MACHINE_NAME

Defined external kernel as linux(https://github.com/analogdevicesinc/linux/tree/adi-4.14.0)

Defined meta-adi-core and meta-adi-xilinx into Yocto Settings-->User Layers

I used not only meta-adi branch 2018_R2 but also master branch

When I deleted these layers, successfully configured project. How can I solve this problem?

Top Replies