Profile loading using iio-oscilloscope throwing error "Failed to load Profile using selected file"

Hello,

I generated profile for 61.44 MHz of the bandwidth of 40 MHz using the profile generator (available in this link). And  I try to load using iio-oscilloscope (I pull the recent update and compiled again) since we are using ZCU102 and ADRV9009.

But it throwing the error as  "Failed to load Profile using selected file". As shown in the screenshot.

What i am missing. How i suppose to load the profile that I generated using the profile wizard.



spell mistake
[edited by: parthi at 9:27 AM (GMT 0) on 17 Feb 2019]