adrv9009-w/pcbz booting problem

i'm trying to boot the my adrv9009-w/pbcz with zcu102 rev 1.0. i followed the user and got to the uboot part(in the "Configure a pre-existing SD-Card"section) and got stuck.
after saving the new mac address and resetting i get two error, and then the booting stops, here is the entire boot sequence:

ZynqMP> Xilinx Zynq MP First Stage Boot Loader
Release 2017.4 Jun 26 2018 - 10:06:15
NOTICE: ATF running on XCZU9EG/silicon v3/RTL5.1 at 0xfffea000, with PMU firmware
NOTICE: BL31: Secure code at 0x0
NOTICE: BL31: Non secure code at 0x8000000
NOTICE: BL31: v1.3(release):47af34b
NOTICE: BL31: Built : 04:15:38, Dec 12 2017
PMUFW: v0.3


U-Boot 2017.01 (May 02 2018 - 15:53:29 +0200) Xilinx ZynqMP ZCU102 rev1.0

I2C: ready
DRAM: 4 GiB
EL Level: EL2
Chip ID: xczu9eg
MMC: sdhci@ff170000: 0 (SD)
reading uboot.env
In: serial@ff000000
Out: serial@ff000000
Err: serial@ff000000
Net: ZYNQ GEM: ff0e0000, phyaddr c, interface rgmii-id

Warning: ethernet@ff0e0000 MAC addresses don't match:
Address in SROM is ff:ff:ff:ff:ff:ff
Address in environment is 00:0a:35:03:45:ac
eth0: ethernet@ff0e0000
## Error: "setup" not defined
Hit any key to stop autoboot: 0
run - run commands in an environment variable

Usage:
run var [...]
- run the commands in the environment variable(s) 'var'
ZynqMP>

thank you for your helps.