本ウェビナーでは、電源設計の評価と特性評価を行うための、ポータブルで高性能なUSB電源駆動ツールキット「LTPowerAnalyzer」システムをご紹介します。参加者の皆様には、LTPowerAnalyzerのハードウェアおよびソフトウェア環境を使って、いかに簡単に電源ソリューションを最適化し、ボード線図応答...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    すべて表示

    What's Brewing?

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    著者:HamedSanogo 本稿は、連載記事「AI用アクセラレータ・カードに最適な電源システム」のPart 3です。今回は、次なる波に目を向けることにします。その先進的な技術は、垂直給電(Vertical Power Delivery)と呼ばれています。まずはこれについて詳しく解説します。その上で...

     

    自律走行ロボット向けのソフトウェア・アーキテクチャの基盤を構築する

    著者:Sarvesh Pimpalkar、Rajesh Mahapatra 自律走行ロボット(AMR:Autonomous Mobile Robot)は、様々な産業の変革に貢献しています。それを支えているのは、AMRが備える自動化用の機能、ナビゲーション機能、複雑なタスクの実行機能などです。こうした多様な機能を実現できるようにするためには...
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
FAQs AD7983: FAQ
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
AD7983: FAQ

AD7983: FAQ
Tags: ad7983 Single Channel A/D Converters Precision A/D Converters
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • AD9783: the function of REFIO
    y_suzuki
    Hello , I have a question about the function of REFIO of AD7983. In the pin descrition tabe, Table 8, REFIO pin is described as "Analog Reference Input/Output (1.2 V Nominal)." This description include...
  • EVAL-AD7983-PMDZ unexpected offset
    kpiterrr
    Hello, I driving EVAL-AD7983-PMDZ by Unipolar, Single-Ended sinusoidal signal (Vpp=4V, Voffset=2 so Vmin=0, Vmax=4). R2 and R4 were removed from the EVAL-AD7983-PMDZ PCB because they give the additional...
  • AD7983 REF Pin behavior
    cm_ele_egr
    I'm working with an AD7983 and hoping to get more information regarding the internal functionality of the REF pin. The datasheet describes how to use this pin from a top-level perspective, but I'm looking...
 
Related Content
  • AD9783: the function of REFIO
    y_suzuki
    Hello , I have a question about the function of REFIO of AD7983. In the pin descrition tabe, Table 8, REFIO pin is described as "Analog Reference Input/Output (1.2 V Nominal)." This description include...
  • EVAL-AD7983-PMDZ unexpected offset
    kpiterrr
    Hello, I driving EVAL-AD7983-PMDZ by Unipolar, Single-Ended sinusoidal signal (Vpp=4V, Voffset=2 so Vmin=0, Vmax=4). R2 and R4 were removed from the EVAL-AD7983-PMDZ PCB because they give the additional...
  • AD7983 REF Pin behavior
    cm_ele_egr
    I'm working with an AD7983 and hoping to get more information regarding the internal functionality of the REF pin. The datasheet describes how to use this pin from a top-level perspective, but I'm looking...