As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...
Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
IEC 61508 appears to include two very similar concepts. Type A and simple, which is referred to as “low complexity”. Anything that isn’t low complexity...
Let’s peel back the curtain on how Analog Devices (ADI) is leading the charge, crafting power solutions that not only keep up with AI’s appetite but redefine...
Technical articles. Blogs. Videos. Your ADI content, all in one place.
Blurb About Content
MAX9271/MAX9273 does not supports crosspoint switch feature. Use MAX96705 which have features like crosspoint switch.