The MAX77860 can be used with a battery that does not have a Battery ID by simply connecting a resistor between DETBATB and GND so that the voltage of DETBATB is pulled below 80% of VIO pin voltage. This may be useful if the battery pack will be permanently attached to the MAX77860, as the battery ID is used to detect if a battery is present or removed.