MAX14748 datasheet document ID 19-100081; Rev 5; 9/18 has the following errors:
- This appears several times throughout the datasheet as a typo: "Ready-Only if AppWrtPrtct = “(1) Protected” (See Table 61)". This should be "Read-Only" rather than "Ready-Only"
- Table 61.
- "MtChTmr" should be "MtChgTmr" (missing "g")
- Register Bit Default Values, the value for BatReChg[1:0] is listed as "100mV". However, that is not a valid value for that register field. Its a typo, it should be 200mV.