Question
What creepage and clearance does the ADM2682E/87E have, and what do these
characteristics refer to?
Answer
The ADM2682E/87E has more than 8 mm of creepage and clearance. Creepage refers
to the shortest path between two conductive parts, or between a conductive part
and the BOUNDING SURFACE of the equipment, measured along the surface of the
insulation. Clearance refers to the shortest distance between two conductive
parts, or between a conductive part and the BOUNDING SURFACE of the equipment,
measured through air.