Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
A checkerboard made as a 7 x 7 matrix has a green basic cell placed in its middle as shown in the above structure. Questions: How many squares, defined...
Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
By Tracey Johnson & Margaret Naughton Imagine a robot stepping out of a safety cage, not to perform a single preprogrammed motion, but to work alongside...
It’s time to look at the next wave: vertical power delivery and the relentless Analog Devices (ADI) innovation that makes it possible. If you’ve joined...
Technical articles. Blogs. Videos. Your ADI content, all in one place.
Blurb About Content
Question
How should I connect Power Valid Pin (PVP) when not using it?
Answer
The ADM2483's Power Valid Pin (PVP) should be pulled high, if not used