For both devices V+ is the output of the voltage doubling charge pump, and the V+ must be bypassed with a reservior capacitor. The reservior capacitor must be connected between V+ and a low-impedance ground or power node. If using ceramic non-polarized capacitors it is ok to connect the reservior capacitor either between V+ and ground or between V+ and VCC. If using polarized capacitors, then the capacitor must only be connected between V+ and ground with the positive terminal connected to V+.