No. Consider for example the MAX3387E T3OUT output is shorted to ground, the component is not necessarily damaged. Note that the page 2 Absolute Maximum Ratings allows a continuous transmitter output short to ground.
Short-Circuit Duration T_OUT to GND........................Continuous
A transmitter output short to ground is a fault condition, and normal device operation should not be expected during this fault condition. Consider that since the charge pump output voltages V+, V- can not provide enough driving power when a transmitter output such as T3OUT is shorted, it will affect the output voltage level of T1OUT and T2OUT.