When DI is logic high, the device drives the bus for a short time, then disables the driver and allows the external pullup/pulldown resistors to hold the bus in the high state. During each low-to-high transition of DI, the driver stays enabled until the A/B bus differential voltage exceeds the driver disable threshold voltage. (i.e A-B > VDT, where VDT is the driver disable threshold).