FAQ MAX96706 correct calculation for eye-width ERRB error output EWM_MIN_THR

There is an error in the datasheet (Document number 19-8248; Rev 1; 3/17, Page 47, ewm(0x13)BITFIELD for EWM_MIN_THR).
The EWM_MIN_THR can have a value from 0 (disabled) to 31. The equation should be:  
EWM_MIN_THR/32 * 100%.  
For example, a value of 13 / 32 = approximately 40%