FAQ Can the line-fault monitors be disabled on the MAX96706?


Yes, the MAX96706 line-fault monitors can be disabled in register 0x08, bits 7 and 6.  If you wish to keep the line-fault monitors disabled permanently, the LMN0 and LMN1 pins can be left unconnected.  The same applies for all Maxim GMSL SerDes parts that have line-fault monitors.