Locale Icon
English
EngineerZone
EngineerZone
Gigabit Multimedia Serial Link (GMSL) Library
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
    Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

Gigabit Multimedia Serial Link (GMSL) Library
  • Interface and Isolation
Gigabit Multimedia Serial Link (GMSL) Library
FAQs
  • FAQs
  • Documents
  • Members
  • Tags
  • Cancel
Browse Categories
  • GMSL1
  • GMSL2
  • GMSL U
  • Features
  • ChannelSpec
  • Documentation
  • EMI
  • Glossary
  • Hardware
  • MAX9205: FAQ
  • MAX9217: FAQ
  • MAX9271: FAQ
  • MAX9275: FAQ
  • MAX9276A: FAQ
  • MAX9277: FAQ
  • MAX9278: FAQ
  • MAX9281: FAQ
  • MAX9286: FAQ
  • MAX9288: FAQ
  • MAX9291: FAQ
  • MAX96705: FAQ
  • MAX96705A: FAQ
  • MAX96706: FAQ
  • MAX96707: FAQ
  • MAX96715: FAQ
  • Safety
  • Software
  • Training
  • Troubleshooting
Manage My Notifications
  • More
  • Cancel
  • FAQs

MAX96706: FAQ

FAQs
  • FAQ

    Can I perform hot swap on systems using GMSL parts with Phantom Power (aka Power over Coax) where one coax cable is used for data and power

    Yes, you can implement a hot swap system with these parts. We have customers with such implementations in production. There are 3 considerations: 1. Voltages spikes. PoC systems use inductors in…
  • FAQ

    Can the line-fault monitors be disabled on the MAX96706?

    Yes, the MAX96706 line-fault monitors can be disabled in register 0x08, bits 7 and 6. If you wish to keep the line-fault monitors disabled permanently, the LMN0 and LMN1 pins can be left unconnected. The…
  • FAQ

    How can I verify the compatibility of a Maxim serializer or deserializer?

    All Maxim GMSL-1 serializers and deserializers (SerDes) are compatible with each other. Our SerDes parts are typically mentioned together (e.g. MAX96705 and MAX96706), but these pairings are only a suggestion…
  • FAQ

    Is there any problem associated with setting the equalizer gain too high in the MAX96706?

    The transmission path is a low-pass filter, it is necessary to amplify the high bandwidth by EQ. When this gain is abnormally high, the slew rate of data becomes faster and overshoot and undershoot occur…
  • FAQ

    MAX96706 correct calculation for eye-width ERRB error output EWM_MIN_THR

    There is an error in the datasheet (Document number 19-8248; Rev 1; 3/17, Page 47, ewm(0x13)BITFIELD for EWM_MIN_THR). The EWM_MIN_THR can have a value from 0 (disabled) to 31. The equation should be…
  • FAQ

    What PRBS type do I use for the MAX96705 (serializer) and the MAX96706 (deserialzer)?

    Q. What PRBS type do I use for the MAX96705 (serializer) and the MAX96706 (deserialzer)? A. For these two parts you should use the default PRBS test as indicated in the data sheet. For these two parts…