The MAXCAMOV10640# is a camera solution that uses the MAX9271 serializer and the OV10640 image sensor. The MAX96705 is pin compatible with the MAX9271, so the MAXCAMOV10640# schematic can be applied to the MAX96705 as well.
MAX96705
Production
The MAX96705 is a compact serializer with features especially suited for automotive camera applications. It is function and pin compatible with the MAX9271...
Datasheet
MAX96705 on Analog.com
MAX9271
Production
The MAX9271 compact serializer is designed to drive 50O coax or 100O shielded twisted-pair (STP) cable. The device pairs with the MAX9272 deserializer...
Datasheet
MAX9271 on Analog.com