Locale Icon
English
EngineerZone
EngineerZone
Gigabit Multimedia Serial Link (GMSL) Library
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
    Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Fast-Track Certification: Leveraging IC Safety App Notes for Functional Safety Designs
    View All Webinars
  • Community Hub

    Challenge Yourself!

      World Engineering Day Quiz!

      By Kuo-Chang A checkerboard made as a 7 x 7 matrix has a green basic cell placed in its middle as shown in the above structure. Questions: How...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

Gigabit Multimedia Serial Link (GMSL) Library
  • Interface and Isolation
Gigabit Multimedia Serial Link (GMSL) Library
FAQs
  • FAQs
  • Documents
  • Members
  • Tags
  • Cancel
Browse Categories
  • GMSL1
  • GMSL2
  • GMSL U
  • Features
  • ChannelSpec
  • Documentation
  • EMI
  • Glossary
  • Hardware
  • MAX9205: FAQ
  • MAX9217: FAQ
  • MAX9271: FAQ
  • MAX9275: FAQ
  • MAX9276A: FAQ
  • MAX9277: FAQ
  • MAX9278: FAQ
  • MAX9281: FAQ
  • MAX9286: FAQ
  • MAX9288: FAQ
  • MAX9291: FAQ
  • MAX96705: FAQ
  • MAX96705A: FAQ
  • MAX96706: FAQ
  • MAX96707: FAQ
  • MAX96715: FAQ
  • Safety
  • Software
  • Training
  • Troubleshooting
Manage My Notifications
  • More
  • Cancel
  • FAQs

MAX96705: FAQ

FAQs
  • FAQ

    Can MAX96705/9/11 Camera Serializers Output on Both Serial Outputs for Splitter Configurations?

    MAX96705/9/11 camera parts do not support splitter configuration however the MAX9271/9273 can be used in COAX Splitter Mode when both OUT+ and OUT- are outputting the same data. For more information see…
  • FAQ

    Can you change the order of the inductors in the GMSL1 Camera Serdes MAX96705 POC filter circuit?

    The combined impedance of the small inductors (L1/330nH and L2/6.8uH) is used to block the high-frequency forward video signal, 10MHz to 750MHz. The big inductor (L3/100uH) impedance is used for low frequency…
  • FAQ

    Does MAX96705 support 1280x1080 resolution?

    If raw data is used and DBL = 1, f or a given image resolution, the corresponding data rate required for the coaxial or twisted pair is: (pixel row * pixel column) /2 * frames per second * 1.25 * 30…
  • FAQ

    Does Maxim have any CSI-1 SERDES products?

    Maxim does not have any products for CSI-1, all Maxim GMSL products will always be CSI-2.
  • FAQ

    For a GMSL serializer or deserializer, what is double mode?

    Double mode (DBL) allows for the serializer to load a GMSL data packet with two half-width serial words instead of one whole-width one. Maxim GMSL parts have three different bus widths: 24, 27, and 32…
  • FAQ

    I want to use features that conflict with the LCCEN pin

    Question: Some GMSL parts have a Local Control Channel ENable (LCCEN) pin so that a microcontroller can be connected directly (locally) to control the serializer. This pin changes the function of other…
  • FAQ

    In a GMSL system, can the remote side I2C bus run at a different speed than the local side?

    Yes, the remote side I2C bus can run at a different speed than the local side. In a GMSL system, the controller is connected to the local device, while the coax/STP cable connects to the remote device…
  • FAQ

    In the MAX96705 and MAX96706 datasheets, what is the meaning of 'X' in the register bit descriptions?

    An 'X' in a bit position can mean two different things depending on the situation: ​ 1) If the 'X' is in a reserved bit position, the value is hidden and not accessible. 2) If the 'X' is in a normally…
  • FAQ

    MAX96705支持1280x1080这个分辨率吗?

    图像分辨率对应的同轴线或双绞线信号传输速率为: (行像素 x 列像素) /2 x 每秒场数 x 1.25 x 30 ( 24-bit 模式) (行像素 x 列像素) /2 x 每秒场数 x 1.25 x 40 ( 32-bit 模式) 对于1280 P ,每秒 30 场的摄像头,同轴线或双绞线传输的最大速率为: ( 1280x1080 ) / 2 x 30 x 1.25 x 30= 777.6Mbps…
  • FAQ

    The MAX96705 is a 16-bit serializer and the MAX96706 is a 14-bit deserializer. How can they be compatible if they have different bit counts?

    All Maxim Gigabit Multimedia Serial Link (GMSL) parts are compatible with each other. However, there are some constraints. If a serializer or deserializer has a feature that its companion does not, just…
>