Locale Icon
English
EngineerZone
EngineerZone
Gigabit Multimedia Serial Link (GMSL) Library
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • COTS SoMs & Phased Array Solutions for Rapid RF Subsystem Integration
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Improving Industrial Functional Safety Compliance with High Performance Supervisory CircuitsPart 5: Sequencers Eliminate Systematic Failures

    This article shifts focus from managing the quantitative metrics of functional safety toward mastering the qualitative yet equally critical challenge:...

Gigabit Multimedia Serial Link (GMSL) Library
  • Interface and Isolation
Gigabit Multimedia Serial Link (GMSL) Library
FAQs
  • FAQs
  • Documents
  • Members
  • Tags
  • Cancel
Browse Categories
  • GMSL1
  • GMSL2
  • GMSL U
  • Features
  • ChannelSpec
  • Documentation
  • EMI
  • Glossary
  • Hardware
  • MAX9205: FAQ
  • MAX9217: FAQ
  • MAX9271: FAQ
  • MAX9275: FAQ
  • MAX9276A: FAQ
  • MAX9277: FAQ
  • MAX9278: FAQ
  • MAX9281: FAQ
  • MAX9286: FAQ
  • MAX9288: FAQ
  • MAX9291: FAQ
  • MAX96705: FAQ
  • MAX96705A: FAQ
  • MAX96706: FAQ
  • MAX96707: FAQ
  • MAX96715: FAQ
  • Safety
  • Software
  • Training
  • Troubleshooting
Manage My Notifications
  • More
  • Cancel
  • FAQs

MAX9288: FAQ

FAQs
  • FAQ

    Are the MAX9263 and MAX9288 compatible?

    The MAX9288 is compatible with the MAX9263 and both can work together. Any features that both do not support will be lost. For example, the MAX9288 does not support HDCP. For more information about compatibility…
  • FAQ

    How to estimate the current consumption when MAX9288 is connected to 4-lane MIPI signal? How does it compare with the 2-lane situation described in the datasheet?

    The power consumption of MIPI is the largest when connected 2 lanes, when connected 4 lanes it will be reduced by about 20mW. The reason is that when the number of lanes is changed, the CSI frequency…
  • FAQ

    MAX9263和MAX9288是否可配对使用?

    MAX9288与MAX9263可以配合使用。但 两者 不同时支持的功能将失效。例如,MAX9288不支持HDCP。详细信息请参靠MAX9288数据手册第84页表格21。
  • FAQ

    MAX9288的HS/VS输入是否必须为高电平有效?

    是的,MAX9288在做GMSL到CSI-2转换时,HS/VS应为高电平有效,若输入为低电平有效需配置INVHSYNC和INVVSYNC寄存器反转HS/VS输入信号。
  • FAQ

    MAX9288连接4 lane MIPI信号时的电流消耗应该如何估算?和datasheet描述的2 lane的情况如何比较?

    连接2 lane MIPI的功耗是最大的,连接4 lane时的功耗会降低大约20mW. 原因是改变lane的数量时,CSI频率和PLL也会发生变化。从2 lane变为4 lane,频率降低,PLL的功耗也随之降低。所以2 lane MIPI的功耗最大。
  • FAQ

    SerDes I2C Reverse Channel Debugging

    The reverse channel in serializer/deserializer pairs can be susceptible to low frequency noise especially when using Power Over Coax. The first thing to check should be the I2C bitrate speed and confirm…