Locale Icon
English
EngineerZone
EngineerZone
Gigabit Multimedia Serial Link (GMSL) Library
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • COTS SoMs & Phased Array Solutions for Rapid RF Subsystem Integration
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Improving Industrial Functional Safety Compliance with High Performance Supervisory CircuitsPart 5: Sequencers Eliminate Systematic Failures

    This article shifts focus from managing the quantitative metrics of functional safety toward mastering the qualitative yet equally critical challenge:...

Gigabit Multimedia Serial Link (GMSL) Library
  • Interface and Isolation
Gigabit Multimedia Serial Link (GMSL) Library
FAQs
  • FAQs
  • Documents
  • Members
  • Tags
  • Cancel
Browse Categories
  • GMSL1
  • GMSL2
  • GMSL U
  • Features
  • ChannelSpec
  • Documentation
  • EMI
  • Glossary
  • Hardware
  • MAX9205: FAQ
  • MAX9217: FAQ
  • MAX9271: FAQ
  • MAX9275: FAQ
  • MAX9276A: FAQ
  • MAX9277: FAQ
  • MAX9278: FAQ
  • MAX9281: FAQ
  • MAX9286: FAQ
  • MAX9288: FAQ
  • MAX9291: FAQ
  • MAX96705: FAQ
  • MAX96705A: FAQ
  • MAX96706: FAQ
  • MAX96707: FAQ
  • MAX96715: FAQ
  • Safety
  • Software
  • Training
  • Troubleshooting
Manage My Notifications
  • More
  • Cancel
  • FAQs

MAX9275: FAQ

FAQs
  • FAQ

    Can GPI/GPO be used for interrupt on the MAX9275

    The GPI input on derserializers is sent in the reverse direction on a GMSL1 link and output on GPO at the serializer. This can be used for getting an interrupt from a touchscreen controller back to an…
  • FAQ

    Can the MAX9275 I2S audio interface pins be used as additional parallel inputs?

    In a MAX9275 application that does not require digital audio transmission, SD can be used as an additional parallel input. Note that SCK and WS cannot be used as additional parallel inputs. For this configuration…
  • FAQ

    How can I update the MAX9275EVKIT firmware, so I can use it with the lastest GUI?

    Our GMSL EVKITS have had three different microcontrollers on them throughout the years. The first GMSL EVKITS that we developed had a Dallas microcontroller on them. Then, we used a Nuvoton microcontroller…
  • FAQ

    How do I run the PRBS test on a GMSL link?

    Some of Maxim serializers and deserializers have a built-in pseudorandom binary sequence (PRBS) generator and receiver for bit error rate (BER) testing on a GMSL link. The serializer generates PRBS data…
  • FAQ

    What do you do with the LMN0 and LMN1 pins on the MAX9275 if you are not using line fault detection?

    If you are not using the line fault detection feature in the MAX9275 then you should leave the LMN0 and LMN1 pins floating by disconnecting the pull-up and pull-down resistors.
  • FAQ

    What is the best GMSL for a 12-bit monochrome display?

    12-bit monochrome video data includes 12 bits of data + HS+VS+DE = 15 parallel into a GMSL device like the MAX9275, per sample. So, BWS = 0 (24-bit mode) configuration allows a pixel clock frequency up…