FAQ Can any error flag be routed to ERRB?

Most errors that have an error status flag can be routed to ERROR/ERRB. When several errors and/or events are configured to drive the ERRB pin, these status registers can be read to determine the source of the ERRB assertion. To determine which errors can be routed to ERROR/ERRB, refer to the device-specific data sheet for the corresponding output enable bit ending with "_OEN".