The DSI and CSI-2 packet-level protocols are different and not interchangeable. A DSI transmitter must be matched to a DSI receiver; a CSI-2 transmitter must be matched to a CSI-2 receiver.
The I2C/UART functions, whether control channel or pass through, are not affected by the speed group settings. The I2C/UART circuitry has a fixed falling-edge slew rate, and the rising-edge slew rate is…
On Dual/Quad deserializers, when some of the links are in tunnel mode and others are in pixel mode, the limitation exists that users cannot aggregate tunnel and pixel mode data streams. Users may aggregate…
Most errors that have an error status flag can be routed to ERROR/ERRB. When several errors and/or events are configured to drive the ERRB pin, these status registers can be read to determine the source…
Yes, GMSL2 devices supporting HDCP and GMSL1 backward compatibility can support HDCP. However, GMSL2 style "auto-HDCP" or "HDCP" is not support in GMSL1 mode. In the case of GMSL1 mode, all HDCP authentication…
No, I2C/UART pass-through cannot access GMSL2 device registers. They only provide access to local device registers and provide control of the peripheral devices. However, the I2C/UART primary control channel…
Yes, it is possible to have one link in crystal mode and other link in RoR mode on the deserializer, refer to device-specific data sheet and user guides for serializers and deserializers that support RoR…
Yes, but only if you do not aggregate the data from the two input ports. You cannot aggregate pixel mode data with tunneling mode data.
There are separate registers for enabling/disabling the tunneling…
Yes, video interface to GMSL link repeater mode is supported by a limited number of devices that include those that may use common consumer connectors which often support HDCP data transmission. In the…