FAQ What are the typical and maximum power consumption values given in GMSL part data sheets?

Typical value of supply current is not a reference for power supply sizing, use the maximum supply value for reference. Typical value of supply current is an indicative value of current consumption which very likely to observe a closer value when measured on a customer application board for the given operating conditions. Maximum supply current value is the guaranteed maximum value based on Lean 6-sigma techniques. There is no margin needed to add on top of this for power supply sizing under given operating conditions.